Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Darkens
Over Time



FAQ
During Application
After Application
- Chipping, Peeling
- Darkens Over Time
- Floor Scuffs Easily
- Finish Wears
- Finish Turns White
- Worn Finish

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Uniformly or Non-Uniformly Darkens Over Time


Color changes/Ambering:

General Comments:
1) All uncoated, bare wood and ALL oil-based polyurethane's get darker in color with time. They darken less and at a slower rate when they are exposed to light. Such as, under area rugs, furniture and areas not exposed to light.

2) Ambering of water-based finishes varies widely however as a general statement waterbased finishes are more color stable than oil based finishes and therefore at a slower rate.

The Problem:
The look of the floor has darkened non-uniformly over time.

The Cause:
Since the wood itself and, sometimes, its topcoat are darkening with time and light exposure, then any areas of the floor covered with area rugs, furniture, etc. will appear darker when uncovered. This is more pronounced if an oil modified polyurethane finish is applied instead of a non-yellowing or non-ambering water-based finish.

How to fix the problem:
1) For an immediate remedy, completely re-sand (If applicable re-stain) and re-coat the entire floor.

2) The condition is substantially but not completely reversible with the passage of time. Removing the items that are blocking the light will allow the previously unexposed, darker areas to lighten and blend somewhat with the rest of the floor. The blend is not perfect, however, because the wood lacks the ability to "recover" fully.


How to avoid in the future:
Finishing with a non-ambering topcoat will eliminate the darkening appearance contributed by the finish. Protecting the wood from the bleaching effects of sunlight is achieved only by minimizing sunlight infiltration via drapes and ultraviolet (UV) light blocking windows. UV light blockers in the finish cannot eliminate color variability problems caused by sunlight.

Note:
This condition can occur on any floor but is more pronounced the lighter the color of the floor.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations