Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Floor Scuffs Easily



FAQ
During Application
After Application
- Chipping, Peeling
- Darkens Over Time
- Floor Scuffs Easily
- Finish Wears
- Finish Turns White
- Worn Finish

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Floor Scuffs Easily

The Problem:
Floor scuffs easily.

The Cause:
New Floors:
This can simply be the result of poor floor maintenance or a poor quality finish having been used. If a quality brand was applied, it is probably the result of the finish not having been fully cured before subjecting it to heavy traffic. A total cure time of seven days is required before heavy traffic is allowed.

Bottom coats, which include stains, require ample time to dry or solvents trapped in the film will continue to migrate up through the film, and often two or more layers of finish, resulting in a tender topcoat.

Old Floors:
As above, plus contaminants such as waxes, sterates and silicones down in-between the boards and end matches can cause a finish coat solvent release to be slowed down, resulting in a tender film.

How to fix the problem:
New Floors:
How long it will take the finish to harden is impossible to predict (this could take up to three months) but be assured soft finish will harden eventually. When the finish is hard the floor should be abraded, vacuumed, tacked and recoated.

Old Floors:
This finish will probably never harden and the finish will have to be completely sanded to the bare wood. Then, protect the floor with Dura Seal Neutral (210) buffed in with steel wool (#2). (Use stain if color change is desired). In addition, apply a coat of DURA SEAL Dura Finish Liquid Floor Wax. Alternately, two coats of Dura Seal Neutral (210) may be used instead.

How to avoid in the future:
New Floors:
Check the temperature and humidity of the floor and alter them if they are not within the product specification, (see label) or give longer dry times. Never apply thick first coats and ensure complete removal of all stains. Good ventilation is always essential for proper cure.

Old Floors:
Inspect the floor prior to sanding. Floors, older than 10 years, should always be suspect for wax's. Checking the corners and scrapping with a knife often reveals the presence of wax. Wax's and other contaminates can also be detected by splashing water on it. If the water beads, know that something is on the floor and pre-sanding removal is essential. Buff the floor with mineral spirits or water, depending on which contaminate is involved.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations