Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Finish Wears



FAQ
During Application
After Application
- Chipping, Peeling
- Darkens Over Time
- Floor Scuffs Easily
- Finish Wears
- Finish Turns White
- Worn Finish

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Wood Floor Preventative Maintenance
(Finish Wears)

The Problem:
Finishes will wear.

Wood Floor Preventative Maintenance:

1. The use of walk off mats at exterior entrances help to prevent sand, grit and water being walked onto the floor. Sand, grit and water are the floor's worst enemy.

2. Install proper floor protectors on furniture used on hardwood floors. Protectors will allow chairs to move over the floor without scuffing. Clean the protectors on a regular basis to remove any grit and sand that may have become imbedded in them.

3. Sweep on a daily basis or as needed but do not use household dust treatments as this may cause your floor to become slick or dull the finish. Vacuum regularly. Do the hardwood floor when the household carpets are being vacuumed. Brush attachments work well on hardwood floors, but do NOT use the beater.

4. Since finishes are designed to protect the stain and face of the wood, they are not designed to protect against excessive water. Never WET-MOP a hardwood floor. Excessive water causes wood to expand, possibly damaging the flooring. Propriety hardwood floor cleaners such as the DURA SEAL Hardwood Floor Cleaner are the industries recommended method for cleaning floors.

5. Keep high heel shoes in good repair. Heels that have lost or worn through their protective cap will expose the fastening nail. This will exert over 8,000lbs. per square inch of pressure on a floor. This pressure will damage all types of floors.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations