Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
White/Gray Lines
Between boards



FAQ
During Application
After Application
- Chipping, Peeling
- Darkens Over Time
- Floor Scuffs Easily
- Finish Wears
- Finish Turns White
- Worn Finish

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

White/Gray Lines Between The Boards

The Problem:
The finish turns white or light gray between the boards.

The Cause:
The wood was not acclimated to room conditions prior to installation. The boards had a higher moisture content when installed than what the room currently has which has caused the finish to be stretched as the boards shrink as they were drying out.

How to fix the problem:
It has to be understood that this is NOT a finish problem. How to know? The finish looks great on the face of the boards the only issue is at the joints. It can be beneficial in some cases for this to happen, by avoiding a panelization issue.

How to avoid in the future:
Apply the sealer, stain and or finish as per manufacturer's recommended instructions using the correct spread rate. Remember more is not better. Watch for excessive cracks. These can be trowel-filled (as per manufacturer's instructions) Also pay attention to the factors that affect dry time. Floors should be installed at normal living conditions. That means, with all windows and doors in place, all wet trades done and the HVAC system running. It is important to control the job site environment. Avoid high humidity, above 90% Relative Humidity and temperatures over 90 degrees F or lower 50 degrees F.

Once the floor is finished allow it to cure appropriately before covering. Check the Dura Seal technical sheets for the correct cure times.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations