Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Crack Beading



FAQ
During Application
- Crack Beading
- Bubbles and Craters
- Drying Too Fast
- Drying Too Slow
- Uneven Color
- Surface Not Smooth

After Application

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Crack Beading or Poly BB's:

The Problem:
Beads of finish forming in the side joints.

The Cause:
Most finishes and stains dry from the top down. When the first coat is applied, whether it is a stain or finish, it seeps down into the cracks between the boards. The material therefore stays comparatively wet because there is no air movement. Usually, at this point three things happen:

  • Additional coats are applied
  • The floor is covered
  • Time elapses

As additional coats are applied, the problem is compounded. Then covering the floor may affect the dry time by locking the solvents down in the cracks. In time the floor expands and contracts. Expansion pushes the boards together and the still wet material down in the gaps is squeezed up, forming the beads.

How to fix the problem:
It has to be understood that this is NOT a finish problem. How to know? The finish looks great on the face of the boards for all coats; the only issue is the cracks.

The solution to the problem is time. Allow the floor to expand and contract and just keep removing the beads that have cured or hardened with a putty knife or scraper. DO NOT attempt to screen the beads off, this will cause circular scratches in the surface of the finish. If there are bb's that are still soft, remove them with a scraper then wipe the area with a rag dampened with mineral spirits.

How to avoid in the future:
Apply the sealer, stain and or finish as per manufacturer's recommended instructions using the correct coverage rate. Remember more is not better. Watch for excessive cracks. These can be trowel-filled (as per manufacturer's instructions) Also pay attention to the factors that affect dry time. Floors should be installed at normal living conditions. That means, with all windows and doors in place, all wet trades done and the HVAC system running. It is important to control the job site environment. Avoid high relative humidity, above 90% R.H. and lower temperatures below 50 degrees F (10 C) that can seriously slow the drying time of sealers, stains and finishes.

Once the floor is finished, allow it to cure appropriately before covering. Check the manufacturers technical sheets for correct dry times.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations