Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Bubbles
and Craters



FAQ
During Application
- Crack Beading
- Bubbles and Craters
- Drying Too Fast
- Drying Too Slow
- Uneven Color
- Surface Not Smooth

After Application

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Bubbles and CratersBubbles and Craters

The Problem:
Topcoat has bumps when dry.

The Cause:
Bubbles:
This can be the result of the finish or the floor being too cold, humidity too high or the previous coat(s) not being dry before this last coat was applied. In addition, not following the coverage rate directions such as, applying too heavy a coat, often lead to this condition. Most finishes cure from the top down. If, the wet coat forms a skin before the air folded into it can escape, the finish forms bubbles and can not level out.
Craters:
Bubbles that have released their air but the finish has then hardened to a point that it can not level out and feels rough to the touch.
Trash in the Finish:
Airborne dust from heating vents, failure to tack efficiently place dust particles in the finish, which look like bubbles until seen under high magnification.

How to fix the problem:
Oil Modified bubbles and craters can usually be screened and re-coated with a thin coat of finish. Water base finishes that have bubbled can be scraped flat but will probably require re-sanding.

How to avoid in the future:
Determining the conditions at the job site and ensuring it is feasible to apply the finish is the responsibility professional sand and finishers. Tools such as hygrometers and moisture meters tell you what the job site conditions are so you can act accordingly. Where possible alter the temperature, humidity and ventilation conditions to those recommended by the specific product directions. Block off all air vents, sweep, vacuum, and tack then apply finish.
If this is not possible to do immediately, it is better to wait until you can.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations