Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Finish Won't Dry



FAQ
During Application
- Crack Beading
- Bubbles and Craters
- Fast Drying
- Slow Drying
- Uneven Color
- Surface Not Smooth

After Application

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Finish won't Dry

The Problem:
Finish drying too slow.

The Cause:
Temperatures below 50 degrees F. (10 C) and relative humidity (over 90%) covering the floor with brown paper or cardboard before it's dry. Oil Modified Polyurethane dries slowly when the floor temperature is at or below 50 degrees F. (10 C) when humidity is over 90% RH. (A combination of both makes conditions worse) all of these points prevent the solvent from leaving the wet film. Contaminants in the grain or between the boards, can also be the cause for slow dry.

How to fix the problem:
Determine which of the above, or combination of, is the cause of the problem.
Remember to stop the A/C (close windows and doors) 30 min.'s prior to application then re-start (reopen) when the finish is tacks free. Which, is usually after about one to two hours for Oil Modified Polyurethane, and 15 to twenty minutes for waterbased. After these corrections to the site conditions have been met, the main ingredient is time. DO NOT attempt to screen the floor until the finish has completely dried since this will cause deep scratches in the finish and will remain visible. You could also experience solvent entrapment, causing a tender topcoat, which is a cause of early wear. A complete re-sand is the alternative.

How to avoid in the future:
A simple tool such as a hygrometer will tell you what the job site condition is and therefore you have the opportunity to act accordingly. Dura Seal recommends changing your expectation of the dry time if your application and drying conditions vary from…

The coverage rate on the label (see Finish and Curing Parameters) (JoeAl please link this)
A temperature above 70 degree F (25 C) and Relative Humidity below 50%.

Note: Dry times either fast or slow are affected by Temperature, Relative Humidity and Air movement, either natural (window) or forced (HVAC) PLUS coverage rate. Attention to these details improves success rates.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations