Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Uneven Color



FAQ
During Application
- Beading
- Bubbles and Craters
- Fast Drying
- Slow Drying
- Uneven Color
- Surface Not Smooth

After Application

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Uneven Color

The Problem:
The look of the stain is uneven.

The Cause:
This can be due to the sanding procedures being uneven. Uneven sanding will cause the color to look uneven. Improper wiping techniques are another reason for uneven staining.

How to fix the problem:
1. If sanding procedures are the cause, then only a complete re-sanding and re-staining of the floor will fix the problem.
2. If improper wiping techniques are the reason for uneven staining, and the floor has not yet been top coated. Buffing the floor with mineral spirits and steel wool, or green synthetic pad under the buffer will even out the color.

How to avoid in the future:
Sand the floor according to NOFMA NWFA standards. Ensure ALL superfluous stain is wiped from the floor.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations