Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Wrinkling, Alligatoring
or Blistering



FAQ
During Application
- Crack Beading
- Bubbles and Craters
- Drying Too Fast
- Drying Too Slow
- Uneven Color
- Surface Not Smooth

After Application

Color & Seal
Fillers
Stains
Sealers

Sport Surface System

Maintain & Beautify

     Warranty

   Quality Products

Wrinkling, Alligatoring or Blistering

The Problem:
Topcoat is not smooth when dry.

The Cause:
This can be the result of the bottom coat(s) not being dry enough to accept an additional coat. Or, a top coats solvents etches (eats) into weaker or uncured bottom coats. The job site conditions and too heavy a first coat are the usual reason for these problems.

Blistering:
Will sometimes occur in spots and could be caused by spotty drying of bottom coats.
Wrinkling:

Will result as blisters over a large area of the floor.
Alligatoring:
Very heavy wrinkling results when the topcoat etches (eats) into the bottom coat and actually lifts it from raw the wood or the stain or sealer.

How to fix the problem:
Blistering and wrinkling can usually be screened and coated with a very thin coat of finish. Alligatoring requires a complete sand and re-coat.

How to avoid in the future:
Determining the conditions at the job site and ensuring it is practical to apply stains and finishes is the fist duty of professional sand and finishers. Tools such as hygrometers and moisture meters tell you what the job site conditions are so you can act accordingly. Should the conditions be borderline it is wise to allow more time than normal to ensure the sealer, stain or finish is dry. Correct temperature, humidity and ventilation are the keys to avoiding these problems. In addition, not following the coverage rate directions such as, applying too heavy a coat, often lead to this condition.


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations