Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Pastels Stain

     Warranty

   Quality Products

DURA SEAL Pastels Stain

Pastel StainsPRODUCT DESCRIPTION:
This line of penetrating, oil-based stains imparts rich pastel colors to the wood that complement today's designer look. Available in Country White, Golden Wheat and Stone Grey, DURA SEAL Pastels Stain highlights rather than hides the natural grain of the wood.

DIRECTIONS:
Surface Preparation:
1. Properly prepare surface according to NOFMA or NWFA approved methods.
2. Final Sanding should be done with eighty (80) grit screen to allow deeper penetration of stain.
3. Remove all dust with a broom and/or vacuum and tack surface with a clean towel moistened with mineral spirits.

Application:
1. Stir material thoroughly before and occasionally during use. Apply a test sample on a small inconspicuous area before proceeding with entire job to insure desired color. Always stain with the grain.
2. Apply the first coat of DURA SEAL Pastels Stain with a brush, lambs wool applicator or cloth. NOTE: Do not use steel wool. To ensure adequate open time and to maintain a wet edge, apply liberally at an application rate of approximately 400 square feet per gallon.
3. Allow to penetrate for 2 to 4 minutes then remove excess by wiping with clean rags.
NOTE: Do not use steel wool. DURA SEAL Pastels Stain dries faster than DURA SEAL Penetrating Finish, 200 Series. If stain becomes tacky, wipe surface with a rag moistened with mineral spirits. Removal of all excess material is essential to ensure proper dry time.
4. A second coat may be applied if greater color density is desired. Allow first coat to dry approximately 8 hours before applying a second coat of non-yellowing top coat. Allow stain to dry 3 days before applying a non-yellowing water borne top coat.

PRECAUTION:
Do not use steel wool. To avoid discoloration, use of a non-yellowing top coat over DURA SEAL Pastels is recommended.

IMPORTANT:
Immediately after use, place rags, steel wool and other waste in a sealed, water filled metal container. See cautionary statement.

PRODUCT PROPERTIES:

COATS REQUIRED Apply only one (1) coat
DRY TIME Approximately 8 hours to overnight. Allow stain to dry 3 days before applying a non-yellowing water borne top coat.
NOTE: Drying time will be increased by high humidity, low temperature, lack of air movement or incomplete removal of excess stain.
COVERAGE Approximately 400 square feet per gallon.
CLEAN UP Clean equipment with mineral spirits.
STORAGE Approximately 400 square feet per gallon.
SOLVENT Non-photochemically reactive.

CAUTION:
COMBUSTIBLE MIXTURE N.Y.F.D. C. OF A. NO.1187

KEEP OUT OF REACH OF CHILDREN.

DANGER:
Contains mineral spirits. Harmful or fatal if swallowed. Do not take internally. Skin irritant. Avoid contact with skin and eyes. Wear rubber gloves and safety glasses when handling. Avoid inhalation and use only with adequate ventilation. If adequate ventilation cannot be maintained, wear respiratory protection [NIOSH/MSHA TC23C or equivalent] or leave the area. Do not use or store near heat, sparks, flame or other sources of ignition. Close container after each use. Rags, steel wool or waste soaked with DURA SEAL Pastels Stain may spontaneously catch fire if improperly discarded. Immediately after use, place rags, steel wool, and other waste in a sealed, water filled metal container. Dispose of in accordance with local fire regulations.

FIRST AID:
If swallowed, do NOT induce vomiting. CALL PHYSICIAN IMMEDIATELY. For skin contact, wash thoroughly with soap and water. If irritation persists, get medical attention. If affected by inhalation, remove to fresh air and CALL PHYSICIAN. In case of eye contact, immediately flush eyes thoroughly with water, then remove any contact lenses. Continue to flush eyes with water for at least 15 minutes. If irritation persists, get medical attention.

Color Size SKU # Case/Pack
COUNTRY WHITE QT 60400 6
COUNTRY WHITE Gal 10400 4
STONE GRAY Gal 10401 4
GOLDEN WHEAT Gal 10402 4

4/30/99
lit # 05990013


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations