Dura Seal™: The Choice of Professionals
 
SITE MAP: Non-Flash Browsers

10 Mountainview Rd., Upper Saddle River NJ  07458-1933
Tel: 1-800-364-1359

Dura Seal is a registered trademark. 
Copyright ©1999 Dura Seal. 
All rights reserved. 
Paste Wax



Color & Seal
Fillers
Stains
Sealers Maintain & Beautify
- Wax & Cleaner
- Touch-up Spray
- Floor Reviver
- Hardwood Floor Cleaner
- Liquid Floor Wax
- Paste Wax
- Renovator Cleaner
- Commerical Floor Maintenance

     Warranty

   Quality Products

DURA SEAL Paste Wax

PRODUCT DESCRIPTION:
DURA SEAL Paste Wax is a special blend of five waxes that gives hardwood floors the hand-rubbed luster of fine furniture. This classic product protects and beautifies with minimal maintenance. Available in Neutral for light surfaces and Coffee Brown for dark surfaces.

DIRECTIONS:
New Floor Preparation:
1. Prepare floor according to NOFMA or NWFA approved methods.
2. Stain and seal with DURA SEAL Penetrating Wood Finish, DURA SEAL Fast Dry Wood Stain, or DURA SEAL 500 Penetrating Fast Dry Sealer, according to label directions.

Old Floor Preparation:
1. Clean flooring using DURA SEAL Renovator Cleaner and Reconditioner, according to label directions.

Application:
1. Place a small amount of DURA SEAL Paste Wax in the center of a piece of cheese cloth. Fold the cloth so the Paste Wax will not come in direct contact with the floor
2. Wipe floor with the cheese cloth in a circular motion applying light pressure to the cloth. This will force the DURA SEAL Paste Wax through the cloth onto the floor yielding a more even application.
NOTE: Apply DURA SEAL Paste Wax in small enough areas so that the surface can be buffed before the wax has set and hardened, approximately five minutes.
3. After applying, buff each area to a soft sheen with a soft, dry cloth, weighted buffer or polisher.

PRECAUTIONS:
Do not use on surfaces other than wood. Do not apply polyurethane over wax. Do not store in warm area.

PRODUCT PROPERTIES:

COVERAGE 500 square feet per pound.
CLEAN UP Clean equipment using paint thinner, turpentine or mineral spirits.
MAINTENANCE Periodically remove dust and grit by sweeping or vacuuming. Wipe up spills as soon as possible. Periodic buffing will renew luster. Exceptionally worn areas will require an additional coat of DURA SEAL Paste Wax. When complete reconditioning is desired, clean surface using DURA SEAL Renovator Cleaner and Reconditioner.
STORAGE Keep containers tightly closed. Isolate from heat, sparks or open flame.
SOLVENT Mineral Spirits (Non-Photochemically Reactive)

PHYSICAL PROPERTIES:

DENSITY (LBS/GAL) 6.8 (Typical)
% SOLIDS 29.5 (Typical)
VISCOSITY Solid at Room Temperature
VOC WGT % 71.0
FLASH POINT 105°F

CAUTION:
COMBUSTIBLE MIXTURE DANGER!

KEEP OUT OF REACH OF CHILDREN.

DANGER:
Contains mineral spirits. Harmful or fatal if swallowed. Do not take internally. Skin irritant. Avoid contact with skin and eyes. Wear rubber gloves and safety glasses when handling. Avoid inhalation and use only with adequate ventilation. If adequate ventilation cannot be maintained, wear respiratory protection [NIOSH/MSHA TC23C or equivalent] or leave the area. Do not use or store near heat, sparks, flame or other sources of ignition. Close container after each use.

HEALTH/SAFETY:

HMIS RATING:  
Health 2
Flammability 2
Reactivity 0

HEALTH:
Effects of overexposure: irritation of eyes, skin and respiratory system.

FIRST AID:
If swallowed, do not induce vomiting. CALL PHYSICIAN IMMEDIATELY. For skin contact, wash thoroughly with soap and water. If irritation persists, get medical attention. In case of eye contact, immediately flush eyes thoroughly with water; then remove any contact lenses. Continue to flush eyes with water for at least 15 minutes. If irritation persists, CONTACT A PHYSICIAN. If affected by inhalation, remove to fresh air and CALL PHYSICIAN.

Color Size SKU # Case/Pack
NEUTRAL 1LB 86710 12
COFFEE BROWN 6LB 81723 4

06/03/99
lit # DS990014


10 Mountainview Rd., Upper Saddle River NJ 07458-1933 Tel: 1-800-364-1359
Dura Seal is a registered trademark. Copyright ©1999 Dura Seal. All rights reserved.
Site Design: JoeAl Creations