Freezer Manufacturers

Freezer Manufacturers directory includes comprehensive cad drawings, BIM families, and csi 3 part freezer specs. Additional content; Freezer Manufacturers videos, details on freezers that contribute to LEED credits, e-Catalogs and Arcat's patented SpecWizard® for accurately creating csi 3-part freezer specifications quickly and easily. Arcat content is free to all architects, spec writers and builders that need to select freezers for projects.   MORE +
 

Freezers for Your Home and Business

The use of freezers is very important to our wellbeing. At a restaurant, commercial freezers keep food fresh and free of spoilage. In a laboratory, an industrial freezer can keep hazardous and explosive materials secure and stabilized. Most importantly, in our homes, a freezer keeps our ice cream from melting.

The Importance of Freezer Maintenance

Freezers for commercial settings need to have proper upkeep, ensuring they stay at the correct temperature and continue to run properly. According to the Food and Drug Administration (the FDA), a freezer must be kept at 0 degrees Fahrenheit or below. Anything above this temperature would be a code violation. In addition to keeping the temperature stable, it is also important not to crowd a freezer. A freezer works best when there are pathways for the air to flow between the items being stocked. Following code guidelines should be followed through all types of freezers, from compact freezers to large, upright freezers.

Having a high-end and dependable freezer or refrigerator with precision temperature control is incredibly important in a laboratory. Unstable materials need to be kept and stored at certain temperatures: if there is too much temperature fluctuation in the freezers they are being kept in, the consequences can be explosive.

Freezers Can Be A Stylish Addition to Any Kitchen

For the freezers we use in our homes, we want something dependable and energy efficient, while looking sleek and stylish. Freezer manufacturers offer models that look at home in any kitchen, no matter what the design scheme. Freezer technology has improved over the years; freezers now have better and more accurate temperature control to keep food evenly frozen and to help defend food against freezer burn. Outdoor bars, patios, and kitchens can be brought to the next level with outdoor freezers.

ARCAT's service are here to lend support to you and your project. Our SpecWizard helps you create a customized 3-Part CSI Specification with ease. Our BIM Objects and CAD Drawings offer visualizations to make planning your projects simpler than ever before. Don't freeze up your project with problems, let ARCAT lend a hand.