Mastic Home Exteriors by Ply Gem -
START HERE
The SpecWizard concept is simple as 1, 2, 3:
1. Select products on the right
by checking check boxes
2. Configure the products
by selecting options
3. Generate Spec
in Word, WP or RTF
Mastic Home Exteriors by Ply Gem ; solid vinyl siding and soffit products.
This section is based on the products of
Mastic Home Exteriors by Ply Gem , which is located at:
2600 Grand Blvd. Suite 900
Kansas City, MO 64108
Toll Free Tel: 800-962-6973
Email: send email
Web: www.mastic.com
[click Here] for additional information.
Alcoa Home Exteriors® combined with Mastic® have set the standard for product quality and innovation for over 40 years. In fact, Mastic all but invented the vinyl siding category. Alcoa Home Exteriors is the leader in vinyl siding color selection with DreamColor™ - over 700 colors in virtually any hue or shade. No other low-maintenance cladding choice comes close. We offer dozens of siding choices from traditional and Dutch-lap styles to a variety of shake and shingle panels and a complete line of high-performance insulated siding plus all of the vinyl and metal accessories, soffits, rainware, gutter protection and trim that you need to specify and finish the job right.
Vinyl siding and accessories from Masic Home Exteriors are a sound environmental choice. NAHB Model Green Home Building Guidelines award 4 points in Section 2.1.5 for using building materials that require no additional finish resources to complete application on site. Builders who use vinyl siding are eligible for these points.
Eco-friendly homebuilders are finding that vinyl siding is green. When comparing fiber cement with vinyl, vinyl comes out ahead when designing an energy-efficient home. The bonus is the surface doesn't need to be repainted every five years like fiber cement siding. Because of its light weight, less energy is consumed in transporting vinyl siding to the home than other heavier exterior cladding materials. In addition, insulated siding from Mastic Home Exteriors can add 10 to 25 percent additional R-value to wall systems.
Mastic Home Exterior product are made in the U.S.A.
Research Building Product info:
[ ARCAT.com ]
[ Comments? ]
[ What would make SpecWizard better? ]