Grohe America, Inc. -
START HERE
The SpecWizard concept is simple as 1, 2, 3:
1. Select products on the right
by checking check boxes
2. Configure the products
by selecting options
3. Generate Spec
in Word, WP or RTF
Grohe America, Inc.; products.
.
This section is based on the products of
Grohe America, Inc., which is located at:
241 Covington Dr.
Bloomingdale, IL 60108-3109
Tel: 630-582-7711
Email: send email
Web: www.groheamerica.com
[ Click Here ] for additional information.
Grohe is recognized as one of the leading faucet brands used in custom homes and upscale remodeling projects. Innovations such as pull-out spray kitchen faucets, solid stainless steel kitchen faucets, single hole centerset lavs that replaced traditional American 4 inch configurations, and thermostatic shower safety valves are just a handful of the European concepts brought to the U.S. by Grohe. Engineered in Germany, Grohe products sold in the U.S. comply with domestic codes and standards.
Research Building Product info:
[ ARCAT.com ]
[ Comments? ]
[ What would make SpecWizard better? ]