COMPANY OVERVIEW

Kingspan Light + Air was founded with a vision; to become the global leader in energy efficient, sustainable lighting, natural ventilation and smoke management solutions for the roof and faCade non-residential sector. Our pledge to sustainability is instilled at every level of the Division and at every step in the manufacturing process.

Our pledge is to provide our customers with energy efficient, safe, sustainable and integrated solutions, that are additionally aesthetically pleasing. We never settle. We always innovate. At Kingspan Light + Air we're creating the products of the future, today. We innovate, so that our customers never have to choose between efficiency, sustainability, style and safety.

We push the boundaries of innovation in every project we're part of. From the Veltins Arena in Germany to the Southwestern Seminary, Texas, U.S.A., our mark spans five continents. Our customers work with us as we enable them to reduce unnecessary energy costs, by offering energy efficient, low carbon alternatives. For your next project, explore the many ways that Kingspan Light + Air can enhance the built environment and human productivity on the path to Net Zero.

ALL PRODUCTS

{{this.show}} {{this.hide}} Commercial Skylights

Bristol Acrylic Aluminum Fixed Unit Skylight image

Bristol Acrylic Aluminum Fixed Unit Skylight - Model: AL

6063-T5 Aluminum skylight comes with acrylic glazing and the option of curb mounted or self flashed.
Bristol Acrylic Aluminum Fixed Unit Skylight (Thermal Barrier Break) image

Bristol Acrylic Aluminum Fixed Unit Skylight (Thermal Barrier Break) - ALB

6063-T5 Aluminum skylight comes with acrylic glazing and a thermal barrier break frame and the option of curb mounted or self flashed.
Bristol Acrylic Aluminum Fixed Unit Skylight (Thermally Broken) image

Bristol Acrylic Aluminum Fixed Unit Skylight (Thermally Broken) - ALIT

6063-T5 Aluminum skylight comes with a thermally broken skylight frame and acrylic glazing. Comes self flashed only.
Coollite Solar Blocking Acrylic Aluminum Fixed Unit Skylight image

Coollite Solar Blocking Acrylic Aluminum Fixed Unit Skylight - AL

6063-T5 Aluminum skylight comes with a specially formulated solar heat blocking acrylic glazing and the option of curb mounted or self flashed.
Coollite Solar Blocking Acrylic Aluminum Fixed Unit Skylight (Thermally Broken) image

Coollite Solar Blocking Acrylic Aluminum Fixed Unit Skylight (Thermally Broken) - ALIT

6063-T5 Aluminum skylight comes with a thermally broken skylight frame and a specially formulated solar heat blocking acrylic glazing. Comes self flashed only.
Energy Star Fiberglass Aluminum Fixed Unit Skylight image

Energy Star Fiberglass Aluminum Fixed Unit Skylight - ES-S

Fiberglass capless skylight comes with a 6063-T5 Aluminum frame and the option of curb mounted or self flashed.
Nano Insulgel Super Insulating Polycarbonate Aluminum Fixed Unit Skylight image

Nano Insulgel Super Insulating Polycarbonate Aluminum Fixed Unit Skylight - AL

6063-T5 Aluminum skylight comes with acrylic prismatic glazing over a super insulating polycarbonate panel and the option of curb mounted or self flashed.
Nano Insulgel Super Insulating Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) image

Nano Insulgel Super Insulating Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) - ALIT

6063-T5 Aluminum skylight comes with a thermally broken skylight frame and acrylic prismatic glazing over a super insulating polycarbonate panel. Comes self flashed only.
Quasar LowE Solar Blocking and Super Insulating Polycarbonate Aluminum Fixed Unit Skylight image

Quasar LowE Solar Blocking and Super Insulating Polycarbonate Aluminum Fixed Unit Skylight - ALB

6063-T5 Aluminum skylight comes with a specially formulated solar heat blocking acrylic glazing over a super insulating polycarbonate panel and a thermal barrier break frame and the option of curb mounted or self flashed.
Quasar LowE Solar Blocking and Super Insulating Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) image

Quasar LowE Solar Blocking and Super Insulating Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) - ALIT

6063-T5 Aluminum skylight comes with a thermally broken skylight frame and a specially formulated solar heat blocking acrylic glazing over a super insulating polycarbonate panel. Comes self flashed only.
Quasar Prismatic Acrylic Aluminum Fixed Unit Skylight image

Quasar Prismatic Acrylic Aluminum Fixed Unit Skylight - AL

6063-T5 Aluminum skylight comes with acrylic prismatic glazing and the option of curb mounted or self flashed.
Quasar Prismatic Acrylic Aluminum Fixed Unit Skylight (Thermal Barrier Break) image

Quasar Prismatic Acrylic Aluminum Fixed Unit Skylight (Thermal Barrier Break) - ALB

6063-T5 Aluminum skylight comes with acrylic prismatic glazing and a thermal barrier break frame and the option of curb mounted or self flashed.
Quasar Prismatic Acrylic Aluminum Fixed Unit Skylight (Thermally Broken) image

Quasar Prismatic Acrylic Aluminum Fixed Unit Skylight (Thermally Broken) - ALIT

6063-T5 Aluminum skylight comes with a thermally broken skylight frame and acrylic prismatic glazing. Comes self flashed only.
Tufflite Polycarbonate Aluminum Fixed Unit Skylight image

Tufflite Polycarbonate Aluminum Fixed Unit Skylight - AL

6063-T5 Aluminum skylight comes with polycarbonate glazing and the option of curb mounted or self flashed.
Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermal Barrier Break) image

Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermal Barrier Break) - ALB

6063-T5 Aluminum skylight comes with polycarbonate glazing and a thermal barrier break frame and the option of curb mounted or self flashed.
Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) image

Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) - ALIT

6063-T5 Aluminum skylight comes with a thermally broken skylight frame and polycarbonate glazing. Comes self flashed only.
Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) image

Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) - HWHS

6063-T5 Aluminum heavy duty skylight comes with polycarbonate glazing suited for heavy weather and high security. Comes with NOA, Florida Building Code, FM, Department of Defence, UL and AAMA approval. Comes curb mounted or self flashed.
Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) image

Tufflite Polycarbonate Aluminum Fixed Unit Skylight (Thermally Broken) - HWHSF5

6063-T5 Aluminum heavy duty skylight comes with polycarbonate glazing suited for heavy weather and high security. Comes with ICC-500, NOA, Florida Building Code, FM, Department of Defence, UL and AAMA approval. Comes curb mounted or self flashed.

{{this.show}} {{this.hide}} Commercial Smoke Vents

Bristol Aluminum Metal Lid Smoke Vent image

Bristol Aluminum Metal Lid Smoke Vent - SVAM

11-Gauge aluminum smoke vent with flat metal lids. Lids can open against a 10, 20 or 30 lb psf uniform load and come as UL Listed & FM Approved. Can be curb mounted or self flashed.
Bristol Aluminum Smoke Vent image

Bristol Aluminum Smoke Vent - SVAA

11-Gauge aluminum smoke vent with acrylic bubble dome lids. Lids can open against a 10 lb psf uniform load and comes as UL Listed. Can be curb mounted or self flashed.
Bristol Galvanized Steel Metal Lid Smoke Vent image

Bristol Galvanized Steel Metal Lid Smoke Vent - SVSM

14-Gauge galvanized steel smoke vent with flat metal lids. Lids can open against a 10, 20 or 30 lb psf uniform load and come as UL Listed & FM Approved. Can be curb mounted or self flashed.
Bristol Galvanized Steel Smoke Vent image

Bristol Galvanized Steel Smoke Vent - SVSA

14-Gauge galvanized steel smoke vent with acrylic bubble dome lids. Lids can open against a 10 lb psf uniform load and comes as UL Listed. Can be curb mounted or self flashed.
Energy Star Aluminum Smoke Vent image

Energy Star Aluminum Smoke Vent - SVAF

11-Gauge aluminum smoke vent with fiberglass bubble dome lids. Lids can open against a 10, 20 or 30 lb psf uniform load and come as UL Listed & FM Approved. Can be curb mounted or self flashed.
Energy Star Galvanized Steel Smoke Vent image

Energy Star Galvanized Steel Smoke Vent - SVSF

14-Gauge galvanized steel smoke vent with fiberglass bubble dome lids. Lids can open against a 10, 20 or 30 lb psf uniform load and come as UL Listed & FM Approved. Can be curb mounted or self flashed.
Quasar Aluminum Smoke Vent image

Quasar Aluminum Smoke Vent - ECO-SVAP

6063-T5 Aluminum smoke vent with prismatic acrylic triarch dome lids. Lids can open against a 10 lb psf uniform load and comes as UL 793 Listed. Can be curb mounted or self flashed.
Quasar Galvanized Steel Smoke Vent image

Quasar Galvanized Steel Smoke Vent - ECO-SVSP

14-Gauge galvanized steel smoke vent with prismatic acrylic triarch dome lids. Lids can open against a 10 lb psf uniform load and comes as UL 793 Listed. Can be curb mounted or self flashed.
Tufflite Aluminum Smoke Vent image

Tufflite Aluminum Smoke Vent - ECO-SVAPC

6063-T5 Aluminum smoke vent with polycarbonate triarch lids. Lids can open against a 10 lb psf uniform load and comes as UL 793 Listed. Can be curb mounted or self flashed.
Tufflite Galvanized Steel Smoke Vent image

Tufflite Galvanized Steel Smoke Vent - ECO-SVSPC

14-Gauge galvanized steel smoke vent with polycarbonate triarch lids. Lids can open against a 10 lb psf uniform load and comes as UL 793 Listed. Can be curb mounted or self flashed.

{{this.show}} {{this.hide}} Commercial Smoke Hatches

Energy Star Aluminum Smoke Hatch - SHD

Aluminum smoke hatch with a fiberglass bubble dome. Can be curb mounted or self flashed.

Energy Star Galvanized Steel Smoke Hatch - SSHD

Galvanized steel smoke hatch with a fiberglass bubble dome. Can be curb mounted or self flashed.

Quasar Aluminum Smoke Hatch - ASHD

Aluminum smoke hatch with a prismatic acrylic triarch dome. Can be curb mounted or self flashed.

{{this.show}} {{this.hide}} Commercial Louvered Skylights

Energy Star Louvered Aluminum Smoke Hatch - ES-SL

Fiberglass capless louvered skylight comes with a 6063-T5 aluminum frame and the option of curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

Energy Star Louvered Galvanized Steel Smoke Hatch - ES-SSL

Fiberglass capless louvered skylight comes with a 20-gauge galvanized steel frame and the option of curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.
Quasar Louvered Aluminum Smoke Hatch image

Quasar Louvered Aluminum Smoke Hatch - SL-CM

Prismatic acrylic louvered skylight comes with a 6063-T5 aluminum frame and the option of curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

{{this.show}} {{this.hide}} Commercial Louvered Smoke Vents

Quasar Louvered Galvanized Steel Smoke Vent - ECO-SVSPL

14-Gauge galvanized steel louvered smoke vent with prismatic acrylic triarch lids. Lids can open against a 10 lb psf uniform load and comes as UL 793 Listed. Can be curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

- ECO-SVAPCL

6063-T5 Aluminum louvered smoke vent with polycarbonate triarch lids. Lids can open against a 10 lb psf uniform load and comes as UL 793 Listed. Can be curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

{{this.show}} {{this.hide}} Commercial Louvered Smoke Hatches

Energy Star Louvered Aluminum Smoke Hatch - SHDL

Aluminum capless fiberglass louvered smoke hatch with a bubble dome. Can be curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

Energy Star Louvered Galvanized Steel Smoke Hatch - SSHDL

Galvanized steel capless fiberglass louvered smoke hatch with a bubble dome. Can be curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

Quasar Louvered Aluminum Smoke Hatch - ASHDL

Aluminum louvered smoke hatch with a prismatic acrylic triarch dome. Can be curb mounted or self flashed. Louver blades are 22-gauge galvanized steel.

{{this.show}} {{this.hide}} Commercial Dropouts

Natural Series Dropout - ESSLDOUL

Aluminum UL Listed dropout with acrylic bubble domes.

{{this.show}} {{this.hide}} Residential Unit Skylights

Alumilite Fixed Unit Skylight image

Alumilite Fixed Unit Skylight - AL

6063-T5 Aluminum skylight comes with acrylic glazing and the option of curb mounted or self flashed.
Alumilite Fixed Unit Skylight (Thermally Broken) image

Alumilite Fixed Unit Skylight (Thermally Broken) - ALT

6063-T5 Aluminum thermally broken skylight comes with acrylic glazing and the option of curb mounted or self flashed.
Alumilite Glass Fixed Unit Skylight image

Alumilite Glass Fixed Unit Skylight - GAL

6063-T5 Aluminum skylight comes with a flat glass panel and the option of curb mounted or self flashed.
Alumilite Glass Fixed Unit Skylight (Thermally Broken) image

Alumilite Glass Fixed Unit Skylight (Thermally Broken) - GALT

6063-T5 Aluminum thermally broken skylight comes with a flat glass panel and the option of curb mounted or self flashed.
Alumilite Multi-Panel Glass Fixed Unit Skylight image

Alumilite Multi-Panel Glass Fixed Unit Skylight - GALM

6063-T5 Aluminum skylight comes with multiple flat glass panels divided by a mullion and the option of curb mounted or self flashed.
Alumilite Multi-Panel Glass Fixed Unit Skylight (Thermally Broken) image

Alumilite Multi-Panel Glass Fixed Unit Skylight (Thermally Broken) - GALTM

6063-T5 Aluminum thermally broken skylight comes with multiple flat glass panels divided by a mullion and the option of curb mounted or self flashed.
Thermoweld Fixed Circular Skylight image

Thermoweld Fixed Circular Skylight - ACS

Circular skylight consisting of a fiberglass frame fused with acrylic domes using a "Thermoweld" process. Can be curb mounted or self flashed.
Thermoweld Fixed Unit Skylight image

Thermoweld Fixed Unit Skylight - AS

Skylight consisting of a fiberglass frame fused with acrylic domes using a "Thermoweld" process. Can be curb mounted or self flashed.
Thermoweld Fixed Unit Skylight (Thermally Broken) image

Thermoweld Fixed Unit Skylight (Thermally Broken) - AST

Skylight consisting of a fiberglass frame fused with acrylic domes using a "Thermoweld" process and a thermally broken 6063-T5 extruded aluminum sub-frame. Can be curb mounted or self flashed.

{{this.show}} {{this.hide}} Residential Openable Skylights

Alumilite Glass Openable Skylight (Electric) image

Alumilite Glass Openable Skylight (Electric) - GAL-ESD

Electrically openable 6063-T5 Aluminum skylight comes with a flat glass panel and the option of curb mounted or self flashed.
Alumilite Glass Openable Skylight (Manual) image

Alumilite Glass Openable Skylight (Manual) - GAL-SD

Manually openable 6063-T5 Aluminum skylight comes with a flat glass panel and the option of curb mounted or self flashed.
Alumilite Multi-Panel Glass Openable Skylight (Electric) image

Alumilite Multi-Panel Glass Openable Skylight (Electric) - GALM-ESD

Electrically openable 6063-T5 Aluminum skylight comes with multiple flat glass panels divided by a mullion and the option of curb mounted or self flashed.
Alumilite Multi-Panel Glass Openable Skylight (Manual) image

Alumilite Multi-Panel Glass Openable Skylight (Manual) - GALM-SD

Manually openable 6063-T5 Aluminum skylight comes with multiple flat glass panels divided by a mullion and the option of curb mounted or self flashed.
Alumilite Openable Skylight (Electric) image

Alumilite Openable Skylight (Electric) - AL-ESD

Electrically openable 6063-T5 Aluminum skylight comes with acrylic glazing and the option of curb mounted or self flashed.
Alumilite Openable Skylight (Manual) image

Alumilite Openable Skylight (Manual) - AL-SD

Manually openable 6063-T5 Aluminum skylight comes with acrylic glazing and the option of curb mounted or self flashed.
Thermoweld Openable Skylight (Electric) image

Thermoweld Openable Skylight (Electric) - AS-ESD

Electric openable skylight consisting of a fiberglass frame fused with acrylic domes using a "Thermoweld" process. Can be curb mounted or self flashed.
Thermoweld Openable Skylight (Manual) image

Thermoweld Openable Skylight (Manual) - AS-SD

Manually openable skylight consisting of a fiberglass frame fused with acrylic domes using a "Thermoweld" process. Can be curb mounted or self flashed.

{{this.show}} {{this.hide}} Tubular Skylights

Quasar Reach Drop Ceiling Skylight image

Quasar Reach Drop Ceiling Skylight - DCS

Aluminum frame with prismatic acrylic outer glazing and inner diffuser. Comes curb mounted or self flashed with options of a Dimmer Kit (DK) and/or Transition Box (TB). Standard length is 4 foot but can be ordered in multiple lengths

{{this.show}} {{this.hide}} Accessories

Airflow Exhaust/Intake Penthouse - EIP

Exhaust/Intake Penthouses provide a protected method of air movement for a building during normal weather conditions. Storm resistant louver blades are utilized to keep out severe weather but keep the air moving. 

Airflow Gravity Vent image

Airflow Gravity Vent - GV

Gravity vents can greatly improve your health, mood and productivity. Gravity vents are installed on areas of the roof where there is a known breeze. This natural ventilation can enter the building and help to reduce odors, eliminate stagnant air and provide cleaner oxygen to breathe improving the lives of the occupants inside the building. Bird screens and optional insect screens are installed in order to keep them out and, yet, allow fresh air into the building. 

Gladiator External Safety Cage image

Gladiator External Safety Cage - SCAGE

Strong. Protective. Gladiator. When it comes to roof safety we are very concious of the needs of the building owners and individuals that have access to the roof. We are proud to offer an external safety cage roof safety product that can be installed at the same time as the skylight or delivered to site factory fitted to the skylight. You can also attach our Gladiator External Safety Cages by means of a retrofit, to new or existing unit skylights or circular skylights, as needed by the local authorities, building owners or general contractors.

Gladiator Roof Access Hatch image

Gladiator Roof Access Hatch - SAH

14-guage steel construction highlighted with yellow and black striped visual warning tape. Comes in either grey paint or safety red paint. For added daylighting benefits an optional acrylic or polycarbonate skylight can be included in the access hatch door. Comes curb mounted or self flashed.
Gladiator Safety Screen image

Gladiator Safety Screen - SSCRN

Strong. Protective. Gladiator. When it comes to roof safety we are very concious of the needs of the building owners and individuals that have access to the roof. We are proud to offer a safety screen roof safety product that can be installed on site prior to the skylight installation or, for ease of installation, the safety screens can be factory fitted with the skylight or smoke vent.

Gladiator Security Grill image

Gladiator Security Grill - SG

Strong. Protective. Gladiator. When it comes to roof safety we are very concious of the needs of the building owners and individuals that have access to the roof. We are proud to offer a security grill roof safety product that can be installed directly on to the roof deck or on to the roof curb prior to the installation of the skylight or smoke vent.

Gladiator Structural Curbs - SC

14-guage galvanized steel construction with optional wood nailer, rigid polyisocyanurate insulation, double wall and/or safety screens.
Solar Breeze Solar Powered Attic Fan image

Solar Breeze Solar Powered Attic Fan - SAF

Black or grey powder coated aluminum housing with a non-corrosive air driven precision pitch 5-blade fan. Operated by a 10W, 20W, 30W or 50W high impact photovoltaic solar panel. Comes curb mounted, gable mounted or self flashed.

{{this.show}} {{this.hide}} Case Studies

Ashland Middle School image

Ashland Middle School

Eneref Institute examines how a rooftop repair program was employed to brighten a Massachusetts middle school.

Lance Camper Manufacturing Facility

Manufacturer of truck campers provides the ultimate facility for productivity and profits through daylighting.


password:  
Last Update: 2019-11-27