Bona QUANTUM FLOW® is a pourable adhesive that has outstanding “green-grab" properties and helps to cover a larger surface area in less time without causing fatigue. Quick and efficient, flooring can be ready in as little as one day for furniture and foot traffic.
Bona QUANTUM™ R851 is a silane-based wood flooring adhesive that provides exceptional "green grab" strength. Its elastomeric characteristics allow the adhesive to move with the wood as it expands and contracts over the life of the floor.
Bona R850T® provides outstanding adhesion to a variety of surfaces, and allows for the natural movement of wood flooring. Use along the leading edge of refinished or solid plank floors, coupled with staple or nail down system. This product is made in the USA and qualifies for Leed 4.1.
Bona QUANTUM™ T is a silane-based wood flooring adhesive that helps reduce voids caused by uneven substrates. Elastomeric characteristics allow the adhesive to move with the wood as it expands and contracts over the life of the floor. The thicker formula mimics a traditional "urethane" feel.
Bona VERTICALTM has an extremely high initial bonding strength and rapid setting formulation. It is perfect for horizontal and vertical applications. The bonding process can be accelerated by lightly misting substrate prior to application, and/or lightly misting the adhesive once applied.
• Rapid set - within a few minutes!
• Great for trim, starter rows, treads, risers, vertical applications, and wall treatments
• 300% improved Green Grab, better vertical adhesion without slump or use of fasteners!
• 10%+ improved sheer strength
• GREENGUARD Gold & zero VOCs
• Addition of multiple substrates including PVC, LVT metal, acrylic paints
Bona® R540 is a polyurethane reactive primer that is compatible with the entire Bona System. It is specially designed to mitigate vapor transmission on absorbent and non-absorbent floors, including Gypsum-based underlayment.
Bona Domo™ is the newest member of the Bona family of finishes. This easy-to-use, entry-level waterborne finish is easy to abrade and has a quick drying formula.
Easy and forgiving to apply with a roller or T-bar, the one-component, non-yellowing formulation comprises all essential properties for finishing and protecting wood floors. And because it's waterborne with low VOCs, Bona Domo provides a healthy environment.
Bona Traffic HD RAW™ is a two-component, waterborne finish that preserves the look and feel of natural wood. This distinct floor finish allows users to get as close to an untreated look and
feel as possible while still maintaining exceptional Bona Traffic HD® level durability. The extremely low, ultra-matte sheen is consistent from all angles and produces a smooth, soft, natural surface with the fell of raw wood beneath your feet.
• Ultra-matte, low sheen that is consistent from every angle
• High durability – Unsurpassed scuff, scratch and chemical resistance at full cure
• Natural anti-slip properties
• Fast dry time – approximately 2-3 hours
• Full cure in 3 days
• VOC compliant
• GREENGUARD GOLD certified
Bona Traffic HD® is for hardwood floor owners with an uncompromising attitude towards durability, lasting beauty and sustainable solutions. Significantly outperforms all urethane finishes, including Bona Traffic, in durability at 24 hours. Very low VOCs - less than 150 g/L, nonflammable and non-offending odor.
The world's leading waterborne finish, providing unsurpassed scuff, scratch and chemical resistance.
Bona Traffic HD® Anti-Slip is a newly formulated finish that features all the same benefits of Bona Traffic® with the added benefit of meeting the highest standards for slip resistance, has low/no odor and is an ideal choice for commercial applications where anti-slip properties are required or in residential settings on stairs, in kitchens or homes occupied with older adults.
Part B Hardener that should be added to a gallon of Bona Traffic HD®.
Bona Traffic HD® Universal Hardener is the Part B to be mixed with Bona Traffic HD®.
Introducing the newest member to the starting lineup of Bona Traffic HD® family of finishes, Traffic HD - Commerical Gloss. Bona Traffic HD - Commerical Gloss brings a whole new level of shine to your hardwood floors with a unique hybrid gloss level, in between a traditional high gloss and semi-gloss sheen, plus all the added benefits you know and love from the Traffic HD Family of products.
Bona Mega ONE® simplifies the craftsman's everyday life, making the job faster and easier with the quality you depend on. Bona Mega ONE is a clear, waterborne one-component finish that dries fast, is easy to use and provides high build for superior protection.
Bona Mega® is the proven performance and value standard waterborne hardwood floor finish in the industry for residential and commercial floors. An oxygen-crosslinking polyurethane (OCP) formula with extraordinary performance.
Bona Retarder is designed to retard the drying/curing process of Bona waterborne finishes, allowing for more open time in less than ideal working environments, such as very hot or dry climates.
Bona ClassicSeal is an exceptionally clear waterborne sealer that highlights the natural color of the wood, minimizes grain raise and tannin bleed. Provides a build layer and prevents the finish from penetrating into the wood surface.
Floor sealer highlighting the wood's natural color. Bona ClearSeal™ is a waterborne sealer that offers easy abradability, great build characteristics and is fast drying. The clear aspect offers a classic appearance which highlights the natural color of wood. Bona ClearSeal provides an initial layer that prevents the finish from penetrating into the wood.
Bona IntenseSeal® is a specifically formulated waterborne sanding sealer that develops a vibrant look and deep, natural tone to individual wood species. Bona waterborne wood floor sealers offer excellent abradability, fast dry times, and reduced potential for side bonding and tannin bleed. They are non-flammable and virtually odorless sealers.
Bona NaturalSeal® is a waterborne sanding sealer designed to retain the appearance of unfinished wood on your floor. Combining Bona NaturalSeal with a matte-sheen finish such as Bona Traffic Naturale preserves that look and gives your floor the durability it needs for everyday life. Bona waterborne wood floor sealers offer excellent abradability, fast dry times, and reduced potential for side bonding and tannin bleed. They are non-flammable and virtually odorless sealers.
Bona AmberSeal® is a non-yellowing, poly-tone waterborne sanding sealer that provides an oil-based look to hardwood floors. Can be used with all Bona waterborne finishes over both stained and unstained floors. Bona waterborne wood floor sealers offer excellent abradability, fast dry times, and reduced potential for side bonding and tannin bleed. They are non-flammable and virtually odorless sealers.
Bona NordicSeal® is a waterborne sanding sealer that is formulated to provide a green alternative to a whitewashed floor without the use of caustic materials such as bleach. A unique way of customizing your floor from a light whitewash to successive coats, providing a truly Scandinavian look. Bona waterborne wood floor sealers offer excellent abradability, fast dry times, and reduced potential for side bonding and tannin bleed. They are non-flammable and virtually odorless sealers.
Bona DriFast® Sealer is a quick drying, oil-modified polyurethane sanding sealer that's designed to penetrate and seal bare wood. It is compatible with all Bona stains, oil-modified and waterborne finishes. It meets ASTM D 1640 for quick-dry sealers and is VOC Compliant under U.S. EPA regulations.
Bona Woodline® Poly provides a tough protective coat and slight amber color to enhance the natural tone of the wood. It will adhere to most solvent-based stains and finishes and most waterborne finishes after proper preparation, drying times, and curing times. It does not require thinning when used under normal environmental and application conditions (65 degrees -75 degrees F, 40-60% relative humidity).
An oil-modified stain that dries and is recoatable in two hours. Advanced technology, quick-drying formula provides speed and high performance for hardwood flooring professionals.
The Metropolitan Collection is comprised of saturated reds, smoky browns, grays and rich, chocolaty black. Each color captures an urban vibe that's just right for today's sophisticate. Compatible with all Bona waterborne systems and all other Bona finish systems. All stain colors are available in quart and gallon sizes.
An oil-modified stain that dries and is recoatable in two hours. Advanced technology, quick-drying formula provides speed and high performance for hardwood flooring professionals.
The Classic Collection is a rich presentation of authentic browns and rich auburns that compliment the heritage of traditional design. This exemplary palette has its roots in the natural appeal of hardwoods. Compatible with all Bona waterborne systems and all other Bona finish systems. All stain colors are available in quart and gallon sizes.
An oil-modified stain that dries and is recoatable in two hours. Advanced technology, quick-drying formula provides speed and high performance for hardwood flooring professionals.
The Essentials Collection is comprised of warm ambers and hints of exotic spices that transport this palette across varied design styles. Find just the right shade for your particular paradise. Compatible with all Bona waterborne systems and all other Bona finish systems. All stain colors are available in quart and gallon sizes.
An oil-modified stain that dries and is recoatable in two hours. Advanced technology, quick-drying formula provides speed and high performance for hardwood flooring professionals.
The Natural Collection is subtle and soft with light tones mixed with warm whites. This easy, breezy collection blends right in with your everyday, everyway living. Compatible with all Bona waterborne systems and all other Bona finish systems. All stain colors are available in quart and gallon sizes.
Capture the ideal expression of your home's personality by combining our know-how and your creativity.
Bona Red Out™ is a simple, easy-to-use solution to remove red and pink hues commonly found in red oak flooring and other wood species with red tones.
Bona Red Out is a two-step waterborne color neutralizer designed to reduce red and pink tones to help mimic the look of white oak wood flooring. Bona Red Out is safe to use on multiple wood species from red oak to Brazilian cherry. This unique product is very low odor, dries quickly, and is compatible with the entire Bona System® to allow easy preparation for staining, sealing, and finishing, making it the perfect first step to achieve lighter tones including a nordic look no matter the color or species of wood.
Bona Red Out is safe for all residential and commercial flooring surfaces where a lighter, natural style is preferred. Because it is a waterborne product, there is also no need to water pop the floor prior to staining, saving valuable time. There is no pot life with Bona Red Out so there is minimal waste and it can be used across multiple jobs. Plus, the product can be diluted with water for easy customization to fit any project needs.
Bona Craft Oil® 2K is made from modified vegetable oils, and catalyzed with a hardener for quicker drying and greater durability. It can be used on its own as a fast-drying, high-performance oil, or can be over-coated with any finish from the Bona Traffic® family, to add gloss and minimize future maintenance. The 2K oil works perfectly with a wide variety of wood species, including cherry, walnut, smoked oak and steamed beech.
This kit includes everything needed for easy and safe cleaning of natural oil treated hardwood floors on a professional level.
A vegetable oil-derived maintenance oil for the professional upkeep of oiled hardwood floors.
Bona Craft Oil 2K® Care is used for the professional maintenance of oiled floors. It is a mixture of vegetable oils that delivers superior protection, allows for great coverage, and penetrates for fast saturation. Indoor air quality is maintained due to extremely low VOCs and its quick drying attribute.
A professional-strength concentrated cleaner specially formulated for oiled hardwood floors.
Bona Craft Oil® 2K Soap gently and safely removes dirt, grime, and marks from oiled hardwood floors. This specially formulated concentrate cleans and nourishes the surface. For professional use only.
Bona Pacific Filler® is a high solids, waterborne compound specifically designed for filling cracks, holes, chips, gouges, and broken edges in hardwood floors prior to finishing. It is a ready-to-use formula, for spot or full-trowel filling. It has excellent adhesion, staining, and finishing properties with minimal shrinkage. For more accurate color matching, Bona Pacific Fillers can be blended together, tinted with universal tints, or mixed with fine edger dust to achieve the closest match possible.
Restore for a longer floor lifetime. Your customers work hard to ensure their hardwood floors look beautiful, but over time, the finish is slowly removed by the friction of daily foot traffic in the home. If the necessary steps to properly maintain them are not met, eventually bare wood will be exposed requiring a complete refinish. Every few years floors can be recoated to maintain their protective layer with the Bona Recoat System. This proved recoat process safely removes contaminants from the floor, rinses the floor clean and refortifies the hardwood floor with a new coat of Bona Traffic or Bona Traffic HD. In less than a day your customers can have a new coat of finish that restores the beauty and prolongs the life of their hardwood floor.
Revive effectively with little downtime. When regular maintenance isn't enough to cut through ground-in-dirt on your customers' hardwood floors, offer them the benefits of a professional cleaning system from the experts in hardwood floor care - the Bona Deep Clean System. This innovative deep cleaning system is the safest, quickest and easiest way to remove all the dirt, grime and build-up on hardwood floors. It's an excellent way to thoroughly clean wire-brushed floors as well. With no need to vacate their home, this system protects their investment and keeps floors looking beautiful.
Refinish for total beauty. When a hardwood floor is severely damaged or yellowed, or your customers simply want to change the color and look of their floor, the Bona Refinish System is the perfect solution. Using our comprehensive sanding equipment, abrasives and dust containment systems, the floor is sanded down to bare wood and then finished with the look and protection they need. It's like providing a whole new floor with endless possibilities.
Bona SuperSport® HD provides a tough, high-build urethane finish. Premium two-component waterborne wood sport floor finish specifically formulated for professional use on maple sport floors.
Bona SuperSport DRIVE® is a one-component finish with the superior features of a premium two-component finishing system. It provides a tough, urethane finish with good build. Bona SuperSport DRIVE is highly durable with a vibrant gloss sheen, is safe for the environment, and is ready for play in just 24-hours.
Bona SuperSport ONE® is one of the leading one-component sport finish for durability and appearance. It is a premium, waterborne wood floor finish specifically formulated for use on professional maple sport floors.
Bona SuperSport DTS® is specially formulated waterborne sanding sealer for use with all Bona waterborne finishes. It seals the wood, develops a deep natural tone and vibrant look, abrades easily and prevents the finish from penetrating into the wood surface.
Bona SuperSport Seal® is a unique, quick-drying, non-ambering formula that reduces grain raise and prepares the floor for a protective top coat of sport floor finish.
Bona SuperSport MVP™ is a two-component, premium waterborne wood sport floor finish for professional use on maple sport floors. It stands up to back-to-back games, community events and large crowds all while maintaining a beautiful design for years to come.
Bona SuperSport ELITE™ is a two-component, premium waterborne sport floor finish specifically formulated for professional use on wood sport floors. It is a low VOC urethane finish that dries quickly and is fully cured in 3 days.
Bona Sport Crosslinker to be used with Bona 2-component Finishes
MIXING INSTRUCTIONS: SHAKE OR STIR WELL BEFORE USING. 1. Open the crosslinker bottle and add an equal part of water to the crosslinker. 2. Shake well. 3. Add the crosslinker/water mixture to the finish within 15 minutes. 4. Shake or stir immediately and let sit 5-10 minutes. POT LIFE: The finish/crosslinker mixture is active for approximately 8 hours. Within 2-3 days of the first use, crosslinker may be added a second time.
Bona Sport® Poly 275 is a premium, oil-modified polyurethane developed specifically for the wood sport floor market. It is low VOC and provides an extremely tough, high-build gloss finish with excellent chemical resistance.
Bona Sport® Poly 350 has low VOC's and provides an extremely tough, high-build gloss finish with excellent chemical resistance. It is specially formulated to meet all federal and state clean air quality standards.
Bona Sport® Poly provides an extremely tough, high-build gloss finish with excellent chemical resistance to protect against perspiration and routine cleaning. Meets federal and most state air quality standards.
Bona All Court® Poly provides an extremely tough, high-build gloss finish with superior flow and leveling. It has a light amber color to enhance the natural color of the wood.
Bona DriFast® Sport Seal is compatible with all Bona® Paints and oil-modified and waterborne sport floor finishes.
Bona Sport® Seal 350 is formulated for use with Bona Sport® Poly 350. It seals the wood, providing a build layer and prevents the finish from penetrating. It is formulated to meet all federal and state clean air quality standards.
Bona Sport® Seal is formulated for use with Bona Sport® Poly and Bona All Court® Poly. It seals the wood, providing a build layer and prevents the finish from penetrating. It meets all federal and most state clean air quality standards.
Bona CourtLines® Sport Floor Paint is for use with both waterborne and oil-modified sport floor sealers and finishes. Available in 15 primary colors and blendable to achieve an endless array of custom colors.
Bona SuperSport Paint® is a fast drying, waterbased game line paint manufactured for use with both Bona® waterborne and oil-modified sport floor sealers and finishes. Domestically sourced pigments allow for a shelf-life of 18 months and offer better hiding.
By combining waterborne and oil-modified finish systems, you are able to reduce dry times and minimize the risk for poly balls while maintaining Bona's durability and beauty of athletic wood floors. Bona's hybrid systems can be applied to newly installed floors, or existing floors, depending on the look your customers want.
With nearly 100 years of heritage, the Bona name captures high recognition among consumers around the world. Synonymous with quality, beauty and durability, Bona opens up a world of trust and confidence proven through market research.
.
A unique product designed for the transformation of resilient floors.
The Bona Commercial System® Resilient Floor Base Color ensures a quick application process with accelerated drying properties and heavy pigmentation for single-coat coverage.
Specifically formulated for the treatment of resilient floors.
Bona Commercial System® Resilient Clear Coat offers a long lasting and extremely durable coating to create a monolithic surface for heavy traffic in schools, industrial and commercial areas, restoring the appearance and simplifying routine maintenance.
Provide improved slip resistance with Bona Commercial System® Antislip Additive. One 5.3 oz. bag treats one 5L of Bona Commercial System™ Resilient Floor Finish. For added slip resistance, a second coat can be appilied.
Provides additional slip protection on wet or dry surfaces;Easy to apply;No additional time applied during coating process
The Bona Commercial System® Multi-Surface Floor Primer is specially formulated to reduce the need for additional coats of color. This formula is designed to lessen the appearance of seams and cracks on resilient and concrete floors creating a seamless and durable look across the floor.
Achieve unique and beautiful design elements when transforming resilient floors.
Bona Commercial System® Premium Color Chips can be added in various concentrations depending on the desired look.
A unique product designed for the renewal of concrete floors.
The Bona Commercial System® Concrete Floor Base Color ensures a quick application process with accelerated drying properties and heavy pigmentation for single-coat coverage.
Specifically formulated for the treatment of concrete floors.
The Bona Commercial System® Concrete Floor Clear Coat provides optimal application and leveling properties as the final step in the renewal process. This formula offers long-term surface protection against heavy traffic on concrete floors.
Hardwood floors add warmth, natural beauty and value to any home. Bona finishes highlight the true color of the wood with unsurpassed beauty and durability. Select from the list on the right to view homes from around the world with Bona High Durability Finishes.
The demands on high traffic areas such as offices and public places are extremely high. For new installations, refinishing and maintaining existing floors, Bona provides the solution for combining high performance with concern for indoor air quality, as well as environmental and personal health.
1,119,446.68 square feet of the Copenhagen Airport are frequently renovated and maintained with Bona's oil and cleaning products.
A hardwood floor plays an important role in the perception of a restaurant or a hotel. Bona finishing systems protect these high traffic floors with long-lasting beauty.
Oak floor that has been installed at the Assembly Hotel with Bona products.
Minimize risk in finishing for basketball, volleyball, racquetball, aerobics, or any hardwood sport floor with products designed to work as a team at each step of the process. Bona Sport systems consistently produce championship appearance and performance for high schools, colleges and professional arenas across North America.
To meet the environmental requirements of Earth Smart B, Bona Traffic was chosen as the finish for their facility. It was used on the maple floors in the cafeteria, entrance and gift shop as well as office premises.