Amarr 3582 Aluminum MultiView doors make a unique design statement with the widest single piece of glass that specifications, safety, and reliability standards allow. Constructed of 2" thick extruded aluminum rails and stiles, these doors are built to last
Since our founding in 1951, Amarr Company has understood the importance of its role in sustaining resources to ensure a positive future for generations to come. As a leader in the garage door industry, we strive to partner with like-minded suppliers whose sustainability goals align with ours. In conjunction with our efforts to preserve natural resources, we also strive to engage in energy efficient manufacturing processes while choosing green products for our garage doors and implementing recycling methods to ensure we meet our defined sustainability goals.
The mechanics that allow your garage door to lift and lower involve the cables on either side of the door frame. The door is lifted through a transmission of energy from the springs attached to the door, the garage door opener, and the tracks. These forces all work together, but if one fails, such as a cable snaps or falls out of a drum, the garage will not function at all and will either fall or be unable to lift.
Garage door cable repair can be difficult and dangerous, but with the right help, it can be done properly.
Are you wanting an upgrade to your home's exterior? Or maybe you're planning to sell your home and you need some guidance on ways to get the most bang for your buck. Updating and replacing outdated or nonfunctional items around the house can help increase the charm of your property, which means buyers may be willing to spend more.
Among the list of renovations to consider, replacing an antiquated or defective garage door can help boost curb appeal by simultaneously improving your home's appearance and functionality. But even if you aren't looking to put your house on the market, updating your garage door can improve the safety and efficiency of your garage — especially if your current door is not working properly.
But how much does it cost to replace a garage door and what type of door is best suited for your home?
For many, the winters are long, dark and cold. We're all trying our best to feel comfortable until the first sight of Summer when the weather clears, the flowers bloom and the sunshine feels warm again. As soon as the sundresses and shorts make their first debut, entertaining guests become top of mind.
Before then, Summer cleaning is an essential part of ushering in the new season and letting go of the clutter of last year. We'll take a look at the tradition of Summer cleaning, where to start and how to reset your garage's organization.
Are you looking for that one-of-a-kind garage door that no one else has? Or maybe you're building your dream home and want that extra WOW factor with a designer garage door; then Amarr has the perfect solution.
The newest Axolotl for Amarr garage door collection gives you the flare and aesthetic you've been searching for with our fancy garage doors. Highly customizable with unique finishes, this collection offers distinctiveness paired with reliable construction.
Mid-century design meets modern garage door innovation with these cleverly placed "window walls" allowing visitors to take in the picturesque views of this vibrant downtown area.
TAKE A LOOK
With a need to withstand high winds sweeping through this mountainous region, Amarr's steel and aluminum full panel overhead sectional doors provided the proper amount of protection for this new fire department.
SEE THE FINALE
With an operable wall approach using Full View Amarr garage doors, Chicken N Pickle combined the indoors with the outdoors so players and spectators could easily enjoy all this entertainment complex had to offer.
JOIN IN THE FUN
Amarr’s hybrid section door solution not only met the LEED Gold Certification requirements but also showcased a beautifully designed architectural facility.
SEE HOW TO GO GREEN
Reaching a specific LEED certification energy savings goal while meeting stringent work safety protocols put Amarr's industry knowledge to the test.
SEE IF WE PASSED
From basic to a state-of-the-art design, this school created a dynamic, multi-purpose learning environment for their students with Amarr commercial doors.
SEE THE TRANSFORMATION
Setting the “bar” high, Amarr’s full view doors provided just what these restaurant owners needed to achieve optimal entertainment space.
SIP OVER THIS STUDY
To embrace the open air, industrial ambiance for this apartment complex, Amarr full view sectional doors were installed allowing light to shine in from all angles.
ENJOY THE READ
Amarr’s full view doors defined the culture of fresh air and open workspaces for all to enjoy at The Move Office Building.
RELAX AND ENJOY THE READ
Everything is bigger in Texas, including this mammoth of a project for a new 392,000 square-foot speculative rear-load industrial development site complete with rapid install lifts and track locks.
GO BIG OR GO HOME
Amarr’s versatile aluminum full view sectional doors eliminated the need for walls and boundaries by creating an open space concept allowing patrons to seamlessly browse throughout the marketplace.
BROWSE THE OPEN CONCEPT
Bringing the outside; inside for their patrons to enjoy all year round was the goal for the owners of Maniac-Mike’s Café. Amarr’s full view sectional doors helped achieve the desired look.
SEE HOW IT WAS DONE
Security meets luxury! The challenge presented was to find an aesthetically appealing commercial door to complete the vehicle storage look while providing a sufficient R-Value.
LEARN HOW WE DID IT
Oversized steel sectional door requirements combined with tenant leasing space was the challenge West Jordan faced before partnering with Amarr.
SCAN THE WIDE SELECTION
Custom painted, high R-value steel sectional doors with a full view panel updated the overall look of the 25 year old fire station.
SEE THE UPGRADE
Customized sectional doors with strong horizontal lines completed the look of industrial sophistication for this high-end car dealership.
SEE THE ULTIMATE RESULTS
ISM Raceway had the ultimate vision to create a versatile venue to support a variety of events using Amarr’s innovative yet functional industrial doors.
RACE TO THE STUDY
Amarr’s distinctive industrial rolling steel doors complemented the architectural style on the art buildings at Southern Utah University.
ROLL INTO THE STUDY