Preferred Solutions, Inc.
CONTENT
Preferred Solutions, Inc.
CONTENT
Staycell ONE STEP Spray Foam Insulation Systems image

Staycell ONE STEP Spray Foam Insulation Systems

Two-layer, Staycell® 265 / Staycell ONE STEP® (Hybrid System)The Hybrid System consists of two separate layers of closed-cell foam: Staycell® 265 as the base layer covered with Staycell ONE STEP® 255 intumescent foam as the exposed surface layer. It is typically specified at greater than a two-inch thickness for insulating walls, metal siding and the underside of roofs and concrete slabs.This System has Class A flame spread and smoke development ratings and is qualified as an Alternative Thermal Barrier Assembly when installed exposed without gypsum board or other fire-protective coverings in accordance with QAI Evaluation Report No. B1020-1, Edition 6.
Rated 5 based on 1 product reviews
Staycell ONE STEP Spray Foam Insulation Systems image

Staycell ONE STEP Spray Foam Insulation Systems

Single-layer, Staycell ONE STEP® 255 (Monolithic System)Staycell ONE STEP® 255 is an intumescent, closed-cell, spray polyurethane foam typically specified up to a two-inch thickness for air sealing and insulating walls, metal siding, structural steel and the underside of roofs and concrete slabs.This product has Class A flame spread and smoke development ratings and is qualified as an AlternativeThermal Barrier Assembly when installed exposed without gypsum board or other fire-protective coverings in accordance with QAI Evaluation Report No. B1020-1, Edition 6.
Rated 5 based on 1 product reviews
Staycell<sup>®</sup> 265 Spray Foam Insulation image

Staycell® 265 Spray Foam Insulation

Staycell® 265 is a closed-cell, spray polyurethane foam having a Class A flame spread and smoke development rating that is code-compliant when fire protected with gypsum board or qualified as an Alternative Thermal Barrier Assembly when covered with Staycell ONE STEP® 255 spray foam insulation or No-Burn Plus ThB intumescent paint in accordance with product listings. Staycell® 265 is typically specified for air sealing and to insulate walls, metal siding and the underside of roofs and concrete slabs.
Rated 5 based on 1 product reviews
Air Sealing Application image

Air Sealing Application

Staycell ONE STEP® Systems are ideal for air sealing new and existing buildings as it's quick and easy to install and can be left exposed without a thermal barrier, saving valuable time and money.
Rated 5 based on 1 product reviews
Crawl Space Application image

Crawl Space Application

Staycell ONE STEP® Systems are the optimal solution for retrofit crawl space applications in commercial and residential buildings as it provides the necessary functions for a safe and dry crawlspace (thermal insulation, air seal, moisture and vapor barrier in one product.
Rated 5 based on 1 product reviews
Metal Roof / Ceiling Application image

Metal Roof / Ceiling Application

Properly insulating metal roofs in cold climates and specialized uses such as gymnasiums, swimming pools and cold storage facilities with fiberglass insulation can be challenging. Over time, moisture penetrates through the seams and failed vapor retarder, condensing on the underside of the roof. This results in poor energy performance and long-term degradation of the roof structure. Staycell ONE STEP® Systems overcome these limitations by forming a seamless, fully-adhered, monolithic insulating air & vapor barrier membrane that will withstand the test of time.
Rated 5 based on 1 product reviews
Metal Wall Application image

Metal Wall Application

Staycell ONE STEP® Systems are the optimal solution for new construction and retrofit applications where compliance with new energy codes make the installation of traditional fiberglass systems increasingly complicated and labor intensive.
Rated 5 based on 1 product reviews
Parking Garage/Concrete Deck Application image

Parking Garage/Concrete Deck Application

Staycell ONE STEP® Systems are the logical choice for insulating the underside of concrete ceilings/floor slabs in parking garages. Seamless, spray-applied and fully-adhered, it eliminates clips, fasteners or suspended ceilings necessary to support traditional insulation materials such as fiberglass and cellulose and installs quickly. Durable, energy efficient, with built in thermal barrier, Staycell ONE STEP® Systems are the most economical, highest performing system on the market.
Rated 5 based on 1 product reviews
Precast/Masonry Wall Application image

Precast/Masonry Wall Application

One of the leading causes of energy loss and excessive moisture in precast/masonry wall cavities is poor exterior wall insulation. Having exceptional energy-efficient performance, Staycell ONE STEP® Systems are multi-functional - insulation, air barrier, water barrier and vapor retarder - and control convective looping within the cavity which can lead to mold growth and wall deterioration. Fully adhered, seamless, fluid application conforms to all shapes & configurations, providing unlimited design flexibility.Staycell ONE STEP® Systems are the optimal solutions for new construction or retrofit applications in all building types and occupancies.
Rated 5 based on 1 product reviews
Williamsport Hospital image

Williamsport Hospital

Williamsport Regional Medical Center, a state-of-the-art facility that's part of the Susquehanna Health System, underwent a $250 million dollar construction and renovation project to improve and expand patient services in central Pennsylvania.
Rated 5 based on 1 product reviews
Foxwoods Casino image

Foxwoods Casino

Foxwoods Resort Casino (the largest in North America) offers a vast array of gaming in seven casinos; AAA Four-Diamond hotels, restaurants from gourmet to quick service, world-renowned spas, award-winning golf, state-of-the-art theaters and exclusive retailers. To expand its shopping offering, Foxwoods partnered with Tanger Factory Outlet Centers, Inc. to build a new $115 million Tanger Outlet adjacent to the casino, providing convenient access for guests.
Rated 5 based on 1 product reviews
Alliance WWTP image

Alliance WWTP

The City of Alliance upgraded its municipal waste water treatment facility for converting waste-to-energy via methane capture to power plant operations. PSI worked with the design/build contractor to design an efficient, economical insulation system for the metal building housing the heat exchangers.
Rated 5 based on 1 product reviews
Scarsdale High School image

Scarsdale High School

The Scarsdale High School renovation was part of the district's school-wide energy efficiency initiative to improve building performance and reduce energy consumption. In addition to upgrades made to the lighting and HVAC equipment, detailed building envelope analysis identified significant heat loss thru uninsulated concrete roof panels and air leakage at the roof/wall transition. To control air leakage and insulate the roof panels, Staycell ONE STEP® 255 intumescent spray foam insulation was applied 2" thick to the sloped portions of the roof sealed to the top of the masonry wall.
Rated 5 based on 1 product reviews
John F. Seiberling Federal Building image

John F. Seiberling Federal Building

The John F. Seiberling Federal Building sits above an unheated multi-floor parking garage. As part of upgrades to improve building performance and reduce energy consumption, portions of the parking garage ceiling (serving as the floor for the offices above) were insulated, reducing energy consumption, improving occupant comfort and eliminating condensation formed during the winter months underneath the office carpeting.
Rated 5 based on 1 product reviews
Global Center for Health Innovation image

Global Center for Health Innovation

Situated near Lake Erie in downtown Cleveland, the 235,000 square foot Global Center for Health Innovation is part of $465 million building project to construct a permanent showroom of medical, surgical and hospital goods along with a new convention center. The goal of the project is to leverage Cleveland's reputation as a world class medical research hub (anchored by the Cleveland Clinic and University Hospitals) by bringing medical shows and conventions to the city.
Rated 5 based on 1 product reviews
Seabrook Middle School image

Seabrook Middle School

The Seabrook Middle School renovation was part of the district's school-wide energy efficiency initiative to improve building performance and reduce energy consumption. In addition to upgrades made to the lighting and HVAC equipment, detailed building envelope analysis identified significant air leakage thru the roof/wall transition joints. According to a study conducted by the Oak Ridge National Laboratory, air leakage is responsible for nearly 40% of heat/cooling loss in an average building.
Rated 5 based on 1 product reviews
Block 38 / CATALYST ONE Building image

Block 38 / CATALYST ONE Building

The Block 38 mixed-use building combines retail, parking and housing into the first high-rise structure built in downtown Lincoln, Nebraska in over 20 years. At 10 stories, the building provides nearly 20,000 SF of retail space on the first level, 650 parking spaces on levels two through seven, and 50 residential units on levels eight through ten.
Rated 5 based on 1 product reviews
South St. Paul Secondary School image

South St. Paul Secondary School

The Packer Hall Gymnasium renovation was part of a campus-wide energy efficiency initiative to improve building performance and reduce energy consumption. The most significant problem with the building related to student safety caused by condensation dripping from the roof structure onto the gymnasium floor. The standing seam metal roof deck was originally insulated with R-30 vinyl-faced fiberglass blanket. Over time the fiberglass lost most of its thermal efficiency from saturation caused by condensation trapped between the metal deck and the insulation's vinyl facer. At the purlins condensation resulted from compression of the fiberglass (resulting in low R-value) between the roof deck and purlin. The application consisted of fiberglass removal and replacement with the R-30 Staycell® HYBRID System, which consists of 4" Staycell® 265 covered with 1/2" Staycell ONE STEP® 255 intumescent spray foam insulation. Finally, the system was top coated white with Sherwin Williams “Fast-Clad" acrylic latex paint. The HYBRID System was chosen because it was more cost-effective than a standard foam and intumescent coating system.
Rated 5 based on 1 product reviews