Introducing the Skyfold Prisma™ experience
Flexible space is the future of architecture. Offering a space that can be adaptive rather than static is simply a priority in today's world.
As the acoustic leader in vertically retractable walls, we pride ourselves on constantly aiming to improve and enthusiastically embrace innovation; therefore, we are extremely excited to introduce our newest addition to the Skyfold family, Prisma™.
Prisma™is an elegant glass flexible space solution with the added luxury of transparency, clean lines, and a lightweight structure - the perfect choice for bright, sophisticated, and welcoming spaces.
By combining precision engineering and outstanding design, the Prisma™ wall takes its design possibilities far beyond the conventional in any space. Prisma™ has a telescopic, straight-down descent, making it the ideal flex space solution for areas with obstructions that limit the usage of vertically folding partition walls. With Prisma's narrow path of travel, there is no need to overhaul furniture placement in the space to operate the partition wall.
Skyfold Prisma™ wall is so easy to operate - with the touch of a button, you can quickly reconfigure any space in minutes. Increasing the aesthetic appeal of any room, Prisma™ also allows daylight to reach into spaces that otherwise would be dark and isolated. Increasing wellness, happiness, productivity, and employee morale creates nothing less than an environment to recharge creativity and stimulate imagination.
Skyfold Prisma™ is not only an elegant design feature for all these reasons - it further boasts an STC of 52 (Rw 52). With finish options such as frosted glass, creating rooms that feel airy and connected that are still quiet and private enough for meetings, collaboration, classes, and autonomous work is perhaps its best feature of all.
Classic™ NRC
Advantages of Skyfold Classic™ Vertically Folding Operable Walls:
The Zenith® Series is cutting-edge, innovative vertical wall technology. Zenith combines the vertically folding elements found in the Classic™ Series at the top portion of the wall with a slick straight down descent thereafter. Zenith is ideal for spaces that may have wall obstructions (such as heavy furniture) which would otherwise limit the use of a vertically folding operable wall. Except for the Zenith 48 models, the Zenith Series is unlimited in length.
Zenith® NRC
Advantages of Skyfold Zenith® Vertically Folding Operable Walls:
Exceptional Safety Features:
With a streamlined straight down deployment, the Zenith® Premium is ideal for spaces with obstructions, such as heavy furniture, which would otherwise limit the use of a vertically folding retractable wall. The ceiling pocket that stores the Skyfold wall is traditionally visible when looking up from the base of a Classic™ or Zenith® model in its down position. The Zenith Premium, however,features closure panels to hide the pocket from view, thereby maintaining the ceiling's flushed and unobtrusive appearance. With this added feature, the Zenith Premium not only functions, but also looks like a permanent fixture.
Including:
Zenith® Premium 51
Zenith® Premium 55
Zenith® Premium 60
Zenith® Premium NRC
Advantages of Skyfold Zenith® Premium Vertically Folding Operable Walls:
Mirage® incorporates Skyfold technology with the added luxury of transparency. Clean lines, a lightweight structure, a wide range of glass and plexiglass panels, high-efficiency acoustic seams, and ease of maintenance all make Mirage the ideal solution for bright, sophisticated and welcoming spaces.
Advantages of Skyfold Mirage Vertically Folding Glass Operable Walls:
Exceptional Safety Features:
With a 17-wall Skyfold configuration, the Walter E. Washington Convention Center was able to capture 48,000 square feet of new flexible meeting and exhibition space within the original building's footprint.
A stepped Skyfold Classic™ 51 transforms a 468-person auditorium into two 156-person lecture halls in Texas A&M's six-story physics building.
A 16-foot high Skyfold Classic™ 51 replaces a former service corridor in between two ballrooms to create a flexible event space that can be reconfigured into one large or two smaller venues at Fairmont Pacific Rim Hotel in Vancouver.
Architect David Preusch and interior designer Jackie Richardson worked together to find a solution to maximize this space's flexibility while preserving the uplifting aesthetics and serene aura of a center dedicated to empowering and supporting cancer survivors through yoga, fitness, nutrition and counseling. Over the center's life cycle, the well-engineered Skyfold system will hold up to multiple daily uses with almost no maintenance.
Anticipating the heavy use of the operable walls and the need for excellent acoustical performance led the project team to choose the highest-quality and easiest-to-use product available: Skyfold. Two 59 ft. Skyfold Classic™ transform a large space into microcosm for the institution that can be used as a coffeehouse, social setting, study area, club space, an auditorium or banquet hall.