Jakob Rope Systems
CONTENT

Stainless Steel Wire Ropes

Wire ropes are made of high-strength cold-drawn wires. The wires 1 area helically wound around the core 2 to form a strand, 3 the strands are then twisted around a steel core 4 to produce the finished ropes. 5 The length of lay L is the measuring value for the pitch of a lay.


The fill factor is the ratio between the metallic cross sections and the total rope cross section.

The metallic cross section (mm2) is the sum of the cross sections A of all wires in the rope.


The nominal strength is the tensile strength of the wire in newton (N) per square millimeter.


The calculated breaking strength is the product of the metallic cross section and the nominal strength of the wires.


The minimal breaking strength of the rope is the product of the calculated breaking strength and the spinning loss factor.


The actual braking strength is determined in a destructive test of the entire rope leg.


The spinning loss factor is a correction value which takes into account the difference between the calculated and the actual breaking strengths.

Rated 5 based on 1 product reviews
BIM SPECS CATALOGS VIDEOS

Webnet

Webnet is a woven product with exceptional tensile resiliency and flexibility. It is weather resistant, extremely robust and requires virtually no maintenance. The stainless steel net is suited for interior and exterior applications.


Installed on railings or in stairways, it provides stability and clear guidance. On faCades, it can serve as a climbing support for plants or it can set delicate accents as a dividing element in large spaces.


Webnet has been assessed according to standard specifications and subjected to many test measurements: As a permanent protection and fall-stop feature for bridges or observation platforms, it is totally UV resistant and weatherproof - in contrast to traditional knotted synthetic-fibre rope nets.


The greatest advantage, however, is its delicate structure. Especially in zoo animal enclosures or protective nets, the visual impairment due to the unavoidable barrier is minimal.

Rated 5 based on 1 product reviews
BIM SPECS CATALOGS VIDEOS

Cable Railing

Cable Railing System is safety railing that use horizontal or vertical
cables in place of spindles, glass, mesh, etc. This type of railing is most often used when an unobstructed view is desired. The Cable Railing can be installed in either metal or wood posts, depending on the customer's likes. Horizontal or vertical cable solutions for railing are an excellent way to achieve a modern look while still maintaining the functionality of traditional railing. Cables also require considerably less maintenance and upkeep than traditional railing systems.


There is a considerable amount of load requirements necessary for cable railing; and because of this, the way the posts are constructed is crucial. The posts should be quite rigid and firm to be able to withstand the amount of force that is applied to the post as a result of the tension of the cables. This is why wood and metal are typically used as posts, because these types provide the most support and rigidity.


For residential railings, the typical diameter of the cables used are either 1/8″ or 3/16″; and 3/16″ and 1/4″ for commercial railings. The strand of cable comes in several different options including stainless steel. The most common cable construction is 1x19 type strand, which houses 19 cables twisted into one bundle.


There are various requirements for constructing the cables, including the spacing between cables, the construction of the top rail, diameter of the cables, post spacing, and cable tension. These requirements vary depending on the state and location in which the cable railing will be placed.






Rated 5 based on 1 product reviews
CAD BIM SPECS CATALOGS VIDEOS

Wire Mesh Railing

Wire Mesh - Webnet is used for railing infills or as a substitute for standard railings. It is equally suitable for such applications in residential, semi-public, and public spaces. Whether in homes, in kindergartens and schools, in museums and offices, on bridges or publicly accessible vantage points: Webnet is always convincing because it combines functionality, aesthetic appeal, economical use of materials, and longevity. And not least, this product is sustainable in the best sense of the term, especially as regards its cost-effectiveness.

Apart from the comparatively low investment, one of the key benefits of Webnet is that it involves virtually no maintenance expenditure.


For architects and builders, the fascination of Webnet as a railing material is based chiefly on its usefulness paired with its uniquely minimal visual impact. Thanks to its discreet and unobtrusive appearance, it can be deployed in practically every style context and for implementing a host of design approaches. In many situations, Webnet gives planners totally new aesthetic and creative options. In staircases that require no handrails, for instance, it can completely replace a railing by stretching it across an oriented surface; this emphasizes the architectural form with impressive purity.


Rated 5 based on 1 product reviews
CAD BIM SPECS CATALOGS VIDEOS

Webnet Modular Railing Systems

  • Webnet stainless steel frames are a high-quality product individually configured and compatible with all type of railings to meet your unique architectural needs.
  • Designed for easy assembly, Webnet frames offer remarkable flexibility and are an excellent turnkey solution for your rope system requirements.
  • Apart from timeless design and unobstructed views, all Webnet frames have built-in
    safety certified features.
  • All components are made from high-grade Stainless Steel (AISI 316) for indoor and
    outdoor applications.
  • Jakob Rope System's Webnet frames are multifunctional and designed for a wide range
    of protective applications with visually stunning appeal.
  • Our years of experience and countless numbers of installations allows us to create a unique solution for you.


Rated 5 based on 1 product reviews
CAD BIM SPECS CATALOGS VIDEOS

Green Walls

Green Walls - Contemporary architecture is increasingly focusing on Vertical Greening Systems as a means to restore the environmental integrity of urban areas, biodiversity and sustainability. Planners and architects who have teamed up with Jakob Rope Systems are already producing outstanding results and are defining new dimensions for “art on buildings" with Jakob Green FaCade System.


Professional and expedient greening faCade requires careful and thoughtful planning, Jakob Rope System has gained an international reputation in this field.


Vertical Green can be classified as faCade greening according to the growing method employed. A Green FaCade use supporting structures and climbing plants that will trail along the structure with soil at the base of the wall. Plants are rooted at the base of these structures, in the ground, in intermediate planters or even on rooftops. Green Facades can be anchored to new construction, existing walls or built as freestanding structures, such as fences or columns.


This techniques have a stunning visual effect and serve to increase the green space of a city. Green facades are typically outdoors and indoor and are limited to species of plant that can climb the structure.


The support structure can be our wire Trellis System, Cable System or Mesh System.



Rated 5 based on 1 product reviews
CAD BIM SPECS CATALOGS VIDEOS LEED

Webnet Enclosures

Enclosures Webnet - A material such as Webnet is the ideal creative and functional alternative to fencing and bars. All over the world, increasing numbers of zoological gardens are using it as the resource of choice for new animal enclosures. Word of the positive experience gained with this material is gradually spreading among the experts. Webnet is safety-certified, weather-resistant and highly durable and requires little or no maintenance. Even the initial investment can be considered comparatively cost-effective.


Rated 5 based on 1 product reviews
BIM CATALOGS VIDEOS

Webnet Safety Nets

Safety Nets - The 

Jakob Webnet

 is practically always a sensible material option for protection approach in the high bridges.

 
Extremely flexible with respect to applications and comparatively easy to install, it is a compelling solution thanks to its discreet and inconspicuous appearance. 

The advantages of Webnet also include its high load-bearing capacity, its impressive longevity, and the fact that it entails virtually no maintenance costs. These benefits have meanwhile been confirmed in a series of projects. 

Jakob experience shows that it can take years to implement a safety concept for bridges. Initially, citixens, a stakeholder group, politicians, or a municipal authority will express the need for sustainable measures. With perseverance and competence, Jakob Rope Systems has complete many projects over the years by attending kick-off meetings with lawmakers, submitting samples, preparing preliminary projects outlines, performing load test series, calculating the feasibility that visualize the proposals, and delivering prototypes for onsite trails. 

We will leverage our experience and accompany you to the approval stage, produce the planned measure to the highest quality standards, and assemble it on site with our specialists. 


Rated 5 based on 1 product reviews
BIM CATALOGS VIDEOS

Webnet Stainless Steel Fences

Fences - As advancements in technology continue, construction products become stronger, better, and lighter. Fencing in particular is making great strides in design improvements. A perfect example of a great new product is the attractive, strong, and flexible wire mesh fence from Webnet.


Webnet is an exciting wire mesh product that is excellent for perimeter fencing and for providing protective netting along staircases. Wire mesh fences are both attractive and strong in design. Specifically, the Jakob® INOX LINE Webnet is constructed of stainless steel and offers strong support for fencing in a property or for guidance on stairwells.

Rated 5 based on 1 product reviews
BIM CATALOGS VIDEOS

HABEGGER Lifting and Pulling Machine

An optimized blend of tradition and functionality (HABEGGER LIFTING EQUIPMENT) 


When heavy loads have to be moved safety and cost-effectively. Original HABEGGER LIFTING EQUIPMENT  products are the first choice for 
lifting and pulling. HABEGGER wire rope hoists have been successfully deployed around the world since 1951. In the 1990s, the product line was extended with motor-powered units.

 
Thanks to superb quality, rugged designs, and longevity, the products can be made fit for service again and again. Apart from the “Swiss Quality” promise, this is another benefit that speaks in favor of Original HABEGGER products. 



Rated 5 based on 1 product reviews

Cable Railing Gallery

Safety railing that use horizontal or vertical cables in place of spindles, glass, mesh, etc. This type of railing is most often used when an unobstructed view is desired. The Cable Railing can be installed in either metal or wood posts, depending on the customer's likes. Horizontal or vertical cable solutions for railing are an excellent way to achieve a modern look while still maintaining the functionality of traditional railing. Cables also require considerably less maintenance and upkeep than traditional railing systems.


Rated 5 based on 1 product reviews
SPECS

Green Walls Gallery

Contemporary architecture is increasingly focusing on Vertical Greening Systems as a means to restore the environmental integrity of urban areas, biodiversity and sustainability. Planners and architects who have teamed up with Jakob Rope Systems are already producing outstanding results and are defining new dimensions for “art on buildings" with Jakob Green FaCade System.



Rated 5 based on 1 product reviews
SPECS

Wire Mesh Gallery

Webnet Frames are a high-quality product individually configured to the application within the scope of a creative architectural approach. As part of our easy-to-assemble rope structure portfolio, they are a remarkable modular element for flexible solutions. Because they are made of stainless steel (AISI 316), Webnet Frames are suitable for indoor and outdoor applications. Webnet is safety-certified, weather-resistant and highly durable and requires little or no maintenance. Site requirements with respect to the loadbearing capability of the web can be accommodated by the selection of different rope diameters and mesh apertures.


The frames themselves are available either in round or square tube material.

Rated 5 based on 1 product reviews
BIM SPECS