Soundproofing Products to Control the Noises of Life! Industrial Facilities - The first and most important reason to control these noisy environments is for the safety of the workers and management at the sites. If workers misinterpret a directive, or are unsure of directions, an injury is imminent. The next issue is productivity; it is medically proven that the human body is adversely affected by long durations of extreme sound pressure or noise. Our nervous systems cannot handle the stress this type of fatigue causes. If a worker is stressed, or fatigued, he is more likely to make a mistake or not work up to his full potential. The third area of concern is surrounding residential areas. The noise from a facility twenty-four hours a day could and would drive someone crazy. If the noise level is too high in surrounding communities, they will complain and get the government involved. If this happens, it may also cause shut downs, and lack of productivity. At the end of the day, all of the above scenarios spell loss of revenue!
Rated 5 based on
1 product reviews