Sumter Coatings, Inc.
CONTENT

Rust Inhibitive & Protective Primers

Rust inhibitive primers are truly our everyday workhorse primers. They have protected more structural steel throughout the southeastern US than any other single primer we produce.
Rated 5 based on 1 product reviews

Universal Steel Primers

These steel primers are versatile by design. They contain a significant amount of rust inhibitive pigment, which translates to protection from corrosion for extended periods of time before top coating or enclosure. Additionally, as a result of resin modification, they may be top coated with coatings containing strong solvents, such as two-part epoxies and polyurethanes, without fear of lifting the primer. This is the primer of choice when the subsequent topcoat is unknown. They may also be used as an intermediate coat over old coatings that may lift if top coated with coatings containing strong solvents.
Rated 5 based on 1 product reviews

Zinc Rich Primers

Our zinc-rich primers offer superior long-term protection for steel from corrosion and have excellent adhesive and protective properties. They perform similarly to galvanizing for structural steel surfaces. These primers contain a high percentage of zinc dust, which acts sacrificially when in direct contact with the steel. The zinc salts, which invariably form, fill the pores of the primer sealing off the steel substrate from moisture. They also are very flexible when applicating, as top coats don't need to be applied immediately after the primer.
Rated 5 based on 1 product reviews

Two-Part Epoxy Primers

Two-part epoxy primers are structural steel primers that require two-components, which cure chemically by cross linking. The resulting film is abrasion, chemical and moisture resistant. These two-part epoxy primers are intended for use over properly prepared steel and concrete. They are suitable for many industrial exposures such as structural steel, power plants, marine applications, water treatment plants, and tank exteriors, to name a few.
Rated 5 based on 1 product reviews

Industrial Water Based Primers

Our water-based primers perform well in helping curb the onslaught of corrosion. In addition, they may help resolve some of the environmental and safety issues facing the steel fabricator. Contact Sumter Coatings today for more information on our water based primer products!
Rated 5 based on 1 product reviews

Specialty Primers

The application of a specialty primer is sometimes overlooked prior to the application of a protective coating. They are used to promote adhesion and seal the substrate prior to the application of a protective coating.
Rated 5 based on 1 product reviews

Enamel Finish Coats

Sumter Coatings manufactures a broad range of enamel finish coats. From OEM to propane tank enamels, we have the solution you need.
Rated 5 based on 1 product reviews

Industrial Epoxy Finish Coats

Sumter Coatings epoxy finish coats are formulated based on the performance requirements for the end product. When properly catalyzed and applied, epoxies produce a hard, chemical and solvent resistant finish.
Rated 5 based on 1 product reviews

Urethane Finish Coats

When it comes to aesthetics, Sumter Coatings urethane finish coats are a smart option when long-term gloss and color retention are needed. Our urethane finish coats are used for OEM, structural steel, industrial maintenance or wherever a high quality, durable, long lasting coating is needed.
Rated 5 based on 1 product reviews

Specialty Finish Coats

For over 20 years, Sumter Coatings has prided itself on being a leader in the manufacture of specialty coatings and primers. Our specialty coatings are designed for optimal performance while meeting customer's requirements.
Rated 5 based on 1 product reviews

Siemens Facility - Charlotte, NC

The new addition to the Siemens Facility in Charlotte, NC needed a lot of structural steel. That steel fabricated by Cooper Steel of Shelbyville, TN needed a lot of protection before and during erection. Sumter's 100W0038 Universal Primer White was chosen for this project for a number of reasons including fast dry, rust inhibitive, light reflectance and the ability to accept a wide variety of topcoats. 100W0038 White Corrosion Resistant Primers meets or exceeds the performance requirements of SSPC Paint No. 25, TT-P-664, and MPI # 76.
Rated 5 based on 1 product reviews

Caterpillar - Winston-Salem, NC

When Caterpillar chose Winston-Salem, NC as the desired location for their new facility, it was a natural to select Lyndon Steel in Winston-Salem to fabricate the structural steel. Lyndon, in turn, chose 100D8814 Inhibitive Primer Gray to protect the steel from corrosion before and during the erection process. 100D8814 Gray Corrosion Resistant Primers meets or exceeds the performance requirements of SSPC Paint No. 25 and MPI # 76.
Rated 5 based on 1 product reviews

Seaside Project - Haskell Steel, Jacksonville, FL

Due to the location of this seaside project, more than just a shopcoat primer was required to protect the exterior steel trusses. A constant salt environment is the enemy to steel. Haskell Steel in Jacksonville, FL did the fabrication and selected to go with a three-coat system from Sumter Coatings. A prime coat of 346D7714 Inhibitive Epoxy Gray was followed with an intermediate coat of 346D7720 Inhibitive Epoxy Light Gray, then topcoated with 318 Series High Build Urethane for additional protection and aesthetics.
Rated 5 based on 1 product reviews

Washington Redskins Training Center - Richmond, VA

The new Washington Redskins Training Center in Richmond, VA is an impressive facility. The structural steel for this venue was fabricated by Weldon Steel Corporation in Weldon, NC. Weldon selected their "go to primer," 100D7714 Inhibitive Shopcoat Primer Dark Gray, to protect the steel during and before erection. 100D7714 meets or exceeds the performance requirements of SSPC Paint No. 15 and MPI #79.
Rated 5 based on 1 product reviews

Michelin plant - Anderson, SC

Structural steel for the new Michelin plant in Anderson, SC was fabricated by Cooper Steel in Shelbyville, TN. Cooper wanted a shop primer that would offer protection from the elements prior to erection. In addition, it had to dry fast to a smooth consistent film. They chose 100D7744 Inhibitive Shopcoat Primer Cooper Gray. 100D7744 meets or exceeds the performance requirements of SSPC Paint No. 15 and MPI # 79.
Rated 5 based on 1 product reviews

Wake Forest University

Lyndon Steel Co. of Winston-Salem, NC was selected to fabricate the steel for the Wake Forest University scoreboard. Lyndon chose Sumter's 100D8814 Inhibitive Primer Gray to protect the steel before and during the erection process. 100D8814 meets or exceeds the performance requirements of SSPC Paint No. 25 and MPI # 76.
Rated 5 based on 1 product reviews

University of North Carolina Wilmington Campus

The new School of Nursing on The University of North Carolina Wilmington campus stands strong and sturdy thanks to the structural steel fabricated by Weldon Steel Corp. of Weldon, NC. To protect the steel prior to and during erection, Weldon used 100D7714 Inhibitive Shopcoat Primer Dark Gray. Weldon depends on 100D7714 for fast dry and corrosion protection. This primer meets or exceeds the performance requirements of SSPC Paint No. 15 and MPI # 79.
Rated 5 based on 1 product reviews

Flex Film's New Plant - Elizabethtown, KY

The structural steel for Flex Film's new plant in Elizabethtown, KY was fabricated by Cooper Steel in Shelbyville, TN. Cooper chose 100D7714 Inhibitive Primer Dark Gray to protect the steel prior to and during erection. A fast dry time and rust inhibitive properties made 100D7714 a great choice. This primer meets or exceeds the performance requirements of SSPC Paint No.15 and MPI #79.
Rated 5 based on 1 product reviews

Mint Hill Community Center - Mint Hill, NC

Mint Hill Community Center in Mint Hill, NC is an important gathering spot for the folks who live there. The structural steel for this facility was fabricated by North State Steel with locations in Greenville and Louisburg, NC. 100D7714 Inhibitive Primer Dark Gray was used to protect the steel prior to and during erection. 100D7714 dries quickly and inhibits corrosion. This primer meets or exceeds the performance requirements of SSPC Paint No. 15 and MPI # 79.
Rated 5 based on 1 product reviews