Stone Farm
CONTENT
New England Blend Reclaimed Thin Brick Veneer image

New England Blend Reclaimed Thin Brick Veneer

Salvaged from old factories, mills, and schools around New England, this blend is an ideal accent material. The color is predominantly deep reds found in the Northeast - however, we mix in white tones and blackened “soot stained" pieces as a result of fire damage and natural weathering. Our New England Mill blend is an incredibly unique offering. See how our thin brick veneer comes to life in recent projects - Interior Brick Projects.
Rated 5 based on 1 product reviews
Vicarage Grey Reclaimed Thin Brick Veneer image

Vicarage Grey Reclaimed Thin Brick Veneer

Our new Vicarage Grey thin brick is a fresh, exciting brick option that offers a unique end result that designers have been asking for. As gray clay is most readily found in the southwest region of China along the banks of the Yangtze River, Stone Farm has partnered with reclamation teams in that area to bring this new product to America.See how our reclaimed thin brick is used in recent projects - Interior Brick Projects.
Rated 5 based on 1 product reviews
Baltimore Blend Reclaimed Thin Brick Veneer image

Baltimore Blend Reclaimed Thin Brick Veneer

The city of Baltimore is currently using the deconstruction of its row houses as a means towards creating employment, reducing waste sent to landfills, and salvaging materials for reuse. The reuse allows us to offer you this exciting blend of reclaimed thin brick! This blend of reclaimed brick is a vibrant flavor of a historic look. The color range includes a mix of reds, blacks, natural clay tones and soft yellows. See how our thin brick veneer comes to life in recent projects - Interior Brick Projects.
Rated 5 based on 1 product reviews
Reclaimed Thin Brick Floor Tile Veneer image

Reclaimed Thin Brick Floor Tile Veneer

Our New England Mill Blend Floor tile is cut from the same bricks as our New England Mill Blend wall veneer. The difference is that we cut the top of the brick (rather than the face). As this is where the mortar lay, you can get more 'whites/grays'. The larger surface area is more consistent with traditional brick floors. Interior Brick Projects.
Rated 5 based on 1 product reviews
New England Mill Blend Floor Tile image

New England Mill Blend Floor Tile

New England Mill Blend is our only color that our Floor Tile comes in, offering you a unique look to any floor.Our New England Mill Blend Floor tile is cut from the same bricks as our New England Mill Blend wall veneer. The difference is that we cut the top of the brick (rather than the face). As this is where the mortar lay, you can get more 'whites/grays'. The larger surface area is more consistent with traditional brick floors. Interior Brick Projects
Rated 5 based on 1 product reviews
Reclaimed Cobblestones image

Reclaimed Cobblestones

The worn patina and subtle colors and textures of Reclaimed Cobblestones speak of a rich, timeless history. Whether harvested directly from an old street or town in America, to a quaint village in Europe, these cobblestones have a story to tell; a history to be discovered and preserved.Project Area
Rated 5 based on 1 product reviews
Domestic - Big Dig Cobbles image

Domestic - Big Dig Cobbles

Typically sourced throughout the Northeast, these cobbles are named after our first reclamation that came from the old streets of Boston. We still harvest in this area today. Often quarried from multiple locations, this material offers a unique range of color, from weathered grays to tan with underlying earth tones. This warm patina, combined with a worn, smooth texture that only time can develop, provide a look not found with new materials.
Rated 5 based on 1 product reviews
European - Porphyry image

European - Porphyry

Belgian Porphyry is referred to as “the Belgian block" and is known for its exceptional hardness and durability. These stones were incredibly fashionable during the 19th and early 20th century and were commonly used in well-known city centers of affluence including Champs-Elysees in Paris, various New York City Avenues and Saint Petersburg in Russia. These cobbles offer beautiful combinations of coloring; green-brown, brown-rusty, green-blue, rusty-red and blue. Shapes include both squares and rectangles. ​
Rated 5 based on 1 product reviews
European - Sandstone image

European - Sandstone

Belgian Sandstone is a very hard and resistant sandstone cobble quarried in the 18th, 19th and 20th centuries in the Walloon region of Belgium. This cobblestone offers a generally smooth and well-worn top face. Colors vary from brown over grey to earthy green as well as lavender. Colors in cobblestones contained within a specific batch offer similar characteristics.
Rated 5 based on 1 product reviews
Reclaimed Paving, Granite Planks image

Reclaimed Paving, Granite Planks

Good design, you know it when you see it. You also understand and appreciate that using natural elements in your designs makes good design even better. Stone Farm gets it too. Our reclaimed stone products are the perfect mix of natural and historic elements that make your great designs stand out.
Rated 5 based on 1 product reviews
New England Granite Planks image

New England Granite Planks

Our New England Granite Planks are harvested around New England and come in a range of dimensions, surface textures and edge treatments. These inherent differences make for a material that can be sorted and utilized for a range of paving applications. Color - Weathered gray and earth tones from New England granites Thickness - Gauged backs (1-3") or non gauged (4-8") with split surface Height - Will vary - typically available (9", 10", 12", 16" and 18") Length - Random from 18" - 8' Finished surface - Can be sorted for heels or no heels Joint - Tight to medium tight
Rated 5 based on 1 product reviews
Antique Asian Granite Planks image

Antique Asian Granite Planks

The textured but very flat surface of this antique stone pavers makes them suitable for applications where the surface needs to be completely flat or the joints need to be nice and tight. Many of these pavers will show many years of wear and weathering, along with hand tooled surfaces. From plank to square shapes, these pavers come in a range of sizes. Color - Natural beige and brown tones to shades of gray Specs -Textured smooth face with natural sides. Dimensions - Planks 9-15" wide 2-5' long and 2-5" thick Surface - High heel compatible, flat surface Joint - Tight Applications - Refined patios and can be sorted for driveway applications. Source - Imported
Rated 5 based on 1 product reviews
Reclaimed Bluestone Sidewalks image

Reclaimed Bluestone Sidewalks

Reclaimed from an old beautiful neighborhood in Pennsylvania. Get your piece of 100+ year old antique bluestone side walk while supply lasts. Color - Deep dark blues, greens, grays and tans Surface finish - walk worn surface Dimensions - Generally 4' x 2-5' x 3-5" Joint - Tightish Source - Domestic Approximately 800 sqft in Stock
Rated 5 based on 1 product reviews
Antique Limestone Planks image

Antique Limestone Planks

Hand hewn limestone has an ancient feel even before it has been worn, weathered and walked on. Centuries of exposure to the elements give this material an almost magical look. Many of these pavers were hand chiseled for traction, providing a very unique surface texture. Color - Charcoal and gray tones Specs - Textured worn face with natural sides Dimensions - Planks 16x18" x 3-4' x 2-4" thick Finished surface - Flat, worn surface. High heel compatible Applications - Refined patios and can be sorted for driveway and step applications Source - Imported
Rated 5 based on 1 product reviews
Reclaimed Sandstone Sidewalks image

Reclaimed Sandstone Sidewalks

Color - Tans, greens, grays and blues Surface finish - walk worn surface Dimensions - Generally 4' x 2-5' x 3-5" Joint - Tightish Source - Domestic
Rated 5 based on 1 product reviews
Full Thickness and Gauged Pavers image

Full Thickness and Gauged Pavers

Often times reclaimed stone will have a beautiful surface or shape, however, the thickness might not work for a particular application. Our gauged pavers are created by sorting material with great paving surfaces and then cutting them to a desired thickness, creating a product that is easier to install and perfect when setting in a bed of mortar.
Rated 5 based on 1 product reviews
Reclaimed Wall Block image

Reclaimed Wall Block

Hammering large pieces of granite into building blocks has been a part of New England's history for hundreds of years. These blocks were used to build railroad trestles, cellar foundations and as the walls of many early American industrial buildings. As these structures are retired from service, Stone Farm harvests their beautiful blocks and re-purposes them for many different applications.
Rated 5 based on 1 product reviews
Colors and Textures image

Colors and Textures

Most of the granite block we harvest today originates from one of the numerous granite quarries scattered throughout New England. Through years of weathering, these quarries produced granite in various shades of gray, blended with underlying earth tones. Combined with a slightly rough, split face, textured surface, the end result is a unique color palette that can't be replicated elsewhere.
Rated 5 based on 1 product reviews
Dimensional Wall Block image

Dimensional Wall Block

Granite Blocks - Dimensional Specs - Blocks that have 6 dimensional sides Dimensions - H (18"x 24") D (18"x 24") L (2-8') Finished wall face - split face or pillowed surface Packaging / trucking - Bulk via 23 ton dump truck or per piece on dunnage on flatbed truck
Rated 5 based on 1 product reviews
Semi Dimension Wall Block image

Semi Dimension Wall Block

Granite Blocks - Roughly Square and Roughly Rectangular Uses - Retaining walls, accent stones Specs - Blocks with at least 2 to 3 square or rectangular flat faces Dimensions - H (18"x 24") D (18"x 24") L (18"- 4') Finished wall face - flat face with rectangular or square shape Packaging / trucking - Bulk via 23 ton dump truck load
Rated 5 based on 1 product reviews
Bench Grade image

Bench Grade

Granite Blocks - Bench Grade Highest quality dimensional block suitable for benches
Rated 5 based on 1 product reviews
Reclaimed Granite Curbing image

Reclaimed Granite Curbing

Reclaimed granite curbing makes a great enhancement to a landscape project. Stone Farm has many products that are created from curbing.
Rated 5 based on 1 product reviews
Step Grade image

Step Grade

Wide, smooth side suitable for steps, split tops and bottoms 4"-7" x 9"-12" or 16"-21" x 2' plus
Rated 5 based on 1 product reviews
Paving Grade image

Paving Grade

Wide, smooth side surface suitable for pavement, split or sawn tops and bottoms 4"-7" x 9"-12" or 16"-21" x 2' plus
Rated 5 based on 1 product reviews
Standard - For Curbing image

Standard - For Curbing

Wide side surface not necessarily suitable for steps or paving, split or sawn tops and bottoms 4"-7" x 9"-12"or 16"-18" x 2' plus
Rated 5 based on 1 product reviews
Architectural Specialties image

Architectural Specialties

Although Stone Farm is known for sourcing reclaimed materials, we also: Create custom products with reclaimed materials; Source new materials to complement / match our reclaimed materials. Applications:Reclaimed Stone for Outdoor DesignsReclaimed Stone Patios and PathwaysSteps, Treads and LandingsPool CopingDriveway, Motor CourtsStone Retaining Wall Blocks
Rated 5 based on 1 product reviews