VASARI™
CONTENT

Luxury Car & SUV Garage Storage Lift for Small Garages

Why choose between your dream home and your treasured vehicles? With a Single-Car Garage Lift from Vasari, you can have it all. Some homeowners do not have the lot size for multi-car surface garages, while others simply prefer a single-space garage. Your personal needs and unique situation can be solved with a car and SUV lift that is perfect for smaller garages, thus providing ample parking for two full-sized vehicles. This type of garage lift accomplishes the job by vertically stacking the vehicles within the same footprint. While one vehicle is kept underground, a second remains on the top platform of the garage lift. As a result, both are stored safely and securely in half the space.


As an industry leader in garage lift design and manufacturing, Vasari can craft garage lift dimensions that deliver the storage space you've always dreamed about. Not all homes can support an addition to the existing garage. Vasari's client-specific solutions, which you can learn more about on this website, always make the most of the available real estate. With a Vasari Single-Car Garage Lift, your small lot size isn't a reality you're forced to accept. By making the most of garage lift dimensions, it's an easy design challenge to solve. Don't lower your standards. Elevate your cars.


Case Study

Rated 5 based on 1 product reviews

Driveway Lift

Do you have limited parking, and are unable to make modifications to your garage? A Driveway Lift from Vasari is your solution. Designed by our engineers for pit installation, a Driveway Lift allows one vehicle to lower below the surface of your driveway, while your other car parks on an upper platform. Because the upper platform can be designed to blend into the driveway, your lift platform is virtually invisible.



Rated 5 based on 1 product reviews

Vault Lift

Your automobile is almost certainly one of your most prized and valuable possessions. Shouldn't you protect it to the utmost? For customers who desire the highest level of security and safety for their vehicle, a Vault Lift from Vasari is the definitive solution. Designed by our engineering experts, a Vault Lift is as simple as it is dependable, securely lowering your vehicle into an underground environment. For added protection, monitoring options are also available.



Rated 5 based on 1 product reviews

Show Room Lifts

Your automobile collection is proof of your singular taste and refinement. Shouldn't your showroom be designed to that same standard? When you choose a Vasari Showroom Lift, you're not simply purchasing a pre-packaged product - you're employing a team of creative problem-solvers, with deep experience and vast capabilities. Drawing from our expertise, we design Showroom Lifts to transport your vehicle below ground, with drive-off capabilities to safely move your vehicle for storage and display. But this is only the beginning.


While all of our Showroom Lifts maintain principal features, our engineers are able to develop creative, customized applications inspired by your objectives. Use your imagination. We can make it reality.


Rated 5 based on 1 product reviews

Underground Parking Lifts

SAFELY STORE AS MANY VEHICLES AS YOUR BASEMENT HAS ROOM.


Your treasured vehicles should not be left vulnerable to the elements or security threats. If your basement has room, why not take advantage of it? A Vasari Underground Lift provides safe, reliable access to your basement, with easy drive on/off capability for access into the basement parking area.


By taking full advantage of your property's basement space, Underground Parking Lifts deliver the utmost in convenience and efficiency. Further proof that Vasari engineers are always looking ahead, even if it means going underground.


Case Study


Rated 5 based on 1 product reviews

Turntable Lifts

Do you believe every part of your car is beautiful and should be showcased? Or is your vehicle in an underground area with space constraints? While each are separate challenges, both share the same solution - a Turntable Lift from Vasari. Simply and exquisitely designed by our engineering experts, a Vasari Turntable Lift is able to rotate 360 degrees. Your car will remain secure as it safely rotates to the ideal drive-off position.


Whether for space-constrained underground areas or a collector's showroom, you'll soon discover that a rotating Vasari Turntable Lift is a smart decision from every direction.


Rated 5 based on 1 product reviews

Shuttle Parking Lift

Your convenience is of paramount importance. Vasari is proud to oblige with an innovative solution for your parking needs. With a design that is as simple as it is functional, a Shuttle Parking Lift uses a moving platform to “shuttle" your vehicle off the lift and into the storage area.

A Shuttle Parking Lift from Vasari is designed and manufactured with your needs in mind. It is proof, once again, that our inspiration is improving your convenience.




Rated 5 based on 1 product reviews

Design Features

At Vasari, we devote ourselves, to the craft of developing quality engineering, construction and exceptional performance of our parking lifts.


We provide a level of innovation, technology, and safety that elevates our parking lifts into a class of their own. Discover the design features that make a Vasari Personal Parking Lift, distinctive.


Structural Integrity

Fail-Safe Hydraulic System

Unique Guide System

Self-Contained Drive System

Easy to Use Control System


Rated 5 based on 1 product reviews

Complete Safety Package

Safety is our # 1 concern, understanding these lifts will be installed in or near your living space, and in the vicinity of the people you love, we have included standard safety devices that are included with all our Vasari parking lifts.

Motion Detector

Wireless Security

Audible Alarm

Maintenance Devices


Rated 5 based on 1 product reviews

Options

Optional equipment features are available to enhance the safety and functionality of your parking lift.


Rotating Turntable

Telescoping Canopy

Touchscreen Controls

Lift System Command Center

Ultrasonic Vehicle Positioning Indicator

High Power Motors

Special Platform Materials


Rated 5 based on 1 product reviews

Conveyor and Storage Rack Car Lift Parking System

A personal car vending machine - deposits one car at a time from storage system.


The Challenge

A homeowner in LA who did not want to give up livable space of their new home construction for the garage space required for their five cars. Under city ordinance, they had limited footprint above ground available. So, our team of talented engineers configured an underground parking system that solved all the homeowner's challenges.


The Vasari Solution
The new home design includes multiple levels, therefore the car lift was designed to travel between three levels in a shaft way with the capacity to move vehicles off by a conveyor system and onto (2) lower-level storage racks. This is achieved by engineering the car lift with an over-sized hydraulic lifting platform embedded with a conveyor system, as well as each slot within the storage racks is also equipped with a conveyor. The homeowner can control the operation of this parking system through a touchscreen HMI panel. This provides a visual screen of the system to allow the homeowner to park a car by selecting which storage space is available and transporting the car to the designated space. They can also select which car should be conveyed off the storage rack and onto the lift, raised up to driveway level for the homeowner's use.


Rated 5 based on 1 product reviews

Showroom Lift with Rotating Turntable

Solving a client's structural Challenge

Challenge
A homeowner wanted his automobile collection incorporated into his new home garage design. However, the new structural design plans prohibited any cars from driving onto the lift in either forward or reverse. If the lift was lowered to the car showroom, a wall would block the cars from driving forward, while a staircase from behind prevented cars from reversing.


Solution
To address this architectural challenge, Vasari's engineer's designed a Vasari 4-Post Parking Lift with a custom rotating turntable. This solved the obstruction in the showroom-garage by allowing vehicles to rotate to the side and exit off the platform.


Rated 5 based on 1 product reviews

Underground Garage Lift

Vasari's Underground Garage Lift Increases Parking Capacity for Homeowners


The Vasari Solution
When traditional parking in a home garage is not available due to space restrictions, Vasari offers an underground solution. Vasari's underground garage lift is designed for residential homes to increase parking capacity. This underground garage lift allows for one vehicle to be transferred safely underground for parking, while a second vehicle can be parked on top.


A homeowner may be faced with parking constraints for various reasons - land restrictions of a new home build to protecting a collector automobile. Whatever the reason, Vasari builds underground garage lifts to solve for these very reason. Working with you and your home builder, we can help determine the requirements for installing an underground garage lift in your new home.


Rated 5 based on 1 product reviews

Residential Car Lift

Vasari's residential car lift guarantees a parking space for every member of the family.


The Challenge
A Colorado family building a new home wanted extra garage parking for their multi-driver household. However, their new home design plans could not accommodate a larger garage. They did not want to leave automobiles outside in inclement weather, so they looked for an alternative solution.


The Vasari Solution
Vasari's residential car lift allows the homeowner to expand their parking options by going underground. The car lift is installed through an excavated pit. The car lift will safely transport a vehicle underground keeping it safe and protected. Vasari's residential car lift is a great solution for existing house plans or new builds.



Rated 5 based on 1 product reviews

Hassle-Free Parking Lift

A perfect parking solution for accessing two vehicles without the hassle of shuffling cars around.


Challenge

When a homeowner was finalizing his floor plans for the construction of his new home, his architect recommended building a one-car garage which is more suitable for the lot size, and also more fitting for the neighborhood characteristics.

The homeowner owning two vehicles, asked his architect to explore alternatives to create more covered parking. The idea of adding an underground garage lift began to take shape with the plans to redesign the garage to include a cathedral style ceiling, so the homeowner will be able to lift two vehicles at the same time.


Solution

After full evaluation of the homeowner's challenges and goals, our engineers designed a high capacity garage lift capable of raising his “everyday" car within the footprint of the garage while accessing his sports car from the basement garage.


Rated 5 based on 1 product reviews

Underground Car Lift Doubles Space

Vasari Delivers Twice the Parking Space By Concealing One Car Underground.


Challenge

New homeowner's were building a new home on a narrow lot that had room for only a standard 2-car garage. They did not want to leave their other vehicle out in the open uncovered or unprotected. They considered installing a pre-packaged stacked car lift in the garage, however, they height requirements would require a redesign of their garage plans.


Solution
Vasari's engineering team designed an underground car lift to fit within the footprint of their garage. The homeowner would not have to sacrifice their design plans. The Vasari lift will be pit installed and transport one vehicle underground where it will be protected. Another car can be parked on top of the lift platform at the garage level.


Rated 5 based on 1 product reviews

Single-Car Garage Lift for Dream Home

Dream home in historic district uses a Vasari single-car garage lift to transfer vehicles to underground storage area.


Challenge

New homeowner's were building their dream home in an historic area where the lot lines were small. They were faced with making a decision of building more living space, or having a multi-car garage. In consulting with their architect, they worked out plans for a single car garage, but one that would include the installation of a car lift to transport their multiple cars to a basement garage for storage.


Solution

To complete their dream home, we custom designed a single-car garage lift for the homeowner's to park multiple cars underground.


To keep the homeowner's family safe when operating the lift, we added a few extra safety features:

  • Emergency Stop Button - immediately stops the lift when pressed.
  • Digital Security Pad - insures operation of the lift is limited to authorize users only.
  • Security Key Switch - the lift will not operate unless key is in place to a turned “On" position.
  • Motion Detectors - the lift will stop if the sensors pick up any interference around the lift and stop its movement.
  • Remote Digital Camera & Monitor - aids in the recognition of potential interference during the lift operation.


Rated 5 based on 1 product reviews

Showroom Lift with Rotating Turntable

Solving a client's Structural Challange.

Challenge
A homeowner wanted his automobile collection incorporated into his new home garage design. However, the new structural design plans prohibited any cars from driving onto the lift in either forward or reverse. If the lift was lowered to the car showroom, a wall would block the cars from driving forward, while a staircase from behind prevented cars from reversing.


Solution
To address this architectural challenge, Vasari's engineer's designed a Vasari 4-Post Parking Lift with a custom rotating turntable. This solved the obstruction in the showroom-garage by allowing vehicles to rotate to the side and exit off the platform.



Rated 5 based on 1 product reviews