SCR Parapet Wall Clamps allow perimeter fall protection railings to be mounted to a parapet wall without the need to mechanically penetrate the wall structure. This clamp-on railing system offers OSHA compliant fall protection without taking up any space on the roof. Railing height is adjusted according to parapet wall height to maintain the OSHA mandated 42" railing height above the walking surface.
SRC EnduraLine Permanent Warning Line System. The EnduraLine Warning Line system is our most robust warning line system we offer. Most commonly used for permanent demarcation on roofs and placed 15 feet in from the roof edge. This type of installation allows coverage of large open areas of roof economically and in areas where there is serviceable equipment within 15 feet of the roof edge, the SRC 360 Mobile Railing System is utilized. This combination of protection systems affords 100% perimeter protection for personnel on the roof. This visual warning line system utilizes heavy-duty cast iron plates, stainless steel cable and aluminum pennants all designed to last for years in the most rugged outdoor environments. Available in powder coated colors or galvanized finish.
|
Global dairy producer Saputo has an immediate need for rooftop safety protection at one of its U.S. facilities. What ensued was an update at more than a dozen plants and an ongoing relationship with Safety Rail Company that ensures Saputo has some of the best protected roofs in the industry.
The SRC Accu-Fit Mobile Safety Rail system is a non-penetrating, passive fall protection barrier system that protects workers from accidental falls. The Accu-Fit Traditional Series railings take versatility and aesthetics into consideration by utilizing 1 1/2” schedule 40 pipe railings supported by vertical stanchions mounted in weighted cast iron base plates. This system offers a continuous, uniform, vertical railing profile which enhances appearance and is often desirable by clients for use in high traffic areas in view of public.
The SRC Accu-Fit PBR Roof Panel Traditional Safety Rail system is a mechanically attached, passive fall protection barrier system that protects workers from accidental falls on flat roofs. The Accu-Fit Traditional Series takes versatility and aesthetics into consideration by utilizing 1 1/2” schedule 40 pipe railings supported by vertical stanchions mounted into base plates. This system offers a continuous, uniform, vertical railing profile which enhances appearance and is often desirable by clients for use in high traffic areas in view of public.
The SRC Accu-Fit Architechtural Standing Seam Safety Rail system is a non-penetrating, clamp-on passive fall protection barrier system that protects workers from accidental falls on flat roofs. The Accu-Fit Architectural Series railings take versatility and aesthetics into consideration by utilizing 1 1/2” schedule 40 pipe railings supported by vertical stanchions mounted into base plates. This system offers a continuous, uniform, curved railing profile which enhances appearance and is often desirable by clients for use in high traffic areas in view of public.
The SRC Accu-Fit Traditional Standing Seam Safety Rail system is a non-penetrating, clamp-on passive fall protection barrier system that protects workers from accidental falls on flat roofs. The Accu-Fit Traditional Series railings take versatility and aesthetics into consideration by utilizing 1 1/2” schedule 40 pipe railings supported by vertical stanchions mounted into base plates. This system offers a continuous, uniform, vertical railing profile which enhances appearance and is often desirable by clients for use in high traffic areas in view of public.
SRC EnduraLine Warning Line Systems are an OSHA compliant visual warning line system designed to alert workers of hazardous areas. Non-penetrating, weighted base plates support a stanchion and 1/8” galvanized wire rope with aluminum pennants placed every 6’ along the line. EnduraLine can be use for permanent or temporary installations.
PASSIVE VS. ACTIVE FALL PROTECTION SYSTEMS: COSTS & COMPARISONS
Some jobs carry with them inherent dangers. We do the best we can to mitigate those dangers and keep worksites as safe as possible. But safety does come at a cost, and that cost is a concern for facility and project managers.
The SRC Hatchguard is an OSHA compliant, passive fall-protection system that installs without welding, drilling or roof membrane penetration. Standard system is a one-piece that drops over the top of the roof hatch and is secured with four compression bolts. Installation takes 15 minutes.
The SRC Skylight Screen is an OSHA compliant fall protection screen for skylights. These screens compression-fit to the aluminum frame of the skylight without any mechanical penetrations. Heavy-duty construction prevents contact with skylight lens in the event of a fall. Installation takes 30 minutes.
The SRC 360 Mobile Safety Rail system is an OSHA compliant, passive fall-protection system that installs without tools, welding, drilling, or roof membranes penetration. Our unique design approach places cast iron bases around workplace safety hazards, creating a ballasted support stand in which steel guardrails are secured.
Many industrial and commercial sites have a variety of equipment and obstacles that personnel must work around - and oftentimes going up and over these barriers is the quickest and safest path. Whether up on the roof or inside the facility, the SRC Modular Crossover Stairs (MCS) system provides the safest, most versatile solution! Perfect for any obstacle, from a dangerous ammonia line to a large complex impediment, the MCS system is a one-product, multi-component solution that can do it all. No other system on the market offers our configurable, plug-and-play design - with components that work seamlessly together and can grow with you as your needs change.