Armatherm
CONTENT
Armatherm™ Z Girt Structural Thermal Break image

Armatherm™ Z Girt Structural Thermal Break

Armatherm thermally broken cladding support connection solutions prevent excessive heat flow and potential condensation problems otherwise associated with thermal bridging. Moreover, wall assemblies using Armatherm attachments will meet the continuous insulation requirement of ASHRAE 90.1 and the effective R value requirements of the Canadian NECB energy code. Modeling results show that using Armatherm Z girts results in several improvements in the thermal efficiency of wall designs, reducing heat flow:The insulation efficiencies of the wall assemblies increase significantly.Some as high as 98%.Higher, effective wall assembly R values are achieved using lower valuesof external insulation. For example, to obtain an R value of R-13 minimumto meet ASHRAE zone 1, steel girts require and external R 20; whereasArmatherm girts require only R 10.Cladding wall assemblies can meet the R value requirements of ALLgeographical zones for both ASHRAE 2013 and NECB 2011 energy codesusing Armatherm Z girts.Reduction in thickness and cost of insulation.Reduces energy consumption.
Rated 5 based on 1 product reviews
Armatherm™ 500 Structural Thermal Break Material image

Armatherm™ 500 Structural Thermal Break Material

Armatherm™ 500 (Thermal Insulation Material - TIM)Reducing heat flow within a building's thermal envelope reduces energy consumption as well as potential condensation issues. Armatherm™ 500 thermal break material (TIM) significantly reduces energy lost from thermal bridging in building envelope connections.Armatherm™ 500 structural thermal break material is a high strength, thermoset polyurethane manufactured in several densities. Armatherm™ 500 is able to transfer a wide range of structural loads with a range from 20 psi - 4000 psi. This wide load range enables designs to keep deflection and creep at a minimum in thermal break connections. Armatherm™ 500 has R values as high as 3.8 per inch which is superior to the properties of aerated concrete and wood blocking.
Rated 5 based on 1 product reviews
Armatherm™ FRR Structural Thermal Break Material image

Armatherm™ FRR Structural Thermal Break Material

Armatherm™ FRR structural thermal break material provides a combination of low thermal conductivity and high compressive strength and has been used in hundreds of structural steel framing connections transferring load in moment and shear conditions. Armatherm™ FRR thermal break material can support up 40,000 psi and has an R value of 0.9 per inch. The material is made of a reinforced, thermoset resin which is fire resistant and has very limited creep under load, making it the ideal material for use in structural steel and faCade thermal break connections.
Rated 5 based on 1 product reviews
Cladding Thermal Bridging Solutions image

Cladding Thermal Bridging Solutions

Continuous insulation is almost always compromised by metallic structural connections such as clips and girts which create thermal bridging when connected to steel stud framing. These connections in conjunction with the steel studs have a significant impact on the U value of wall assemblies. Insulation effectiveness can be reduced by as much as 50% due to these heat flow paths. Armatherm™ Z GIRTs improve the U value of cladding and wall panel assemblies by eliminating the use of highly conductive metal girts and aluminum brackets creating wall assemblies that are up to 98% efficient.Cladding Thermal BreakArmatherm cladding attachments significantly reduce thermal bridging and improve wall assembly thermal performance. Armatherm FRR Z Girt, clip and structural thermal break materials provide a combination of low thermal conductivity and high compressive strength transferring load and reducing heat loss. The thermal break material is made of a reinforced, thermoset resin that is fire resistant and exhibits very limited creep under load, making it the ideal material for use in structural and faCade thermal break connections.
Rated 5 based on 1 product reviews
Column Base Thermal Bridging Solution image

Column Base Thermal Bridging Solution

Internal steel columns traditionally extend through the building envelope floor slab and insulation at their base. In low temperature buildings such as freezer rooms and cold storage facilities, this creates a thermal bridge and point transmittance (heat loss) at the steel column base. This is also the case for exterior columns which support floors or roof overhangs. The column to roof connection interrupts the continuous insulation creating heat loss due to thermal bridging. Column Base Thermal BreakArmatherm™ 500, structural thermal break material can support and transfer column loads while providing an effective thermal break at the column connection. With R values as low as R 3.8 per inch, Armatherm™ 500 can help to meet the ASHRAE requirement for continuous insulation as well as the baseline insulation requirements for floors in refrigerated storage facilities.
Rated 5 based on 1 product reviews
Foundation Wall Thermal Bridging Solution image

Foundation Wall Thermal Bridging Solution

Thermal Bridging at foundation wall transitions creates heat loss at the foundation perimeter. This reduces the exterior wall's effective R Value. Foundations are part of a buildings' thermal envelope. The intersection at a slab on grade to foundation wall and exterior wall to foundation transition are both areas where heat flows out of a building. This is due primarily to non-continuous insulation details. Foundation Wall Thermal BreakThe linear transmittance (heat loss) at the base of the foundation wall can be reduced by as much as 60% by using an efficient, structural thermal break. Armatherm™ 500 is a load bearing, thermal break material manufactured in several densities to provide a range of load capacities with R values as high as R 3.8 per inch.Thermal bridging at a foundation wall transition can be reduced further by increasing the length of the slab insulation.
Rated 5 based on 1 product reviews
Masonry Shelf Angle Thermal Bridging Solution image

Masonry Shelf Angle Thermal Bridging Solution

Masonry veneer walls require tie-backs and shelf angles which form significant thermal bridges and can reduce a walls' R value by as much as 50% making it difficult to meet energy codes. Shelf angles transfer the masonry load back to the buildings' structural steel or concrete slab edge interrupting the continuous insulation of the wall assembly creating a linear thermal bridge. To improve the U value of a masonry wall assembly, the shelf angle can be connected to the structure at discreet, evenly spaced points such as plate “blades" allowing the insulation to pass behind the steel angle, thus reducing the effects of a continuous thermal bridge. However, building the shelf angle outwards requires larger geometries and additional material to support the cantilevered load. Masonry Shelf Angle Thermal BreakAlternatively, Armatherm™ FRR structural thermal break material can be used directly behind the masonry shelf angle as a thermal break within the insulating layer. The Armatherm™ thermal break significantly reduces the linear transmittance (heat loss) of the shelf angle connection. Rigid, metal flashing used as waterproofing can also be replaced with a non-conductive, self-adhered membrane to reduce the effects of thermal bridging further.
Rated 5 based on 1 product reviews
Parapet Roof Penetration Thermal Bridging Solution image

Parapet Roof Penetration Thermal Bridging Solution

The roof is part of the building envelope where penetrations such as davits, anchors and supports for dunnage extend through the thermal envelope and roof insulation creating non-continuous insulation. These interface details are typically connected to interior trusses or structural elements creating a thermal bridge and point transmittance (heat flow). The R value of the roof can be reduced by up to 40% in these areas.Parapet Roof Penetration Thermal BreakA structural thermal break at these locations will improve the U value of the roof assembly and prevent potential condensation problems at the structural connection. Armatherm™ FRR and 500 series thermal break materials can transfer the loading conditions at these locations while significantly reducing heat flow, creating continuous insulation. The heat loss can be improved by as much as 80%.
Rated 5 based on 1 product reviews
Balcony Canopy Thermal Bridging Solution image

Balcony Canopy Thermal Bridging Solution

The most common interface details for structural framing are canopies and balconies that use cantilevered steel or aluminum elements. These elements are typically connected to slab edges or spandrel beams on the interior side of the thermal envelope passing through insulation and air barrier layers. The R value of a wall assembly can be reduced by as much as 60% due to thermal bridging at balcony and canopy connections. The point transmittance (heat flow) at these connections can be reduced by as much as 70% by using Armatherm™ FRR structural thermal break material. Balcony Thermal BreakArmatherm™ FRR is capable of transferring load in moment and shear connections without creating significant rotation. In structural testing, Armatherm™ FRR has been evaluated in balcony connections for creep, rotation and any impact on bolt force. A structural thermal break must maintain the structural integrity of the balcony or canopy connection, while also minimizing heat flow.
Rated 5 based on 1 product reviews