Modular Elevator Manufacturing, Inc.
CONTENT
Modular Elevator Manufacturing, Inc.
CONTENT
Modular Elevator Manufacturing Builds the Most Current State of the Art Hydraulic System in the Industry. image

Modular Elevator Manufacturing Builds the Most Current State of the Art Hydraulic System in the Industry.

Our Hydraulic Elevator System is available with in-ground and holeless jacks. We are the only manufacturer to build a steel cab that complies with ASME 17.1. This can eliminate putting sprinklers, heat sensors and shunting in the hoist way. Please refer to our CAD and PDF drawings in ARCAT. We build elevators from 2000 lb. capacity to 5000 lb. capacity to meet all of the vertical requirements for your project. We provide seven colors of high pressure laminate as standard cab finishes. We offer over 2000 upgraded cab interiors that can installed onsite in one day. The Modular Elevator System by Modular Elevator Manufacturing can be used as a permanent in-place construction elevator. This can eliminate hundreds of thousands of dollars from the requirement to have a construction elevator on your project.
Rated 5 based on 1 product reviews
Modular Elevator Hoistways - A Pre-fabricated Pre-engineered Faster Solution image

Modular Elevator Hoistways - A Pre-fabricated Pre-engineered Faster Solution

Our modular Hoist way is made from 4x4 HSS structural steel. We include the code required overhead space within this structure. We build three hoist ways, an HW-1, HW-2 and HW-3. If you refer to page S3 in our PDF plan set you will see the elevators that fit into each hoist way. Our most popular size is the HW-2 with a 3500 lb. gurney complaint cab. This is the smallest footprint available for diagonal gurney compliance. There is no hoist beam required as the elevator comes pre-installed within the structure. The hoist way walls come standard with a one-hour fire rating. We can provide up to a three hour fire rating if required in your project. We use 5/8ths green board on the interior of our hoist way walls. Green board is mold and mildew resistant for moist environments. We use 5/8ths brown board on the exterior of the hoist way walls. Brown board is ideal for external walls because it has some water resistant properties and can support almost any type of exterior finish. The hoist way and pre-installed elevator can be set in as little as four hours. Once the structure is set the installation is 90% complete. All that is left to complete the Installation is the final adjustment and inspection. This takes another two or three days. Total installation time should be less than one-week. Modular Elevator Manufacturing builds a modular equipment room that can sit adjacent to the hoist way or up to thirty feet in a remote location. This modular machine room is only designed for exterior applications. If your project requires an interior elevator our elevator and hoist way typically sets during the early stages of the construction phase. This normally occurs before the walls are erected and after the poured foundation.
Rated 5 based on 1 product reviews
County of Riverside image

County of Riverside

Project Location: Riverside, CaliforniaProject Owner: County of RiversideGeneral Contractor: McCarthy ConstructionArchitect: International Parking Design A Modular Elevator Manufacturing modular elevator system will save your clients weeks of design and agency review time, cut installation time, and save you tens of thousands of dollars in maintenance fees and parts. Our elevator is also nonproprietary, and will save your clients more than $100,000 over the life of the elevator on maintenance and parts. Our production times are 10-12 weeks and the system installs in one day.
Rated 5 based on 1 product reviews
Jesuit High School image

Jesuit High School

Project Location: Carmichael, CaliforniaProject Owner: Jesuit High SchoolGeneral Contractor: Roebbelen ConstructionArchitect: Williams Paddon Architects & PlannersJesuit High School is a fully accredited Jesuit, Catholic, college preparatory, private high school that serves the greater Sacramento area. As part of a campus modernization project, the school added a MEM modular elevator connecting the main floor to the second floor.
Rated 5 based on 1 product reviews
City of Orange Parking Structure image

City of Orange Parking Structure

Project Owner: The City of Orange, California. General Contractor: Bomel Construction. Architect: Choate Parking Design.This project is a five story pre-engineered, pre-designed Modular Elevator for the Parking Structure at the Town and County Mall. Modular Elevator Manufacturing was the only Company that could stay ahead of the construction schedule for this project. Each deck of the parking structure was built in a week. The Modular Elevator System set the elevator at the beginning of the project.
Rated 5 based on 1 product reviews
Columbia Street Apartments - San Diego, CA image

Columbia Street Apartments - San Diego, CA

Project Owner: Parikh Properties. General Contractor: Cannon ConstructorsArchitect: Dess PartnersConstruction Manager: Boretto + Merrill Consulting. This project is a ground -up urban infill project in the heat of Little Italy in San Diego. This project is an 18 unit, zero lot line residential building on a 3500 square foot parcel. The small size of the parcel provides a variety of construction challenges.To offset impacts of small lot infill development Modular Elevator Manufacturing was contracted to provide a cutting-edge modular elevator. The cab and entire elevator shaft were brought into Downtown on a flatbed truck and installed in a single day. The building will be constructed around the elevator shaft and the elevator will operate as an OSHA compliant man lift during construction. The installation will save over 6 weeks of construction times well as provide a significant dollar savings to the overall cost of the project.
Rated 5 based on 1 product reviews
Mullin Automotive Museum image

Mullin Automotive Museum

Project Location: Oxnard, CaliforniaProject Owner: Peter W. Mullin Family Trust UDT General Contractor: Interscape Construction, Inc.Architect: David Hertz Archtect, SEAThe Mullin Automotive Museum is a private museum in Oxnard, California which focuses on rare and exquisite european automobiles. They wanted a very special elevator to match the decor of the museum. They selected an MEM elevator with glass wall panels in the hoistway and cab, with all components powdercoated or painted black. The museum added custom wrought iron panels integrated into the hoistway to complete the package.
Rated 5 based on 1 product reviews
Citrus Residential Dormitories at The University of La Verne -  La Verne CA image

Citrus Residential Dormitories at The University of La Verne - La Verne CA

Location: La Verne CA.Owner: The University of La VerneGeneral Contractor: Bernards BuilderArchitect: Steinberg Architects.This project had three modular elevators. Two elevators in a duplex configuration and one elevator in a simplex configuration. These were five stop elevators.
Rated 5 based on 1 product reviews
Modular Elevator Applications Gallery image

Modular Elevator Applications Gallery

Modular Elevators are the perfect solution for many applications as shown below. ClassroomsStadiumsLight Rail StationsParking StructuresPedestrian BridgesConvention CentersCruise Ship TerminalsIndoor MallsOutdoor MallsMedical OfficesHospitalsOther Custom Applications
Rated 5 based on 1 product reviews