SECTION 05 52 10 SAFETY RAILINGS AND GATES Copyright 2015 - 2026 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** Tractel Ltd.; safety railings and gates. . This section is based on the products of Tractel Ltd., which is located at: 6300 W. By NorthWest Blvd. , Suite 100 Houston, TX 77040 Toll Free Tel: 800-962-6111 Email: jim.nowaczewski@alimakgroup.com Web: https://www.tractel.com/us [ https://arcat.com/company/tractel-ltd-36094 ] for additional information. The FabEnCo FabRail safety rail system is a component, highly versatile and effective safety solution engineered to install quickly and easily in virtually any kind of environment. Constructed of long-lasting 1-1/2' (1.90 OD) Flo-Coat, FabRail is built to serve your needs. With nothing more than a hex key needed to install, FabRail enables you to create a permanent, durable OSHA-compliant barrier in no time. In 1972, FabEnCo introduced its first patented self-closing safety gate to meet the OSHA requirement for fall protection at platform and ladderway openings. Today, FabEnCo has sold more than 600,000 self-closing safety gates and is recognized as the world's leading manufacturer of industrial safety gates. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for Project. A. Modular safety rails. (FabRail) B. Self-closing safety gates of the following types: 1. Self-closing safety gates. (A Series) 2. Extended coverage self-closing safety gates. (XL Series) 3. Standard bolt-on safety gates. (R Series) 4. Standard bolt-on extended coverage safety gates. (RX Series) 5. Safety gates for new construction. (Z Series) 6. Full coverage safety gates. (ZT Series) 7. Universal hinge mount safety gates. (G Series) 8. Mezzanine-pivot safety gates. (MZ Series) 1.2 RELATED SECTIONS ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this Project; add others as required. A. Section 05 50 00 - Metal Fabrications. 1.3 REFERENCES ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited Section. A. OSHA 29 CFR 1910.23 - Guarding Floor and Wall Openings and Holes. 1.4 SUBMITTALS A. Submit under provisions of Section 01 30 00 - Administrative Requirements. B. Product Data: Manufacturer's data sheets on each product to be used, including: 1. Preparation instructions and recommendations. 2. Storage and handling requirements and recommendations. 3. Installation methods. ** NOTE TO SPECIFIER ** Delete paragraph below if shop drawings not required. C. Shop Drawings: Drawings showing plans, elevations, sections and details of components. 1.5 QUALITY ASSURANCE A. Provide safety gates which meet or exceed OSHA 29CFR 1910.23 standards as applicable. 1.6 PROJECT CONDITIONS A. Field Measurements: Where safety railings are indicated to fit to other construction, check actual dimensions of other construction by accurate field measurements before delivery. 1.7 WARRANTY A. Warranty: Provide manufacture's standard limited warranty. PART 2 PRODUCTS 2.1 MANUFACTURERS A. Acceptable Manufacturer: Tractel Ltd., which is located at: 6300 W. By NorthWest Blvd. , Suite 100 Houston, TX 77040 Toll Free Tel: 800-962-6111 Email: jim.nowaczewski@alimakgroup.com;Web: https://www.tractel.com/us ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 Section on product options and substitutions. B. Substitutions: Not permitted. C. Requests for substitutions will be considered in accordance with provisions of Section 01 60 00 - Product Requirements. ** NOTE TO SPECIFIER ** The FabEnCo FabRail safety rail system is a component, highly versatile and effective safety solution engineered to install quickly and easily in virtually any kind of environment. Constructed of long-lasting 1-1/2" (1.90 OD) Flo-Coat,(R) FabRail is built to serve your needs. With nothing more than a hex key needed to install, FabRail enables you to create a permanent, durable OSHA-compliant barrier in no time. Delete if not required. 2.2 MODULAR SAFETY RAILS A. Product: FabRail by FabEnCo, Inc. 1. System: Modular components of top rail, midrail, posts and fittings. Designed with 42 inches (1067 mm) toprail height and 21 inches (533 mm) midrail height with posts on 7 feet (2134 mm) centers, anchors and fittings. 2. Compliance: OSHA-compliant barrier, and BOCA building code. ** NOTE TO SPECIFIER ** Standard size. Delete if not required. 3. Rail and Post Material: 1-1/2 inches (38 mm) Flo-Coat (1.90 O.D). ** NOTE TO SPECIFIER ** Optional size. Delete if not required. 4. Rail and Post Material: 1-1/4 inches (32 mm) Flo-Coat (1.66 O.D). 5. Fittings: Pre-assembled to posts for installation of rails. Fittings secured by hex nut and key wrench. 6. Finish: Factory-applied powder coated finish selected from manufacturer's standard colors. 2.3 SELF-CLOSING SAFETY GATES ** NOTE TO SPECIFIER ** The FabEnCo A Series Self-Closing Safety Gate can be easily installed in minutes on all types of handrails (angle, flatbar, pipe) or to existing walls. It can be mounted left or right, on either side of a handrail. The Safety Gate's stainless steel spring automatically closes the gate after each passage and adjustment bolts provide positive stop without handrail contact. Delete model if not required. A. Self-Closing Safety Gates: A Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. A71. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. A71-PC. 3. Material: 6061-T6 aluminum, Model No. A82. 4. Material: 316L stainless steel, Model No. A94. 5. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 6. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** The FabEnCo XL Series Self-Closing Safety Gate can be easily installed in minutes on all types of handrails (angle, flatbar, pipe) or to existing walls. It can be mounted left or right, on either side of a handrail. The Safety Gate's stainless steel spring automatically closes the gate after each passage and adjustment bolts provide positive stop without handrail contact. Delete model if not required. B. Extended Coverage Self-Closing Safety Gates: XL Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. XL71. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. XL71-PC. 3. Material: 6061-T6 aluminum, Model No. XL82. 4. Material: 316L stainless steel, Model No. XL94. 5. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 6. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** Delete optional toe board kit if not required. 7. Clamp-on Toe Board Kit: A36 carbon steel galvanized. 8. Clamp-on Toe Board Kit: A36 carbon steel with safety yellow powder coat. ** NOTE TO SPECIFIER ** The FabEnCo R Series Self-Closing Safety Gate can be installed on all types of handrails (angle, flatbar, pipe). Choose standard or 90 degrees stop positions. Delete model if not required. C. Standard Bolt-on Safety Gates: R Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. R70. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. R70-PC. 3. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 4. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** Delete stop position not required. 5. Stop Position: Standard. 6. Stop Position: 90 degrees. ** NOTE TO SPECIFIER ** The FabEnCo RX Series Self-Closing Safety Gate can be installed on all types of handrails (angle, flatbar, pipe). The RX Series is the only gate that requires a swing direction to be specified because the mounting plate is at the top of the gate rather than the center. The left-hand or right-hand swing designation indicates the direction the gate swings when you push the gate open to walk through the protected opening. Choose standard or 90 degree stop positions. Delete model if not required. D. Standard Bolt-on Extended Coverage Safety Gates: RX Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. RX70. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. RX70-PC. 3. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 4. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** Delete stop position not required. 5. Stop Position: Standard. 6. Stop Position: 90 degrees. ** NOTE TO SPECIFIER ** Delete swing not required. 7. Swing: Left-hand swing. 8. Swing: Right-hand swing. ** NOTE TO SPECIFIER ** Delete optional toe board kit if not required. 9. Clamp-on Toe Board Kit: A36 carbon steel galvanized. 10. Clamp-on Toe Board Kit: A36 carbon steel with safety yellow powder coat. ** NOTE TO SPECIFIER ** The FabEnCo Z Series Self-Closing Safety Gate can be installed on all types of handrails (angle, flatbar, pipe) or to existing walls. It can be mounted left or right, on either side of a handrail. You can choose a standard or 90 degree stop position. Once installed, our custom stainless steel spring automatically closes the gate after each passage Delete model if not required. E. Safety Gates for New Construction. Z Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. Z70. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. Z70-PC. 3. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 4. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** Delete stop position not required. 5. Stop Position: Standard. 6. Stop Position: 90 degrees. ** NOTE TO SPECIFIER ** Delete optional toe board kit if not required. 7. Clamp-on Toe Board Kit: A36 carbon steel galvanized. 8. Clamp-on Toe Board Kit: A36 carbon steel with safety yellow powder coat. ** NOTE TO SPECIFIER ** The FabEnCo ZT Series Self-Closing Safety Gate can be installed on all types of handrails (angle, flatbar, pipe) or to existing walls. It can be mounted left or right, on either side of a handrail. You can choose a standard or 90 degree stop position. Once installed, our custom stainless steel spring automatically closes the gate after each passage. Delete model if not required. F. Full Coverage Safety Gates: ZT Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. ZT70. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. ZT70-PC. 3. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 4. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** Delete stop position not required. 5. Stop Position: Standard. 6. Stop Position: 90 degrees. ** NOTE TO SPECIFIER ** The FabEnCo Self-Closing safety gate can be easily installed in minutes on all types of handrails (angle, flatbar, pipe) or to existing walls. It can be mounted left or right, on either side of a handrail. The safety gate's stainless steel springs automatically close the gate after each passage. Delete model if not required. G. Universal Hinge Mount Safety Gates: G Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. G70. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. G70-PC. 3. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 4. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. 5. Lateral Adjustment: 6 inches (152 mm). ** NOTE TO SPECIFIER ** The MZ-Pivot Gate protects employees in elevated mezzanine loading areas. Its counterbalanced gates ensure that one gate is always between your employees and the edge of the platform. The MZ-Pivot Gate is available in single or double pallet widths, breaks down for shipping efficiency and assembles easily with basic tools. Delete model if not required. H. Mezzanine-Pivot Safety Gates: MZ Series by FabEnCo, Inc. ** NOTE TO SPECIFIER ** Delete materials not required. 1. Material: A36 carbon steel galvanized, Model No. MZ14. 2. Material: A36 carbon steel with safety yellow powder coat, Model No. MZ14-PC. 3. Material: 316L stainless steel. 4. Height and Width: As selected from manufacturer's standard sizes, to fit clear opening indicated on the Drawings. 5. Hardware: Stainless steel spring and zinc-plated bolts, nuts and washers. ** NOTE TO SPECIFIER ** Delete pallet width not required. 6. Pallet Width: Single. 7. Pallet Width: Single. PART 3 EXECUTION 3.1 EXAMINATION A. Do not begin installation until substrates have been properly prepared. B. If substrate preparation is the responsibility of another installer, notify Architect of unsatisfactory preparation before proceeding. 3.2 PREPARATION A. Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions. 3.3 INSTALLATION A. Install in accordance with manufacturer's instructions and in proper relationship with adjacent construction. Test for proper operation and adjust until satisfactory results are achieved. 3.4 PROTECTION A. Protect installed products until completion of project. B. Touch-up, repair or replace damaged products before Substantial Completion. END OF SECTION