SECTION 09 67 00 FLUID-APPLIED FLOORING Copyright 2020 - 2025 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** Dudick Inc., fluid-applied flooring. This section is based on the products of Dudick Inc., which is located at: 1818 Miller Pkwy. Streetsboro, OH 44241 Toll Free: 800-322-1970 Phone: 330-562-1970 Fax: 330-562-7638 Email: sales@dudick.com Web: dudick.com [Click Here] for additional information. Dudick Inc. located in Northeast Ohio is a world leader in High Performance Coatings, Floorings, and Tank Linings. For over 40 years we have provided solutions in corrosion resistance and chemical containment systems for food processing, steel production, chemical processing, pulp and paper, electronics, power, and biological research labs. Our products meet the stringent requirements of FDA, USDA, and NSF. We currently manufacture in Streetsboro, Ohio; Kaohsiung, Taiwan; Seoul, Korea; and Buenos Aires, Argentina. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for project. A. Industrial Solid Coatings of the Following Types: 1. Polymer Alloy Series. 2. Protecto Coat Series. 3. Protecto Crete Series. 4. Protecto Flake Series. 5. Protecto Flex Series. 6. Protecto Glass Series. 7. Protecto Line Series. 8. Shock Crete Series. B. Architectural Solid Coatings of the Following Types: 1. Steri Flor Series. 2. Steri Coat Series. 3. Steri Glass. 4. Steri Seal Series. 5. Sealers. C. Architectural Flake Floor Coatings of the Following Types: 1. Steri Flake Series. D. Architectural Quartz Floor Coatings: Steri Quartz Series. E. Other Coatings of the Following Types: 1. Polymer Concrete Series. 2. Polymer Steel Series. 3. Vapor-Stop Series. F. Accessories and Components of the Following Types: 1. Polymer concrete. 2. Underlayment. 3. Block filler. 4. Sealants. 5. Fillers. 6. Concrete repair mortar. 7. Gel-Coat Series. 8. Membranes. 9. Hardener. 10. Primers. 11. Solvents. 12. Scratch-Coat Series. 13. Steri-Cove Gel. 14. Styrene. 1.2 RELATED SECTIONS ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required. A. Section 03 30 00 - Cast-in-Place Concrete. B. Section 03 63 00 - Epoxy Grouting. C. Section 05 10 00 - Structural Metal Framing. D. Section 05 50 00 - Metal Fabrications. E. Section 07 90 00 - Joint Protection. F. Section 09 90 00 - Painting and Coating. 1.3 REFERENCES ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited section. A. ASTM International (ASTM): 1. ASTM C307 - Standard Test Method For Tensile Strength of Chemical-Resistant Mortar, Grouts, And Monolithic Surfacings. 2. ASTM C413 - Standard Test Method for Absorption of Chemical-Resistant Mortars, Grouts, Monolithic Surfacings, and Polymer Concretes. 3. ASTM C423 - Standard Test Method for Sound Absorption and Sound Absorption Coefficients by the Reverberation Room Method. 4. ASTM C579 - Standard Test Methods for Compressive Strength of Chemical-Resistant Mortars, Grouts, Monolithic Surfacings, and Polymer Concretes. 5. ASTM C580 - Standard Test Method for Flexural Strength and Modulus of Elasticity of Chemical-Resistant Mortars, Grouts, Monolithic Surfacings, and Polymer Concretes. 6. ASTM D307 - Method of Test for Spectral Characteristics and Color of Objects and Materials. 7. ASTM D412 - Standard Test Methods for Vulcanized Rubber and Thermoplastic Elastomers - Tension. 8. ASTM D635 - Standard Test Method for Rate of Burning and/or Extent and Time of Burning of Plastics in a Horizontal Position. 9. ASTM D638 - Standard Test Method for Tensile Properties of Plastics. 10. ASTM D695 - Standard Test Method for Compressive Properties of Rigid Plastics. 11. ASTM D1894 - Standard Test Method for Static and Kinetic Coefficients of Friction of Plastic Film and Sheeting. 12. ASTM D4060 - Standard Test Method for Abrasion Resistance of Organic Coatings by the Taber Abraser. 13. ASTM D4541 - Standard Test Method for Pull-Off Strength of Coatings Using Portable Adhesion Testers. 14. ASTM D7234 - Standard Test Method for Pull-Off Adhesion Strength of Coatings on Concrete Using Portable Pull-Off Adhesion Testers. 15. ASTM E84 - Standard Test Method for Surface Burning Characteristics of Building Materials. 16. ASTM F150 - Standard Test Method for Electrical Resistance of Conductive and Static Dissipative Resilient Flooring. B. Food and Drug Administration (FDA). C. National Fire Protection Association (NFPA): 1. NFPA 99 - Health Care Facilities Code. D. United States Department of Agriculture (USDA). E. US Military Standard 810E - Environmental Engineering Considerations and Laboratory Tests. 1.4 SUBMITTALS A. Submit under provisions of Section 01 30 00. B. Product Data: 1. Manufacturer's data sheets on each product to be used. 2. Preparation instructions and recommendations. 3. Storage and handling requirements and recommendations. 4. Typical installation methods. ** NOTE TO SPECIFIER ** Delete if not applicable to product type. C. Verification Samples: Two representative units of each type, size, pattern and color. D. Shop Drawings: Include details of materials, construction and finish. Include relationship with adjacent construction. 1.5 QUALITY ASSURANCE A. Manufacturer Qualifications: Company specializing in manufacturing products specified in this section with a minimum five years documented experience. B. Installer Qualifications: Company specializing in performing Work of this section with minimum two years documented experience with projects of similar scope and complexity. C. Source Limitations: Provide each type of product from a single manufacturing source to ensure uniformity. ** NOTE TO SPECIFIER ** Include mock-up if the project size or quality warrant the expense. The following is one example of how a mock-up on might be specified. When deciding on the extent of the mock-up, consider all the major different types of work on the project. D. Mock-Up: Construct a mock-up with actual materials in sufficient time for Architect's review and to not delay construction progress. Locate mock-up as acceptable to Architect and provide temporary foundations and support. 1. Intent of mock-up is to demonstrate quality of workmanship and visual appearance. 2. If mock-up is not acceptable, rebuild mock-up until satisfactory results are achieved. 3. Retain mock-up during construction as a standard for comparison with completed work. 4. Do not alter or remove mock-up until work is completed or removal is authorized. 1.6 PRE-INSTALLATION CONFERENCE A. Convene a conference approximately two weeks before scheduled commencement of the Work. Attendees shall include Architect, Contractor and trades involved. Agenda shall include schedule, responsibilities, critical path items and approvals. 1.7 DELIVERY, STORAGE, AND HANDLING A. Store and handle in strict compliance with manufacturer's written instructions and recommendations. B. Protect from damage due to weather, excessive temperature, and construction operations. 1.8 PROJECT CONDITIONS A. Maintain environmental conditions (temperature, humidity, and ventilation) within limits recommended by manufacturer for optimum results. Do not install products under environmental conditions outside manufacturer's recommended limits. 1.9 WARRANTY A. Manufacturer's standard limited warranty unless indicated otherwise. PART 2 PRODUCTS 2.1 MANUFACTURERS A. Acceptable Manufacturer: Dudick Inc., which is located at: 1818 Miller Pkwy.; Streetsboro, OH 44241; ASD Toll Free Tel: 800-322-1970; Tel: 330-562-1970; Fax: 330-562-7638; Email: sales@dudick.com; Web: www.dudick.com ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions. B. Substitutions: Not permitted. C. Requests for substitutions will be considered in accordance with provisions of Section 01 60 00. ** NOTE TO SPECIFIER ** Delete Article if not required. 2.2 INDUSTRIAL SOLID COATINGS ** NOTE TO SPECIFIER ** Delete basis of design options not required. A. Basis of Design: Polymer Alloy 2000. 100 Percent Solids, Multi-Functional Epoxy Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Standards Compliance: USDA compliant. b. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, aliphatic organic solvents, mineral oils, salt solutions. c. Low odor and low-VOC. d. Compressive Strength, ASTM C579: Greater than 12,000 psi (82,740 kPa). e. Tensile Strength, ASTM D638: 5000 psi (34,470 kPa). f. Flexural Strength, ASTM C580: 7200 psi (49,640 kPa). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). h. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. i. Water Absorption, ASTM C413: 0.0324 percent. 2. Polymer Alloy 2000: Semi-self-leveling. Thickness: 0.020 inch (0.51 mm). 3. Finish: High-gloss. B. Basis of Design: Polymer Alloy 2000C, 100 Percent Solids, Multi-Functional, Conductive, Semi-Self Leveling Epoxy Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Standards Compliance: USDA compliant. b. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, aliphatic organic solvents, mineral oils, salt solutions. c. Low odor and low-VOC. d. Compressive Strength, ASTM C579: Greater than 6,000 psi (41,370 kPa). e. Tensile Strength, ASTM D307: 2200 psi (15,170 kPa). f. Flexural Strength, ASTM C580: 1800 psi (12,410 kPa). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). h. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. i. Resistivity, ASTM F150: 25,000 to 1,000,000 Ohms. 2. Thickness: 0.020 inch (0.51 mm). 3. Finish: High-gloss. C. Basis of Design: Polymer Alloy 2000LE, 100 Percent Solids, Flexible, Semi-Self Leveling Epoxy Monolithic Floor Topping; as manufactured by Dudick Inc. Develops a cured strength 2 to 3 times that of the concrete base to which it is applied. 1. Can be Seeded for Anti-Skid Surface. 2. Performance Requirements: a. Standards Compliance: USDA compliant. b. Low odor and low-VOC. VOC Values: 0 g per l. c. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, aliphatic organic solvents, mineral oils, salt solutions. d. Compressive Strength, ASTM C579: Greater than 12,000 psi (82,737 kPa). e. Tensile Strength, ASTM D307: 5000 psi (34,474 kPa). f. Flexural Strength, ASTM C580: 11500 psi (79,290 kPa). g. Fungus Resistance: No growth. h. Shore D Hardness, ASTM D2240: 80 - 90. i. Taber Abrasion, ASTM D4060: 33 mg. j. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). k. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. l. Water Absorption, ASTM C413: 0.0324 percent. 3. Thickness: 0.020 to 0.030 inches (0.51 to 0.76 mm) DFT. 4. Finish: High-gloss. D. Basis of Design: Polymer Alloy 2000SD, 100 Percent Solids, Static Dissipative, Multi-Functional, Semi-Self Leveling Epoxy Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Standards Compliance: USDA compliant. b. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, aliphatic organic solvents, mineral oils, salt solutions. c. Low odor and low-VOC. d. Compressive Strength, ASTM C579: Greater than 6,000 psi (41,370 kPa). e. Tensile Strength, ASTM D307: 2200 psi (15,170 kPa). f. Flexural Strength, ASTM C580: 1800 psi (12,410 kPa). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). h. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. i. Resistivity, ASTM F150: 1,000,000 to 1,000,000,000 Ohms. 2. Thickness: 0.015 inch (0.38 mm). 3. Finish: High-gloss. E. Basis of Design: Protecto-Coat 100XT, Flake Filled, High Performance, 100 Percent Solids, Novolac Epoxy Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, salts, sulfuric acid, oils, solvents. b. Low odor and low-VOC. c. Compressive Strength, ASTM C579: Minimum 9,000 psi (62,050 kPa). d. Tensile Strength, ASTM D307: Minimum 3000 psi (20,680 kPa). e. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). f. Taber Abrasion, ASTM D4060: 0.0018 ounces (50 mg). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Applied in two coats. 3. Total Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). F. Basis of Design: Protecto-Coat 1130, High Solids, High Performance, Multi-Function Epoxy Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, salts, oils, solvents. b. Low odor and low-VOC. c. Compressive Strength, ASTM C579: 12,000 psi (82,740 kPa). d. Tensile Strength, ASTM D307: 4000 psi (27,580 kPa). e. Taber Abrasion, ASTM D4060: 0.0020 ounces (58 mg). f. Flexural Strength, ASTM C580: 6000 psi (41,370 kPa). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Applied in two coats. 3. Total Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). G. Basis of Design: Protecto-Coat 306DTR, High Solids, Flake Filled, Self-Priming, Direct-to-Rust Epoxy Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acid fumes, dilute alkali fumes, organic solvent fumes, salt solutions, mineral oils. b. Taber Abrasion, ASTM D4060: 0.0036 ounces (101 mg). c. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Thickness: 0.008 to 0.010 inch (0.20 to 0.25 mm). H. Basis of Design: Protecto-Coat 800, Flake-Filled, Vinyl Ester Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: FDA compliant. b. Chemical Resistance: Organic acids, inorganic acids, alkali solutions, salts, oils. c. Protective against fluorides and higher caustic concentrations. d. Tensile Strength, ASTM C307: Minimum 2500 psi (17,240 kPa). e. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). f. Taber Abrasion, ASTM D4060: 0.00081 ounces (23 mg). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Applied in two coats. 3. Total Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). I. Basis of Design: Protecto-Coat 805, Flake-Filled, Vinyl Ester Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: FDA compliant. b. Chemical Resistance: Organic acids, inorganic acids, alkali solutions, salts, oils. ** NOTE TO SPECIFIER ** Protecto-Coat 805 offers more protection than Protecto-Coat 800. c. Highly protective against fluorides and higher caustic concentrations. d. Tensile Strength, ASTM C307: Minimum 2500 psi (17,240 kPa). e. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). f. Taber Abrasion, ASTM D4060: 0.00081 ounces (23 mg). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Applied in two coats. 3. Total Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). J. Basis of Design: Protecto-Coat 800HT, Glass Flake-Filled, Spray Applied Vinyl Ester Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: FDA compliant. b. Chemical Resistance: Organic acids, inorganic acids, alkali solutions, salts, oils. c. Tensile Strength, ASTM C307: Minimum 2500 psi (17,240 kPa). d. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). e. Taber Abrasion, ASTM D4060: 0.00071 ounces (20 mg). f. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Applied in two or three coats. 3. Total Thickness: 0.030 to 0.060 inch (0.76 to 1.4 mm). K. Basis of Design: Protecto-Coat 900, Flake-Filled, Novolac Vinyl Ester Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, alkali solutions, solvents, salts, oils. b. Tensile Strength, ASTM C307: Minimum 2500 psi (17,240 kPa). c. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). d. Taber Abrasion, ASTM D4060: 0.0008 ounces (23 mg). e. Flame Spread Index, ASTM E84: 35. f. Smoke Development Index, ASTM E84: 130. 2. Applied in two coats. 3. Total Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). L. Basis of Design: Protecto-Coat 905, Flake-Filled, Novolac Vinyl Ester Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, alkali solutions, solvents, salts, oils. b. Increased protection against fluorides and higher caustic concentrations. c. Electrical Properties, ASTM F150 and NFPA 99: 1.5 to 2.0 Megaohms. d. Tensile Strength, ASTM C307: Minimum 2500 psi (17,240 kPa). e. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). f. Taber Abrasion, ASTM D4060: 0.0008 ounces (23 mg). g. Flame Spread Index, ASTM E84: 35. h. Smoke Development Index, ASTM E84: 130. 2. Applied in two coats. 3. Total Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). M. Basis of Design: Protecto-Coat 900HT, Glass Flake Filled, High Performance, Spray Applied, Novolac Vinyl Ester Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, alkali solutions, solvents, salts, oils. b. Tensile Strength, ASTM C307: Minimum 2500 psi (17,240 kPa). c. Flexural Strength, ASTM C580: Minimum 5000 psi (34,470 kPa). d. Taber Abrasion, ASTM D4060: 0.0007 ounces (20 mg). e. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). f. Friction Coefficient, ASTM D1894: Static 0.12, Kinetic 0.17. 2. Applied in two or three coats. 3. Total Thickness: 0.030 to 0.060 inch (0.76 to 1.4 mm). N. Basis of Design: Protecto-Coat EPG, Epoxy Phenolic Glass Flake Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Sour and sweet crude, waste water, salt water, MTBE, weak acids and weak caustics with PH of 2.5 to 11, most aliphatic and aromatic compounds. b. Self-priming. 2. Applied in two coats. 3. Total Thickness: 0.012 to 0.014 inch (0.30 to 0.36 mm). O. Basis of Design: Protecto-Coat PS, Elastomeric Polysulfide Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Aliphatic hydrocarbons, toluene and higher boiling aromatics, fuel oil, crude oil, butyl acetate and higher boiling esters, most acids and bases. b. Self-priming. c. Tensile Strength, ASTM D412: Minimum 450 psi (3100 kPa). d. Elongation, ASTM D412: 20 percent. 2. Thickness: 0.015 to 0.020 inch (0.38 to 0.51 mm). P. Basis of Design: Protecto-Crete 140T, Trowel Applied or Seeded Novolac Epoxy Topping and Resurfacer; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, alkaline solutions, solvents, salts, oils, sulfuric acid 98 percent. b. Compressive Strength, ASTM C579: Minimum 5000 psi (34,470 kPa). c. Tensile Strength, ASTM C307: Minimum 1500 psi (10,340 kPa). d. Flexural Strength, ASTM C580: Minimum 2200 psi (15,170 kPa). e. Taber Abrasion, ASTM D4060: 0.0021 ounces (60 mg). f. Cohesive Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Applied in one coat. 3. Total Thickness: 3/16 inch (4.8 mm). Q. Basis of Design: Protecto-Flake 800, Glass Flake-Filled, Trowel Applied, High Molecular Weight Vinyl Ester Tank Lining; as manufactured by Dudick Inc. 1. Performance Requirements: a. Protecto-Flake 800 Compliance: FDA compliant. b. Chemical Resistance: Sulfuric acid, chromic acid, hydrochloric acid, phosphoric acid, nitric acid, acetic acid, fatty acids, chlorides, phosphates, sulfides, aliphatic solvents, aromatic solvents. 2. Tensile Strength, ASTM C307: 3900 psi (26,890 kPa). a. Flexural Strength, ASTM C580: 9300 psi (64,120 kPa). b. Elongation, ASTM C307: 1 percent. c. Taber Abrasion, ASTM D4060: 0.0024 ounces (68 mg). d. Flame Spread, ASTM D635: 3.9 inches (100 mm). e. Adhesion to Steel, ASTM D4541: 2200 psi (15,170 kPa). 3. Thickness: 0.060 to 0.080 inch (1.5 to 2.0 mm). R. Basis of Design: Protecto-Flake 900, Glass Flake-Filled, Trowel Applied, High Molecular Weight Vinyl Ester Tank Lining; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: FDA compliant. b. Protecto-Flake 900: Improved chemical resistance to salts, acids, and organic solvents. c. Chemical Resistance: Sulfuric acid, chromic acid, hydrochloric acid, phosphoric acid, nitric acid, acetic acid, fatty acids, chlorides, phosphates, sulfides, aliphatic solvents, aromatic solvents. d. Tensile Strength, ASTM C307: 3900 psi (26,890 kPa). e. Flexural Strength, ASTM C580: 9300 psi (64,120 kPa). f. Elongation, ASTM C307: 1 percent. g. Taber Abrasion, ASTM D4060: 0.0024 ounces (68 mg). h. Flame Spread, ASTM D635: 3.9 inches (100 mm). i. Adhesion to Steel,ASTM D4541: 2200 psi (15,170 kPa). 2. Thickness: 0.060 to 0.080 inch (1.5 to 2.0 mm). S. Basis of Design: Protecto-Flex 100XT, Trowel Applied, Glass Reinforced, Epoxy Lining with Novolac Epoxy Topcoat; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, solvents, alkali solutions, salts, oils. b. Compressive Strength, ASTM C579: 6000 psi (41,370 kPa). c. Tensile Strength, ASTM C307: Minimum 4500 psi (31,030 kPa). d. Tensile Elongation, ASTM C307: 12 to 15 percent. e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Base Coat: Flexibilized epoxy resin with silica fillers. 3. Reinforcement: Fiberglass mat. 4. Topcoat: Novolac epoxy binder and overlapping flake fillers. 5. Total Thickness: 0.100 to 0.110 inch (2.2 to 2.4 mm). T. Basis of Design: Protecto-Flex 325HB, Trowel Applied, Glass Reinforced, Epoxy Lining; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: FDA acceptable. b. Chemical Resistance: Dilute inorganic acids, mineral oils, ammonium hydroxide, sodium hydroxide, brine solutions. c. Compressive Strength, ASTM C579: 6000 psi (41,370 kPa). d. Tensile Strength, ASTM C307: Minimum 4500 psi (31,030 kPa). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Base Coat: Flexibilized epoxy resin with silica fillers. 3. Reinforcement: Fiberglass mat. 4. Topcoat: Amine cured epoxy resin and overlapping fillers. 5. Total Thickness: 0.100 to 0.110 inch (2.2 to 2.4 mm). U. Basis of Design: Protecto-Flex 800, Trowel Applied, Glass Reinforced, Flexible Epoxy Lining with a Vinyl Ester Topcoat; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: FDA compliant. b. Chemical Resistance: Organic acids, inorganic acids, mineral oils, ammonium hydroxide, sodium hydroxide, brine solutions, solvents. c. Compressive Strength, ASTM C579: 6000 psi (41,370 kPa). d. Tensile Strength, ASTM C307: Minimum 4500 psi (31,030 kPa). e. Tensile Elongation, ASTM C307: 12 to 15 percent. f. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Base Coat: Flexibilized epoxy resin with silica fillers. 3. Reinforcement: Fiberglass mat. 4. Topcoat: Vinyl ester resin. ** NOTE TO SPECIFIER ** Broadcast is optional. Delete broadcast options not required. 5. Broadcast: Sand. 6. Broadcast: Aluminum oxide. 7. Total Thickness: 0.100 to 0.110 inch (2.2 to 2.4 mm). V. Basis of Design: Protecto-Flex 805, Trowel Applied, Glass Reinforced, Epoxy Lining with a Graphite Filled Vinyl Ester Topcoat; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, mineral oils, ammonium hydroxide, sodium hydroxide, brine solutions, solvents, sodium hypochlorite. b. Compressive Strength, ASTM C579: 6000 psi (41,370 kPa). c. Tensile Strength, ASTM C307: Minimum 4500 psi (31,030 kPa). d. Tensile Elongation, ASTM C307: 12 to 15 percent. e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Base Coat: Flexibilized epoxy resin with silica fillers. 3. Reinforcement: Fiberglass mat. 4. Topcoat: Vinyl ester resin. ** NOTE TO SPECIFIER ** Broadcast is optional. Delete broadcast options not required. 5. Broadcast: Sand. 6. Broadcast: Aluminum oxide. 7. Total Thickness: 0.100 to 0.110 inch (2.2 to 2.4 mm). W. Basis of Design: Protecto-Flex 900, Trowel Applied, Glass Reinforced, Flexible Epoxy Lining with a Flake Filled Vinyl Ester Intermediate Coat and Novolac Vinyl Ester Topcoat; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, mineral oils, ammonium hydroxide, sodium hydroxide, brine solutions, solvents. b. Compressive Strength, ASTM C579: 6000 psi (41,370 kPa). c. Tensile Strength, ASTM C307: Minimum 4500 psi (31,030 kPa). d. Tensile Elongation, ASTM C307: 12 to 15 percent. e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Base Coat: Flexibilized epoxy resin with silica fillers. 3. Reinforcement: Fiberglass mat. 4. Intermediate Coat: Vinyl ester resin. 5. Topcoat: Novolac vinyl ester resin. ** NOTE TO SPECIFIER ** Broadcast is optional. Delete broadcast options not required. 6. Broadcast: Sand. 7. Broadcast: Aluminum oxide. 8. Total Thickness: 0.100 to 0.110 inch (2.2 to 2.4 mm). X. Basis of Design: Protecto-Flex 905, Trowel Applied, Glass Reinforced, Flexible Epoxy Lining with a Graphite Filled Novolac Vinyl Ester Topcoat; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, mineral oils, ammonium hydroxide, sodium hydroxide, brine solutions, solvents. b. Compressive Strength, ASTM C579: 6000 psi (41,370 kPa). c. Tensile Strength, ASTM C307: Minimum 4500 psi (31,030 kPa). d. Tensile Elongation, ASTM C307: 12 to 15 percent. e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Base Coat: Flexibilized epoxy resin with silica fillers. 3. Reinforcement: Fiberglass mat. 4. Intermediate Coat: Vinyl ester resin. 5. Topcoat: Novolac vinyl ester resin. ** NOTE TO SPECIFIER ** Broadcast is optional. Delete broadcast options not required. 6. Broadcast: Sand. 7. Broadcast: Aluminum oxide. 8. Total Thickness: 0.100 to 0.110 inch (2.2 to 2.4 mm). Y. Basis of Design: Protecto-Glass 1130, Trowel Applied, Reinforced, High Performance, Multi-Functional, 100 Percent Solids Epoxy Lining; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, solvents, salts, oils. b. Compressive Strength, ASTM C579: Minimum 6000 psi (41,370 kPa). c. Tensile Strength, ASTM C307: Minimum 4000 psi (27,580 kPa). d. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. e. Flame Spread, ASTM D635: 0.2 inches (5 mm). f. Taber Abrasion, ASTM D4060: 0.0020 ounces (58 mg). 2. Basecoat: Epoxy resin and silica fillers. 3. Reinforcement: Fiberglass mat. 4. Topcoat: Epoxy resin with flake fillers. 5. Thickness: 0.090 inch (2.3 mm). Z. Basis of Design: Protecto-Glass 160XT, Trowel Applied, Reinforced, 100 Percent Solids, Novolac Epoxy Lining; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Sulfuric acid, dilute inorganic acids, alkali solutions, solvents, salts, oils. b. Compressive Strength, ASTM C579: Minimum 6000 psi (41,370 kPa). c. Tensile Strength, ASTM C307: Minimum 4000 psi (27,580 kPa). d. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. e. Flame Spread, ASTM D635: 1.3 inches (33 mm). f. Taber Abrasion, ASTM D4060: 0.0025 ounces (72 mg). 2. Basecoat: Novolac epoxy resin and silica fillers. 3. Reinforcement: Fiberglass mat. 4. Topcoat: Novolac epoxy resin and overlapping flake fillers. 5. Thickness: 0.090 inch (2.3 mm). AA. Basis of Design: Protecto-Glass 860, Trowel Applied, Reinforced Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, fluorides, alkali solutions, salts, oils. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Flexural Strength, ASTM C580: 8600 psi (59,290 kPa). 2. Base Coat: Vinyl ester resin and silica fillers. 3. Reinforcement: Fiberglass mat. 4. Protecto-Glass 860 Topcoat: Flake filled. 5. Total Thickness: 0.090 inch (2.3 mm). AB. Basis of Design: Protecto-Glass 865, Trowel Applied, Reinforced Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, fluorides, alkali solutions, salts, oils. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Flexural Strength, ASTM C580: 8600 psi (59,290 kPa). 2. Base Coat: Vinyl ester resin and silica fillers. 3. Reinforcement: Fiberglass mat. 4. Protecto-Glass 865 Topcoat: Graphite filled. 5. Total Thickness: 0.090 inch (2.3 mm). AC. Basis of Design: Protecto-Glass 960, Trowel Applied, Reinforced Novolac, Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, fluorides, alkali solutions, salts, oils, solvents. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Flexural Strength, ASTM C580: 8600 psi (59,290 kPa). ** NOTE TO SPECIFIER ** Delete if not required. e. Protecto-Glass 960 Electrical Properties, ASTM F150 and NFPA 99: 1.5 to 2.0 Megaohms. 2. Base Coat: Novolac vinyl ester resin and silica fillers. 3. Reinforcement: Fiberglass mat. 4. Protecto-Glass 960 Topcoat: Flake filled. 5. Total Thickness: 0.090 inch (2.3 mm). AD. Basis of Design: Protecto-Glass 965, Trowel Applied, Reinforced Novolac, Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Organic acids, inorganic acids, fluorides, alkali solutions, salts, oils, solvents. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Flexural Strength, ASTM C580: 8600 psi (59,290 kPa). ** NOTE TO SPECIFIER ** Delete if not required. e. Protecto-Glass 965 Electrical Properties, ASTM F150 and NFPA 99: 1.5 to 2.0 Megaohms. 2. Base Coat: Novolac vinyl ester resin and silica fillers. 3. Reinforcement: Fiberglass mat. 4. Protecto-Glass 965 Topcoat: Graphite filled. 5. Total Thickness: 0.090 inch (2.3 mm). AE. Basis of Design: Protecto-Line 100XT, Trowel Applied, 100 Percent Solids, Reinforced, Novolac Epoxy Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Concentrated inorganic acids, dilute organic acids, alkali solutions, salts, oils, solvents. b. Compressive Strength, ASTM C579: 14,000 psi (96,530 kPa). c. Tensile Strength, ASTM C307: 2700 psi (18,620 kPa). d. Flame Spread, ASTM D635: 0.39 inches (10 mm). e. Taber Abrasion, ASTM D4060: 0.00071 ounces (20 mg). 2. Base Coat: Filled with graded silica. 3. Reinforcement: Fiberglass or synthetic fabric. 4. Protecto-Line 100XT Topcoat: Silica filled. 5. Total Thickness: 0.125 inch (3.17 mm). AF. Basis of Design: Protecto-Line 100XT AR, Trowel Applied, 100 Percent Solids, Reinforced, Novolac Epoxy Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Concentrated inorganic acids, dilute organic acids, alkali solutions, salts, oils, solvents. b. Compressive Strength, ASTM C579: 14,000 psi (96,530 kPa). c. Tensile Strength, ASTM C307: 2700 psi (18,620 kPa). d. Flame Spread, ASTM D635: 0.39 inches (10 mm). e. Taber Abrasion, ASTM D4060: 0.00071 ounces (20 mg). 2. Base Coat: Filled with graded silica. 3. Reinforcement: Fiberglass or synthetic fabric. 4. Protecto-Line 100XT AR Topcoat: Aluminum oxide filled. 5. Total Thickness: 0.125 inch (3.17 mm). AG. Basis of Design: Protecto-Line 800, Trowel Reinforced, Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Concentrated inorganic acids, dilute organic acids, alkali solutions, salts, oils, solvents. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Flexural Strength, ASTM C580: 8600 psi (59,290 kPa). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. f. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). g. Taber Abrasion, ASTM D4060: 0.0014 ounces (40 mg). ** NOTE TO SPECIFIER ** Delete if not required. h. Protecto-Line 805 Electrical Properties, ASTM F150 and NFPA 99: 0 to 200,000 Ohms. ** NOTE TO SPECIFIER ** Delete base coat option not required. 2. Protecto-Line 800 Base Coat: Silica filled. 3. Protecto-Line 805 Base Coat: Carbon filled. 4. Protecto-Line 800 Reinforcement: Fiberglass roving. 5. Protecto-Line 800 Topcoat: Silica filled. 6. Total Thickness: 0.125 inch (3.17 mm). AH. Basis of Design: Protecto-Line 800 AR, Trowel Reinforced, Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Concentrated inorganic acids, dilute organic acids, alkali solutions, salts, oils, solvents. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Flexural Strength, ASTM C580: 8600 psi (59,290 kPa). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. f. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). g. Taber Abrasion, ASTM D4060: 0.0014 ounces (40 mg). ** NOTE TO SPECIFIER ** Delete if not required. h. Protecto-Line 805 Electrical Properties, ASTM F150 and NFPA 99: 0 to 200,000 Ohms. ** NOTE TO SPECIFIER ** Delete base coat option not required. 2. Protecto-Line 800AR Base Coat: Silica filled. 3. Protecto-Line 805 Base Coat: Carbon filled. 4. Protecto-Line 800AR Reinforcement: Fiberglass roving. 5. Protecto-Line 800AR Topcoat: Aluminum oxide filled. 6. Total Thickness: 0.125 inch (3.17 mm). AI. Basis of Design: Protecto-Line 900, Trowel Reinforced, Novolac Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, organic acids, dilute alkali solutions, fluorides, salts, oils, solvents. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. e. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). f. Taber Abrasion, ASTM D4060: 0.0014 ounces (40 mg). ** NOTE TO SPECIFIER ** Delete if not required. g. Protecto-Line 905 Electrical Properties, ASTM F150 and NFPA 99: 0 to 200,000 Ohms. ** NOTE TO SPECIFIER ** Delete base coat option not required. 2. Protecto-Line 900 Base Coat: Silica filled. a. Protecto-Line 900 Reinforcement: Fiberglass roving. 3. Protecto-Line 905 Base Coat: Carbon filled. a. Protecto-Line 905 Reinforcement: Synthetic fabric. 4. Protecto-Line 900 Top coat: Silica filled. 5. Total Thickness: 0.125 inch (3.17 mm). AJ. Basis of Design: Protecto-Line 900 AR, Trowel Reinforced, Novolac Vinyl Ester Lining and Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, organic acids, dilute alkali solutions, fluorides, salts, oils, solvents. b. Compressive Strength, ASTM C579: 12,500 psi (86,180 kPa). c. Tensile Strength, ASTM C307: 2400 psi (16,550 kPa). d. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. e. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). f. Taber Abrasion, ASTM D4060: 0.0014 ounces (40 mg). ** NOTE TO SPECIFIER ** Delete if not required. g. Protecto-Line 905 Electrical Properties, ASTM F150 and NFPA 99: 0 to 200,000 Ohms. ** NOTE TO SPECIFIER ** Delete base coat option not required. 2. Protecto-Line 900AR Base Coat: Silica filled. a. Protecto-Line 900AR Reinforcement: Fiberglass roving. 3. Protecto-Line 905 Base Coat: Carbon filled. a. Protecto-Line 905 Reinforcement: Synthetic fabric. 4. Protecto-Line 900AR Topcoat: Aluminum oxide filled. 5. Total Thickness: 0.125 inch (3.17 mm). AK. Basis of Design: Shock-Crete HD, Cementitious urethane flooring mortar as manufactured by Dudick Inc. Liquid nitrogen resistant for splash and spill, trowel applied cementitious urethane mortar. Contains antimicrobial additives that protect it from degradation caused by microorganisms. Demonstrates excellent resistance to thermal shock, mechanical damage, and chemical attack. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, organic acids, alkali solutions, salts, oils, aliphatic solvents. b. Dry Temperature Resistance: -350 to 400 degrees F (-212 to 204 degrees C). c. Coefficient of Thermal Expansion, ASTM C531: 1.1 x 10-5. d. Compressive Strength, ASTM C579: 7,300 psi (50 MPa). e. Density: 130 lbs/cu ft (2082.4 kg/cu meter). f. Flexural Strength, ASTM C580: 1,800 psi (12.4 MPa). g. Modulus of Elasticity, ASTM C580: 1.7 x 105 psi. h. Taber Abrasion, ASTM D4060: 70 mg. i. Tensile Bond Strength, ASTM C7234: Cohesive Failure of Concrete. j. Tensile Strength, ASTM C307: 825 psi (5.7 MPa). 2. Thickness: 1/4 to 1/2 inches (6 to 13 mm). 3. Topcoat: Shock-Crete Topcoat. 4. Topcoat: Shock-Crete TCUV. 5. Topcoat: Sealer 985. 6. Topcoat: Sealer 985 HB. 7. Topcoat: As recommended by a Dudick representative. AL. Basis of Design: Shock-Crete HF, Cementitious urethane flooring mortar as manufactured by Dudick Inc. Moisture move through material at a safe rate.Contains Polygiene with antimicrobial properties. Protection from thermal shock, mechanical damage, and chemical attack. Typically a single coat solution or used for sloping and patching in conjunction with Shock-Crete SR or SL2. 1. Performance Requirements: a. Dry Temperature Resistance: 1) Continuous: 220 degrees F (104 degrees C) 2) Non-Continuous: 250 degrees F (121 degrees C). b. Abrasion Resistance, ASTM D4060, CS 17 Wheel, 1000 cycles: 50 mg loss c. Adhesion, ASTM D4541: 400 PSI (2.8 MPa). 100 percent concrete failure d. Friction Coefficient, ASTM D2047: Exceeds ADA recommendations. e. Thermal Expansion Coefficient, ASTM C531: 1.1 x10-5 inches/inch/ degree F f. Compressive Strength, ASTM C 579: 8,000 psi (55 MPa) g. Flexural Strength, ASTM C 580: 2,900 psi (20 MPa) h. Tensile Strength, ASTM C307: 1,450 psi (10 MPa) 2. Thickness: 1/4 to 38 inches (6 to 13 mm). AM. Basis of Design: Shock-Crete IF, Iron filled cementitious urethane mortar as manufactured by Dudick Inc. Exceptionally heavy duty and trowel applied. Contains Polygiene, an antimicrobial. Excellent zresistance to mechanical damage, heavy machinery, thermal shock, and chemical attack. 1. Performance Requirements: a. Dry Temperature Resistance: 1) Continuous: 220 degrees F (104 degrees C) 2) Non-Continuous: 250 degrees F (121 degrees C). b. Abrasion Resistance, ASTM D4060, CS 17 Wheel, 1000 cycles: 50 mg loss c. Adhesion, ASTM D4541: 400 PSI (2.8 MPa). 100 percent concrete failure d. Friction Coefficient, ASTM D2047: Exceeds ADA recommendations. e. Thermal Expansion Coefficient, ASTM C531: 1.1 x10-5 inches/inch/ degree F f. Compressive Strength, ASTM C 579: 8,000 psi (55 MPa) g. Flexural Strength, ASTM C 580: 2,900 psi (20 MPa) h. Tensile Strength, ASTM C307: 1,450 psi (10 MPa) 2. Thickness: 3/8 to 1/2 inch (10 to 13 mm). AN. Basis of Design: Shock-Crete MD, Cementitious urethane flooring mortar as manufactured by Dudick Inc. An aggregate filled system. Develops a cure strength 2 times that of the concrete base to which it is applied. Exhibits physical and mechanical strength and chemical resistance. 1. Performance Requirements: a. Dry Temperature Resistance: -120 to 200 degrees F (-84 to 93 degrees C), b. Thermal Expansion Coefficient, ASTM C531: 1.7x10-5 inches / inch / degree F, c. Compressive Strength, ASTM C 579: 8,000 psi (55 MPa), d. Density: 127 lbs/cu ft (2034 kg/cu m). e. Flexural Strength, ASTM C 580: 2,200 psi (15 MPa). f. Modulus of Elasticity, ASTM C580: 2.2 x 10^8 psi. g. Taber Abrasion, ASTM D4060: 70 mg. h. Tensile Bond Strength ASTM D7234: Cohesive Failure of Concrete. i. Tensile Strength, ASTM C307: 1,000 psi (6.9 MPa). 2. Thickness: 3/16 to 3/8 inch (5 to 10 mm). 3. Topcoats: Depends on exposure. Contact Manufacturer for recommendations. AO. Basis of Design: Shock-Crete SL2, Semi-Self Leveling or Seeded, Water Dispersed Polyurethane Floor Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, organic acids, alkali solutions, salts, oils, aliphatic solvents. b. Compressive Strength, ASTM C579A: 6800 psi (46,880 kPa). c. Tensile Strength, ASTM C307: 1050 psi (7239 kPa). d. Flexural Strength, ASTM C580: 2600 psi (17,930 kPa). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. ** NOTE TO SPECIFIER ** Delete coating option not required. 2. Shock-Crete SL Coating: Urethane. 3. Shock-Crete SF Coating: Seeded urethane. 4. Thickness: 1/16 to 3/16 inch (1.6 to 4.8 mm). AP. Basis of Design: Shock-Crete SR, Semi-self-leveling cementitious urethane floor coating as manufactured by Dudick Inc. 1. Allows moisture to move through the material at a safe rate. contains Polygiene, an antimicrobial. Provides protection from thermal shock, mechanical damage, and chemical attack. Typically broadcast with sand as part of a robust anti-skid flooring system. 2. Performance Requirements: a. Dry Temperature Resistance: 1) Continuous: 200 degrees F (93 degrees C) 2) Non-Continuous: 250 degrees F (121 degrees C). b. Abrasion Resistance, ASTM D4060, CS 17 Wheel, 1000 cycles: 50 mg loss c. Adhesion, ASTM D4541: 400 PSI (2.8 MPa). 100 percent concrete failure d. Friction Coefficient, ASTM D2047: Exceeds ADA recommendations. e. Thermal Expansion Coefficient, ASTM C531: 1.5 x10-5 inches/inch/ degree F f. Compressive Strength, ASTM C 579: 8,128 psi (206 MPa) g. Flexural Strength, ASTM C 580: 2,900 psi (20 MPa) h. Impact Resistance: No visible damage or deterioration at minimum 160 in-lb. i. Modulus of Elasticity, ASTM C469: 1.7 x 10^5. j. Tensile Strength, ASTM C307: 1,450 psi (10 MPa). k. Water Absorption: Less than 0.1 percent. 3. Thickness: 3/16 to 1/4 inch (5 to 6 mm). 4. Topcoat: Shock-Crete Topcoat. 5. Topcoat: Shock-Crete TCUV. 6. Topcoat: Sealer 985. 7. Topcoat: Sealer 985 HB. 8. Topcoat: Sealer 30. 9. Topcoat: As recommended by Dudick. AQ. Basis of Design: Shock-Crete Topcoat, polyurethane high performance cementitious urethane floor sealer as manufactured by Dudick Inc. Excellent primer for cementitious urethane systems due to outstanding resistance to moisture vapor transmission. Contains Polygiene, an antimicrobial. 1. Performance Requirements: a. Abrasion Resistance, ASTM D4060, CS 17 Wheel, 1000 cycles: 50 mg loss. b. Adhesion, ASTM D4541: 400 PSI (2.8 MPa). 100 percent concrete failure. c. Friction Coefficient, ASTM D2047: Exceeds ADA recommendations. d. Thermal Expansion Coefficient, ASTM C531: 2.2 x10-5 inches/inch/ degree F. e. Compressive Strength, ASTM C 579: Greater than 7,250 psi (50 MPa). f. Flexural Strength, ASTM C 580: 2,900 psi (20 MPa). g. Impact Resistance: No visible damage or deterioration at minimum 160 in-lb. h. Modulus of Elasticity, ASTM C469: 1.7 x 10^5. i. Tensile Strength, ASTM C307: 1,740 psi (12 MPa). j. Water Absorption: Less than 0.1 percent. 2. Thickness: 20 to 30 mils (0.50 to 0.75 mm). AR. Basis of Design: Shock-Crete TCUV, high performance cementitious urethane floor sealer as manufactured by Dudick Inc. A high performance, UV stable, semi-gloss topcoat for cementitious urethane floor systems. Contains Polygiene an antimicrobial. 1. Performance Requirements: a. Compressive Strength, ASTM C 579: Greater than 7,000 psi (48.26 MPa). b. Flexural Strength, ASTM C 580: 1200 psi (8.27 MPa). c. Tensile Strength, ASTM C307: 1500 psi (10.34 MPa). d. Static or Dynamic Coefficient of Friction: System can be built to meet or exceed testing requirements for ANSI B101.1 of greater than 0.6 and dynamic coefficient of friction (DCOF). Wet ANSI A326.3 of greater than 0.42. 2. Thickness: 12 mils (300 mm). AS. Basis of Design: Shock-Crete Vertical, cementitious urethane cove base mortar as manufactured by Dudick Inc. Provides a durable finish for use with Shock-Crete flooring systems. Contains Polygiene, an antimicrobial Demonstrates excellent resistance to thermal shock, mechanical damage, and chemical attack. 1. Performance Requirements: a. Dry Temperature Resistance: 1) Continuous: 220 degrees F (104 degrees C) 2) Non-Continuous: 250 degrees F (121 degrees C). b. Abrasion Resistance, ASTM D4060, CS 17 Wheel, 1000 cycles: 0.079 g loss. c. Adhesion, ASTM D4541: 400 PSI (2.8 MPa). 100 percent concrete failure. d. Bond Strength, ASTM D4541: Greater than 300 psi (2 MPa). e. Coefficient of Friction, ASTM D2047: Exceeds ADA Recommendations. f. Coefficient of Thermal Expansion, ASTM C531: 1.1 x 10-5 inches/inch/degree F g. Compressive Strength, ASTM C579: 8,000 psi (55 MPa). h. Flexural Strength, ASTM C580: 2,900 psi (20 MPa). i. Microbial / Fungal Inhibition: AATCC 147-193: 100 percent. j. Tensile Strength, ASTM C307: 1,450 psi (10 MPa). 2. Thickness: 1/8 to 3/16 inches (3 to 5 mm). 3. Topcoat: Shock-Crete Topcoat 4. Topcoat: Shock-Crete TCUV 5. Topcoat: As recommended by Dudick Representative AT. Primer and Sealer: ** NOTE TO SPECIFIER ** Delete primer options not required. 1. Primer: As indicated on Drawings. 2. Primer: _____. ** NOTE TO SPECIFIER ** Confirm if sealer is required. Delete sealer options not required. 3. Sealer: As indicated on Drawings. 4. Sealer: _____. 5. Color: To be selected by Architect. ** NOTE TO SPECIFIER ** Delete Article if not required. 2.3 ARCHITECTURAL SOLID COATINGS ** NOTE TO SPECIFIER ** Delete basis of design options not required. A. Basis of Design: Steri-Flor GP, Semi Self-Leveling or Seeded High Solids General Purpose Epoxy Topping; as manufactured by Dudick Inc. 1. Performance Requirements: a. Recycled Content: 15 percent. b. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, mineral oils, salt solutions, cleaning and sanitizing solutions. c. Low odor and low-VOC. d. Compressive Strength, ASTM C579: 12,000 psi (82,740 kPa). e. Tensile Strength, ASTM D638: 7200 psi (49,640 kPa). f. Flexural Strength, ASTM C580: 11,500 psi (79,290 kPa). g. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. h. Taber Abrasion, ASTM D4060: 0.0011 ounces (32 mg). 2. Thickness: 0.010 to 0.015 inch (0.25 to 0.38 mm). B. Basis of Design: Steri-Flor T, Hybrid Epoxy, Heavy Duty Industrial Floor System; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compliance: USDA compliant. b. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, mineral oils, salt solutions, aliphatic organic solvents. c. Low odor and low-VOC. d. Compressive Strength, ASTM C579: Minimum 7000 psi (48,260 kPa). e. Tensile Strength, ASTM C307: Minimum 1800 psi (12,410 kPa). f. Flexural Strength, ASTM C580: Minimum 2500 psi (17,240 kPa). g. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. h. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Body Coat: Resin. 3. Topcoat: UV and chemical resistant with stippled texture. 4. Total Thickness: 3/16 to 1/4 inch (4.8 to 6.4 mm). C. Basis of Design: Steri-Flor UV, 100 percent Solids, Self-Leveling Epoxy Floor Topping; as manufactured by Dudick Inc. Increased UV stability. Good resistance to common chemicals and daily traffic. Used as a base/color coat, receiving coat, or grout coat for decorative broadcast floors. 1. Color: Clear, unless pigmented. 2. Performance Requirements: a. Compliance: USDA compliant. b. Chemical Resistance: Dilute inorganic acids, dilute alkali solutions, mineral oils, salt solutions, cleaning and sanitizing solutions. c. Low odor and low-VOC. VOC: 90 g per l. 3. Thickness: 0.008 to 0.020 inch (0.20 to 0.51 mm) dry film thickness. 4. Finish: Gloss. D. Basis of Design: Steri-Coat P, Multi-Functional, Pigmented, High-Build Epoxy Novolac Coating, for Wall and Ceiling Applications; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, aliphatic hydrocarbons, sodium hydroxide, salt and brine solutions, mineral oils. b. Low odor and low-VOC. c. Taber Abrasion, ASTM D4060: 0.0032 ounces (92 mg). d. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Thickness: 0.012 to 0.016 inch (0.30 to 0.41 mm). E. Basis of Design: Steri-Coat 200, Two Component, Water Borne, Alipathic Urethane Wall Coating, Class A Fire Rating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Low odor and low-VOC. b. Tensile Strength, ASTM D638: 8500 psi (58,610 kPa). c. Flame Spread Index, ASTM E84: 5. d. Smoke Developed Index, ASTM E84: 5. 2. Thickness: 0.006 to 0.008 inch (0.15 to 0.20 mm). F. Basis of Design: Steri-Glass, High Solids, Fiberglass Reinforced, High Build Epoxy Wall System; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, aliphatic hydrocarbons, sodium hydroxide, salt and brine solutions, mineral oils. b. Low odor and low-VOC. c. Taber Abrasion, ASTM D4060: 0.0032 ounces (92 mg). d. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Body Coat: Fiberglass reinforced hybrid binder. 3. Thickness: 0.025 to 0.035 inch (0.64 to 0.89 mm). G. Basis of Design: Steri-Seal HB, High Solids, Multi-Functional, Spray Applied, Pigmented, High Build, Chemically Resistant Epoxy Coating, for Ceiling and Wall Applications; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, aliphatic hydrocarbons, sodium hydroxide, salt and brine solutions, mineral oils. b. Low odor and low-VOC. c. Taber Abrasion, ASTM D4060: 0.0021 ounces (60 mg). d. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Thickness: 0.030 to 0.040 inch (0.76 to 1.0 mm). H. Basis of Design: Steri-Seal HC, Multi-Functional, Pigmented, High Chemically Resistant Epoxy Coating, for Floor Applications; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Dilute inorganic acids, aliphatic hydrocarbons, sodium hydroxide, salt and brine solutions, mineral oils. b. Low odor and low-VOC. c. Taber Abrasion, ASTM D4060: 0.0042 ounces (120 mg). d. Tensile Strength, ASTM D638: 2870 psi (19,790 kPa). e. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). f. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Thickness: 0.010 to 0.020 inch (0.25 to 0.51 mm). I. Basis of Design: Sealer 30, High Solids, Two Component, Aliphatic, Polyurethane Sealer; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Water, solvents, sodium hydroxide, dilute organic acids, dilute inorganic acids, oils, gasoline, jet fuel. b. Low VOC. c. Pencil Hardness: 2H. 2. Thickness: 0.004 to 0.005 inch (0.10 to 0.13 mm). J. Basis of Design: Sealer 30 SD, Two Component, Aliphatic, Electrostatic Dissipative, Polyurethane Sealer; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Water, solvents, sulfuric acid, sodium hydroxide, oils, gasoline, jet fuel, skydrol. b. Low VOC. c. Pencil Hardness: 2H. d. Surface Resistivity: 1,000,000 to 1,000,000,000 ohms. K. Basis of Design: Sealer 35. High solids, multi-component hard-wearing, aliphatic polyurethane sealer. Color stable, UV resistant, Toughness, impact and stain resistance are inherent qualities of this topcoat. 1. Chemical Resistance: N-Methylpyrrolidone(NMP), Betadine, Beer, Brake Fluid, Citric Acid, Iodine, Water, Solvents, Sodium Hydroxide-50 percent, Sulfuric Acid-20 percent, Dilute Organic/Inorganic Acids, Oils, Gasoline, and Jet Fuel. 2. Dry Film Thickness: 3 to 4 mils (76 to 102 microns) DFT. Do not exceed 6 mils wet. 3. Low odor and VOC compliant. 4. Performance Requirements: a. Abrasion, ASTM D-4060, CS-17 Wheel: 20 mg. b. Gloss at 60 degrees F: 85 to 90. c. Pencil Hardness: 2H. 5. Color: Clear. 6. Color: ________. Pigmented with Universal Color Packs. 7. Color: As determined by the Architect. Pigmented with Universal Color Packs. L. Basis of Design: Sealer 50, Two Component, Nano Enhanced, Hybrid Fluoropolymer Sealer with High Stain and Wear Resistance; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Betadine, oils, gasoline, jet fuel, sodium hydroxide, peroxide, bleach solutions, solvents, sulfuric acid, skydrol, hydrogen. b. Outstanding color stability. c. Low VOC. d. Pencil Hardness: 2H. M. Basis of Design: Sealer 50 TSD. Two-component, nano enhanced, static dissipative, hybrid fluoropolymer sealer. A fluoropolymer urethane sealer/topcoat. Color stable, UV and stain resistant. 1. Chemical Resistance: N-Methylpyrrolidone (NMP), Dimethyl Sulfoxide (DMSO), Betadine, Oils, Gasoline, Jet Fuel, Sodium Hydroxide: 50 percent, Bleach Solutions, Solvents, Sulfuric Acid: 50 percent, Skydrol, and Hydrogen Peroxide. 2. Meets California Department of Public Health CDPH/EHLB Standard Method Version 1.2 2017; compliance certificates available upon request. 3. Meets SCAQMD Rule 1113 for VOC content. 4. Performance Requirements: a. VOC: Volatile Organic Content. 1) As Supplied: Less than 50 grams per liter. b. Solids by Volume: 45 percent. c. Finish: Satin. d. ASTM D7234: Greater than 350 psi; substrate failure. e. Impact Resistance (Direct), ASTM D2794: 160 inch-lbs. f. Impact Resistance (Indirect), ASTM D2794: 160 inch-lbs. 5. Dry Film Thickness: 2 to 4 mils (51 to 102 microns) DFT. 6. Color: Translucent clear. N. Basis of Design: Sealer 80, Two Component, Engineered Hybrid Sealer; as manufactured by Dudick Inc. An isocyanate free, ultra-durable, fast-cure coating. Combines the chemical resistant properties of epoxies with the weathering characteristics of acrylic-polyurethanes giving it a tightly cross-linked film resulting in a finish with barrier properties against Vaporized Hydrogen Peroxide. volatile organic content. 1. Performance Requirements: a. VOC: Volatile Organic Content. 1) As Supplied: 1.8 lbs/gal (216 g/L) mixed. 2) Thinner 10: 13 oz/gal: 2.29 lbs/gal (275 g/L). b. Solids Volume: 75 percent. +/- 2 percent. c. Finish: Gloss. d. Abrasion resistant. e. Resists dirt pickup, and easily cleaned. f. Isocyanate free. g. Fast cure. h. Meets IEEE ANSI C57.12.29-2005 Standard For Pad Mounted Equipment. i. Dry Temperature Resistance: 1) Continuous: 302 degrees F (150 degrees C). 2) Non-Continuous: 338 degrees F (170 degrees C). 2. Thickness: 0.003 to 0.007 inch (0.08 to 0.18 mm). O. Basis of Design: Sealer 200 SD, Two Component, Water Borne, Aliphatic Urethane, Floor Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Low odor and low VOC. b. Tensile Strength, ASTM D638: 8500 psi (58,610 kPa). c. Tear Strength, ASTM D624: 450 psi (3100 kPa). d. Surface Resistivity: 1,000,000 to 1,000,000,000 ohms. 2. Thickness: 0.006 to 0.008 inch (0.15 to 0.20 mm). P. Basis of Design: Sealer 200 WB, Two Component, Water Borne, Aliphatic Urethane, Electrostatic Dissipative Floor Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Low odor and low VOC. b. Tensile Strength, ASTM D638: 8500 psi (58,610 kPa). c. Tear Strength, ASTM D624: 450 psi (3100 kPa). 2. Thickness: 0.005 to 0.006 inch (0.13 to 0.15 mm). Q. Basis of Design: Sealer 985, High-Solids Polyaspartic Floor Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Low odor and low VOC. b. Finish: Gloss. c. Dry Film Thickness: 10 - 15 mils (254 - 381 microns) per coat. d. Solids Volume: 95 percent. +/- 2 percent. e. Tensile Strength, ASTM D412: 3000 psi (20684 kPa). f. Tear Strength, ASTM D624: 450 psi (3100 kPa). R. Basis of Design: Sealer 985 HB, High-Solids, High-Build Polyaspartic Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Low odor and low VOC. b. Finish: Gloss. c. Dry Film Thickness: 10 - 15 mils (254 - 381 microns) per coat. d. Solids Volume: 95 percent. +/- 2 percent. S. Primer and Sealer: ** NOTE TO SPECIFIER ** Delete primer options not required. 1. Primer: As indicated on Drawings. 2. Primer: _____. ** NOTE TO SPECIFIER ** Confirm if sealer is required. Delete sealer options not required. 3. Sealer: As indicated on Drawings. 4. Sealer: _____. 5. Color: To be selected by Architect. ** NOTE TO SPECIFIER ** Delete Article if not required. 2.4 ARCHITECTURAL FLAKE COATINGS ** NOTE TO SPECIFIER ** Delete basis of design options not required. A. Basis of Design: Steri-Flake, General Purpose, Light-Medium Traffic, Decorative Acrylic Flake Filled Floor System; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Salts, dilute inorganic acids, cleansing and sanitizing solutions, alkaline solutions, oils. b. Low odor and low VOC. c. Minimum 15 percent post industrial recycled content. d. Compressive Strength, ASTM C579: Minimum 8000 psi (55,160 kPa). e. Tensile Strength, ASTM C307: Minimum 1500 psi (10,340 kPa). f. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. g. Taber Abrasion, ASTM D4060: 0. 0021 ounces (60 mg). 2. Body Coat: Pigmented mineral filled. 3. Topcoat: UV and chemical resistant. Coats as required to encapsulate acrylic flake. 4. Thickness: 1/16 to 1/8 inch (1.6 to 3.2 mm). B. Primer and Sealer: ** NOTE TO SPECIFIER ** Delete primer options not required. 1. Primer: As indicated on Drawings. 2. Primer: _____. ** NOTE TO SPECIFIER ** Confirm if sealer is required. Delete sealer options not required. 3. Sealer: As indicated on Drawings. 4. Sealer: _____. C. Colors: 1. Color: To be selected by Architect. ** NOTE TO SPECIFIER ** Delete Article if not required. 2.5 ARCHITECTURAL QUARTZ COATINGS ** NOTE TO SPECIFIER ** Delete basis of design options not required. A. Basis of Design: Steri-Quartz, General Purpose, Broadcast, UV Resistant, Light-Medium, Decorative Quartz Floor System; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Salts, dilute inorganic acids, cleaning and sanitizing solutions, alkaline solutions, and oils. b. Low odor and very low VOC. c. Compressive Strength, ASTM C579: 12,000 psi (82,740 kPa). d. Tensile Strength, ASTM C307: 2200 psi (15,170 kPa). e. Flexural Strength, ASTM C580: 3800 psi (26,200 kPa). f. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Body Coat: Quartz broadcast. 3. Grout Coat: UV and chemical resistant. Coats as required to achieve approved texture. 4. Thickness: 1/16 to 3/16 inch (1.6 to 4.8 mm). B. Basis of Design: Steri-Quartz T, Solvent Free, Light-Medium Traffic, Decorative Quartz Floor System; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Salts, dilute inorganic acids, alkaline solutions, oils. b. Low odor and low VOC. c. Compressive Strength, ASTM C579: Minimum 8000 psi (55,160 kPa). d. Tensile Strength, ASTM C307: Minimum 1500 psi (10,340 kPa). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. f. Taber Abrasion, ASTM D4060: 0.0021 ounces (60 mg). g. Flame Spread, ASTM D635: Less than 0.2 inches (5 mm). 2. Body Coat: Quartz broadcast. 3. Grout Coat: UV and chemical resistant, fills porosity in body coat. 4. Thickness: 3/16 to 1/6 inch (4.8 to 6.4 mm). C. Primer and Sealer: ** NOTE TO SPECIFIER ** Delete primer options not required. 1. Primer: As indicated on Drawings. 2. Primer: _____. ** NOTE TO SPECIFIER ** Confirm if sealer is required. Delete sealer options not required. 3. Sealer: As indicated on Drawings. 4. Sealer: _____. D. Color: 1. Color: To be selected by Architect. ** NOTE TO SPECIFIER ** Delete Article if not required. 2.6 OTHER COATINGS ** NOTE TO SPECIFIER ** Delete basis of design options not required. A. Basis of Design: Polymer Concrete 100, Epoxy Polymer Concrete, Dilute Acids Resistance; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compressive Strength, ASTM C579: 16,500 psi (113,800 kPa). b. Tensile Strength, ASTM C307: 5400 psi (37,230 kPa). c. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Description: Three-component epoxy polymer concrete used for construction of chemical resistant floors, pads, curbing, trenches, and sumps. B. Basis of Design: Polymer Concrete 100XT, Novolac Epoxy Strong Sulfuric Resistance; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compressive Strength, ASTM C579: 16,500 psi (113,800 kPa). b. Tensile Strength, ASTM C307: 5400 psi (37,230 kPa). c. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Description: Three-component, novolac epoxy polymer concrete used for construction of chemical resistant floors, pads, curbing, trenches, and sumps. C. Basis of Design: Polymer Concrete 800, Non-Shrink, Vinyl Ester Polymer Concrete; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compressive Strength, ASTM C579: 14,500 psi (99,970 kPa). b. Tensile Strength, ASTM C307: 1800 psi (12,410 kPa). c. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Description: Three-component, vinyl ester polymer concrete used for construction of chemical resistant floors, pads, curbing, trenches, and sumps. D. Basis of Design: Polymer Concrete 900, Non-Shrink, Novolac Vinyl Ester Polymer Concrete, Solvent and Organic Acid Resistance; as manufactured by Dudick Inc. 1. Performance Requirements: a. Compressive Strength, ASTM C579: 14,500 psi (99,970 kPa). b. Tensile Strength, ASTM C307: 1900 psi (13,100 kPa). c. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Description: Three-component, novolac vinyl ester polymer concrete used for construction of chemical resistant floors, pads, curbing, trenches, and sumps. E. Basis of Design: Polymer Steel EG, 100 Percent Solids, Aluminum Oxide-Filled, Fast Setting Epoxy Putty, Highbuild Capabilities; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, some solvents, salts, oils. b. Zero VOC. c. Compressive Strength, ASTM D695: 26,000 psi (179,260 kPa). d. Tensile Adhesion, ASTM D4541: Minimum 1800 psi (12,410 kPa). e. Taber Abrasion, ASTM D4060: 0.00078 ounces (22 mg). 2. Description: 100 percent solids, aluminum oxide filled, polymer steel epoxy putty. 3. Thickness: 1/16 to 1/2 inch (1.6 to 13 mm). 4. Color: Dark Green. F. Basis of Design: Polymer Steel MG, 100 Percent Solids, Metal Filled, Machinable Epoxy Putty; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, some solvents, salts, oils. b. Zero VOC. c. Compressive Strength, ASTM D695: 15,500 psi (106,870 kPa). d. Tensile Adhesion, ASTM D4541: Minimum 1850 psi (12,760 kPa). 2. Description: 100 percent solids, metal filled, polymer steel epoxy putty. 3. Thickness: 1/16 to 1/2 inch (1.6 to 13 mm). ** NOTE TO SPECIFIER ** Delete color option not required. 4. Color: Light Gray. 5. Color: Dark Gray. G. Basis of Design: Polymer Steel RG, 100 Percent Solids, Aluminum Oxide-Filled, Multi-Functional, Epoxy Putty, Highbuild Capabilities; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, some solvents, salts, oils. b. Zero VOC. c. Compressive Strength, ASTM D695: 22,700 psi (156,510 kPa). d. Tensile Adhesion, ASTM D4541: Minimum 1800 psi (12,410 kPa). e. Taber Abrasion, ASTM D4060: 0.00078 ounces (22 mg). 2. Description: 100 percent solids, aluminum oxide filled, polymer steel epoxy putty. 3. Thickness: 1/16 to 1/2 inch (1.6 to 13 mm). 4. Color: Gray. H. Basis of Design: Polymer Steel SG, 100 Percent Solids, Aluminum Oxide-Filled, Multi-Functional, Epoxy Coating; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, some solvents, salts, oils. b. Zero VOC. c. Compressive Strength, ASTM D695: 20,500 psi (141,340 kPa). d. Tensile Adhesion, ASTM D4541: Minimum 1800 psi (12,410 kPa). e. Taber Abrasion, ASTM D4060: 0.00078 ounces (22 mg). 2. Description: 100 percent solids, aluminum oxide filled, polymer steel epoxy coating. Can be used over Polymer Steel RG for a smoother finish. 3. Thickness: 0.020 to 0.040 inch (0.51 to 1.0 mm). ** NOTE TO SPECIFIER ** Delete color option not required. 4. Color: Light Gray. 5. Color: Black. I. Basis of Design: Polymer Carbide, 100 Percent Solids, High Abrasion Resistant, Ceramic Filled, Epoxy Putty; as manufactured by Dudick Inc. 1. Performance Requirements: a. Chemical Resistance: Inorganic acids, alkali solutions, some solvents, salts, oils. b. Low VOC. c. Compressive Strength, ASTM D695: 15,500 psi (106,870 kPa). d. Tensile Adhesion, ASTM D4541: Minimum 1850 psi (12,760 kPa). 2. Description: 100 percent solids, ceramic filled, polymer steel epoxy putty. Can be used over Polymer Steel RG for a smoother finish. 3. Thickness: Approximately 1/4 inch (6.4 mm). ** NOTE TO SPECIFIER ** Delete color option not required. 4. Color: Light Gray. 5. Color: Dark Gray. J. Basis of Design: Vapor-Stop, Semi-Self Leveling, Seeded Moisture Vapor Reduction Coating for Vertical and Horizontal Applications, Low Odor; as manufactured by Dudick Inc. 1. Performance Requirements: a. Low odor and low VOC. b. Compressive Strength, ASTM C579: 6800 psi (46,880 kPa). c. Tensile Strength, ASTM C307: 1050 psi (7240 kPa). d. Flexural Strength, ASTM C580: 2600 psi (17,930 kPa). e. Tensile Bond Strength, ASTM D7234: Cohesive failure of concrete. 2. Description: Polyurethane moisture control system seeded with silica sand. 3. Thickness: Minimum 0.060 inch (1.4 mm). ** NOTE TO SPECIFIER ** Medium Grey color is standard. Delete color options not required. 4. Color: Medium Grey. 5. Color: _____. ** NOTE TO SPECIFIER ** Delete Article if not required. 2.7 ACCESSORIES AND COMPONENTS ** NOTE TO SPECIFIER ** Delete products not required. A. Polymer Concrete: 1. Product: Polymer Concrete 100. A three-component, epoxy used for the construction of chemical resistant floors, pads, curbing, trenches and sumps. a. Tensile Strength per ASTM C307: 5,400 psi (37232 kPa). b. Compressive Strength per ASTM C579: 16,500 psi (113763 kPa). c. Shrinkage: Less than 0.05 percent; varies with amount of filler used. d. Coefficient of Expansion per ASTM C531: 12x10^-6 inches / inch degree F. e. Bond Strength of Concrete per ASTM D7234: Greater than cohesive strength of concrete. 2. Product: Polymer Concrete 100XT. A three-component, novolac epoxy used for the construction of floors, pads, curbing, trenches and sumps. High resistance to strong acids and alkalis. Ideal for heavy traffic and abuse areas. a. Tensile Strength per ASTM C307: 5,400 psi (37232 kPa). b. Compressive Strength per ASTM C579: 16,500 psi (113763 kPa). c. Shrinkage: Less than 0.05 percent; varies with amount of filler used. d. Coefficient of Expansion per ASTM C531: 12x10^-6 inches / inch / degree F. e. Bond Strength of Concrete per ASTM D7234: Greater than cohesive strength of concrete. 3. Product: Polymer Concrete 800. A three-component, vinyl ester epoxy used for the construction of chemical resistant floors, pads, curbing, trenches and sumps. High resistance to strong acids and alkalis. Ideal for heavy traffic and abuse areas. a. Tensile Strength per ASTM C307: 1,800 psi (12411 kPa). b. Compressive Strength per ASTM C579: 14,500 psi (99,974 kPa). c. Shrinkage: Less than 0.05 percent; varies with amount of filler used. d. Coefficient of Expansion per ASTM C531: 13x10^-6 inches / inch / degree F. e. Bond Strength of Concrete per ASTM D7234: Greater than cohesive strength of concrete. 4. Polymer Concrete 900: A three-component, vinyl ester epoxy used for the construction of chemical resistant floors, pads, curbing, trenches and sumps. High resistance to strong acids and alkalis. Ideal for heavy traffic and abuse areas. a. Tensile Strength per ASTM C307: 1,900 psi (13,100 kPA). b. Compressive Strength per ASTM C579: 14,500 psi (99,974 kPa). c. Shrinkage: Less than 0.05 percent; varies with amount of filler used. d. Coefficient of Expansion per ASTM C531: 13x10^-6 inches / inch / degree F. e. Bond Strength of Concrete per ASTM D7234: Greater than cohesive strength of concrete. B. Underlayment: High performance cement base. 1. Product: Carbocrete 4000. A trowel-applied, fast cure and high performance underlayment for sloping and patching floors. Can be overcoated with a variety of finishes including tiles, vinyl and polymer flooring. Protein-free formulation prevents the growth and spread of bacteria. a. Recommended Thickness: 0.25 to 4.0 inches (6.4 to 101.6 mm). 1) Addition of pea gravel is required for thicknesses over 1 inch (25 mm). ** NOTE TO SPECIFIER ** The figures and test results below are typical properties achieved in laboratory tests at 75 degrees F (24 degrees C) and at 50 percent Relative Humidity. b. Bond Strength per ASTM C882: 1) 1 Day: 2,000 psi(13789 kPa). 2) 7 Days: 2,500 psi (17237 kPa). c. Chloride Ion Permeability per ASTM C1202: 1) 3 Days: Less than 500 coulombs. 2) 28 Days: Less than 300 coulombs. d. Compressive Strength per ASTM C109: 1) 3 Hours: 2,500 psi (17237 kPa). 2) 28 Days: 8,000 psi (55,158 kPa). e. Length Change (ASTM C157): 1) 28 Days Wet: +0.03 percent. 2) 28 Days Dry: +0.05 percent. C. Block Filler: Trowel, squeegee or roller applied epoxy material for concrete. D. Sealants: 1. Caulk 100XT: Two-component, fluoroelastomer joint sealant. 2. Caulk 149: 100 percent solids, two-component polysulfide expansion and control joint sealant. 3. Caulk PSC: Elastomeric polysulfide caulk. 4. Caulk PJS: UV Resistant, 100 Percent Solids Polyurea Joint Sealant. a. Durable, two component, heavy duty, semi-rigid polyurea joint sealant designed for filling and protecting control joints and saw cut construction joints in industrial and commercial floors. b. Features: 1) UV resistant. 2) 10-20 minute shave time with a long open shaving window. 3) Cure Temperatures: As low as -20 degrees F (-29 degrees C). 4) Suitable for use in USDA inspected facilities. c. Performance Data: 1) Adhesion to Concrete at 7 days, ASTM D4541: 250 psi. 2) Elongation at Break at 14 days, ASTM D638: 249 percent. 3) Shore A Hardness, ASTM D2240: 84 Shore A. 4) Shore D Hardness, ASTM D2240: 33 Shore D. 5) Tensile Strength at 14 days, ASTM D638: 1,200 psi (8.9 MPa). 6) Viscosity, ASTM D2196: Part A: 2,000 cP. Part B: 1,800 cP. ** NOTE TO SPECIFIER ** Delete color options not required. d. Color: Light Grey (Q700). e. Color: Medium Grey (Q701). f. Color: Black (Q900). g. Color: Red (Q500). h. Color: Black (Q900). i. Color: Beige (Q201). E. Fillers: 1. G-1 Filler: Protecto-Line filler. 2. G-2 Filler: Scratch-Coat 800 filler. F. Concrete Repair Mortar: 1. Product: Steri-Flor Fast Patch. Fast curing epoxy, low temp, concrete repair mortar. Easy application in low temperature environments. 2. Performance Requirements: a. Chemical Resistance: A broad range of acidic and caustic chemicals, including organic and inorganic substances, oils, and salts. b. Temperature Resistance: Continuous Dry Heat: 150 degrees F. Excursions of up to 200 degrees F c. Bond Strength to Concrete ASTM D7234: Greater than cohesive strength of concrete d. Compressive Strength ASTM C579: 10,000 psi. e. Flame Spread ASTM D635: Less than 5 mm. Self Extinguishing. f. Flexural Strength ASTM D4060: 5,000 psi. g. Taber Abrasion ASTM D4060, CS-17 Wheel, 1000 Rev: 60 mg h. Tensile Strength ASTM C307: 2,800 psi i. Water Vapor Transmission ASTM E96: 0.0018 Perms/in. G. Gel-Coat Series: 1. Gel-Coat 800: Provides smooth surface and added protection for chemical contamination over Protecto-Flake 800. 2. Gel-Coat 900: Provides smooth surface and added protection for chemical contamination over Protecto-Flake 900. H. Membranes: 1. Product: Semstone 805.Flexible novolac epoxy coating and lining for steel and concrete. Can also be used as a high build coating and lining system with the addition of a third component. Low odor, two-component system applied as a neat system (unfilled), a reinforced system, an aggregate-filled system or as an aggregate filled reinforced system. It is most often used with reinforcing fabric, No. 100 over expansion joints. a. Self-leveling. b. Highly flexible. c. Chemical resistant. d. Water resistant. e. Abrasion Resistant per ASTM D1044: 120 mg lost (CS17 wheels - 1000 cycle, 1000 gram load). f. Bond Strength over Concrete per ASTM D4541: Greater than 350 psi; Cohesive failure in concrete substrate. g. Hardness per ASTM D2240: 55 Shore A. h. Tensile Elongation ASTM D638: 100 percent. i. Tensile Strength per ASTM D638: 1050 psi. j. Solids: 99 percent +/- 2 percent. k. Color: Gray. l. Finish: N/A. m. VOC: 7 grams per liter; as supplied. n. Primer: Semstone 110. o. Dry Film Thickness: 0.020 to 0.040 mils (0.5 - 1 mm) per coat 2. Product: Semstone 806. Self-leveling, rubberized, low odor, chemically resistant epoxy membrane for concrete. When reinforced with flexible fabrics provides a system for bridging working cracks and expansion joints. When reinforced with Semstone 100 Fabric: Bridge crack expansion joint movement up to 1/2 inch without cracking. May be used as a high build coating system by the addition of a third component. Ideal for use as a secondary containment membrane. a. Flexible. b. Waterproof. c. Abrasion Resistant per ASTM D1044: 26 mg lost (CS17 wheels - 1000 cycle, 1000 gram load). d. Bond Strength per ASTM D4541: Greater than 3500 psi; Cohesive failure in concrete 2 inch overlap joint strength reinforced with fabric. e. Hardness per ASTM D2240: 55. f. Tensile Elongation ASTM D638: 75 percent. 1) Reinforced with Fabric: 60 percent. g. Tensile Strength per ASTM D638: 1500 to 2000 psi. 1) Reinforced with Fabric: 3000 to 3500 psi h. Solids: 99 percent +/- 2 percent. i. Color: Gray. j. VOC: 2 grams per liter; as supplied. k. Primer: Optional. l. Dry Film Thickness: 0.050 to 0.060 mils (1.27 to 1.52 mm) after saturation of fabric No. 100. I. PH-1 Hardener: Polyester and vinyl ester hardener. J. Primers: 1. Primer 27: Vinyl ester primer for steel and concrete, 0.003 to 0.004 inches (0.08 to 0.10 mm) thick. 2. Primer 27C: Conductive vinyl ester primer for concrete, 0.003 to 0.004 inches (0.08 to 0.10 mm) thick. 3. Primer 67: High solids, moisture tolerant epoxy primer for steel and concrete, 0.003 to 0.004 inches (0.08 to 0.10 mm) thick. 4. Primer 67 DP: Deep penetrating, moisture tolerant epoxy primer for dense high compressive strength concrete, 0.002 to 0.003 inches (0.05 to 0.08 mm) thick. 5. Primer 67DP LV: Low VOC, Deep penetrating, moisture tolerant epoxy primer for dense high compressive strength concrete, 0.003 to 0.004 inches (0.08 to 0.10 mm) thick. 6. Primer 67 DTO: 100 percent solids, moisture tolerant epoxy primer for concrete contaminated with vegetable and petroleum oils, 0.004 to 0.006 inches (0.10 to 0.15 mm) thick. 7. Primer 67 C: High solids, moisture tolerant epoxy primer for steel and concrete, 0.003 to 0.004 inches (0.08 to 0.10 mm) thick. 8. Primer 67 LV: Low VOC, high solids, moisture tolerant, epoxy primer for steel and concrete, 0.003 to 0.004 inches (0.08 to 0.10 mm) thick. 9. Primer 67 SD: High solids, static dissipative epoxy primer for concrete. Used as part of static dissipative flooring system, intended to dissipate stray electrical current by running excess current to ground. Increases adhesion and reduces the potential for outgassing on concrete substrates. a. Tolerance to Moisture Vapor Transmission: Less than 5 lbs per 1000 sq ft (24.4 grams per sq m) b. Dry Film Thickness: 3 to 4 mils (76 to 102 microns) per coat. c. Performance Data: 1) Adhesion to Concrete, ASTM D4541: Cohesive Failure of concrete. 2) Electrical, NFPA 99 and ASTM F150: 106 to 109 ohms. 3) Tensile Elongation, ASTM C307: 15 to 25 percent. 4) Tensile Strength, ASTM C307: 2,000 to 2,500 psi (15.2 to 17.2 MPa). d. Color: Black. 10. Steri-Prime: High solids epoxy primer for concrete. Designed to increase adhesion and reduce the potential for outgassing in high performance flooring or containment systems. a. Tolerance to Moisture Vapor Transmission: Less than 5 lbs per 1000 sq ft (24.4 grams per sq m). b. Dry Film Thickness: 3 to 4 mils (76 to 102 microns) per coat. c. Performance Data: 1) Adhesion to Concrete, ASTM D7234: Cohesive Failure of Concrete. 2) Tensile Elongation, ASTM C307: 20 to 25 percent. 3) Tensile Strength, ASTM C307: 2.000 to 2,500 psi (13.8 to 17.2 MPa). d. Color: Clear. 11. Steri-Prime DTO: High solids epoxy primer for concrete that has been exposed to oils, grease, or fats. Increases adhesion and reduces outgassing potential in high performance flooring or containment systems. a. Tolerance to Moisture Vapor Transmission: Less than 5 lbs per 1000 sq ft (24.4 grams per sq m) b. Dry Film Thickness: 4 to 6 mils (102 to 152 microns) per coat. c. Performance Data: 1) Adhesion to Concrete, ASTM D7234: Cohesive Failure of Concrete. 2) Tensile Elongation, ASTM C307: 10 to 15 percent. 3) Tensile Strength, ASTM C307: 1,400 to 2,200 psi. d. Color: Translucent Grey. 12. Steri-Prime WB: Water-Based Epoxy Emulsion Primer. Increases adhesion and reduce the potential for outgassing in high performance flooring systems. a. Dry Film Thickness: 1 to 2 mils (25 to 51 microns) per coat b. Performance Data: 1) Adhesion to Concrete, ASTM D-7234: Cohesive Failure of concrete. c. Color: Clear. K. S-10 Solvent: Cleaning solvent for tools and equipment. L. Scratch-Coat Series: 1. Scratch-Coat 300: Trowel or squeegee applied, epoxy material for concrete. 2. Scratch-Coat 800: Trowel or squeegee applied, vinyl ester material for concrete. M. Steri-Cove Gel: An epoxy system designed for installation as integral cove base, 1/16 to 1/4 inch (1.6 to 6.4 mm) thick. N. Styrene: Smoothing liquid for Protecto-Flake 800 and Protecto-Flake 900. PART 3 EXECUTION 3.1 EXAMINATION A. Do not begin installation until substrates have been properly constructed and prepared. B. If substrate preparation is the responsibility of another installer, notify Architect in writing of unsatisfactory preparation before proceeding. 3.2 PREPARATION A. Clean surfaces thoroughly prior to installation. B. Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions. 3.3 INSTALLATION A. Install in accordance with manufacturer's instructions approved submittals and in proper relationship with adjacent construction. 3.4 FIELD QUALITY CONTROL A. Field Inspection: Coordinate field inspection in accordance with appropriate sections in Division 01. ** NOTE TO SPECIFIER ** Include if manufacturer provides field quality control with onsite personnel for instruction or supervision of product installation, application, erection or construction. Delete if not required. B. Manufacturer's Services: Coordinate manufacturer's services in accordance with appropriate sections in Division 01. 3.5 CLEANING AND PROTECTION A. Clean products in accordance with the manufacturer's recommendations. B. Touch-up, repair or replace damaged products before Substantial Completion. END OF SECTION