SECTION 01 70 00 EXECUTION AND CLOSEOUT REQUIREMENTS Copyright 2015 - 2026 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** This is a generic ARCAT specification, provided in the style and format of all ARCAT manufacturer's specifications. The Notes to Specifier are intended to provide guidance in editing the text. Delete and add text as required for your individual project. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for project. A. Cutting and patching. B. Substantial Completion: The following are prerequisites to substantial completion. Provide the following. 1. Punch list prepared by Contractor and subcontractors as applicable. 2. Supporting documentation. 3. Warranties. 4. Certifications. 5. Occupancy permit. 6. Start-up and testing of building systems. 7. Change over of locks. 8. Meter readings. 9. Commissioning documentation. C. Final Acceptance: Provide the following prerequisites to final acceptance. 1. Final payment request with supporting affidavits. 2. Completed punch list. D. As-Built Drawings: Provide a marked-up set of drawings including changes, which occurred during construction. E. Project Closeout: Provide the following during project closeout. 1. Submission of record documents. 2. Submission of maintenance manuals. 3. Training and turnover to Owner's personnel. 4. Final cleaning and touch-up. 5. Removal of temporary facilities. PART 2 PRODUCTS - Not applicable to this Section PART 3 EXECUTION 3.1 CUTTING AND PATCHING A. Cutting and Patching: Provide cutting and patching work to properly complete the work of the project, complying with project requirements for: 1. Structural work. 2. Mechanical/electrical systems. 3. Visual requirements, including detailing and tolerances. 4. Operational and safety limitations. 5. Fire resistance ratings. 6. Inspection, preparation, and performance. 7. Cleaning. B. Means and Methods: Do not cut and patch in a manner that would result in a failure of the work to perform as intended, decrease energy performance, increase maintenance, decrease operational life, or decrease safety performance. C. Inspection: Inspect conditions prior to work to identify scope and type of work required. Protect adjacent work. Notify Owner of work requiring interruption to building services or Owner's operations. D. Performance of Operations: Perform work with workmen skilled in the trades involved. Prepare sample area of each type of work for approval. E. Cutting: Use cutting tools, not chopping tools. Make neat holes. Minimize damage to adjacent work. Inspect for concealed utilities and structure before cutting. F. Patching: Make patches, seams, and joints durable and inconspicuous. Comply with tolerances for new work. G. Cleaning: Clean work area and areas affected by cutting and patching operations. END OF SECTION