SECTION 07 46 33 VINYL SIDING Copyright 2010 - 2026 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** MITTEN Building Products; windows, doors, patio doors, and siding. This section is based on the products of MITTEN Building Products, which is located at: 5A - 225 Henry St. Brantford, ON, Canada N3S 7R4 Toll Free Tel: 888-648-8364 Email: request info (marketing@mittenbp.com) Web: https://www.mittensiding.com [ https://arcat.com/company/mitten-building-products-50582 ] for additional information. MITTEN Building Products is the original Canadian manufacturer and market leader of vinyl siding. Our continued focus on operational excellence has set the industry benchmark for service, quality, performance and design, backed by the best in class life time warranty. As a coast to coast distributor of premium exterior building products we are the link between architects, builders and installers providing an endless variety of business and design solutions. As part of the Cornerstone Building Brands family, we are the largest manufacturer of exterior building products in North America. Our Canadian made vinyl siding has the largest and boldest colour pallet in the industry and our colour matched aluminum, shake, stone, and accessories provide the perfect complements and finishing touches to any project. Our products maximize curb appeal and benefit installers by minimizing labour requirements. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for project. A. Vinyl Siding including: 1. Horizontal and vertical vinyl siding. (West Ridge) 2. Horizontal vinyl siding. (Sentry) 3. Vertical vinyl board and batten. (Sentry) 4. Horizontal vinyl siding. (Highland) 5. Horizontal vinyl siding. (Oregon Pride) 6. Horizontal color matched single course shakes. 7. Vertical vinyl siding. (Double 5 inch) B. Vinyl Soffits: 1. Beaded. 2. Triple 4 inch. 3. Double 5 inch. 4. Jamb-Fit 8 inch. C. Vinyl skirting. (Pleasant View) D. Accessories and trim. 1.2 RELATED SECTIONS ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required. A. Section 06 10 00 - Rough Carpentry. B. Section 07 27 19 - Plastic Sheet Air Barriers . C. Section 07 90 00 - Joint Protection. 1.3 REFERENCES ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited section. A. ASTM International (ASTM): 1. ASTM C1363 - Standard Test Method for Thermal Performance of Building Materials and Envelope Assemblies by Means of a Hot Box Apparatus. 2. ASTM D1929 - Standard Test Method for Ignition Properties of Plastics. 3. ASTM D2244 - Standard Practice for Calculations of Color Tolerances and Color Differences from Instrumentally Measured Color Coordinates. 4. ASTM D3679 - Standard Specification for Rigid Poly (Vinyl Chloride) (PVC) Siding. 5. ASTM D4216 - Standard Specification for Rigid Poly (Vinyl Chloride) (PVC) Compounds and Related Plastic Building Product Compounds. 6. ASTM E84 - Standard Test Method for Surface Burning Characteristics of Building Materials. 7. ASTM E96 - Standard Test Methods for Water Vapor Transmissions of Materials. 8. ASTM E119 - Standard Test Methods for Fire Tests of Building Construction and Materials. B. Canadian Construction Materials Centre (CCMC): 1. CCMC Acceptance No. 06419L. C. Vinyl Siding Institute (VSI): 1. Certified Installer Program. 2. Installation Manual. 3. Cleaning and Maintenance Guide. 1.4 SUBMITTALS A. Submit under provisions of Section 01 30 00. B. Product Data: Manufacturer's data sheets on each product to be used, including: 1. Preparation instructions and recommendations. 2. Storage and handling requirements and recommendations. 3. Installation methods. C. Shop Drawings: 1. Provide project specific shop drawings including layout, orientation, patterns, extents of installation, and details. 2. Show material layers and thicknesses, flashing, terminations, and penetrations. ** NOTE TO SPECIFIER ** Delete below if colors have already been selected. D. Selection Samples: For each finish product specified, two complete sets of color chips representing manufacturer's full range of available colors and patterns. E. Verification Samples: For each finish product specified, two samples, minimum size 12 inches (300 mm) long, representing actual product, color, and patterns. 1.5 QUALITY ASSURANCE A. Fire Resistance: Provide products that meet or exceed the following ratings: 1. ASTM E84: a. Flame Spread Index: 20. b. Fuel Contribution: 0. c. Smoke Development Rating: 360. 2. ASTM D1929: a. Self-Ignition Temperature: 824 degrees F (440 degrees C). 3. ASTM E119: a. Fire Endurance Classification: 1 hour, as wall assembly. B. Canada Code/Standard Compliance: 1. CAN/CGSB-41.24.95. 2. CCMC Acceptance No. 06419L. C. Manufacturer Qualifications: Minimum 20 years' experience manufacturing similar products. 1. Manufacturer's custom work process will include the following steps: a. Project concept. b. Job evaluation. c. Design and engineering. d. Fabrication and delivery. e. Installation and training. D. Installer Qualifications: Provide installer with not less than 3 years of experience with products specified or has passed the Vinyl Siding Institute's (VSI) Certified Installer Program. ** NOTE TO SPECIFIER ** Include a mock-up if the project size or quality warrant taking such a precaution. The following is one example of how a mock-up on a large project might be specified. When deciding on the extent of the mock-up, consider all the major different types of work on the project. E. Mock-Up: Provide a mock-up for evaluation of surface preparation techniques and application workmanship. 1. Finish areas designated by Architect. 2. Do not proceed with remaining work until workmanship is approved by Architect. 3. Refinish mock-up area as required to produce acceptable work. 1.6 PRE-INSTALLATION MEETINGS A. Convene minimum two weeks prior to starting work of this section. 1.7 DELIVERY, STORAGE, AND HANDLING A. Deliver and store products in manufacturer's unopened packaging bearing the brand name and manufacturer's identification until ready for installation. B. Handling: Handle materials to avoid damage. 1.8 PROJECT CONDITIONS A. Maintain environmental conditions (temperature, humidity, and ventilation) within limits recommended by manufacturer for optimum results. Do not install products under environmental conditions outside manufacturer's recommended limits. 1.9 WARRANTY A. Vinyl Siding: Provide manufacturer's standard, lifetime, non-prorated, transferable warranty that products are free from manufacturing defects, hail damage, and uniform weathering. 1. Color-Rich Coverage: Calculated according to ASTM D2244: a. Premium colors will not change in excess of 3 Hunter units. b. Standard colors will not change in excess of 4 Hunter units. ** NOTE TO SPECIFIER ** Include below for foam backed siding. Delete if not required. 2. Thermal and Permeability Performance: a. Thermal resistance will not vary more than 10 percent from published R-values when tested in accordance with ASTM C1363. b. Permeability will not vary more than 5 perms per inch (25 mm) from published values when tested in accordance with ASTM E96. 3. Warranty Period: Lifetime. PART 2 PRODUCTS 2.1 MANUFACTURERS A. Acceptable Manufacturer: MITTEN Building Products, which is located at: 5A - 225 Henry St.; Brantford, ON, Canada N3S 7R4; ASD Toll Free Tel: 888-648-8364; Email: request info; Web: https://www.mittensiding.com ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions. B. Substitutions: Not permitted. C. Requests for substitutions will be considered in accordance with provisions of Section 01 60 00. 2.2 MATERIALS A. Polyvinyl Chloride: PVC compound with cell classification of 13344B, as defined by ASTM D4216, that meets or exceeds the following properties: 1. Impact Strength: 2.20 ft-lbs per inch (2.98 nM per 25 mm) at test temperature of 73 degrees F. (22.7 degrees C.), and 1.30 ft-lbs per inch (1.76 nM per 25 mm) at test temperature of 32 degrees F (0 degrees C), per ASTM D4226. 2. Tensile Strength: 7,344 psi (50,637 kPa). 3. Flexural Modulus of Elasticity in Tension: 455,750 psi (3,142,396 kPa). 4. Deflection Temperature Under Load of 264 psi (1820 kPa): 168 degrees F (76 degrees C). 5. Coefficient of Expansion: .000034 in/in/degree F. 6. Chemical resistance: Excellent. B. Vinyl Components: Provide products made of extruded polyvinyl chloride as specified in this section and manufactured to comply with requirements of ASTM D3679 including: 1. Provide elongated nailing slots on nailing flanges to allow for movement. 2. Factory-notch ends of horizontal panels to form overlapping joints. 3. Meet weathering requirements of ASTM D3679. ** NOTE TO SPECIFIER ** Delete below if West Ridge horizontal and vertical vinyl siding is not used. 2.3 HORIZONTAL AND VERTICAL VINYL SIDING (WEST RIDGE) A. Vinyl Siding Type ___: West Ridge Siding, Single 8 inch (203 mm). Mounting Profile: Horizontal or vertical. 1. Product Description: Premium product line offering a 0.046 inch (1.17 mm) thick panel and a selection of 1 Black, 4 Rustic, 3 Bold, and 1 Standard, color options. Profile: Features a well-defined wood-grain texture. Stacked Locking System: Connects panels securely to walls. Ridged Foam Backing: Provides added strength to the panel. 2. Piece Dimensions: Length: 12 foot-6 inch (3.81 m). Width: 8 inch (203 mm). 3. Material Thickness: Nominal 0.046 inch (1.17 mm). B. Manufacturer�s Accessories: ** NOTE TO SPECIFIER ** *Accessories available in select colors. Delete accessories not required. 1. J-Channel. 2. Finish Trim. 3. H-Trim. 4. Drip Cap. 5. Inside Corner Post. 6. Apex Outer Corner Post. C. Color: ** NOTE TO SPECIFIER ** Delete colors not required. 1. Black: Black. 2. Rustic: Drift. 3. Rustic: Teak. 4. Rustic: Arctic Grey. 5. Rustic: Farmhouse. 6. Bold: Gunmetal Grey. 7. Bold: Rockaway Grey. 8. Bold: Huron Blue. 9. Standard: Frost. ** NOTE TO SPECIFIER ** Delete below if Sentry horizontal vinyl siding is not used. 2.4 HORIZONTAL VINYL SIDING (SENTRY) ** NOTE TO SPECIFIER ** Delete below if Sentry Double 4 inch (101 mm) horizontal siding is not used. A. Vinyl Siding Type ___: Sentry Siding, Double 4 inch (101 mm) Horizontal Profile. 1. Product Description: Premium product line offering a 0.044 inch (1.12 mm) thick panel and a complete selection of 17 Bold Premium, 14 Natural Standard, and 6 Rustic color options. Profiles feature a cedar-grain texture in a low-gloss finish with a distinctive deep silhouette for rich shadow lines. Board and Batten profile is also available for vertical applications. Contoured lock system connects panels securely to walls. Withstands winds up to 180 miles per hour (80 meters per second). 2. Piece Dimensions: 12 foot-6 inch (3.81 m) piece length, 8 inch (203 mm) piece width. 3. Material Thickness: Nominal 0.044 inch (1.12 mm). ** NOTE TO SPECIFIER ** Delete below if Sentry Double 4.5 inch (114 mm) Dutchlap siding is not used. B. Vinyl Siding Type ___: Sentry Siding, Double 4.5 inch (114 mm) Dutchlap Profile. 1. Product Description: Premium product line offering a 0.044 inch (1.12 mm) thick panel and a complete selection of 17 Bold Premium, 14 Natural Standard, and 6 Rustic color options. Profiles feature a cedar-grain texture in a low-gloss finish with a distinctive deep silhouette for rich shadow lines. Board & Batten profile is also available for vertical applications. Contoured lock system connects panels securely to walls. Withstands winds up to 180 miles per hour (80 meters per second). 2. Piece Dimensions: 12 foot 1 inch (3.68 m) piece length, 9 inch (228 mm) piece width. 3. Material Thickness: Nominal 0.044 inch (1.12 mm). ** NOTE TO SPECIFIER ** Select accessories. Delete accessories not required. C. Provide manufacturer's recommended accessories including: 1. 5/8 inch (17 mm) J-Channel. 2. 5/8 inch (17 mm) J-Channel. Color: Black. 3. 7/8 inch (22 mm) J-Channel. 4. Belt Line. 5. Crown Molding. 6. Drip Cap. 7. Finish Trim. 8. H-Trim. 9. H-Trim. Color: Black. 10. Inside Corner Post. 11. Inside Corner Post. Color: Black. 12. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. 13. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. Color: Black. 14. 3 inch (76 mm) Outside Corner Post, 12 feet (3.65 m) long. 15. 5-1/2 inch (139 mm) Outside Corner Post, 20 feet (6.09 m) long. 16. 5-1/2 inch (139 mm) Fluted Outside Corner Post, 20 feet (6.09 m) long. 17. Recessed Window and Door Trim. 18. 3-1/2 inch (89 mm) Window and Door Trim. 19. Window Casing Trim. 20. Starter Strip. 21. Transition Trim. ** NOTE TO SPECIFIER ** Select color. Delete colors not required. D. Color and Texture: 1. Cedar-Grain texture, color as selected from manufacturer's full range. 2. Cedar-Grain texture, color Yukon Grey. 3. Cedar-Grain texture, color Huron Blue. 4. Cedar-Grain texture, color Drift. 5. Cedar-Grain texture, color Teak. 6. Cedar-Grain texture, color Burnt Sienna. 7. Cedar-Grain texture, color Farmhouse. 8. Cedar-Grain texture, color Hemlock. 9. Cedar-Grain texture, color Arctic Grey. 10. Cedar-Grain texture, color Ash. 11. Cedar-Grain texture, color Regatta Blue. 12. Cedar-Grain texture, color Gunmetal Grey. 13. Cedar-Grain texture, color Eggplant. 14. Cedar-Grain texture, color Annapolis Blue. 15. Cedar-Grain texture, color Aviator Green. 16. Cedar-Grain texture, color Richmond Red. 17. Cedar-Grain texture, color Coffee Bean. 18. Cedar-Grain texture, color Nickel. 19. Cedar-Grain texture, color Khaki Brown. 20. Cedar-Grain texture, color Rockaway. 21. Cedar-Grain texture, color Grenadier Green. 22. Cedar-Grain texture, color Muskoka Green. 23. Cedar-Grain texture, color Indigo. 24. Cedar-Grain texture, color Caribou Brown. 25. Cedar-Grain texture, color Frost. 26. Cedar-Grain texture, color Bone. 27. Cedar-Grain texture, color Cypress. 28. Cedar-Grain texture, color Stratus. 29. Cedar-Grain texture, color Flagstone. 30. Cedar-Grain texture, color Brownstone. 31. Cedar-Grain texture, color Hearthstone. 32. Cedar-Grain texture, color Sandcastle. 33. Cedar-Grain texture, color Saffron. 34. Cedar-Grain texture, color Satin Grey. 35. Cedar-Grain texture, color Sage. 36. Cedar-Grain texture, color Timber bark. 37. Cedar-Grain texture, color Sapphire Blue. 38. Cedar-Grain texture, color Lighthouse Red. ** NOTE TO SPECIFIER ** Delete below if Sentry Board and Batten vertical vinyl siding is not used. 2.5 VERTICAL VINYL BOARD AND BATTEN SIDING (SENTRY) ** NOTE TO SPECIFIER ** Select below for standard colors. Delete not required. A. Vinyl Siding Type ___: Sentry Board and Batten Vertical Siding. 1. Product Description: Board and Batten profile combines wide and narrow vertical panels in a simple, yet beautiful, design well suited to distinctive architectural styles. Available in 14 Natural Standard color options. 2. Piece Dimensions: 10 foot (3.04 m) piece length, 7 inch (117 mm) piece width. 3. Material Thickness: Nominal .045 inch (1.14 mm). ** NOTE TO SPECIFIER ** Select below for rustic and premium colors. Delete not required. B. Vinyl Siding Type ___: Sentry Board and Batten Vertical Siding. 1. Product Description: Board and Batten profile combines wide and narrow vertical panels in a simple, yet beautiful, design well suited to distinctive architectural styles. Available in 1 Black color, 6 Rustic colors, and 17 Bold Premium color options. 2. Piece Dimensions: 10 foot (3.04 m) piece length, 7 inch (117 mm) piece width. 3. Material Thickness: Nominal .050 inch (1.27 mm). 4. Color: Black. ** NOTE TO SPECIFIER ** Select accessories. Delete not required. C. Provide manufacturer�s recommended accessories including: 1. 1/2 inch (12 mm) J-Channel. 2. 5/8 inch (17 mm) J-Channel. 3. 5/8 inch (17 mm) J-Channel. Color: Black. 4. Belt Line. 5. Crown Molding. 6. Drip Cap. 7. Finish Trim. 8. H-Trim. 9. H-Trim. Color: Black. 10. Inside Corner Post. 11. Inside Corner Post. Color: Black. 12. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. 13. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long Color: Black. 14. 3 inch (76 mm) Outside Corner Post, 12 feet (3.65 m) long. 15. 5-1/2 inch (139 mm) Traditional Outside Corner Post, 20 feet (6.09 m) long. 16. 5-1/2 inch (139 mm) Fluted Outside Corner Post, 20 feet (6.09 m) long. 17. Recessed Window and Door Trim. 18. 3-1/2 inch (89 mm) Window and Door Trim. 19. Window Casing Trim. 20. Starter Strip. 21. Transition Trim. ** NOTE TO SPECIFIER ** Select color. Delete colors not required. D. Color and Texture: 1. Cedar-Grain texture, color as selected from manufacturer's full range. 2. Standard: Cedar-Grain texture, color Indigo. 3. Standard: Cedar-Grain texture, color Nickel. 4. Standard: Cedar-Grain texture, color Sage. 5. Standard: Cedar-Grain texture, color Saffron. 6. Standard: Cedar-Grain texture, color Cypress. 7. Standard: Cedar-Grain texture, color Stratus. 8. Standard: Cedar-Grain texture, color Flagstone. 9. Standard: Cedar-Grain texture, color Satin Grey. 10. Standard: Cedar-Grain texture, color Brownstone. 11. Standard: Cedar-Grain texture, color Ash. 12. Standard: Cedar-Grain texture, color Hearthstone. 13. Standard: Cedar-Grain texture, color Sandcastle. 14. Standard: Cedar-Grain texture, color Bone. 15. Standard: Cedar-Grain texture, color Frost. 16. Rustic: Cedar-Grain texture, color Drift. 17. Rustic: Cedar-Grain texture, color Teak. 18. Rustic: Cedar-Grain texture, color Hemlock. 19. Rustic: Cedar-Grain texture, color Arctic Grey. 20. Rustic: Cedar-Grain texture, color Burnt Sienna. 21. Rustic: Cedar-Grain texture, color Farmhouse. 22. Premium: Cedar-Grain texture, color Richmond Red. 23. Premium: Cedar-Grain texture, color Khaki Brown. 24. Premium: Cedar-Grain texture, color Caribou Brown. 25. Premium: Cedar-Grain texture, color Coffee Bean. 26. Premium: Cedar-Grain texture, color Eggplant. 27. Premium: Cedar-Grain texture, color Rockaway Grey. 28. Premium: Cedar-Grain texture, color Aviator Green. 29. Premium: Cedar-Grain texture, color Grenadier Green. 30. Premium: Cedar-Grain texture, color Muskoka Green. 31. Premium: Cedar-Grain texture, color Gunmetal Grey. 32. Premium: Cedar-Grain texture, color Annapolis Blue. 33. Premium: Cedar-Grain texture, color Regatta Blue. 34. Premium: Cedar-Grain texture, color Lighthouse Red. 35. Premium: Cedar-Grain texture, color Timber Bark. 36. Premium: Cedar-Grain texture, color Sapphire Blue. 37. Premium: Cedar-Grain texture, color Huron Blue. 38. Premium: Cedar-Grain texture, color Yukon Grey. ** NOTE TO SPECIFIER ** Delete below if Highland horizontal vinyl siding is not used. 2.6 HORIZONTAL VINYL SIDING (HIGHLAND) ** NOTE TO SPECIFIER ** Delete below if Highland Double 4 inch (101 mm) horizontal siding is not used. A. Vinyl Siding Type ___: Highland Siding, Double 4 inch (101 mm) Horizontal Profile. 1. Product Description: Mitten's most complete product line offering a wide selection of 6 different profiles in 3 bold and 14 natural standard colors. Attractive profiles feature a satin finish wood-grain texture and complement a variety of architectural styles. 2. Piece Dimensions: 12 foot-6 inch (3.81 m) piece length, 8 inch (203 mm) piece width. 3. Material Thickness: Nominal 0.042 inch (1.07 mm). ** NOTE TO SPECIFIER ** Delete below if Highland Double 4.5 inch (101 mm) horizontal siding is not used. B. Vinyl Siding Type ___: Highland Siding, Double 4.5 inch (114 mm) Horizontal Profile. 1. Product Description: Mitten's most complete product line offering a wide selection of 6 different profiles in 3 bold and 13 natural standard colors. Attractive profiles feature a satin finish wood-grain texture and complement a variety of architectural styles. 2. Piece Dimensions: 12 foot-1 inch (3.68 m) piece length, 9 inch (229 mm) piece width. 3. Material Thickness: Nominal 0.042 inch (1.07 mm). ** NOTE TO SPECIFIER ** Delete below if Highland Double 5 inch (127 mm) horizontal siding is not used. C. Vinyl Siding Type ___: Highland Siding, Double 5 inch (127 mm) Horizontal Profile. 1. Product Description: Mitten's most complete product line offering a wide selection of 6 different profiles in 3 bold and 13 natural standard colors. Attractive profiles feature a satin finish wood-grain texture and complement a variety of architectural styles. 2. Piece Dimensions: 14.7 foot (4.5 m) piece length, 4-1/2 inch (114 mm) piece width. 3. Material Thickness: Nominal 0.042 inch (1.07 mm). ** NOTE TO SPECIFIER ** Delete below if Highland Double 4.5 inch (101 mm) dutchlap siding is not used. D. Vinyl Siding Type ___: Highland Siding, Double 4.5 inch (114 mm) Dutchlap Profile. 1. Product Description: Mitten's most complete product line offering a wide selection of 6 different profiles in 3 bold and 14 natural standard colors. Attractive profiles feature a satin finish wood-grain texture and complement a variety of architectural styles. 2. Piece Dimensions: 12 foot-1 inch (3.68 m) piece length, 9 inch (229 mm) piece width. 3. Material Thickness: Nominal 0.042 inch (1.07 mm). ** NOTE TO SPECIFIER ** Delete below if Highland Double 5 inch (127 mm) Dutchlap siding is not used. E. Vinyl Siding Type ___: Highland Siding, Double 5 inch (127 mm) Dutchlap Profile. 1. Product Description: Mitten's most complete product line offering a wide selection of 6 different profiles in 3 bold and 14 natural standard colors. Attractive profiles feature a satin finish wood-grain texture and complement a variety of architectural styles. 2. Piece Dimensions: 12 foot (3.66 m) piece length, 10 inch (254 mm) piece width. 3. Material Thickness: Nominal 0.042 inch (1.07 mm). ** NOTE TO SPECIFIER ** Delete below if Highland Triple 3 inch (76 mm) siding is not used. F. Vinyl Siding Type ___: Highland Siding, Triple 3 inch (76 mm) Dutchlap Profile. 1. Product Description: Mitten's most complete product line offering a wide selection of 6 different profiles in 3 bold and 14 natural standard colors. Attractive profiles feature a satin finish wood-grain texture and complement a variety of architectural styles. 2. Piece Dimensions: 12 foot (3.66 m) piece length, 10 inch (254 mm) piece width. 3. Material Thickness: Nominal 0.040 inch (1.02 mm). ** NOTE TO SPECIFIER ** Select accessories. Delete not required. G. Provide manufacturer's recommended accessories including: 1. Roll-over nail rail. 2. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. 3. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long Color: Black. 4. 3 inch (76 mm) Outside Corner Post, 12 feet (3.65 m) long. 5. 5.5 inch (139 mm) Fluted Outside Corner Post, 20 feet (6.09 m) long. 6. 5.5 inch (139 mm) Traditional Outside Corner Post, 20 feet (6.09 m) long. 7. 3-1/2 inch (89 mm) Window and Door Trim. 8. Recessed Window and Door Trim. 9. Window Casing Trim. 10. 5/8 inch (17 mm) J-Channel. 11. 5/8 inch (17 mm) J-Channel. Color: Black. 12. Belt Line. 13. Crown Molding. 14. Drip Cap. 15. Finish Trim. 16. H-Trim. 17. H-Trim. Color: Black. 18. Inside Corner Post. 19. Inside Corner Post. Color: Black. 20. Starter Strip. 21. Transition Trim. ** NOTE TO SPECIFIER ** Select color. Not all colors are available in all Highland profiles, confirm with the manufacturer. Indigo is not available in the Double 4.5 inch and Double 5 inch Horizontal profiles. Delete colors not required. H. Color and Finish: 1. Satin finish, wood-grain texture, color as selected from manufacturer's full range. 2. Satin finish, wood-grain texture, color Sandcastle. 3. Satin finish, wood-grain texture, color Saffron. 4. Satin finish, wood-grain texture, color Satin Grey. 5. Satin finish, wood-grain texture, color Sage. 6. Satin finish, wood-grain texture, color Nickel. 7. Satin finish, wood-grain texture, color Indigo. 8. Satin finish, wood-grain texture, color Ash. 9. Satin finish, wood-grain texture, color Khaki Brown. 10. Satin finish, wood-grain texture, color Rockaway Grey. 11. Satin finish, wood-grain texture, color Grenadier Green. 12. Satin finish, wood-grain texture, color Frost. 13. Satin finish, wood-grain texture, color Bone. 14. Satin finish, wood-grain texture, color Cypress. 15. Satin finish, wood-grain texture, color Stratus. 16. Satin finish, wood-grain texture, color Flagstone. 17. Satin finish, wood-grain texture, color Brownstone. 18. Satin finish, wood-grain texture, color Hearthstone. ** NOTE TO SPECIFIER ** Delete below if Oregon Pride horizontal vinyl siding is not used. 2.7 HORIZONTAL VINYL SIDING (OREGON PRIDE) ** NOTE TO SPECIFIER ** Delete below if Oregon Pride Double 4 inch (101 mm) horizontal siding is not used. A. Vinyl Siding Type ___: Oregon Pride Siding, Double 4 inch (101 mm) Horizontal Profile. 1. Product Description: Mitten's traditional product line, offering a wide selection of profiles in classic 0.040 inch (1.02 mm) thick panels. Profiles feature a subtle wood-grain appearance in 14 colors. 2. Piece Dimensions: 12 foot-6 inch (3.81 m) piece length, 8 inch (203 mm) piece width. 3. Material Thickness: Nominal 0.040 inch (1.02 mm). ** NOTE TO SPECIFIER ** Delete below if Oregon Pride Double 4 inch (101 mm) Dutchlap siding is not used. B. Vinyl Siding Type ___: Oregon Pride Siding, Double 4 inch (101 mm) Dutchlap Horizontal Profile. 1. Product Description: Mitten's traditional product line, offering a wide selection of profiles in classic 0.040 inch (1.02 mm) thick panels. Profiles feature a subtle wood-grain appearance in 8 colors. 2. Piece Dimensions: 12 foot-6 inch (3.81 m) piece length, 8 inch (203 mm) piece width. 3. Material Thickness: Nominal 0.040 inch (1.02 mm). ** NOTE TO SPECIFIER ** Delete below if Oregon Pride Double 4-1/2 inch (114 mm) Dutchlap siding is not used. C. Vinyl Siding Type ___: Oregon Pride Siding, Double 4-1/2 inch (114 mm) Dutchlap Profile. 1. Product Description: Mitten's traditional product line, offering a wide selection of profiles in classic 0.040 inch (1.02 mm) thick panels. Profiles feature a subtle wood-grain appearance in 14 colors. 2. Piece Dimensions: 12 foot-1 inch (3.68 m) piece length, 9 inch (228 mm) piece width. 3. Material Thickness: Nominal 0.040 inch (1.02 mm). ** NOTE TO SPECIFIER ** Select accessories. Delete not required. D. Provide manufacturer's recommended accessories including: 1. 5/8 inch (17 mm) J-Channel. 2. 5/8 inch (17 mm) J-Channel. Color: Black. 3. Belt Line. 4. Crown Molding. 5. Drip Cap. 6. Finish Trim. 7. H-Trim. 8. H-Trim. Color: Black. 9. Inside Corner Post. 10. Inside Corner Post. Color: Black. 11. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. 12. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. Color: Black. 13. 3 inch (76 mm) Outside Corner Post, 12 feet (3.65 m) long. 14. 5-1/2 inch (139 mm) Traditional Outside Corner Post, 20 feet (6.09 m) long. 15. 5-1/2 inch (139 mm) Fluted Outside Corner Post, 20 feet (6.09 m) long. 16. Recessed Window and Door Trim. 17. 3-1/2 inch (89 mm) Window and Door Trim. 18. Window Casing Trim. 19. Starter Strip. 20. Transition Trim. ** NOTE TO SPECIFIER ** Select color. Not all colors are available in all Oregon Pride profiles, confirm with the manufacturer. The colors Indigo, Ash, Sandcastle, Saffron, Satin Gray, and Sage are not available in the Double 4 inch Dutchlap profile. Delete colors not required. E. Color and Finish: 1. Realistic, wood-grain texture, color as selected from manufacturer's full range. 2. Realistic, wood-grain texture, color Nickel. 3. Realistic, wood-grain texture, color Indigo. 4. Realistic, wood-grain texture, color Ash. 5. Realistic, wood-grain texture, color Frost. 6. Realistic, wood-grain texture, color Bone. 7. Realistic, wood-grain texture, color Cypress. 8. Realistic, wood-grain texture, color Stratus. 9. Realistic, wood-grain texture, color Flagstone. 10. Realistic, wood-grain texture, color Brownstone. 11. Realistic, wood-grain texture, color Hearthstone. 12. Realistic, wood-grain texture, color Sandcastle. 13. Realistic, wood-grain texture, color Saffron. 14. Realistic, wood-grain texture, color Satin Gray. 15. Realistic, wood-grain texture, color Sage. ** NOTE TO SPECIFIER ** Delete below if color matched, single course 8-1/2 inch (216 mm) horizontal shake is not required. 2.8 HORIZONTAL COLOR MATCHED SINGLE COURSE SHAKES A. Polymer Siding Type ___: Single Course 8-1/2 inch (216 mm) Horizontal Profile. 1. Product Description: Replicates appearance of real wood. Engineered to withstand extreme temperatures. Sturdy and lightweight. Color throughout panel. Superior UV Inhibitors. Test results exceed industry standards for fire rating, wind resistance, impact resistance and fading. Traditional seamless finish. Never needs to be painted. Available in 23 colors. 2. Piece Dimensions: 8 foot-1 inch (2.44 m) piece length, 8.45 inch (215 mm) piece width. 3. Material Thickness: Nominal 0.090 inch (2.29 mm). 4. Wind and Impact resistance per ASTM D4226. B. Rough Sawn Shake Corner: 1. Piece Dimensions (HxW): 15.18 x 4.5 inches (386 x 114 mm). 2. Material Thickness: 0.085 inch (2.16 mm). 3. Wind and Impact resistance per ASTM D4226. ** NOTE TO SPECIFIER ** Select accessories. Delete not required. C. Provide manufacturer's recommended accessories including: 1. 7/8 inch (22 mm) J-Channel. 2. Starter Strip. ** NOTE TO SPECIFIER ** Delete colors not required. D. Color and Finish: 1. Cedar-Grain texture, color as selected from manufacturer's full range. 2. Cedar-Grain texture, color Annapolis Blue. 3. Cedar-Grain texture, color Bone. 4. Cedar-Grain texture, color Brownstone. 5. Cedar-Grain texture, color Coffee Bean. 6. Cedar-Grain texture, color Flagstone. 7. Cedar-Grain texture, color Frost. 8. Cedar-Grain texture, color Grenadier Green. 9. Cedar-Grain texture, color Gunmetal Grey. 10. Cedar-Grain texture, color Hearthstone. 11. Cedar-Grain texture, color Huron Blue. 12. Cedar-Grain texture, color Indigo. 13. Cedar-Grain texture, color Khaki Brown. 14. Cedar-Grain texture, color Muskoka Green. 15. Cedar-Grain texture, color Nickel. 16. Cedar-Grain texture, color Regatta Blue. 17. Cedar-Grain texture, color Richmond Red. 18. Cedar-Grain texture, color Rockaway Grey. 19. Cedar-Grain texture, color Sage. 20. Cedar-Grain texture, color Sapphire Blue. 21. Cedar-Grain texture, color Satin Grey. 22. Cedar-Grain texture, color Stratus. 23. Cedar-Grain texture, color Timber Bark. 24. Cedar-Grain texture, color Yukon Grey. ** NOTE TO SPECIFIER ** Delete below if Double 5 inch (127 mm) vertical vinyl siding is not used. 2.9 VERTICAL VINYL SIDING (DOUBLE 5 INCH) A. Vinyl Siding Type ___: Double 5 inch (127 mm) Vertical Siding. 1. Product Description: Durable vinyl siding with vertical orientation available in 4 Rustic colors and 5 Natural Standard colors. 2. Piece Dimensions: 12 foot (3.66 m) piece length, 10 inch (254 mm) piece width. 3. Material Thickness: Nominal ____ inch (____ mm). ** NOTE TO SPECIFIER ** Select accessories. Delete not required. B. Provide manufacture'rs recommended accessories including: 1. 1/2 inch (12 mm) J-Channel. 2. 5/8 inch (17 mm) J-Channel. 3. Belt Line. 4. Crown Molding. 5. Drip Cap. 6. Finish Trim. 7. H-Trim. 8. Inside Corner Post. 9. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. 10. 3 inch (76 mm) Outside Corner Post, 12 feet (3.65 m) long. 11. 5-1/2 inch (139 mm) Traditional Outside Corner Post, 20 feet (6.09 m) long. 12. 5-1/2 inch (139 mm) Fluted Outside Corner Post, 20 feet (6.09 m) long. 13. Recessed Window and Door Trim. 14. 3-1/2 inch (89 mm) Window and Door Trim. 15. Window Casing Trim. 16. Starter Strip. 17. Transition Trim. ** NOTE TO SPECIFIER ** Select color. Delete colors not required. C. Color and Finish: 1. Manufacturer's standard finish, color as selected from manufacturer's full range. 2. Manufacturer�s standard finish, color Drift. 3. Manufacturer�s standard finish, color Teak. 4. Manufacturer�s standard finish, color Arctic Grey. 5. Manufacturer's standard finish, color Bone. 6. Manufacturer's standard finish, color Brownstone. 7. Manufacturer�s standard finish, color Burnt Sienna. 8. Manufacturer's standard finish, color Farmhouse. 9. Manufacturer's standard finish, color Frost. 10. Manufacturer's standard finish, color Hearthstone. 11. Manufacturer�s standard finish, color Hemlock. 12. Manufacturer's standard finish, color Stratus. ** NOTE TO SPECIFIER ** Delete below if Beaded Vinyl Soffits are not required. 2.10 VINYL SOFFITS (BEADED) A. Soffit Type ___: 7 inch (178 mm) Beaded Vinyl Soffits. 1. Product Description: Maximizes the net free air intake per foot. Aids in air circulation through attic. Can help prevent early roof failure. Comply with local building code for venting requirements. ** NOTE TO SPECIFIER ** Delete soffit type option not required. 2. Soffit Type: Solid. 3. Soffit Type: Hidden Vent, 8.4 square inch (213 square mm) net free air intake per foot (304 mm). 4. Piece Dimensions: 12 foot (3.658 m) piece length, 7 inch (178 mm) piece width. ** NOTE TO SPECIFIER ** Select accessories. Delete not required. B. Provide manufacturer's recommended accessories including: 1. 1/2 inch (13 mm) F-Channel. 2. 1/2 inch (13 mm) J-Channel. 3. Crown Molding. 4. Fascia. 5. Fascia J. ** NOTE TO SPECIFIER ** Select colors. Delete not required. C. Color and Finish: 1. Manufacturer's standard finish, color as selected from manufacturer's full range. 2. Manufacturer's standard finish, Frost white color. ** NOTE TO SPECIFIER ** Delete below if Triple 4 inch (101 mm) Soffits are not required. 2.11 VINYL SOFFITS (TRIPLE 4 INCH) A. Soffit Type ___: Triple 4 inch (101 mm) Vinyl Soffits. 1. Product Description: Maximizes the net free air intake per foot. Aids in air circulation through attic. Can help prevent early roof failure. Comply with local building code for venting requirements. ** NOTE TO SPECIFIER ** Delete soffit type options not required. 2. Soffit Type: Solid. 3. Soffit Type: Perforated Full Vent, 5.89 square inch (149 square mm) net free air intake per foot (304 mm). 4. Soffit Type: Perforated Center Vent, 1.96 square inch (49 square mm) net free air intake per foot (304 mm). 5. Piece Dimensions: 12 foot-6 inch (3.81 m) piece length, 6 inch (152 mm) piece width. ** NOTE TO SPECIFIER ** Select accessories. Delete not required. B. Provide manufacturer's recommended accessories including: 1. 1/2 inch (13 mm) F-Channel. 2. 1/2 inch (13 mm) J-Channel. 3. Crown Molding. 4. Fascia. 5. Fascia J. ** NOTE TO SPECIFIER ** Select colors. Delete not required. C. Color and Finish: 1. Manufacturer's standard finish, color as selected from manufacturer's full range. 2. Manufacturer's standard finish, Black color. 3. Manufacturer's standard finish, Musket Brown color. 4. Manufacturer's standard finish, Frost color. 5. Manufacturer's standard finish, Bone color. 6. Manufacturer's standard finish, Stratus color. 7. Manufacturer's standard finish, Brownstone color. 8. Manufacturer's standard finish, Hearthstone color. ** NOTE TO SPECIFIER ** Delete below if Double 5 inch (127 mm) Soffits are not required. 2.12 VINYL SOFFITS (DOUBLE 5 INCH) A. Soffit Type ___: Double 5 inch (127 mm) Vinyl Soffits. 1. Product Description: Maximizes the net free air intake per foot. Aids in air circulation through attic. Can help prevent early roof failure. Comply with local building code for venting requirements. ** NOTE TO SPECIFIER ** Select type. Designate Types if both are used. Delete not required. 2. Soffit Type: Solid. 3. Soffit Type: Perforated, 4.2 square inch (106 square mm) net free air intake per foot (304 mm). 4. Piece Dimensions: 12 foot-6 inch (3.81 m) piece length, 6 inch (152 mm) piece width. ** NOTE TO SPECIFIER ** Select accessories. Delete not required. B. Provide manufacturer's recommended accessories including: 1. 1/2 inch (12.7 mm) F-Channel. 2. 1/2 inch (12.7 mm) J-Channel. 3. Crown Molding. 4. Fascia. 5. Fascia J. ** NOTE TO SPECIFIER ** Select colors. Delete not required. C. Color and Finish: 1. Manufacturer's standard finish, color as selected from manufacturer's full range. 2. Manufacturer�s standard finish, Drift color. 3. Manufacturer�s standard finish, Teak color. 4. Manufacturer's standard finish, Burnt Sienna color. 5. Manufacturer's standard finish, Farmhouse color. 6. Manufacturer's standard finish, Hemlock color. 7. Manufacturer's standard finish, Arctic Grey color. 8. Manufacturer's standard finish, Frost color. 9. Manufacturer's standard finish, Bone color. 10. Manufacturer's standard finish, Stratus color. 11. Manufacturer's standard finish, Brownstone color. 12. Manufacturer's standard finish, Hearthstone color. 2.13 JAMB-FIT VINYL SOFFIT A. Soffit Type ___: Jamb-Fit Vinyl Soffits. 1. Product Description: A durable soffit with an easy to install slide lock. Comply with local building code for venting requirements. ** NOTE TO SPECIFIER ** Delete profile option not required. Then delete soffit type and color options not required. The colors Bone and Brownstone are not available for the Solid soffit type. 2. Profile: 4 inch (102 mm), 8 inches (203 mm) wide. 0.04 inches (1.02 mm) thick. a. Piece Length: 12 foot (3.66 m) piece length. b. Soffit Type: Solid. c. Soffit Type: Perforated, 3.1 square inches (2000 square mm) net free air intake per foot (304 mm). d. Color and Finish: 1) Manufacturer's standard finish. Color selected from manufacturer's range. 2) Manufacturer's standard finish, Black color. 3) Manufacturer's standard finish, Bone color. 4) Manufacturer's standard finish, Brownstone color. 5) Manufacturer's standard finish, Frost color. 6) Manufacturer�s standard finish, Stratus color. ** NOTE TO SPECIFIER ** Delete below if vinyl skirting is not required. 2.14 VINYL SKIRTING (PLEASANT VIEW) A. Skirting Type ___: Pleasant View Vinyl Skirting. 1. Product Description: Great alternative to wooden lattice. Easily secures to the perimeter of mobile homes, cottages, decks or foundations. Special front rail design allows access to be maintained. Will not attract termites. 2. Skirting Panel: 12 foot (3.66 m) length, 12 inch (304 mm) width. 3. Bottom Rail: 12 foot (3.66 m) length. 4. Trim Back: 12 foot (3.66 m) length. 5. Trim Front: 12 foot (3.66 m) length. ** NOTE TO SPECIFIER ** Select accessories. Delete not required. B. Provide manufacturer's recommended accessories including: 1. 1/2 inch (13 mm) J-Channel. 2. 3 inch (76 mm) Outside Corner Post, 10 feet (3.04 m) long. C. Color and Finish: 1. Manufacturer's standard finish and color, Frost. 2.15 ACCESSORIES AND TRIM A. Provide manufacturer's inside corners, outside corners, posts, channels, nailers, under sill trim, starter strips, finish trim and other accessories as shown on the drawings and as recommended by the manufacturer for a complete installation. 1. Colors: As indicated on the drawings. 2. Materials: Of the same materials and finish with similar properties as vinyl siding. B. Fasteners: Galvanized steel, stainless steel or other corrosion-resistant fasteners as recommended by the manufacturer. PART 3 EXECUTION 3.1 EXAMINATION A. Do not begin installation until substrates have been properly prepared. B. Confirm critical dimensions and existing structure are within the manufacturer's limits and tolerances. C. If substrate preparation is the responsibility of another installer, notify Architect of unsatisfactory preparation before proceeding. 3.2 PREPARATION A. Clean surfaces thoroughly prior to installation. B. Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions. C. Where required, repair substrate flaws and defects to ensure even installation surfaces, free from obstructions. 3.3 INSTALLATION A. Install in accordance with manufacturer's instructions, the latest edition of the Vinyl Siding Institute (VSI) Installation Manual and details shown on the drawings. B. Install wood shims at building corners to bring cut edges of vertical siding out to correct and even planes. C. Attach panels by placing fastener in the center of slots for horizontal panels, and top slot for vertical panels. Drive fasteners straight leaving 1/16 inch (1.6 mm) space between heads and panel flanges. D. Panels and joints will be plumb and true. Stagger joints in a uniform pattern as successive courses are installed. E. Allow space between both ends of siding panels and trim for thermal movement. Overlap horizontal panel ends one-half the width of factory pre-cut notches. F. Securely attach panel components, accessories and trim using methods recommended by the manufacturer. 3.4 CLEANING A. Remove fingerprints and tool marks, clean soiled areas in accordance with the manufacturer's instructions and the Vinyl Siding Institute (VSI) Cleaning and Maintenance Guide. B. Remove packaging and unused materials from the project site. 3.5 PROTECTION A. Protect installed products until completion of project. B. Touch-up, repair or replace damaged products before Substantial Completion. END OF SECTION