SECTION 07 42 13 METAL WALL PANELS Copyright 2026 - 2026 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** Morin by Kingspan; Architectural Metal Wall Panel Systems. This section is based on the products of Morin by Kingspan, which is located at: 685 Middle St. Bristol, CT 06010-8416 Toll Free Tel: 800-640-9501 Tel: 800-640-9501 Fax: 860-582-7503 Email: request info (sales@morincorp.com) Web: https://www.morincorp.com [ https://arcat.com/company/morin-by-kingspan-34322 ] for additional information. Morin Corporation specializes in the roll-forming of architectural heavy-gauge metals and aluminum panels for single-skin wall and roof systems. With over 100 profiles and four manufacturing facilities, Morin is equipped to handle projects of any size and complexity. The Morin story is about more than panels - we excel at turning bold architectural visions into reality. Our product offerings include perforations, seamless corners, integrated louvers, trimless ends, and custom extrusions, delivering a cohesive and sophisticated look. Our on-site technical team provides expert support with drawings, design insights, cost-saving strategies, and solutions for complex challenges. Additionally, we offer on-site installation guidance from professionals with decades of hands-on experience. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for project. A. Matrix Series metal wall panel system. B. Integrity Series metal wall panel system. C. Pulse Series metal wall panel system. D. Exposed Series metal wall panel system. 1.2 RELATED SECTIONS ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required. A. Section 07 41 13 - Metal Roof Panels. B. Section 07 42 00 - Wall Panels. C. Section 07 42 43 - Composite Wall Panels. D. Section 07 42 93 - Soffit Panels. E. Section 07 62 00 - Sheet Metal Flashing and Trim. 1.3 REFERENCES ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited section. A. ASTM International (ASTM): 1. ASTM A792 - Standard Specification for Steel Sheet, 55 Percent Aluminum-Zinc Alloy-Coated by the Hot-Dip Process. 2. ASTM B209 - Standard Specification for Aluminum and Aluminum-Alloy Sheet and Plate. 3. ASTM E283 - Standard Test Method for Determining Rate of Air Leakage Through Exterior Windows, Skylights, Curtain Walls, and Doors Under Specified Pressure Differences Across the Specimen. 4. ASTM E331 - Standard Test Method for Water Penetration of Exterior Windows, Skylights, Doors, and Curtain Walls by Union Static Air Pressure Difference. 5. ASTM E1592 - Standard Test Method for Structural Performance of Sheet Metal Roof and Siding Systems by Uniform Static Air Pressure Difference. B. American Society of Civil Engineers (ASCE): 1. ASCE 7 - Minimum Design Loads and Associated Criteria for Buildings and Other Structures. C. National Fire Protection Association (NFPA): 1. NFPA 285 - Standard Fire Test Method for Evaluation of Fire Propagation Characteristics of Exterior Non-Load-Bearing Wall Assemblies Containing Combustible Components. 1.4 ACTION SUBMITTALS A. Submit under provisions of Section 01 30 00. B. Product Data: 1. Manufacturer's data sheets and product attributes on each metal panel product to be used. 2. Preparation instructions and recommendations. 3. Storage and handling requirements and recommendations. 4. Typical installation methods. 5. Maintenance instructions. ** NOTE TO SPECIFIER ** Delete if not applicable to product type. C. Verification Samples: Two representative units of each type, size, pattern, and color. D. Shop Drawings: Illustrate products and installation. Include details of materials, construction, and finish. Include relationship with adjacent construction. E. Panel Calculations: Sealed calculations for panel structural integrity by engineer licensed in the State of project's location. F. Environmental Product Declaration: Manufacturers third-party verified EPD, conforming to standard ISO 14025, Type III Environmental Declaration, and Product Category Rule. Registration Number SCS-EPD-09034. 1.5 INFORMATIONAL SUBMITTALS A. Certificate of Compliance: Certification that installed products meet specified design and performance requirements. 1.6 QUALITY ASSURANCE A. Manufacturer Qualifications: Company specializing in manufacturing products specified in this section with a minimum of five (5) years documented experience. B. Installer Qualifications: Company specializing in performing Work of this section with minimum five years documented experience with projects of similar scope and complexity. C. Source Limitations: Provide each type of product from a single manufacturing source to ensure uniformity. ** NOTE TO SPECIFIER ** Include mock-up if the project size or quality warrant the expense. The following is one example of how a mock-up might be specified. When deciding on the extent of the mock-up, consider all the major different types of work on the project. Delete mock-up dimensions and mock-up to remain or not remain as part of the work that are not applicable. D. Mock-Up: Construct a mock-up with actual materials in sufficient time for Architect's review and to not delay construction progress. Locate mock-up as acceptable to Architect and provide temporary foundations and support. ** NOTE TO SPECIFIER ** Delete dimension option not required. 1. Mock-Up Dimensions: 8 x 8 ft (2.44 x 2.44 m). 2. Mock-Up Dimensions: As directed by the Architect. 3. The intent of a mock-up is to demonstrate quality of workmanship and visual appearance. 4. If the mock-up is not acceptable, rebuild the mock-up until satisfactory results are achieved. 5. Retain mock-up during construction as a standard for comparison with completed work. 6. Do not alter or remove mock-up until work is completed or removal is authorized. 7. Approved mock-up may remain as part of the work. 8. Approved mock-up may not remain as part of the work. 1.7 PRE-INSTALLATION CONFERENCE A. Convene a conference approximately two weeks before scheduled commencement of the Work. Attendees must include Architect, Owner, Contractor, Construction Manager, Installer and trades involved. Agenda must include project conditions, manufacturer requirements, delivery and storage, staging and sequencing, schedule, responsibilities, critical path items, approvals and protection of completed work. 1.8 DELIVERY, STORAGE, AND HANDLING A. Store and handle in strict compliance with manufacturer's written instructions and recommendations. B. Protect from damage due to weather, excessive temperature, and construction operations. 1.9 PROJECT CONDITIONS A. Maintain environmental conditions (temperature, humidity, and ventilation) within limits recommended by manufacturer for optimum results. Do not install products under environmental conditions outside manufacturer's recommended limits. ** NOTE TO SPECIFIER ** Delete Installer's 2 year warranty if not applicable. Installer's 2 year warranty is applicable to Pulse, Matrix, and Integrity Series panels. 1.10 WARRANTY A. Manufacturer's two (2) year warranty against defects in materials and workmanship. B. Manufacturer's twenty (20) year warranty against chipping, cracking, fading or delamination of panel finish. C. Installer's two (2) year warranty against leakage through wall system. PART 2 PRODUCTS 2.1 MANUFACTURERS A. Acceptable Manufacturer: Morin by Kingspan, which is located at: 685 Middle St. Bristol, CT 06010-8416 Toll Free Tel: 800-640-9501 Tel: 800-640-9501 Fax: 860-582-7503 Email: request info (sales@morincorp.com);Web: https://www.morincorp.com ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions. B. Substitutions: Not permitted. C. Requests for substitutions will be considered in accordance with the provisions of Section 01 60 00. 2.2 DESIGN REQUIREMENTS A. Design Requirements: 1. Live and dead loads in accordance with Building Code and authorities having jurisdiction. ** NOTE TO SPECIFIER ** Delete deflection and LEED conformance sub-paragraphs if not applicable. 2. Maximum Allowable Deflection: L/180. 3. Movement caused by ambient temperature range of 120 to 180 degrees F (49 to 82 degrees C). 4. LEED v 4.1: Third-Party Verified EPDs conforming to ISO 14025. 2.3 METAL WALL PANELS ** NOTE TO SPECIFIER ** Delete basis of design options not required. A. Basis of Design: Matrix Series Panels, a concealed fastener rainscreen wall panel system as manufactured and supplied by the Morin Corporation. 1. Performance and Design Requirements: a. Standards Compliance: ASTM E283, ASTM E331, and NFPA 285. b. Performance Requirements: ** NOTE TO SPECIFIER ** Delete air leakage option not required. 1) Air Leakage: ASTM E283: Aluminum: Maximum 0.008 cfm (0.00022 cu m per min) of wall area measured at reference differential pressure across assembly of 40 psf (1915 Pa). 2) Air Leakage: ASTM E283: Galvalume: Maximum 0.020 cfm psf (0.00057 cu m per min) of wall area measured at reference differential pressure across assembly of 40 psf (1915 Pa). 3) Water Leakage: ASTM E331: None, at test pressure of 40 psf (1915.21 Pa). 2. Concealed clips and fasteners with side joints allowing mixed profiles. a. Panel Attachment: MIP clip and fastener. ** NOTE TO SPECIFIER ** Delete application options not required. 3. Application: Weather resistant. 4. Application: Rainscreen rear ventilation for horizontal application. 5. Application: Rainscreen rear ventilation for vertical application. 6. Surface Finish: Smooth, Stucco Embossed. 7. Panel Joint: Tongue and groove interlock. ** NOTE TO SPECIFIER ** Delete panel length option not required. Panel lengths are 5 to 30 ft (1.52 to 6.10 m), Custom lengths are available. Consult manufacturer for options and NFPA 285 compliant fire performance assembly requirements. 8. Panel Length: ____ft (___ m). 9. Panel Length: As selected by the Architect. ** NOTE TO SPECIFIER ** Delete panel depth and width option not required. Then delete panel profile options not required. 10. Panel Depth: 1-1/2 inch (38 mm). Panel Width: 12 inch (305 mm). a. Matrix Panel Profile: MX-1. b. Matrix Panel Profile: MX-2. c. Matrix Panel Profile: MX-3. d. Matrix Panel Profile: MX-4. e. Matrix Panel Profile: Multi-Depth: MX-5. f. Matrix Panel Profile: MX-6. g. Matrix Panel Profile: MX-7. h. Matrix Panel Profile: MX-8. i. Matrix Panel Profile: MX-9. j. Matrix Panel Profile: MX-10. k. Matrix Panel Profile: MX-11. l. Matrix Panel Profile, Multi-Depth: MX-12. 11. Panel Depth: 2 inches (51 mm). Panel Width: 12 inch (305 mm). a. Matrix Panel Profile, Multi-Depth: MX-13. b. Matrix Panel Profile, Multi-Depth: MX-14. c. Matrix Panel Profile, Multi-Depth: MX-15. ** NOTE TO SPECIFIER ** Delete material options not required. 24 gage (0.60 mm) galvalume and 0.032 inch (0.80 mm) aluminum roll form panels are not available for MX-5, MX-6, MX-7, MX-8, MX-9, MX-10, and MX-11 profiles. 12. Material: Galvalume. Roll form panels from minimum 18 ga. (1.19 mm) aluminum-zinc alloy coated steel sheet. 13. Material: Galvalume. Roll form panels from minimum 20 ga. (1.0 mm) aluminum-zinc alloy coated steel sheet. 14. Material: Galvalume. Roll form panels from minimum 22 ga. (0.80 mm) aluminum-zinc alloy coated steel sheet. 15. Material: Galvalume. Roll form panels from minimum 24 ga. (0.60 mm) aluminum-zinc alloy coated steel sheet. 16. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.032 inch (0.80 mm) sheet. 17. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.040 inch (1 mm) sheet. 18. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.050 inch (1.27 mm) sheet. 19. Accessories: a. Closure Strips: Closed cell, minimum 1 inch (25 mm) thick, matching wall panel profile, and fabricated from same material, gage and finish as panels. b. Tapes and Sealers: As recommended by the manufacturer. ** NOTE TO SPECIFIER ** Factory applied caulking is optional. Delete if not required. c. Factory applied caulking. ** NOTE TO SPECIFIER ** Trimless ends and ribs are available only for MX-6, MX-7 and MX-8 profiles. For trimless ends and ribs, check availability with manufacturer's representative. For products manufactured in Florida, consult manufacturer's representative for available manufacturing locations. Delete if not required. d. Trimless ends. e. Ribs. ** NOTE TO SPECIFIER ** Delete manufacture locations not required. Matrix MX-12 is not manufactured in Arkansas. Matrix MX -5, MX-12, MX-13, MX-14, and MX-15 are not manufactured in Florida. 20. Manufacture Location: Connecticut. 21. Manufacture Location: California. 22. Manufacture Location: Arkansas. 23. Manufacture Location: Florida. B. Basis of Design: Integrity Series Panels as manufactured and supplied by the Morin Corporation. 1. Performance and Design Requirements: a. Standards Compliance: ASTM E283, ASTM E331, and NFPA 285. b. Performance Requirements: ** NOTE TO SPECIFIER ** Delete air leakage option not required. 1) Air Leakage: ASTM E283: Aluminum: Maximum 0.012 cfm (0.00033 cu m per min) of roof area measured at reference differential pressure across assembly of 15 psf (718 Pa). 2) Air Leakage: ASTM E283: Galvalume: Maximum 0.002 CFM psf (0.00006 cu m per min) of roof area measured at reference differential pressure across assembly of 15 psf (718 Pa). 3) Water Leakage: ASTM E331: None, at test pressure of 1.57 psf (75 Pa). 2. Concealed clips and fasteners with common side joints allowing mixed profiles. a. Panel Attachment: MIP clip and fastener. ** NOTE TO SPECIFIER ** Delete application options not required. 3. Application: Weather resistant. 4. Application: Rainscreen rear ventilation for horizontal application. 5. Application: Rainscreen rear ventilation for vertical application. 6. Surface Finish: Smooth, standard. 7. Panel Joint: Tongue and groove interlock. ** NOTE TO SPECIFIER ** Delete panel length option not required. 8. Panel Length: ____ft (___ m). 9. Panel Length: As selected by the Architect. ** NOTE TO SPECIFIER ** Delete panel depth and width option not required. Then delete panel profile options not required. 10. Panel Depth: .875 inch (22 mm). Panel Width: 12 inch (305 mm). a. Integrity Panel Profile: X-12. b. Integrity Panel Profile: XA-12. c. Integrity Panel Profile: XB-12. d. Integrity Panel Profile: XC-12. e. Integrity Panel Profile: XD-12. f. Integrity Panel Profile: XE-12. g. Integrity Panel Profile: XF-12. h. Integrity Panel Profile: XG-12. 11. Panel Depth: .875 inch (22 mm). Panel Width: 16 inch (406 mm). a. Integrity Panel Profile: X-16. b. Integrity Panel Profile: XA-16. c. Integrity Panel Profile: X-16. d. Integrity Panel Profile: XAB-16. e. Integrity Panel Profile: XAAB-16. f. Integrity Panel Profile: XABB-16. g. Integrity Panel Profile: S-16. ** NOTE TO SPECIFIER ** Delete material options not required. 18-gauge XABB-16 is currently being tested. Please refer to the 24-gauge span chart for all applicable span limitations until testing is complete. 24 gage (0.60 mm) galvalume roll form and 0.032 inch (0.80 mm) aluminum panels are not available for XC-12, XAB-16, XA-16, XB-16, and XD-12 profiles. 12. Material: Galvalume. Roll form panels from minimum 18 ga. (1.19 mm) aluminum-zinc alloy coated steel sheet. 13. Material: Galvalume. Roll form panels from minimum 20 ga. (1.0 mm) aluminum-zinc alloy coated steel sheet. 14. Material: Galvalume. Roll form panels from minimum 22 ga. (0.80 mm) aluminum-zinc alloy coated steel sheet. 15. Material: Galvalume. Roll form panels from minimum 24 ga. (0.60 mm) aluminum-zinc alloy coated steel sheet. 16. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.032 inch (0.80 mm) sheet. 17. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.040 inch (1 mm) sheet. 18. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.050 inch (1.27 mm) sheet. 19. Accessories: a. Closure Strips: Closed cell, minimum 1 inch (25 mm) thick, matching wall panel profile, and fabricated from same material, gage and finish as panels. b. Tapes and Sealers: As recommended by the manufacturer. ** NOTE TO SPECIFIER ** Factory applied caulking is optional. Delete if not required. c. Factory applied caulking. ** NOTE TO SPECIFIER ** Delete manufacture locations not required. Integrity Profile S-16 is manufactured in Connecticut and California only. 20. Manufacture Location: Connecticut. 21. Manufacture Location: California. 22. Manufacture Location: Arkansas. 23. Manufacture Location: Florida. C. Basis of Design: Pulse Series Panels as manufactured and supplied by Morin Corporation. 1. Performance and Design Requirements: a. Standards Compliance: ASTM E283, ASTM E331, and NFPA 285. b. Performance Requirements: 1) Air Leakage: ASTM E283: Aluminum: Maximum 0.135 cfm (0.00382 cu m per min) of wall area measured at reference differential pressure across assembly of 30 psf (1436 Pa). 2) Air Leakage: ASTM E283: Galvalume: Maximum 0.251 cfm psf (0.00711 cum per min) of wall area measured at reference differential pressure across assembly of 30 psf (1436 Pa). 3) Water Leakage: ASTM E331: None, at test pressure of 30 psf (1436 Pa). 2. Concealed clips and fasteners with common side joints allowing mixed profiles. a. Panel Attachment: MIP clip and fastener. ** NOTE TO SPECIFIER ** Delete application options not required. 3. Application: Weather resistant. 4. Application: Rainscreen rear ventilation for horizontal application. 5. Application: Rainscreen rear ventilation for vertical application. 6. Surface Finish: Smooth, standard. 7. Panel Joint: Tongue and groove interlock. ** NOTE TO SPECIFIER ** Delete panel length option not required. 8. Panel Length: ____ft (___ m). 9. Panel Length: As selected by the Architect. 10. Panel Depth: 1-1/2 inch (38.1 mm). Panel Width: 12 inch (304.8 mm). ** NOTE TO SPECIFIER ** Delete profile options not required. a. Pulse Panel Profile: P-1. b. Pulse Panel Profile: P-2. c. Pulse Panel Profile: P-3. d. Pulse Panel Profile: P-4. e. Pulse Panel Profile: P-9. f. Pulse Panel Profile: P-10. g. Pulse Panel Profile: P-11. ** NOTE TO SPECIFIER ** Delete material options not required. 24 gage (0.60 mm) galvalume roll form and 0.032 inch (0.80 mm) aluminum panels are not available for P-2 profiles. 11. Material: Galvalume. Roll form panels from minimum 18 ga. (1.19 mm) aluminum-zinc alloy coated steel sheet. 12. Material: Galvalume. Roll form panels from minimum 20 ga. (1.0 mm) aluminum-zinc alloy coated steel sheet. 13. Material: Galvalume. Roll form panels from minimum 22 ga. (0.80 mm) aluminum-zinc alloy coated steel sheet. 14. Material: Galvalume. Roll form panels from minimum 24 ga. (0.60 mm) aluminum-zinc alloy coated steel sheet. 15. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.032 inch (0.80 mm) sheet. 16. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.040 inch (1 mm) sheet. 17. Material: Aluminum per ASTM B209. Alloy and Temper: 3003- H14: Roll form panels from minimum 0.050 inch (1.27 mm) sheet. 18. Accessories: a. Closure Strips: Closed cell, minimum 1 inch (25.4 mm) thick, matching wall panel profile, and fabricated from same material, gage and finish as panels. b. Tapes and sealers recommended by the manufacturer. ** NOTE TO SPECIFIER ** Factory applied caulking is optional, delete if not required. c. Factory applied caulking. ** NOTE TO SPECIFIER ** Delete manufacturer locations not required. Pulse Profiles are not manufactured in Florida. 19. Manufacturer Location: Connecticut. 20. Manufacturer Location: California. 21. Manufacturer Location: Arkansas. 22. Manufacturer Location: Florida. D. Basis of Design: Exposed Fastener Series Panels as manufactured and supplied by Morin Corporation. 1. Concealed clips and fasteners with common side joints allowing mixed profiles. a. Panel Attachment: Exposed fastening. ** NOTE TO SPECIFIER ** Delete application options not required. 2. Application: Weather resistant. 3. Application: Rainscreen rear ventilation for horizontal application. 4. Application: Rainscreen rear ventilation for vertical application. 5. Panel Joint: Overlapping side joint configuration. ** NOTE TO SPECIFIER ** Delete panel length option not required. 6. Panel Length: ____ft (___ m). 7. Panel Length: As selected by the Architect. ** NOTE TO SPECIFIER ** Delete panel depth and width options not required. Then delete panel profiles not required. 8. Panel Depth: 1-1/2 inch (38.1 mm). Panel Width: 28 inch (711 mm). a. Exposed Panel Profile: BR-28 Profile A. b. Exposed Panel Profile: BR-28 Profile B. 9. Panel Depth: 1-1/2 inch (38.1 mm). Panel Width: 35 inch (889 mm). a. Exposed Panel Profile: BR-35 Profile A. b. Exposed Panel Profile: BR7-35 Profile A. c. Exposed Panel Profile: BR-35 Profile B. d. Exposed Panel Profile: BR7-35 Profile B. 10. Panel Depth: 1-1/2 inch (38.1 mm). Panel Width: 36 inch (889 mm). a. Exposed Panel Profile: Exposed Panel: BR9-36 Profile A. b. Exposed Panel Profile: Exposed Panel: BR9-36 Profile B. 11. Panel Depth : 7/8 inch (22.2 mm). Panel Width: 29 inch (737 mm). a. Exposed Panel Profile: C-29 Profile A. b. Exposed Panel Profile: C-29 Profile B. 12. Panel Depth: 7/8 inch (22.2 mm). Panel Width: 37 inch (940 mm). a. Exposed Panel Profile: C-37 Profile A. b. Exposed Panel Profile: C-37 Profile B. 13. Panel Depth: 1 inch (25.4 mm). Panel Width: 36 inch (914 mm). a. Exposed Panel Profile: E-36 Profile A. b. Exposed Panel Profile: E-36 Profile B. c. Exposed Panel Profile: VB-36 Profile A. d. Exposed Panel Profile: VB-36 Profile B. 14. Panel Depth: 1 inch (25.4 mm). Panel Width: 40 inch (1016 mm). a. Exposed Panel Profile: E8-40 Profile A. b. Exposed Panel Profile: E8-40 Profile B. 15. Panel Depth: 1-1/2 inch (38.1 mm). Panel Width: 29 inch (737 mm). a. Exposed Panel Profile: Y-29 Profile A. b. Exposed Panel Profile: Y-29 Profile B. 16. Panel Depth: 1-1/2 inch (38.1 mm). Panel Width: 36 inch (914 mm). a. Exposed Panel Profile: Y-36 Profile A. b. Exposed Panel Profile: Y-36 Profile B. 17. Panel Depth: 2 inch (50.8 mm). Panel Width: 31 inch (787 mm). a. Exposed Panel Profile: VB-31 Profile A. b. Exposed Panel Profile: VB-31 Profile B. 18. Panel Depth: 3 inch (76.2 mm). Width: 24 inch (609.6 mm). a. Exposed Panel Profile: U-24 Profile A. b. Exposed Panel Profile: U-24 Profile B. 19. Panel Depth: 3 inch (76.2 mm). Width: 36 inch (914 mm). a. Exposed Panel Profile: MR-36 Profile A. b. Exposed Panel Profile: MR-36 Profile B. 20. Panel Depth: 4 inch (102 mm). Width: 24 inch (610 mm). a. Exposed Panel Profile: O-24-E Profile A. b. Exposed Panel Profile: O-24-E Profile B. c. Exposed Panel Profile: O-24-W Profile A. d. Exposed Panel Profile: O-24-W Profile B. 21. Panel Depth: 1/2 inch (13 mm). Width: 40 inch (1016 mm). a. Exposed Panel Profile: C-40 Profile A. b. Exposed Panel Profile: C-40 Profile B. ** NOTE TO SPECIFIER ** Delete material options not required. 22. Material: Galvalume: Roll form panels from minimum 18 gage (1.19 mm) aluminum-zinc alloy coated steel sheet. 23. Material: Galvalume: Roll form panels from minimum 20 gage (1.0 mm) aluminum-zinc alloy coated steel sheet. 24. Material: Galvalume: Roll form panels from minimum 22 gage (0.80 mm) aluminum-zinc alloy coated steel sheet. 25. Material: Galvalume: Roll form panels from minimum 24 gage (0.60 mm) aluminum-zinc alloy coated steel sheet. 26. Material: Aluminum: ASTM B209: Alloy and Temper: 3003- H14: Roll form panels from minimum 0.032 inch (0.80 mm) sheet. 27. Material: Aluminum: ASTM B209: Alloy and Temper: 3003- H14: Roll form panels, minimum 0.040 (1 mm) thick sheet. 28. Material: Aluminum: ASTM B209: Alloy and Temper: 3003- H14: Roll form panels, minimum 0.050 inch (1.27 mm) sheet. 29. Accessories: a. Closure Strips: Closed cell, minimum 1 inch (25 mm) thick, matching wall panel profile, and fabricated from same material, gage and finish as panels. b. Tapes and Sealers: As recommended by the manufacturer. ** NOTE TO SPECIFIER ** Delete manufacturer locations not required. c. California Manufactured Profiles: BR9-36A, BR9-36B, BR7-35A, BR7-35B, C-29A, C-29B, C-37A, C-40A, C-40B, E-36A, E-36B, E8-40A, E8-40B, MR-36A, MR-36B, C-37B, O-24-WA, O-24-WB, U-24A U-24B, VB-36A, VB-36B, Y-29A, Y-29B, Y-36A, and Y-36B. d. Connecticut Manufactured Profiles: BR-28A, BR-28B, C-29A, C-29B, C-40A, C-40B, MR-36A, MR-36B, O-24-EA, O-24-EB, Y-29A, Y-29B, Y3-6A, and Y-36B. e. Florida Manufactured Profiles: BR-35A, BR-35B, BR-28A, BR-28B, C-29A, C-29B, C-37A, C-37B, VB-31A, VB-31B, Y-29A, Y-29B, Y-36A, and Y-36B. f. Arkansas Manufactured Profiles: C-29A, C-29B, C-37A, C-37B, U-24A, U-24B, Y-29A, Y-29B, Y-36A, and Y-36B. 30. Manufacturer Location: Connecticut. 31. Manufacturer Location: California. 32. Manufacturer Location: Arkansas. 33. Manufacturer Location: Florida. ** NOTE TO SPECIFIER ** Delete the perforations paragraph if not required, or delete open area and diameter options not required. All profiles are available with perforations. 34. Manufacturer's Suggested Materials: a. Aluminum: .032 inch (0.81 mm), 0.040 inch (1.02 mm), and 0.050 inch (1.27 mm). b. Stainless Steel: 20, 22, and 24 gauge. 1) Zinc: and 0.039 inch (0.8 and 1.0 mm) with a minimum hole size of 3/16 (4.76 mm) inch. 2) Galvalume: Available for Interior applications only. This material is subject to rust in exterior conditions. Consult with manufacturer's representative for other perforation capabilities. E. Perforations: 1. Open Area: 10 percent. a. Diameter: 1/8 inch (3.18 mm). Center Spacing: 3/8 inch (9.52 mm). 2. Open Area: 23 percent. a. Diameter: 1/8 inch (3.18 mm). Center Spacing: 1/4 inch (6.35 mm). b. Diameter: 1/4 inch (6.35 mm). Center Spacing: 1/2 inch (12.70 mm). 3. Open Area: 30 percent. a. Diameter: 1/8 inch (3.18 mm). Center Spacing: 7/32 inch (5.56 mm). 4. Open Area: 33 percent. a. Diameter: 3/16 inch (4.76 mm). Center Spacing: 5/16 inch (7.94 mm). 5. Open Area: 40 percent. a. Diameter: 1/8 inch (3.18 mm). Center Spacing: 3/16 inch (4.76 mm). b. Diameter: 3/8 inch (9.52 mm). Center Spacing: 9/16 inch (14.29 mm). 6. Open Area: 51 percent. a. Diameter: 3/16 inch (4.76 mm). Center Spacing: 1/4 inch (6.35 mm). b. Diameter: 3/8 inch (9.52 mm). Center Spacing: 1/2 inch (12.70 mm). 7. Open Area: ________. a. Diameter: ___ inch (___ mm). Center Spacing: ___ inch (___ mm). ** NOTE TO SPECIFIER ** Delete finish options not required. Consult manufacturer for available colors, SR, E and SRI values, and for custom and additional panel and trim finish options. F. Finish: Panel and Trim Finish: 1. Galvalume-Zincalume Plus per ASTM A792 and ASTM AZ55. 2. Anodized Aluminum: Clear Matte. 3. Anodized Aluminum: Black Matte. 4. Anodized Aluminum: Dark Bronze. 5. Anodized Aluminum: Medium Bronze. 6. Anodized Aluminum: Light Bronze. 7. Anodized Aluminum: Copper Penny. 8. Anodized Aluminum: Dark Copper. 9. Anodized Aluminum: Antique Brass. 10. Anodized Aluminum: Champagne Gold. 11. Anodized Aluminum: Silver White. 12. Anodized Aluminum: As selected by the Architect. 13. Fluropon: AAMA 2605: 70 Percent Polyvinylidene, Two Coats: 0.2 mil primer, 0.8 mil color. a. Color: Regal White - SR: 0.70, E: 0.86, SRI: 85. b. Color: Ascot White - SR: 0.69, E: 0.85, SRI: 83. c. Color: Bone White - SR: 0.69, E: 0.84, SRI: 83. d. Color: Sandstone - SR: 0.61, E: 0.85, SRI: 72. e. Color: Dove Gray - SR: 0.47, E: 0.86, SRI: 53. f. Color: Zinc Gray - SR: 0.35, E: 0.86, SRI: 53. g. Color: Chromium Gray - SR: 0.48, E: 0.85, SRI: 54. h. Color: Surrey Beige - SR: 0.48, E: 0.86, SRI: 54. i. Color: Driftwood - SR: 0.45, E: 0.86, SRI: 50. j. Color: Parchment - SR: 0.53, E: 0.85, SRI: 61. k. Color: Antique Bronze - SR: 0.43, E: 0.86, SRI: 61. l. Color: Regal Blue - SR: 0.26, E: 0.85, SRI: 24. m. Color: Spartan Bronze - SR: 0.31, E: 0.85, SRI: 31. n. Color: Dark Bronze - SR: 0.29, E: 0.88, SRI: 30. o. Color: Patina Green - SR: 0.41, E: 0.84, SRI: 44. p. Color: Evergreen - SR: 0.26, E: 0.85, SRI: 24. q. Color: Slate Blue - SR: 0.28, E: 0.85, SRI: 27. r. Color: Bristol Black - SR: 0.26, E: 0.86, SRI: 25. s. Color: Blue Gray - SR: 0.27, E: 0.85, SRI: 26. t. Color: As selected by the Architect. 14. Fluropon Classic: AAMA 2605: High Performance Primer, 70 Percent Polyvinylidene Difluoride with Aluminum Flake Pigments, 70 Percent Polyvinylidene Difluoride, Three Coats: 0.2 mil primer, 0.8 mil color, 0.5 mil topcoat. a. Color: Medium Gray - SR: 0.36, E: 0.85, SRI: 38. b. Color: Bright Silver - SR: 0.57, E: 0/81, SRI: 65. c. Color: Champagne Gold - SR: 0.51, E: 0.85, SRI: 58. d. Color: As selected by the Architect. 15. Fluropon Classic II: AAMA 2605: 70 Percent Polyvinylidene Difluoride, Mica Based, Two Coats: 0.2 mil primer, 0.8 mil color. a. Color: Silversmith - SR: 0.53, E: 0.79, SRI: 59. b. Color: Champagne Bronze - SR: 0.44, E: 0.78, SRI: 46. c. Color: Weathered Zinc - SR: 0.33, E: 0.84, SRI: 33. d. Color: Copper Penny - SR: 0.48, E: 0.84, SRI: 54. e. Color: Champagne Pearl - SR: 0.48, E: 0.81, SRI: 53. f. Color: As selected by the Architect. 16. Fluoropon Coastal PVDF: AAMA 2605: High Performance Primer, 70 Percent Polyvinylidene Difluoride, Mica Based, Two Coats: 0.8-1.0 mil primer, 0.7-0.8 mil color. ** NOTE TO SPECIFIER ** Delete custom Fluoropon color options not required. 17. Custom Fluoropon Color: Grande Rust. 18. Custom Fluoropon Color: White Rust. 19. Custom Fluoropon Color: Venetian Pewter. 20. Custom Fluoropon Color: Vintage Medallion. 21. Custom Fluoropon Color: Rustic Ridge. 22. Custom Fluoropon Color: Azure Patina. 23. Custom Fluoropon Color: Midnight Tarnish. 24. Custom Fluoropon Color: Midnight Oxide. 25. Custom Fluoropon Color: Midnight Hour. 26. Custom Fluoropon Color: Black Oxide Steel. 27. Custom Fluoropon Color: Black Etched Steel. 28. Custom Fluoropon Color: Forged Steel. 29. Custom Fluoropon Color: Black Ore. 30. Custom Fluoropon Color: Golden Bamboo. 31. Custom Fluoropon Color: Light Oak. 32. Custom Fluoropon Color: Light Natural Walnut. 33. Custom Fluoropon Color: Pickled Ironwood. 34. Custom Fluoropon Color: Weathered Wood. 35. Custom Fluoropon Color: Honey Teak. 36. Custom Fluoropon Color: Eucalyptus. PART 3 EXECUTION 3.1 EXAMINATION A. Do not begin installation until the substrates have been properly constructed and prepared. B. If substrate preparation is the responsibility of another installer, notify Architect in writing of unsatisfactory preparation before proceeding. 3.2 PREPARATION A. Clean surfaces thoroughly prior to installation. B. Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions. 3.3 INSTALLATION A. Install in accordance with manufacturer's instructions, approved submittals, and in proper relationship with adjacent construction. ** NOTE TO SPECIFIER ** Delete installation tolerance not required or include maximum variation from plane if different from variation listed below. B. Installation Tolerances: 1. Maximum Variation From Plane: 1/4 inch (6.35 mm) in 20 ft (6.10 m), non-cumulative. 2. Maximum Variation From Plane: _______ inch in 20 ft (6.10 m), non-cumulative. 3.4 FIELD QUALITY CONTROL A. Field Inspection: Coordinate field inspection in accordance with appropriate sections in Division 01. ** NOTE TO SPECIFIER ** Include if manufacturer provides field quality control with onsite personnel for instruction or supervision of product installation, application, erection, or construction. Delete if not required. B. Manufacturer's Services: Coordinate manufacturer's services in accordance with appropriate sections in Division 01. 3.5 CLEANING AND PROTECTION A. Clean products in accordance with the manufacturers recommendations. B. Touch-up, repair or replace damaged products before Substantial Completion. END OF SECTION