MasterFormat: 2020 Switch to 95
Download this Protective Covers - Awnings, Canopies, and Sunshades Specification for
WORD | WORD-Canadian | WP | RTF | TEXT
Find over 500 more construction specifications | Arcat.com
          SKYSCAPE Architectural Canopies Protective Covers - Awnings, Canopies, and Sunshades
 
         
SECTION 10 73 00
 
         
PROTECTIVE COVERS - AWNINGS, CANOPIES, AND SUNSHADES
 
         
 
         
Copyright 2025 - 2025 ARCAT, Inc. - All rights reserved

          ** NOTE TO SPECIFIER ** SKYSCAPE Architectural Canopies; Aluminum Canopy systems.
This section is based on the products of SKYSCAPE Architectural Canopies, which is located at:
4575 River Green Pkwy., Suite 200
Duluth, GA 30096
Tel: 770-674-6452
Email: request info (sales@skyscapecanopies.com)
Web: https://www.skyscapecanopies.com
[ Click Here ] for additional information.
SKYSCAPE is on a mission to be the nation's leading provider of aluminum canopy systems. With a focus on exceptional customer support, we deliver pre-engineered canopies distinguished by uncompromising quality. From design to engineering to execution, we're here to assist you every step of the way.
Unlike brake-formed aluminum or bolt-together canopy systems, SKYSCAPE® Canopies are fabricated using extruded aluminum components for unbeatable strength and durability. Capable of withstanding even the harshest weather conditions, they can last years without rusting or corroding. And because our manufactured canopies are welded, not thru-fastened, field installation is simplified to ensure a top-quality product with a fast completion time.
SKYSCAPE® offers specialized services for architects, engineers, general contractors, facility managers and property managers. In addition to engineering and installation support, we also provide design assistance. We can configure a custom canopy system based on most design concepts and size needs, load, and engineering requirements. Plus, our wide selection of standard profiles, design options and finishes, gives you the flexibility to enhance virtually any architectural aesthetic.
So whether you're an architect looking for design inspiration, a general contractor with a tight completion schedule, an engineer concerned with code requirements, or a property owner in need of an "update" solution, you can trust SKYSCAPE® to deliver for you.
 
          PART 1GENERAL
 
          1.1SECTION INCLUDES
          ** NOTE TO SPECIFIER ** Delete items below not required for project.
 
          A.Awnings:
          1.Fabric covered.
          2.Metal covered.
 
          B.Canopies:
          1.Cantilevered.
          2.Hangar supported.
          3.Post supported.
 
          C.Sunshades:
          1.Cantilevered.
          2.Hangar supported.
          3.Post supported.
 
          1.2RELATED SECTIONS
          ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required.
 
          A.Section 03 30 00 - Cast-in-Place Concrete. Concrete footings, anchor bolts.
 
          B.Section 04 20 00 - Unit Masonry.
 
          C.Section 06 20 00 - Finish Carpentry.
 
          D.Section 09 91 13 - Exterior Painting. Paint finish on framing members.
 
          E.Section 26 27 26 - Wiring Devices. Finish requirements for wall controls specified in this section.
 
          1.3SUBMITTALS
 
          A.Submit under provisions of Section 01 30 00.
 
          B.Product Data:
          1.Manufacturer's data sheets and technical specifications for each product to be used.
          2.Preparation instructions and recommendations.
          3.Storage and handling requirements and recommendations.
          4.Typical installation methods.
          ** NOTE TO SPECIFIER ** Delete if not applicable to product type.
 
          C.Color Verification Samples: Two representative units of each color.
 
          D.Shop Drawings: Include details of materials, construction, and finish. Include relationship with adjacent construction.
          1.Show structural component locations/positions, material dimensions and details of construction and assembly.
 
          1.4QUALITY ASSURANCE
 
          A.Manufacturer Qualifications: Company specializing in manufacturing products specified in this section with a minimum of five years documented experience.
 
          B.Installer Qualifications: Company specializing in performing Work of this section with minimum two years documented experience with projects of similar scope and complexity.
 
          C.Source Limitations: Provide each type of product from a single manufacturing source to ensure uniformity.
          ** NOTE TO SPECIFIER ** Include mock-up if the project size or quality warrant the expense. The following is one example of how a mock-up might be specified. When deciding on the extent of the mock-up, consider all the major different types of work on the project.
 
          D.Mock-Up: Construct a mock-up with actual materials in sufficient time for Architect's review and to not delay construction progress. Locate mock-up as acceptable to Architect and provide temporary foundations and support.
          1.The intent of a mock-up is to demonstrate quality of workmanship and visual appearance.
          2.If the mock-up is not acceptable, rebuild the mock-up until satisfactory results are achieved.
          3.Retain mock-up during construction as a standard for comparison with completed work.
          4.Do not alter or remove mock-up until work is completed or removal is authorized.
 
          1.5PRE-INSTALLATION CONFERENCE
 
          A.Convene a conference approximately two weeks before scheduled commencement of the Work. Attendees shall include Architect, Contractor and trades involved. Agenda shall include schedule, responsibilities, critical path items and approvals.
 
          1.6DELIVERY, STORAGE, AND HANDLING
 
          A.Store and handle in strict compliance with manufacturer's written instructions and recommendations.
 
          B.Protect from damage due to weather, excessive temperature, and construction operations.
 
          1.7PROJECT CONDITIONS
 
          A.Maintain environmental conditions (temperature, humidity, and ventilation) within limits recommended by manufacturer for optimum results. Do not install products under environmental conditions outside manufacturer's recommended limits.
 
          1.8WARRANTY
 
          A.Manufacturer's standard limited warranty unless indicated otherwise.
 
          PART 2PRODUCTS
 
          2.1MANUFACTURERS
 
          A.Acceptable Manufacturer: SKYSCAPE Architectural Canopies, which is located at:
4575 River Green Pkwy., Suite 200
Duluth, GA 30096
Tel: 770-674-6452
Email: request info (sales@skyscapecanopies.com);Web: https://www.skyscapecanopies.com
          ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions.
 
          B.Substitutions: Not permitted.
 
          C.Requests for substitutions will be considered in accordance with the provisions of Section 01 60 00.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.2AWNINGS; FABRIC COVERED
 
          A.Performance and Design Requirements:
          1.Awnings: Must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          2.Engineering Certification: PE Stamped calculations and drawings.
          3.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          4.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the awning, other than fixture locations.
          5.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the awning manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry awning loads where required.
          d.Water drainage away from awning where necessary.
          e.Outrigger: Profile as selected by architect.
 
          B.Materials:
          1.Awning Fabric:
          a.Fire retardant treated Sunbrella fabric, or similar, soft textured canvas.
          b.Fabric Color: As selected by Architect from Manufacutrer's standard range.
          ** NOTE TO SPECIFIER ** Delete either of the two paragraphs if it is not required.
          1)Provide color sample cards showing full range of available colors.
          2)Samples of specific fabric for final color selection.
          2.Frame:
          a.Structure: 6063-T5 aluminum extrusions.
          b.Framing Profiles: Sized to withstand live, dead, and superimposed loads.
          c.Fasteners: Non-corrosive, non-staining bolts, shims, and accessory items.
          3.PVC Trim:
          a.PVC ZipStrip: Used to cover staple seams unless otherwise specified.
          b.DividerBead: Used where structure modules are joined.
          c.FlashStrip: Used on top of awning where it contacts substrate to provide weatherproof seal.
          4.Staples: 18 gauge galvanized or stainless steel.
          a.Crown: 5/16 inch (8 mm) width. Length: 3/8 or 1/2 inch (9.5 or 13 mm).
 
          C.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          D.Fabrication:
          1.Factory weld and paint assemblies, Deliver ready to install.
          a.Not Acceptable: Field assembly of awning frame components ("stick-built") using mechanical fasteners.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.3AWNINGS; METAL COVERED
 
          A.Performance and Design Requirements:
          1.Awnings: Must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          2.Engineering Certification: PE Stamped calculations and drawings.
          3.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          4.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the awning, other than fixture locations.
          5.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the awning manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry awning loads where required.
          d.Water drainage away from awning where necessary.
          e.Outrigger: Profile as selected by architect.
 
          B.Materials:
          1.Standing Seam Metal:
          a.Material: Galvalume, 24 ga minimum.
          b.Panel Width Minimum: 12 inches (305 mm).
          c.Color: As selected by Architect from Manufacutrer's standard range.
          ** NOTE TO SPECIFIER ** Delete either of the two paragraphs if it is not required.
          1)Provide color sample cards showing full range of available colors.
          2)Samples of specific colors for final color selection.
          2.Frame:
          a.Structure: 6063-T5 aluminum extrusions.
          b.Framing Profiles: Sized to withstand live, dead, and superimposed loads.
          c.Fasteners: Non-corrosive, non-staining bolts, shims, and accessory items.
          3.PVC Trim:
          a.DividerBead: Used where structure modules are joined.
          b.FlashStrip: Used on top of awning where it contacts substrate to provide weatherproof seal.
 
          C.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          D.Fabrication:
          1.Factory weld and paint assemblies, Deliver ready to install.
          a.Not Acceptable: Field assembly of awning frame components ("stick-built") using mechanical fasteners.
          ** NOTE TO SPECIFIER ** Delete articles if not required.
 
          2.4CANOPIES; CANTILEVERED
 
          A.Performance and Design Requirements:
          1.Canopy: Must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete canopy profile options not required.
          2.Canopy Profile: Flat.
          3.Canopy Profile: Curved.
          4.Canopy Profile: Arched.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          5.Engineering Certification: PE Stamped calculations and drawings.
          6.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          7.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the awning, other than fixture locations.
          8.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the canopy manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry canopy loads where required.
          d.Water drainage away from canopy where necessary.
          e.Outrigger: Profile as selected by architect.
          f.Concealed Drainage: Water is to drain from covered surfaces into internal fascia/gutter and directed out and away from the canopy.
          ** NOTE TO SPECIFIER ** Delete drainage options not required.
          1)Drainage: Scuppers.
          2)Drainage: Downspouts.
          3)Drainage: As detailed on the Drawings.
          4)Drainage: As selected by Architect.
 
          B.Materials:
          ** NOTE TO SPECIFIER ** Delete decking options not required.
 
          C.1 x 12 inch (25 x 305 mm) standing seam is not available for curved canopies.
 
          D.1 x 12 inch (25 x 305 mm) standing seam and corrugated material are the only decking profiles that can be used on arched canopies.
          1.Decking: 6 inch (152 mm) flat deck extruded aluminum.
          2.Decking: 6 inch (152 mm) V-deck extruded aluminum.
          3.Decking: Corrugated extruded aluminum.
          4.Decking: 1.5 x 16 inch (38 x 406 mm) flat extruded aluminum.
          5.Decking: 2 x 16 inch (51 x 406 mm) flat extruded aluminum.
          6.Decking: 1 x 12 inch (25 x 305 mm) standing seam extruded aluminum.
          7.Fascia, Perimeter, Outrigger, and Intermediate Framing Members:
          a.Material: Aluminum.
          ** NOTE TO SPECIFIER ** Delete extrusion and extension options not required.
          b.Extrusion: As selected by architect.
          c.Extrusion: C-8 inch (203 mm).
          d.Extrusion: C-12 inch (305 mm).
          e.Extrusion: J-8 inch (203 mm).
          1)Extension: 2 inches (51 mm).
          2)Extension: 4 inches (102 mm).
          3)Extension: 6 inches (152 mm).
          4)Extension: 8 inches (203 mm).
          f.Extrusion: J-12 inch (305 mm).
          1)Extension: 2 inches (51 mm).
          2)Extension: 4 inches (102 mm).
          3)Extension: 6 inches (152 mm).
          4)Extension: 8 inches (203 mm).
          ** NOTE TO SPECIFIER ** The following fascia options are for curved and arched canopies.
          8.Fascia: Frame and Formed Metal: 8 inch (23 mm).
          9.Fascia: Frame and Formed Metal: 10 inch (254 mm).
          10.Fascia: Frame and Formed Metal: 12 inch (305 mm).
          11.Fascia: Frame and Formed Metal: 16 inch (406 mm).
          12.Aluminum Plate Thickness: To be determined by manufacturer.
 
          E.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          F.Fabrication:
          1.Factory welded and painted assemblies, prior to delivery.
          a.Not Acceptable: Field assembled frame components ("stick-built") using mechanical fasteners.
          2.Decking: Interlocking extruded or roll-formed panels, as selected by architect.
          ** NOTE TO SPECIFIER ** Delete plate options not required.
          3.Escutcheon Plates: Aluminum as detailed: 6 x 6 x 0.375 inches (152 x 152 x 9.5 mm).
          4.Escutcheon Plates: Aluminum as detailed: 8 x 8 x 0.375 inches (203 x 203 x 9.5 mm).
          5.Escutcheon Plates: Aluminum as detailed.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.5CANOPIES; HANGAR SUPPORTED
 
          A.Performance Requirements:
          1.Canopy must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete canopy profile options not required.
          2.Canopy Profile: Flat.
          3.Canopy Profile: Flat.
          4.Canopy Profile: Curved.
          5.Canopy Profile: Arched.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          6.Engineering Certification: PE Stamped calculations and drawings.
          7.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          8.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the awning, other than fixture locations.
          9.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the canopy manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry canopy loads where required.
          d.Water drainage away from canopy where necessary.
          e.Outrigger: Profile as selected by architect.
          f.Concealed Drainage: Water is to drain from covered surfaces into internal fascia/gutter and directed out and away from the canopy.
          ** NOTE TO SPECIFIER ** Delete drainage options not required.
          1)Drainage: Scuppers.
          2)Drainage: Downspouts.
          3)Drainage: As detailed on the Drawings.
          4)Drainage: As selected by Architect.
 
          B.Materials:
          ** NOTE TO SPECIFIER ** Delete decking options not required.
 
          C.1 x 12 inch (25 x 305 mm) standing seam is not available for curved canopies.
 
          D.1 x 12 inch (25 x 305 mm) standing seam and corrugated material are the only decking profiles that can be used on arched canopies.
          1.Decking: 6 inch (152 mm) flat deck extruded aluminum.
          2.Decking: 6 inch (152 mm) V-deck extruded aluminum.
          3.Decking: Corrugated extruded aluminum.
          4.Decking: 1.5 x 16 inch (38 x 406 mm) flat extruded aluminum.
          5.Decking: 2 x 16 inch (51 x 406 mm) flat extruded aluminum.
          6.Decking: 1 x 12 inch (25 x 305 mm) standing seam extruded aluminum.
          7.Fascia, Perimeter, Outrigger, and Intermediate Framing Members:
          a.Material: Aluminum.
          ** NOTE TO SPECIFIER ** Delete extrusion and extension options not required.
          b.Extrusion: As selected by architect.
          c.Extrusion: C-8 inch (203 mm).
          d.Extrusion: C-12 inch (305 mm).
          e.Extrusion: J-8 inch (203 mm).
          1)Extension: 2 inches (51 mm).
          2)Extension: 4 inches (102 mm).
          3)Extension: 6 inches (152 mm).
          4)Extension: 8 inches (203 mm).
          f.Extrusion: J-12 inch (305 mm).
          1)Extension: 2 inches (51 mm).
          2)Extension: 4 inches (102 mm).
          3)Extension: 6 inches (152 mm).
          4)Extension: 8 inches (203 mm).
          ** NOTE TO SPECIFIER ** The following fascia options are for curved and arched canopies.
          8.Fascia: Frame and Formed Metal: 8 inch (23 mm).
          9.Fascia: Frame and Formed Metal: 10 inch (254 mm).
          10.Fascia: Frame and Formed Metal: 12 inch (305 mm).
          11.Fascia: Frame and Formed Metal: 16 inch (406 mm).
 
          E.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          F.Fabrication:
          1.Factory welded and painted assemblies, prior to delivery.
          a.Not Acceptable: Field assembled frame components ("stick-built") using mechanical fasteners.
          2.Decking: Interlocking extruded or roll-formed panels, as selected by architect.
          ** NOTE TO SPECIFIER ** Delete plate options not required.
          3.Escutcheon Plates: Aluminum as detailed: 6 x 6 x 0.375 inches (152 x 152 x 9.5 mm).
          4.Escutcheon Plates: Aluminum as detailed: 8 x 8 x 0.375 inches (203 x 203 x 9.5 mm).
          5.Escutcheon Plates: Aluminum as detailed.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.6CANOPIES; POST SUPPORTED
 
          A.Performance Requirements:
          1.Canopy must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete canopy type options not required.
          2.Canopy Type: Flat.
          3.Canopy Type: Curved.
          4.Canopy Type: Arched.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          5.Engineering Certification: PE Stamped calculations and drawings.
          6.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          7.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the awning, other than fixture locations.
          8.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the canopy manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry canopy loads where required.
          d.Water drainage away from canopy where necessary.
          e.Outrigger: Profile as selected by architect.
          f.Concealed Drainage: Water is to drain from covered surfaces into internal fascia/gutter and directed out and away from the canopy.
          ** NOTE TO SPECIFIER ** Delete drainage options not required.
          1)Drainage: Scuppers.
          2)Drainage: Downspouts.
          3)Drainage: As detailed on the Drawings.
          4)Drainage: As selected by Architect.
 
          B.Materials:
          ** NOTE TO SPECIFIER ** Delete decking options not required.
 
          C.1 x 12 inch (25 x 305 mm) standing seam is not available for curved canopies.
 
          D.1 x 12 inch (25 x 305 mm) standing seam and corrugated material are the only decking profiles that can be used on arched canopies.
          1.Decking: 6 inch (152 mm) flat deck extruded aluminum.
          2.Decking: 6 inch (152 mm) V-deck extruded aluminum.
          3.Decking: Corrugated extruded aluminum.
          4.Decking: 1.5 x 16 inch (38 x 406 mm) flat extruded aluminum.
          5.Decking: 2 x 16 inch (51 x 406 mm) flat extruded aluminum.
          6.Decking: 1 x 12 inch (25 x 305 mm) standing seam extruded aluminum.
          7.Fascia, Perimeter, Outrigger, and Intermediate Framing Members:
          a.Material: Aluminum.
          ** NOTE TO SPECIFIER ** Delete extrusion and extension options not required.
          b.Extrusion: As selected by architect.
          c.Extrusion: C-8 inch (203 mm).
          d.Extrusion: C-12 inch (305 mm).
          e.Extrusion: J-8 inch (203 mm).
          1)Extension: 2 inches (51 mm).
          2)Extension: 4 inches (102 mm).
          3)Extension: 6 inches (152 mm).
          4)Extension: 8 inches (203 mm).
          f.Extrusion: J-12 inch (305 mm).
          1)Extension: 2 inches (51 mm).
          2)Extension: 4 inches (102 mm).
          3)Extension: 6 inches (152 mm).
          4)Extension: 8 inches (203 mm).
          ** NOTE TO SPECIFIER ** The following fascia options are for curved and arched canopies.
          8.Fascia: Frame and Formed Metal: 8 inch (23 mm).
          9.Fascia: Frame and Formed Metal: 10 inch (254 mm).
          10.Fascia: Frame and Formed Metal: 12 inch (305 mm).
          11.Fascia: Frame and Formed Metal: 16 inch (406 mm).
          12.Support Posts: Aluminum support posts, height as required to adequately secure the canopy, unless otherwise specified by architect
          ** NOTE TO SPECIFIER ** Delete post size options not required.
          a.Support Post Size: 4 x 4 inch (102 x 102 mm)
          b.Support Post Size: __ x __ inch (__ x __ mm)
          c.Support Post Size: As detailed on the Drawings.
          13.Outrigger Design: Profile as selected by architect.
          14.Aluminum Plate Thickness: To be determined by manufacturer.
 
          E.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          F.Fabrication:
          1.Factory welded and painted assemblies, prior to delivery.
          a.Not Acceptable: Field assembled frame components ("stick-built") using mechanical fasteners.
          2.Decking: Interlocking extruded or roll-formed panels, as selected by architect.
          ** NOTE TO SPECIFIER ** Delete plate options not required.
          3.Escutcheon Plates: Aluminum as detailed: 6 x 6 x 0.375 inches (152 x 152 x 9.5 mm).
          4.Escutcheon Plates: Aluminum as detailed: 8 x 8 x 0.375 inches (203 x 203 x 9.5 mm).
          5.Escutcheon Plates: Aluminum as detailed.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.7SUNSHADES; CANTILEVERED
 
          A.Performance and Design Requirements:
          1.Sunshades: Must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          2.Engineering Certification: PE Stamped calculations and drawings.
          3.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          4.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the sunshades, other than fixture locations.
          5.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the sunshades manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry sunshades loads where required.
          d.Outrigger: Profile as selected by architect.
 
          B.Materials: Extruded aluminum unless specified otherwise.
          1.Airfoils: 1.5 x 6 inches (38 x 152 mm).
          2.Airfoils: 2 x 8 inches (51 x 203 mm).
          3.Louver Blades: No. L-1. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          4.Louver Blades: No. L-1F. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          5.Louver Blades: No. L-7. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          6.Fascia, Perimeter, Outrigger, and Intermediate Framing Members: Extruded aluminum, in profile and thickness shown in current manufacturer's details and/or literature.
          ** NOTE TO SPECIFIER ** Delete the fascia extruded tube options not required.
          7.Fascia: Extruded Tube. 2 x 4 inches (51 x 102 mm).
          8.Fascia: Extruded Tube. 2 x 6 inches (51 x 152 mm).
          9.Fascia: Extruded Tube. 2 x 8 inches (51 x 203 mm).
          10.Aluminum Plate Thickness: To be determined by manufacturer.
 
          C.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          D.Fabrication:
          1.Factory welded and painted assemblies, prior to delivery.
          a.Not Acceptable: Field assembled frame components ("stick-built") using mechanical fasteners.
          2.Framing: Interlocking extruded or roll-formed panels, as selected by architect.
          ** NOTE TO SPECIFIER ** Delete plate options not required.
          3.Escutcheon Plates: Aluminum as detailed: 6 x 6 x 0.375 inches (152 x 152 x 9.5 mm).
          4.Escutcheon Plates: Aluminum as detailed: 8 x 8 x 0.375 inches (203 x 203 x 9.5 mm).
          5.Escutcheon Plates: Aluminum as detailed.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.8SUNSHADES; HANGAR SUPPORTED
 
          A.Performance and Design Requirements:
          1.Sunshades: Must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          2.Engineering Certification: PE Stamped calculations and drawings.
          3.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          4.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the sunshades, other than fixture locations.
          5.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the sunshades manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry sunshades loads where required.
          d.Outrigger: Profile as selected by architect.
 
          B.Materials: Extruded aluminum unless specified otherwise.
          1.Airfoils: 1.5 x 6 inches (38 x 152 mm).
          2.Airfoils: 2 x 8 inches (51 x 203 mm).
          3.Louver Blades: No. L-1. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          4.Louver Blades: No. L-1F. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          5.Louver Blades: No. L-7. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          6.Fascia, Perimeter, Outrigger, and Intermediate Framing Members: Extruded aluminum, in profile and thickness shown in current manufacturer's details and/or literature.
          7.Fascia:
          ** NOTE TO SPECIFIER ** Delete the following options not required.
          a.Extruded Tube: 2 x 4 inches (51 x 102 mm).
          b.Extruded Tube: 2 x 6 inches (51 x 152 mm).
          c.Extruded Tube: 2 x 8 inches (51 x 203 mm).
          d.Extruded Tube: Size as selected by architect.
          8.Aluminum Plate Thickness: To be determined by manufacturer.
 
          C.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
 
          D.Fabrication:
          1.Factory welded and painted assemblies, prior to delivery.
          a.Not Acceptable: Field assembled frame components ("stick-built") using mechanical fasteners.
          2.Framing: Interlocking extruded or roll-formed panels, as selected by architect.
          ** NOTE TO SPECIFIER ** Delete plate options not required.
          3.Escutcheon Plates: Aluminum as detailed: 6 x 6 x 0.375 inches (152 x 152 x 9.5 mm).
          4.Escutcheon Plates: Aluminum as detailed: 8 x 8 x 0.375 inches (203 x 203 x 9.5 mm).
          5.Escutcheon Plates: Aluminum as detailed.
          ** NOTE TO SPECIFIER ** Delete article if not required.
 
          2.9SUNSHADES; POST SUPPORTED
 
          A.Performance and Design Requirements:
          1.Sunshades: Must conform to local building codes.
          ** NOTE TO SPECIFIER ** Delete engineering certification if not required.
          2.Engineering Certification: PE Stamped calculations and drawings.
          3.Field Measurements: Confirm prior to preparation of shop drawings when possible.
          4.Allow for installation of electrical conduit, lighting, plumbing, sprinkler components, etc., concealed above the decking, not visible from beneath the sunshades, other than fixture locations.
          5.Design Considerations:
          a.Flashing: Generic and/or specialty designs will be required and may be supplied by the sunshades manufacturer or by the installer.
          b.Determine wall construction, make-up, and thickness.
          c.Ensure adequate wall condition to carry sunshades loads where required.
          d.Outrigger: Profile as selected by architect.
 
          B.Materials: Extruded aluminum unless specified otherwise.
          1.Airfoils: 1.5 x 6 inches (38 x 152 mm).
          2.Airfoils: 2 x 8 inches (51 x 203 mm).
          3.Louver Blades: No. L-1. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          4.Louver Blades: No. L-1F. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          5.Louver Blades: No. L-7. Dimensions: 5.5 x 3.75 inches (140 x 95 mm).
          6.Fascia, Perimeter, Outrigger, and Intermediate Framing Members: Extruded aluminum, in profile and thickness shown in current manufacturer's details and/or literature.
          ** NOTE TO SPECIFIER ** Delete the fascia extruded tube options not required.
          7.Fascia: Extruded Tube. 2 x 4 inches (51 x 102 mm).
          8.Fascia: Extruded Tube. 2 x 6 inches (51 x 152 mm).
          9.Fascia: Extruded Tube. 2 x 8 inches (51 x 203 mm).
          10.Support Posts: Aluminum support posts, height as required to adequately secure the canopy, unless otherwise specified by architect.
          ** NOTE TO SPECIFIER ** Delete size options not required.
          a.Support Post Size: 4 x 4 inch (102 x 102 mm).
          b.Support Post Size: __ x __ inch (__ x __ mm).
          c.Support Post Size: As detailed on the Drawings.
          11.Aluminum Plate Thickness: To be determined by manufacturer.
 
          C.Finish: Factory applied by the awning manufacturer.
          1.Quality Level: Meet or Exceed AAMA 2604.
          ** NOTE TO SPECIFIER ** Delete the powder coat or the Kynar option. Whichever is not required.
          2.Powder coated. Color: As determined by the Architect from the Manufacturer's offerings.
          3.Kynar: Color: As determined by the Architect from the Manufacturer's offerings.
          4.LEED Certified.
          5.Paint Finish Specified: To be factory applied and quality controlled by the awning manufacturer as the single source supplier of the awning.
 
          D.Fabrication:
          1.Factory welded and painted assemblies, prior to delivery.
          a.Not Acceptable: Field assembled frame components ("stick-built") using mechanical fasteners.
          2.Framing: Interlocking extruded or roll-formed panels, as selected by architect.
          ** NOTE TO SPECIFIER ** Delete plate options not required.
          3.Escutcheon Plates: Aluminum as detailed: 6 x 6 x 0.375 inches (152 x 152 x 9.5 mm).
          4.Escutcheon Plates: Aluminum as detailed: 8 x 8 x 0.375 inches (203 x 203 x 9.5 mm).
          5.Escutcheon Plates: Aluminum as detailed.
 
          PART 3EXECUTION
 
          3.1EXAMINATION
 
          A.Do not begin installation until the substrates have been properly constructed and prepared.
 
          B.If substrate preparation is the responsibility of another installer, notify Architect in writing of unsatisfactory preparation before proceeding.
 
          3.2PREPARATION
 
          A.Clean surfaces thoroughly prior to installation.
 
          B.Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions.
 
          3.3INSTALLATION
 
          A.Install in accordance with manufacturer's instructions, approved submittals, and in proper relationship with adjacent construction.
 
          3.4FIELD QUALITY CONTROL
 
          A.Field Inspection: Coordinate field inspection in accordance with appropriate sections in Division 01.
          ** NOTE TO SPECIFIER ** Include if manufacturer provides field quality control with onsite personnel for instruction or supervision of product installation, application, erection, or construction. Delete if not required.
 
          B.Manufacturer's Services: Coordinate manufacturer's services in accordance with appropriate sections in Division 01.
 
          3.5CLEANING AND PROTECTION
 
          A.Clean products in accordance with the manufacturers recommendations.
 
          B.Touch-up, repair or replace damaged products before Substantial Completion.
 
         
END OF SECTION