MasterFormat: 2020 Switch to 95
Download this Wood Treatment Specification for
WORD | WORD-Canadian | WP | RTF | TEXT
Find over 500 more construction specifications | Arcat.com
          TechWood by ChemTech Wood Treatment
 
         
SECTION 06 05 73
 
         
WOOD TREATEMENT
 
         
 
         
Copyright 2025 - 2025 ARCAT, Inc. - All rights reserved

          ** NOTE TO SPECIFIER ** TechWood; Factory applied wood protection treatment, Lumber Treatment, Softwood Protection, Plywood and OSB Sheathing Treatment, Factory Applied, Beams, Columns, Headers, Joists, Rafters, Chords and Webs of Trusses, I-Joist, Rim Boards, Wall Studs, Sill Plate, Fire Rating, Fire Retardant.
This section is based on the products of TechWood, located at:
7397 Commercial Circle
Fort Pierce, Florida 34954
Toll Free: () 835-9663 (833-TEKWOOD)
Email:
Treatment Inquiries: Connect@TechWoodTreatments.com
Architectural Inquiries: DesignPro@TechWoodTreatments.com
Web: www.techwoodtreatments.com
[Click Here] for additional information.
We are a company focused on the continuous development of wood treatment technology and solutions.
Our mission is to provide innovation and critical wood treatment solutions for the safer development of residential and commercial structures and those who utilize them. We are driven to lead the industry in safer material protection for long-term durability, cost-effectiveness and ownership peace of mind by meeting and exceeding existing building codes and practices.
TechWood is dedicated to developing new innovations in wood treatment processes, solutions and partnerships with like-minded organizations focused on a safer future and safer buildings. Working with builders, engineers, contractors and architectswe are paving the way for better, safer, more durable, and more efficient buildings.
 
          PART 1GENERAL
 
          1.1SECTION INCLUDES
          ** NOTE TO SPECIFIER ** Delete items below not required for project.
 
          A.Shop-Applied Wood Treatment.
 
          B.RELATED SECTIONS
          ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required.
          1.Section 01 61 16 - Volatile Organic Compound (VOC) Content Restrictions.
          2.Section 06 10 00 - Rough Carpentry.
          3.Section 06 12 19 - Structural Insulated Panels.
          4.Section 06 13 23 - Heavy Timber Framing.
          5.Section 06 15 00 - Wood Decking.
          6.Section 06 16 00 - Sheathing.
          7.Section 06 17 33 - Wood I-Joists
          8.Section 06 17 36 - Metal-Web Wood Joists.
          9.Section 06 17 53 - Shop-Fabricated Wood Trusses.
          10.Section 06 18 00 - Glued-Laminated Construction.
          11.Section 07 45 23 - Wood Siding.
 
          1.2REFERENCES
          ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited section.
 
          A.ASTM International (ASTM):
          1.ASTM D198 - Standard Test Methods of Static Tests of Lumber in Structural Sizes; 2022a.
          2.ASTM D3273 - Standard Test Method for Resistance to Growth of Mold on the Surface of Interior Coatings in an Environmental Chamber; 2021.
          3.ASTM D4587 - Standard Practice for Fluorescent UV-Condensation Exposures of Paint and Related Coatings; 2023.
          4.ASTM D5116 - Standard Guide for Small-Scale Environmental Chamber Determinations of Organic Emissions from Indoor Materials/Products; 2017.
          5.ASTM D5197 - Standard Test Method for Determination of Formaldehyde and Other Carbonyl Compounds in Air (Active Sampler Methodology); 2021.
          6.ASTM D5590 - Standard Test Method for Determining the Resistance of Paint Films and Related Coatings to Fungal Defacement by Accelerated Four-Week Agar Plate Assay; 2021.
          7.ASTM E84 - Standard Test Method for Surface Burning Characteristics of Building Materials; 2023d.
 
          B.American Wood Council (AWC):
          1.AWC NDS - National Design Specification (NDS) for Wood Construction; Most Recent Edition Adopted by Authority Having Jurisdiction, Including Applicable Amendments and Supplements.
 
          C.American Wood Protection Association (AWPA):
          1.AWPA E1 - Laboratory Methods for Evaluating the Termite Resistance of Wood-Based Materials: Choice and No-Choice Tests; 2023.
          2.AWPA E10 - Laboratory Method for Evaluating the Decay Resistance of Wood-Based Materials Against Pure Basidiomycete Cultures: Soil/Block Test; 2022.
          3.AWPA E12 - Standard Method of Determining Corrosion of Metal in Contact with Treated Wood; 2020.
          4.AWPA E21 - Standard Field Test for Evaluation of Wood Preservatives to be Used for Interior Applications (UC1 and UC2); Full-Size Commodity Termite Test; 2018 (R2024).
          5.AWPA M4 - Standard for the Handling, Storage, Field Fabrication and Field Treatment of Preservative-Treated Wood Products; 2023.
          6.AWPA U1 - Use Category System: User Specification for Treated Wood; 2024.
 
          D.International Code Council (ICC):
          1.International Building Code; 2021.
 
          E.International Organization for Standardization (ISO):
          1.ISO/IEC 17065 - Conformity Assessment - Requirements for Bodies Certifying Products, Processes and Services, 2012.
 
          F.National Fire Protection Association (NFPA):
          1.NFPA 255 - Standard Method of Test of Surface Burning Characteristics of Building Materials; 2006.
 
          G.National Institute of Standards and Technology (NIST):
          1.Doc PS 1 - Structural Plywood.
          2.Doc PS 2 - Performance Standard for Wood-based Structural-use Panels.
 
          H.Underwriters Laboratories (UL):
          1.UL 723 - Test for Surface Burning Characteristics of Building Materials; 2023.
          2.UL 2818 - GREENGUARD Certification Program For Chemical Emissions For Building Materials, Finishes And Furnishings; 2022.
 
          I.Uniform Building Code (UBC):
          1.Fire-Resistive Standards for Fire Protection; Current Edition.
 
          1.3SUBMITTALS
 
          A.Submit under provisions of Section 01 30 00, Administrative Requirements.
 
          B.Product Data:
          1.Manufacturer's data sheets for each product.
          2.Preparation instructions and recommendations.
          3.Storage and handling requirements and recommendations.
          4.Typical installation methods.
          5.Maintenance data.
 
          C.Applicators qualification statement.
 
          D.Warranty: Submit manufacturer warranty and ensure that forms are completed in Owner's name and registered with the manufacturer.
 
          1.4QUALITY ASSURANCE
 
          A.Applicator Qualifications: Company specializing in performing Work of this section with minimum 2-years of documented experience with projects of similar scope and complexity and licensed by manufacturer.
 
          1.5DELIVERY, STORAGE, AND HANDLING
 
          A.Store and handle materials in strict compliance with manufacturer's written instructions and recommendations.
 
          B.Protect from damage due to weather, moisture, excessive temperature, and construction operations.
 
          C.Cover wood products to protect against moisture.
 
          D.Support stacked products to prevent deformation and to allow air circulation.
 
          E.Fire Retardant Treated Wood: Prevent exposure to precipitation during shipping, storage, and installation.
 
          1.6PROJECT CONDITIONS
 
          A.Maintain environmental conditions including temperature, humidity, and ventilation within limits recommended by the manufacturer for optimum results. Do not install products under environmental conditions outside of manufacturer's recommended limits.
 
          1.7WARRANTY
 
          A.See Section 01 78 00, Closeout Submittals for additional requirements.
 
          B.Manufacturer's standard 20-year limited warranty.
 
          PART 2PRODUCTS
 
          2.1MANUFACTURERS
 
          A.Acceptable Manufacturer: TechWood by ChemTech, which is located at:
7397 Commercial Cir.
Fort Pierce, FL 34954
Toll Free Tel: 833-835-9663 (833-TEKWOOD)
Email: request info (DesignPro@TechWoodTreatments.com);Web: https://techwoodtreatments.com
          1.Email for Treatment Inquiries: Connect@TechWoodTreatments.com.
          2.Email for Architectural Inquiries: DesignPro@TechWoodTreatments.com
          3.Web: www.techwoodtreatments.com.
          ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions.
 
          B.Substitutions: Not permitted.
 
          C.Requests for substitutions will be considered in accordance with the provisions of Division 01.
          ** NOTE TO SPECIFIER ** Delete articles not required.
 
          2.2PRODUCT TYPES
 
          A.Basis-of-Design: TechWood 2200; www.techwoodtreatments.com.
          1.Factory applied wood protection treatment for treating solid sawn, plywood, OSB, and engineered wood products used for floor, roof, and wall structural members.
          a.Structural Applications:
          1)Beams.
          2)Columns.
          3)Headers.
          4)Joists.
          5)Rafters.
          6)Chords and Webs of Trusses.
          7)I-joist flanges.
          8)Rim Boards.
          9)Wall Studs.
          2.Use as sill plates in direct contact with concrete or masonry is allowed.
          3.Duration of Load Increase: in accordance with the Authorities Having Jurisdiction but no greater than 1.6.
          4.Application: Above ground applications not subject to contact with water.
          a.Interior.
          b.Exterior:
          1)Protect from direct wetting.
          2)Flashing required for exterior applications.
          3)Primer and a minimum of two finish coats are required for exterior applications.
          a)Primer:
          1)Manufacturer: [_________].
          2)Product: [_________].
          b)Finish Coat:
          1)Manufacturer: [_________].
          2)Product: [_________].
          5.Color: [_____].
          6.Use Category:
          a.UC1 Interior/Dry Construction: Millwork and Finishing
          b.UC2 Interior/Damp Construction: Interior beams, timbers, flooring, framing, millwork, and sill plates.
          c.UC3a Exterior siding and trim.
          7.Connections: Lateral loads for nails, screws, and bolts, and withdrawal loads for nails and screws in accordance with NDS using species specific gravity.
          8.Fasteners:
          a.In accordance with IBC 2304.10.5.
          b.Aluminum fasteners are permitted in interior applications.
          c.Plain carbon steel fasteners including nuts and washers are permitted in SBX/DOT and zinc borate preservative-treated wood in an interior, dry environment.
 
          B.Basis-of-Design: TechWood 2200EX; www.techwoodtreatments.com.
          1.Factory applied wood protection treatment and water repellant additive for use including but not limited to fence pickets installed vertically.
          2.Duration of Load Increase: in accordance with the Authorities Having Jurisdiction but no greater than 1.6.
          3.Material Use:
          a.Southern Pine.
          b.Spruce Pine Fir.
          c.Hem-Fir.
          d.Douglas-Fir.
          4.Application:
          a.Interior.
          b.Exterior:
          1)Above ground UC3a and UC3b application exposed to all weather cycles, including intermittent wetting and in direct contact with concrete or masonry is allowed.
          5.Color: [_____].
          6.Use Category:
          a.UC1, Interior/Dry Construction: Millwork and Finishing
          b.UC2, Interior/Damp Construction: Interior beams, timbers, flooring, framing, millwork, and sill plates.
          c.UC3a, Above Ground Exterior Protected: Coated millwork, siding, fence pickets, and trim in a vertical state.
          7.Connections: Lateral loads for nails, screws, and bolts, and withdrawal loads for nails and screws in accordance with NDS using species specific gravity.
          8.Fasteners:
          a.In accordance with IBC 2304.10.5.
          b.Stainless steel.
          c.Aluminum.
          d.Hot-dipped galvanized.
          e.Electro-galvanized.
 
          C.Basis-of-Design: TechWood 3300; www.techwoodtreatments.com.
          1.Factory-applied wood protection treatment and fire-retardant additive for treating wood members including solid sawn wood and engineered wood products used as floor, roof, and wall structural members.
          a.Structural Applications:
          1)Structural Panels including OSB and Plywood.
          2)Beams.
          3)Columns.
          4)Headers.
          5)Joists.
          6)Rafters.
          7)Chords and Webs of Trusses.
          8)I-joist flanges.
          9)Rim Boards.
          10)Wall Studs.
          2.Extended Fire Rating: Class A, ASTM E84.
          3.Use as sill plates in direct contact with concrete or masonry is allowed.
          4.Duration of Load Increase: in accordance with the Authorities Having Jurisdiction but no greater than 1.6.
          5.Material Use:
          a.Kiln Dried or Green Dimensional Lumber up to 30 percent Moisture Content:
          1)Southern Pine.
          2)Spruce Pine Fir.
          3)Hem-Fir.
          4)Douglas-Fir.
          b.Laminated Veneer Lumber.
          c.Glued Laminated Beams.
          d.Parallel strand Lumber.
          e.Oriented Strand Board Rim Board.
          f.Plywood Complying with PS1.
          g.OSB Complying with PS2.
          6.Application: Above ground applications not subject to contact with water.
          a.Interior.
          b.Exterior:
          1)Protect from direct wetting.
          2)Flashing required for exterior applications.
          3)Primer and a minimum of two finish coats are required for exterior applications.
          a)Primer:
          1)Manufacturer: [_________].
          2)Product: [_________].
          b)Finish Coat:
          1)Manufacturer: [_________].
          2)Product: [_________].
          7.Color: [_____].
          8.Use Category:
          a.UC1, Interior/Dry Construction: Millwork and Finishing
          b.UC2, Interior/Damp Construction: Interior beams, timbers, flooring, framing, millwork, and sill plates.
          c.UC3a, Above Ground Exterior Protected: Treated millwork, siding, fence pickets, and trim in a vertical state.
          9.Connections: Lateral loads for nails, screws, and bolts, and withdrawal loads for nails and screws in accordance with NDS using species specific gravity.
          10.Fasteners:
          a.In accordance with IBC 2304.10.5.
          b.Aluminum fasteners are permitted in interior applications.
          c.Plain carbon steel fasteners including nuts and washers are permitted in SBX/DOT and zinc borate preservative-treated wood in an interior, dry environment.
 
          D.Basis-of-Design: TechWood 4400; www.techwoodtreatments.com.
          1.Factory-applied wood protection treatment and fire-retardant additive for treating wood members including solid sawn lumber used as floor, roof, and wall structural members.
          a.Structural Applications:
          1)Beams.
          2)Columns.
          3)Headers.
          4)Joists.
          5)Rafters.
          6)Chords and Webs of Trusses.
          7)Wall Studs.
          2.Flame Spread Index: 15.
          3.Smoke Developed Index: 10.
          4.Use as sill plates in direct contact with concrete or masonry is allowed.
          5.Duration of Load Increase: in accordance with the Authorities Having Jurisdiction but no greater than 1.6.
          6.Material Use:
          a.Kiln Dried or Green Dimensional Lumber up to 30 percent Moisture Content:
          1)Southern Pine.
          2)Spruce Pine Fir.
          3)Hem-Fir.
          4)Douglas-Fir.
          b.Glued Laminated Beams Manufactured from Douglas-Fir.
          c.Southern Pine Plywood.
          7.Application: Above ground applications not subject to contact with water.
          a.Interior.
          b.Exterior:
          1)Protect from direct wetting.
          2)Flashing required for exterior applications.
          3)Primer and a minimum of two finish coats are required for exterior applications.
          a)Primer:
          1)Manufacturer: [_________].
          2)Product: [_________].
          b)Finish Coat:
          1)Manufacturer: [_________].
          2)Product: [_________].
          8.Color: [_____].
          9.Use Category:
          a.UC1, Interior/Dry Construction: Millwork and Finishing
          b.UC2, Interior/Damp Construction: Interior beams, timbers, flooring, framing, millwork, and sill plates.
          c.UC3a, Above Ground Exterior Protected: Coated millwork, siding, fence pickets, and trim in a vertical state.
          10.Connections: Lateral loads for nails, screws, and bolts, and withdrawal loads for nails and screws in accordance with NDS using species specific gravity.
          11.Fasteners:
          a.In accordance with IBC 2304.10.5.
          b.Aluminum fasteners are permitted in interior applications.
          c.Plain carbon steel fasteners including nuts and washers are permitted in SBX/DOT and zinc borate preservative-treated wood in an interior, dry environment.
 
          PART 3EXECUTION
 
          3.1EXAMINATION
 
          A.Remove dust, dirt and other contaminants from treatment surfaces.
 
          B.Remove tarpaulins, drop cloths, strippable protection films and other items prior to treatment of materials.
 
          C.Do not begin installation until substrates or adjoining construction is properly prepared and constructed.
 
          D.If substrate preparation is the responsibility of another installer, notify Architect in writing of unsatisfactory preparation before proceeding.
 
          3.2PREPARATION
 
          A.Clean surfaces thoroughly prior to treatment.
 
          B.Prepare surfaces using methods recommended in writing by the manufacturer.
 
          3.3INSTALLATION
 
          A.Comply with manufacturer's written instructions and approved submittals.
 
          B.Treat field cuts, notches, or bored holes in accordance with manufacturer's written instructions and AWPA M4.
 
          3.4FIELD QUALITY CONTROL
 
          A.Field Inspection: Coordinate field inspection in accordance with appropriate sections in Division 01.
          ** NOTE TO SPECIFIER ** Include if manufacturer provides field quality control with onsite personnel for instruction or supervision of product installation, application, erection, or construction. Delete if not required.
 
          B.Manufacturer's Services: Coordinate manufacturer's services in accordance with appropriate sections in Division 01.
 
          3.5CLEANING AND PROTECTION
 
          A.Clean products in accordance with the manufacturer's written recommendations.
 
          B.Touch-up, repair or replace damaged products prior to Substantial Completion.
 
         
END OF SECTION