SECTION 06 73 00 COMPOSITE DECKING AND RAILINGS Copyright 2019 - 2021 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** Trex Railing and Decking; composite decking and railings. This section is based on the products of Trex Railing and Decking, which is located at: 160 Exeter Dr. Winchester, VA 22603-8605 Tel: (540) 542-6300 Fax: (540) 542-6890 Email: marketing@trex.com Web: http://www.trex.com [ https://arcat.com/company/trex-company-incorporated-36113 ] for additional information. Since 1996 Trex has invented, defined and perfected the composite deck category, becoming the world's largest manufacturer of wood-alternative decking products. Never content to settle, we continue to make strides in outdoor engineering, melding innovation with environmental responsibility and beautiful form with powerful function. Formed in 1996 through the buyout of a division of Mobil Corporation, our company went public in 1999. Today we offer the industry's widest array of high-performance composite products, which are available in more than 42 countries around the world. With the largest market share of composite decking in North America, a growing international footprint and more than $740,000,000 in annual sales, we lead the industry on a global scale. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for project. A. Composite Decking (Trex Transcend and Trex Enhance). B. Composite Decking (Trex Select). C. Composite Railing (Trex Transcend and Select). 1.2 RELATED SECTIONS ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required. A. Section 05 73 05 - Decorative Stainless Steel Railings. (Trex) B. Section 06 11 16 - Mechanically Graded Lumber. C. Section 05 40 00 - Cold-Formed Metal Framing. 1.3 REFERENCES ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited section. A. ASTM International (ASTM): 1. ASTM D1037: Water Absorption of Plastics. 2. ASTM D1761: Mechanical Fasteners in Wood. 3. ASTM D1413: Test method for Wood Preservatives by Laboratory Soil-block Cultures. 4. ASTM D7031: Standard Guide for Evaluating Mechanical and Physical Properties of Wood-Plastic Composite Products, ASTM International. 5. ASTM D7032: Standard Specification for Establishing Performance Ratings for Wood-Plastic Composite Deck Boards and Guardrail Systems (Guards or Handrails). 6. ASTM E84: Test Method for Surface Burning Characteristics of Building Materials, ASTM International. B. Code Reports: 1. Nationally Recognized Testing Facilities: a. Intertek: 1) CCRR-0301 Trex Enhance Basic and Naturals Decking. 2) CCRR-0132 Transcend, Enhance, and Select Railing. b. ICC Evaluation Services: 1) ESR-3168 Trex Transcend and Select Decking. 2) ESR-3947 Trex Transcend and Select Railing. 1.4 SUBMITTALS A. Submit under provisions of Section 01 30 00 - Administrative Requirements. B. Product Data: Manufacturer's data sheets on each product to be used, including: 1. Preparation instructions and recommendations. 2. Storage and handling requirements and recommendations. 3. Installation methods. C. Shop Drawings: 1. Provide plans and details which include layout, spacing, and sizes of decking and railings. ** NOTE TO SPECIFIER ** Delete selection samples if colors have already been selected. D. Selection Samples: For each finish product specified, two complete sets of color chips representing manufacturer's full range of available colors and patterns. E. Verification Samples: For each finish product specified, two samples, representing actual product color, size, and finish. 1.5 QUALITY ASSURANCE A. Manufacturer Qualifications: Minimum 5 year experience manufacturing similar products. B. Installer Qualifications: Minimum 2 year experience installing similar products. ** NOTE TO SPECIFIER ** Include a mock-up if the project size and/or quality warrant taking such a precaution. The following is one example of how a mock-up on a large project might be specified. When deciding on the extent of the mock-up, consider all the major different types of work on the project. C. Mock-Up: Provide a mock-up for evaluation of surface preparation techniques and application workmanship. 1. Finish areas designated by Architect. 2. Do not proceed with remaining work until workmanship is approved by Architect. 3. Refinish mock-up area as required to produce acceptable work. 1.6 PRE-INSTALLATION MEETINGS A. Convene minimum two weeks prior to starting work of this section. 1.7 DELIVERY, STORAGE, AND HANDLING A. Deliver and store products in manufacturer's unopened packaging bearing the brand name and manufacturer's identification until ready for installation. B. Store products on a flat and level surface. Adjust support blocks accordingly. C. Support bundles on supplied dunnage. D. When stacking bundles, supports should start approximately 8 inches from each end and be spaced approximately 2 feet on center. Supports shall line up vertically/perpendicular to the decking product. E. Do not stack Transcend decking more than 14 bundles. Do not stack Select or Enhance decking more than 12 bundles. F. Keep material covered using the provided bundle cover until time of installation. G. Handle materials to avoid damage. 1.8 PROJECT CONDITIONS A. Maintain environmental conditions (temperature, humidity, and ventilation) within limits recommended by manufacturer for optimum results. Do not install products under environmental conditions outside manufacturer's recommended limits. 1.9 SEQUENCING A. Ensure that products of this section are supplied to affected trades in time to prevent interruption of construction progress. 1.10 WARRANTY A. Provide manufactures warranty against rot, decay, splitting, checking, splintering, fungal damage, and termite damage for a period of 25 years for a residential installation and 10 years for a commercial installation. In addition provide the Trex Fade and Stain Warranty against food staining and fading beyond 5 Delta E (CIE units) for a period of 25 years for a residential installation and 10 years for a commercial installation. PART 2 PRODUCTS 2.1 MANUFACTURERS A. Acceptable Manufacturer: Trex Railing and Decking; 160 Exeter Dr., Winchester, VA 22603-8605. Tel: (540) 542-6300. Fax: (540) 542-6890. Email: marketing@trex.com Web: http://www.trex.com. ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions. B. Substitutions: Not permitted. C. Requests for substitutions will be considered in accordance with provisions of Section 01 60 00 - Product Requirements. 2.2 Design/Performance Requirements: A. Structural Performance: 1. Deck: Uniform Load - 100lbf/sq.ft. 2. Tread of Stairs: Concentrated Load: 750 lbf on area of 4 sq. in., and 1/8 inch maximum deflection at a concentrated load of 300 lbf. 3. Railing: Trex Railing Systems meet various IRC and IBC requirements. Consult the label and published code evaluation reports for the performance levels of each system. B. Fire-Surface Burning Characteristics per ASTM E-84. ** NOTE TO SPECIFIER ** Delete if not required. 2.3 COMPOSITE DECKING A. Wood-Plastic Composite Lumber: ** NOTE TO SPECIFIER ** With Trex's flagship Transcend(r) decking you can pair elevated aesthetics with the highest level of performance. Ten premium tropical and monochromatic shades - Island Mist, Tiki Torch, Havana Gold, Spiced Rum, Lava Rock, Gravel Path, Rope Swing, Vintage Lantern - feature high-definition grain patterns and 25-Year Limited General and Fade & Stain warranties. Transcend combines second-to-none performance and hassle-free maintenance with the beauty of exotic teak and ipe. Unlike wood, this low-maintenance composite decking line never needs sanding, staining, sealing or painting and cleans up easily with just soap and water. Transcend, like all of the Trex decking collections, is made from 95% recycled material, including reclaimed wood fiber and plastic film. Delete if not required. 1. Product: Trex Transcend Decking Boards as manufactured by Trex Railing and Decking. 2. Material Description: Composite Decking consisting of recycled Linear Low Density Polyethylene (LLDPE) and recycled wood. The product is extruded into shapes and sizes as follows: a. Width: 1 inch x 5.5 inches (25 mm x 140 mm). b. Lengths - 12 feet (3658 mm) 16 feet (4877 mm), and 20 feet (6096 mm). c. Color - To be specified by owner from Trex' standard list of colors. 3. Physical and Mechanical Properties as follows: a. Flame Spread, ASTM E 84: 70. b. Thermal Expansion, ASTM D 1037: 0.000019 inch/inch/degree F. c. Moisture Absorption, ASTM D 1037: Less than 1percent. d. Screw Withdrawal, ASTM D1761: 588 lbs/in. e. Fungus Resistance, ASTM D1413: Rating - no decay. f. Termite Resistance, AWPAE1-72: Rating: 9.6. g. Compression Parallel, ASTM D198: 1588 psi ultimate, 540 psi design. h. Compression Perpendicular, ASTM D143: 1437 psi ultimate, 540 psi design. i. Bending Strength, ASTM D198: 3280 psi ultimate, 500 psi design. j. Shear Strength, ASTM D143: 1761 psi ultimate, 360 psi design. k. Modulus of Elasticity, ASTM D4761: 412,000 psi ultimate, 200,000 psi design. l. Modulus of Rupture, ASTM D4761: 3280 psi ultimate, 500 psi design. m. Ultimate strength values are not meant for design analysis. Design values are for temperatures up to 125 degree F (52 degree C). ** NOTE TO SPECIFIER ** Trex Enhance(r) decking is comprised of two color collections - Basics and Naturals. Enhance Naturals come in five contemporary, multi-tonal hues that resemble the streaked looks of natural wood. Foggy Wharf, Rocky Harbor, Toasted Sand, and Coastal Bluff feature the authentic charm and color variations of wood, without the hassles of ongoing maintenance and upkeep. Enhance Basics boards are offered in three proven and popular monochromatic shades, Clam Shell, Beach Dune and Saddle. Enhance boards are also made from more than 95% recycled material and are backed by Trex's 25-year Limited General and Fade & Stain warranties. B. Wood-Plastic Composite Lumber 1. Product: Trex Enhance Decking Boards as manufactured by Trex Railing and Decking. 2. Material Description: Composite Decking consisting of recycled Linear Low Density Polyethylene (LLDPE) and recycled wood. The product is extruded into shapes and sizes as follows: a. Width: 1 inch x 5.5 inches (25 mm x 140 mm). b. Lengths - 12 feet (3658 mm) 16 feet (4877 mm), and 20 feet (6096 mm). c. Color - To be specified by owner from Trex' standard list of colors. 3. Physical and Mechanical Properties as follows: a. Flame Spread, ASTM E 84: 125 b. Thermal Expansion, ASTM D 1037: 0.000019 inch/inch/degree F. c. Moisture Absorption, ASTM D 1037: Less than 1 percent. d. Screw Withdrawal, ASTM D1761: 588 lbs/in. e. Fungus Resistance, ASTM D1413: Rating - no decay. f. Termite Resistance, AWPAE1-72: Rating: 9.6. g. Compression Parallel, ASTM D198: 1588 psi ultimate, 540 psi design. h. Compression Perpendicular, ASTM D143: 1437 psi ultimate, 540 psi design. i. Bending Strength, ASTM D198: 3280 psi ultimate, 500 psi design. j. Shear Strength, ASTM D143: 1761 psi ultimate, 360 psi design. k. Modulus of Elasticity, ASTM D4761: 412,000psi ultimate, 200,000 psi design. l. Modulus of Rupture, ASTM D4761: 3280 psi ultimate, 500 psi design. m. Ultimate strength values are not meant for design analysis. Design values are for temperatures up to 125-degree F (52-degree C). ** NOTE TO SPECIFIER ** Trex Select(r) decking is the perfect combination of price, minimal maintenance and design flexibility. This collection features our high-performance shell technology and a solid profile that allows the boards to be shaped for one-of-a-kind curved deck designs. The boards also can be incorporated into Trex railing to create a convenient cocktail/beverage rail. Select is available in five nature-inspired colors, including Madeira, Pebble Grey, Winchester Grey, Saddle and Woodland Brown - all backed by Trex's 25-year Limited General and Fade & Stain warranties. Select is also made from more than 95% recycled material. Delete if not required. C. Wood-Plastic Composite Lumber: 1. Product: Select as manufactured by Trex Railing and Decking. 2. Pattern: Consistent patterns board to board reveal a flawless finish. 3. Material Description: Composite Decking consisting of recycled Linear Low Density Polyethylene (LLDPE) and recycled wood. The product is extruded into shapes and sizes as follows: a. Trex Select Decking Boards; 0.875 inches x 5.5 inches (22 mm x 140 mm). b. Lengths - 12 feet (3658 mm) 16 feet (4877 mm), and 20 feet (6096 mm). c. Color - To be specified by owner from Trex' standard list of colors. 4. Physical and Mechanical Properties as follows: a. Flame Spread, ASTM E 84: 70. b. Thermal Expansion, ASTM D 1037: 0.000019 inch/inch/degree F. c. Moisture Absorption, ASTM D 1037: Less than 1.2 percent. d. Screw Withdrawal, ASTM D1761: 388 lbs/in. e. Fungus Resistance, ASTM D1413: Rating - no decay. f. Termite Resistance, AWPAE1-72: Rating: 9.7. g. Compression Parallel, ASTM D198: 1588 psi ultimate, 540 psi design. h. Compression Perpendicular, ASTM D143: 1437 psi ultimate, 540 psi design. i. Bending Strength, ASTM D198: 3280 psi ultimate, 500 psi design. j. Shear Strength, ASTM D143: 1761 psi ultimate, 360 psi design. k. Modulus of Elasticity, ASTM D4761: 412,000psi ultimate, 200,000 psi design. l. Modulus of Rupture, ASTM D4761: 3280 psi ultimate, 500 psi design. m. Ultimate strength values are not meant for design analysis. Design values are for temperatures up to 125 degree F (52 degree C). ** NOTE TO SPECIFIER ** When it comes to finishing the sides of your deck, nothing beats the beauty, durability and low maintenance of high-performance Trex Fascia and stair risers now available to match every one of our Trex decking lines, and for the first time ever, a go-with-anything high-performance white. Delete if not required. D. Fascia Boards 1. Product: Trex Fascia. ** NOTE TO SPECIFIER ** When it comes to building stairs for your deck, sometimes it's best to stray from the straight and narrow. Whether confronted with tight quarters or conflicting styles, you may require stairs that are a little less conventional. That's why we're introducing the next step in elevated living: the spatially efficient and customizable Trex(R) Spiral Stairs(TM) system. Engineered with the same combination of durability and ease that makes us the world's #1 decking brand, Trex Spiral Stairs offer all of the space-saving advantages of traditional spiral staircases with Trex signature style, strength and simplicity. And with a range of design options like two material choices and custom, high-performance composite treads the Trex Spiral Stairs system is the ultimate staircase alternative. Space Saving and Stylish; Aluminum Powder-Coated or Galvanized Options; Available in All Trex Transcend Colors; Optional Trex Boards and Trex Lighting; Easy to Install; 25-year Limited Warranty. Delete if not required. E. Stairs: 1. Product: Spiral Stairs(tm) system as manufactured by Trex Railing and Decking. ** NOTE TO SPECIFIER ** Explore our decking colors and put your imagination to work. Delete if not required. Colors are available in all three composite deck boards: TrexSelect (Good), TrexEnhance (Better), TrexTranscend. Delete color nor required. F. Composite Decking Color: ** NOTE TO SPECIFIER ** Greys palette. Delete if not required. 1. Color: Gravel Path; (Transcend Earth Tones). 2. Color: Pebble Grey (Select). 3. Color: Island Mist (Transcend Tropicals). 4. Color: Clam Shell (Enhance Basics). 5. Color: Winchester Grey (Select). 6. Color: Foggy Wharf (Enhance Naturals). 7. Color: Rocky Harbor (Enhance Naturals). ** NOTE TO SPECIFIER ** Browns palette. Delete if not required. 8. Color: Rope Swing (Transcend Earth Tones). 9. Color: Beach Dune (Enhance Basics). 10. Color: Saddle (Enhance Basics). 11. Color: Saddle (Select). 12. Color: Tiki Torch (Transcend Tropicals). 13. Color: Havana Gold (Transcend Tropicals). 14. Color: Spiced Rum (Transcend Tropicals). 15. Color: Toasted Sand (Enhance Naturals). 16. Color: Coastal Bluff (Enhance Naturals). 17. Color: Woodland Brown (Select). 18. Color: Vintage Lantern (Transcend Earth Tones). ** NOTE TO SPECIFIER ** Reds palette. Delete if not required. 19. Color: Madeira (Select). 20. Color: Lava Rock (Transcend Tropicals). ** NOTE TO SPECIFIER ** Everything you need to get busy building - from fasteners to saw blades - features Trex-grade engineering. Delete if not required. G. Accessory Hardware: 1. Fasteners: a. Trex Universal Hideaway Hidden Fasteners. See - http://s7d4.scene7.com/is/content/Trex/Installation%20Guide%202013pdf for the updated recommendations on fasteners. b. Composite Decking Screws: 1) Refer to Trex.com for recommended composite screws. ** NOTE TO SPECIFIER ** Delete if not required. 2.4 DECK RAILING A. Composite Railing: ** NOTE TO SPECIFIER ** Composite boards and railing take this outside space beyond the ordinary. Our highest-performance railing option offers more colors in more component profiles than any railing out there. Won't rot, warp, peel or splinter (which trumps sanding row after row of wooden balusters any day) and it never needs painting or staining, ever. Talk about luxurious. Delete if not required. 1. Product: a. Transcend Railing as manufactured by Trex Railing and Decking. b. Select Railing as manufactured by Trex Railing and Decking. The Trex ADA-Compliant Handrail system is designed to seamlessly blend with all Trex railing options, offering an extra level of safety, strength and accessibility for any deck design. Available in three colors - Charcoal Black, Bronze and Classic White - this heavy-duty aluminum system features a full complement of components to accommodate easy installation. Made with a high-quality powder-coated finish to meet AAMA-2604 test compliant, our components resist fading, chipping and corrosion. Wall mounts and wall returns include fasteners for both wood post and aluminum post installations. Aluminum collars hide railing seams for a smooth transition between components, and aluminum cap ends conceal open rail ends. B. ADA-Compliant Handrail as manufactured by Trex Railing and Decking. ** NOTE TO SPECIFIER ** Trex post sleeves, post sleeve caps and post sleeve skirts are the hub of all our railing lines and are available in our seven Transcend railing colors. Meaning you can pair these universal components with components from every other Trex railing line for countless ways to achieve your unique vision. All high-performance. All low maintenance. Any which way you like. Delete if not required. C. Railing Post Components: 1. Product: Post sleeves, post sleeve caps, post sleeve skirts. ** NOTE TO SPECIFIER ** Delete if not required. 2.5 DECK DRAINAGE SYSTEMS ** NOTE TO SPECIFIER ** Trex RainEscape is a unique under-deck drainage system network of troughs and gutters keeps rain, spills and snow melt from dripping through elevated deck boards, creating a dry patio area on the ground level below. It can even be installed on an existing deck by removing the flooring before installation. Once the Trex RainEscape deck drainage system is installed, utilities can be added then covered with the soffit or ceiling of your choice. Delete if not required. A. Under-Deck Drainage System: 1. Product: Trex RainEscape as manufactured by Trex Railing and Decking. ** NOTE TO SPECIFIER ** In our survey of deck builders, we learned that 98% of 8-10 year-old decks have splitting, rotting and decay. For the $8,000 to $10,000 price of the average deck*, wouldn't it be wise to spend a few extra dollars to protect the life of your deck? Trex Protect acts as a moisture barrier between wood and galvanized metal, helping screws hold longer and stronger so you get the full life out of your deck. Delete if not required. B. Moisture Barrier: 1. Product: Trex Protect Tape as manufactured by Trex Railing and Decking. ** NOTE TO SPECIFIER ** Delete if not required. 2.6 OUTSIDE LIGHTING ** NOTE TO SPECIFIER ** Get the right mood right under the moonlight with our sophisticated deck lights. Easy to build into a new or existing deck, Trex Deck Lighting is even easier to set up with the Trex LightHub connection system. To take the look up another notch, try the optional timer and dimmer for total lighting control. Whether safely illuminating your stairways with LED step lights or proudly highlighting the perimeter of your domain with deck post lighting, our lights offers a long-lasting glow that never fails to match the beauty of a Trex deck. Delete if not required. A. Product: Trex Outdoor Lighting as manufactured by Trex Railing and Decking. PART 3 EXECUTION 3.1 EXAMINATION A. Do not begin installation until substrates have been properly prepared. B. If substrate preparation is the responsibility of another installer, notify Architect of unsatisfactory preparation before proceeding. 3.2 PREPARATION A. Clean surfaces thoroughly prior to installation. B. Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions. 3.3 INSTALLATION ** NOTE TO SPECIFIER ** Click on "Trex Decking 2021 Installation Guide" link to download the guide. A. Install in accordance with manufacturer's instructions, approved submittals, and in proper relationship with adjacent construction. B. Cut, drill, and rout using carbide tipped blades. C. Do not use composite wood material for structural applications. 3.4 Cleaning ** NOTE TO SPECIFIER ** Click on "Trex 2020 Full Installation Guide" link to download the guide. A. Cleaning as required by manufacturer for warranty compliance. 3.5 PROTECTION A. Protect installed products until completion of project. B. Touch-up, repair or replace damaged products before Substantial Completion. END OF SECTION DISCLAIMER: Trex Company, Inc. Guide Specifications have been written as an aid to the professionally qualified Specifier and Design Professional. The use of this Guideline Specification requires the sole professional judgment and expertise of the qualified Specifier and Design Professional to adapt the information to the specific needs for the Building Owner and the Project, to coordinate with their Construction Document Process, and to meet all the applicable building codes, regulations and laws.