SECTION 11 23 00 COMMERCIAL LAUNDRY EQUIPMENT Copyright 2004 - 2025 ARCAT, Inc. - All rights reserved ** NOTE TO SPECIFIER ** UniMac/Alliance Laundry Systems; heavy-duty industrial laundry equipment. This section is based on the products of UniMac/Alliance Laundry Systems, which is located at: Shepard St. P. O. Box 990 Ripon, WI 54971-0990 Tel: 800-587-5458 Fax: 920-748-1664 Email: leads@alliancels.com Web: https://www.unimac.com [Click Here] for more information. UniMac provides a full line of heavy-duty industrial equipment for the laundry industry. As key players in the success of on-premises laundry facilities, UniMac laundry equipment continuously achieves high levels of efficiency, quality, and durability. PART 1 GENERAL 1.1 SECTION INCLUDES ** NOTE TO SPECIFIER ** Delete items below not required for project. A. Washer extractors. B. Drying tumblers. C. Automatic drying cabinets. D. Fireman's personal protection equipment (PPE) drying cabinet. 1.2 RELATED SECTIONS ** NOTE TO SPECIFIER ** Delete any sections below not relevant to this project; add others as required. A. Section 03 30 00 - Cast-in-Place Concrete. B. Section 05 50 00 - Metal Fabrications. C. Division 23 Sections for supply and exhaust fans; exhaust ductwork; service roughing-ins; drain traps; valves, pipes, and fittings; and other materials required to complete commercial laundry equipment installation. D. Division 26 Sections for wiring disconnect switches, and other electrical materials required to complete commercial laundry equipment installation. 1.3 REFERENCES ** NOTE TO SPECIFIER ** Delete references from the list below that are not actually required by the text of the edited section. A. UL Certification: Provide electric equipment and components that are evaluated by UL for fire, and electric shock according to applicable safety standards and that are UL certified for compliance and labeled for intended use. 1.4 SUBMITTALS A. Submit under provisions of Section 01 30 00 - Administrative Requirements. B. Product Data: Manufacturer's data sheets on each product to be used, including: 1. Preparation instructions and recommendations. 2. Storage and handling requirements and recommendations. C. Shop Drawings: Include plans, elevations, sections, roughing-in dimensions, fabrication details, utility service requirements, and attachments to other work. D. Coordination Drawings: Indicate locations of laundry equipment and connections to utilities, and clearance requirements for equipment access and maintenance. E. Operation and Maintenance Data: For laundry equipment to include in emergency, operation, and maintenance manuals. Include a schedule with the following: 1. Designation indicated on Drawings. 2. Manufacturer's name and model number. 3. List of factory-authorized service agencies including their addresses and telephone numbers. 1.5 DELIVERY, STORAGE, AND HANDLING A. Store equipment on site protected from weather, direct sunlight and temperature extremes. Do not remove packaging prior to storage. B. Consult manufacturer if machines are to be stored for an extended period of time. 1.6 PROJECT CONDITIONS A. Maintain environmental conditions (temperature, humidity, and ventilation) within limits recommended by manufacturer for optimum results. Do not install products under environmental conditions outside manufacturer's absolute limits. 1.7 WARRANTY ** NOTE TO SPECIFIER ** Delete the first two paragraphs following if washer extractors are not required. Delete the third paragraph following if dryer tumblers are not required. A. Washer Extractor Parts Only: Manufacturer's standard form in which manufacturer agrees to repair or replace any part of the equipment assembly that fails within specified warranty period. 1. Warranty Period: Three years from date of Substantial Completion. B. Washer Extractor Parts Only, Mainframe, Cylinder Shaft Assembly, and Bearings Warranty: Manufacturer's standard form in which manufacturer agrees to repair or replace main frame, bearing, cylinder or cylinder shaft assembly that fails within specified warranty period. 1. Warranty Period: Five years from date of Substantial Completion. C. Dryer Tumbler Parts Only: Manufacturer's standard form in which manufacturer agrees to repair or replace any part of the equipment assembly that fails within specified warranty period. 1. Warranty Period: Three years from date of Substantial Completion. D. Automatic Drying Cabinets Parts Only: Manufacturer's standard form in which manufacturer agrees to repair or replace any part of the equipment assembly that fails within specified warranty period. 1. Warranty Period: Three years from date of Substantial Completion. PART 2 PRODUCTS 2.1 MANUFACTURERS A. Acceptable Manufacturer: UniMac, which is located at: Shepard St., P. O. Box 990 Ripon, WI 54971-0990 Toll Free Tel: 800-587-5458 Fax: 920-748-1664 Email: request info (franchella.ales@alliancels.com);Web: http://www.unimac.com ** NOTE TO SPECIFIER ** Delete one of the following two paragraphs; coordinate with requirements of Division 1 section on product options and substitutions. B. Substitutions: Not permitted. C. Requests for substitutions will be considered in accordance with provisions of Section 01 60 00. 2.2 MATERIALS ** NOTE TO SPECIFIER ** Delete the following paragraph if washer extractors are not required. Dryer tumblers are fabricated from galvanized steel. A. Washer Extractors - Stainless Steel: ASTM A 666, Type 304 with No. 4 finish, directional satin finish, on exposed surfaces. ** NOTE TO SPECIFIER ** Delete the following paragraph if dryer tumblers are not required. Washer extractors are fabricated from stainless steel. B. Dryer Tumblers - Galvanized Steel: ASTM A 653/A 653M, G90 (Z275) coating designation; commercial-quality, cold-rolled steel that is zinc coated by the hot-dip process and chemically treated. 2.3 UW SERIES HIGH PERFORMANCE HARDMOUNT WASHER EXTRACTORS ** NOTE TO SPECIFIER ** Use the following if any of the UWT - high performance washer extractor models are specified. Delete all UWT washer extractor model numbers not required. A. Model No. UWT045V40V: 1. Capacity: 45 lbs (20 kg). 2. Cylinder Volume: 7.3 cu. ft. (185 liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 400. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 10. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. B. Model No. UWT065V40V: 1. Capacity: 65 lbs (29.5 kg). 2. Cylinder Volume: 9.7 cu. ft. (246 liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 400. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 10. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. C. Model No. UWT085V40V: 1. Capacity: 85 lbs (38.6 kg). 2. Cylinder Volume: 13 cu. ft. (368 liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 6. Drive Motor: 7.5 hp (5.6 kW). 7. G Force: 300. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. D. Model No. UWT105V40V: 1. Capacity: 105 lbs (47.6 kg). 2. Cylinder Volume: 15.9 cu. ft. (450 liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 6. Drive Motor: 7.5 hp (5.6 kW). 7. G Force: 300. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. E. Model No. UWT130V40V: 1. Capacity: 130 lbs (59.0 kg). 2. Cylinder Volume: 19.6 cu. ft. (555 liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Two, 1 inch (25 mm) and 2 x 3/4 inch (51 x 19 mm) all NH male connectors. 5. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 6. Drive Motor: 10 hp (7.5 kW). 7. G Force: 300. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. F. Model No. UWT160V40V: 1. Capacity: 160 lbs (72.6 kg). 2. Cylinder Volume: 24.1 cu. ft. (682 liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Two, 1 inch (25 mm) and two, 3/4 inch (19 mm), all NH male connectors. 5. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 6. Drive Motor: 10 hp (7.5 kW). 7. G Force: 300. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. G. Model UWT200V: ** NOTE TO SPECIFIER ** Delete model not required. 1. Model without Soapbox: Model UWT200V40M. 2. Model with Soapbox: Model UWT200V30M. 3. Capacity: 200 lbs (90.7 kg). 4. Cylinder Volume: 30.1 cu.ft. (852 liters) minimum. 5. Number of Speeds: 9. 6. Number and Size of Water Inlet Connections: Two (main fill) connections x 1 inch (25 mm) NH male connections and Two (spray rinse) connections x 3/4 inch (19 mm) NH male connections. 7. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 8. Drive Motor: 10 hp (7.5 kW). 9. G Force: 200. ** NOTE TO SPECIFIER ** Delete voltage not required. 10. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 11. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. 12. Electrical Requirements: 380 - 415 V / 60 Hz / 3 phase. H. Model UWT V40L, UWT V40M, and UWT V40V General Characteristics: 1. Frame: Heavy-duty structural plate steel frame. 2. Construction: Cabinet front, top, sides and inner and outer tubs, 304 grade stainless steel. 3. Control System: a. Programming Methods: Control Interface, Wi-Fi, Infrared or USB (PC). b. 99-Cycle Capability with graphic display of words and icons. c. 34 languages supported. d. 30 programmable water levels, plus overflow. e. Graphic display with words and icons. f. Automatic maintenance reminders by day, week and month. g. Wi-Fi and PC software with management reports. h. Internet connectivity for off-site diagnostic and remote programming capabilities. i. Real-time clock allows time and date stamp to 100+ items. j. Cycle counter. k. Displays a count up timer after the end of cycle. l. Temperature controlled fill and thermal cool down. m. Water Monitoring: Fill value, slow drain and automatic leak detection system. n. Diagnostic capabilities. 4. Chemical Supply System: a. Automatic flushing and 8 external supply signals. b. Manually filled 5 compartment dry chemical dispensing system. 5. Cylinder Drive: Programmable inverter drive. 6. Rapid jet-spray rinse system. 7. Drain Valve: Automatically opens in event of power failure. 8. Bearing Protection: Ozone resistant seals. I. Model No. UWT045V40L: 1. Capacity: 45 lbs (20 kg). 2. Cylinder Volume: 7.3 cu. ft. (185 Liters) minimum. 3. Number of Speeds: 5. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 100. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. J. Model No. UWT065V40L: 1. Capacity: 65 lbs (29.5 kg). 2. Cylinder Volume: 9.7 cu. ft. (246 Liters) minimum. 3. Number of Speeds: 5. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 100. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. K. Model No. UWT065V40M: 1. Capacity: 65 lbs (29.5 kg). 2. Cylinder Volume: 9.7 cu. ft. (246 Liters) minimum. 3. Number of Speeds: 6. 4. Number and Size of Water Inlet Connections: Four, 3/4 inch (19 mm) NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 10. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. L. Model No. UWT200V40M: 1. Capacity: 200 lbs (90.7 kg). 2. Cylinder Volume: 30.1 cu. ft. (852 Liters) minimum. 3. Number of Speeds: 9. 4. Number and Size of Water Inlet Connections: Two (main fill) connections x 1 inch (25 mm) NH male connections and Two (spray rinse) connections x 3/4 inch (19 mm) NH male connections. 5. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 6. Drive Motor: 10 hp (7.5 kW). 7. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if no UWT*** washer extractor models are selected. 2.4 UW SERIES MID PERFORMANCE WASHER EXTRACTOR MODELS AND COMPONENTS A. Model UWT N2 General Characteristics: 1. Frame: Heavy-duty structural plate steel frame. 2. Construction: Cabinet front, top, sides and inner and outer tubs, 304 grade stainless steel. 3. Control System: UniMac M30. a. Programmable microprocessor: machine keypad, Windows PDA/laptop. 4. Cylinder Drive: Programmable inverter drive with rotation. 5. Chemical Supply System: Automatic flushing and connections for 4 external supply lines and control signals for 4 external supplies. a. UWT N1 adds 5 cup manual fill soap box option for dry chemical dispensing. Also deletes external supply signals and external connections. 6. Drain Valve: Automatically opens in event of power failure. ** NOTE TO SPECIFIER ** Delete all UWT*** washer extractor model numbers not required. B. Model No. UWT045N2M: 1. Capacity: 45 lbs (20 kg). 2. Cylinder Volume: 7.3 cu. ft. (185 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 100. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. C. Model No. UWT045N2L: 1. Capacity: 45 lbs (20 kg). 2. Cylinder Volume: 7.3 cu. ft. (185 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 100. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. D. Model No. UWT065N2M: 1. Capacity: 65 lbs (30 kg). 2. Cylinder Volume: 9.7 cu. ft. (246 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 10. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. E. Model No. UWT065N2L: 1. Capacity: 65 lbs (30 kg). 2. Cylinder Volume: 9.7 cu. ft. (246 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 5 hp (3.7 kW). 7. G Force: 100. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. F. Model No. UWT085N2M: 1. Capacity: 85 lbs (38.6 kg). 2. Cylinder Volume: 13 cu. ft. (368 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 7.5 hp (5.6 kW). 7. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. G. Model No. UWT105N2M: 1. Capacity: 105 lbs (47.6 kg). 2. Cylinder Volume:15.9 cu. ft. (450 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 7.5 hp (5.6 kW). 7. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. H. Model No. UWT130N2M: 1. Capacity: 130 lbs (59.0 kg). 2. Cylinder Volume: 19.6 cu. ft. (555 liters) minimum. 3. Control: M30 system. 4. Number and Size of Water Inlet Connections: Two, 1 inch (25 mm), NH male connectors. 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor: 10 hp (7.5 kW). 7. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if Models UC washer extractor models are not required. 2.5 UC SERIES CABINET HARDMOUNT WASHER EXTRACTORS ** NOTE TO SPECIFIER ** Use the following if any of the UC washer extractor models are specified. A. Model UCT**** General Characteristics: 1. Frame: Heavy-duty structural steel A-frame. 2. Construction: Cabinet front, top, and inner and outer tubs, 304 grade stainless steel. ** NOTE TO SPECIFIER ** This nine-cycle control, available with 100 G-Force and 200 G-Force, is designed to be easy-to-use, while offering the programming flexibility to meet the needs of special applications. Three water level settings and up to four supply signals for automatic laundry chemical dispensing offer even more flexibility, while self diagnostic and cycle counter tools help ensure that your laundry keeps running as efficiently as possible. Delete the control system option not required. 3. Control System: Nine-cycle Control. M9 with 100 G-Force. a. Programmable microprocessor, with cycle time remaining and cycle counter. b. Programmable microprocessor: machine keypad, Windows PDA/laptop. c. 9 cycle capability. d. 3 programmable water levels. e. Real-time clock to record events by date and time. f. Cycle counter. g. Water monitoring: slow drain and automatic leak detection system. h. Diagnostic capabilities. 4. Control System: Nine-cycle Control. M9 with 200 G-Force. a. Programmable microprocessor, with cycle time remaining and cycle counter. b. Programmable microprocessor: machine keypad, Windows PDA/laptop. c. 9 cycle capability. d. 3 programmable water levels. e. Real-time clock to record events by date and time. f. Cycle counter. g. Water monitoring: slow drain and automatic leak detection system. h. Diagnostic capabilities. 5. Chemical Supply System: a. Automatic flushing and connections for 4 external supply lines and control signals for 4 external supplies. b. Four compartment, manually filled self-cleaning dry chemical dispensing system. 6. Drain Valve: Automatic opening in event of power failure. ** NOTE TO SPECIFIER ** Delete all UC washer extractor model options not required. B. Model No. UCT020: 1. Capacity: 20 lbs (9 kg). 2. Cylinder Volume: 2.8 cu. ft. (79 L). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) NH male connectors. 4. Number and Size of Drain Outlets: One, 2 inch (52 mm). 5. Drive Motor: 1 hp. 6. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. C. Model No. UCT030: 1. Capacity: 30 lbs (13.6 kg). 2. Cylinder Volume: 4.2 cu. ft. (119 L). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) NH male connectors. 4. Number and Size of Drain Outlets: One, 2 inch (51 mm). 5. Drive Motor: 1 hp (0.75 kW). 6. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. D. Model No. UCT040: 1. Capacity: 40 lbs (18 kg). 2. Cylinder Volume: 6.3 cu. ft. (178 L). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) NH male connectors. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 2 hp (1.5 kW). 6. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. E. Model No. UCT060: 1. Capacity: 60 lbs (27 kg). 2. Cylinder Volume: 9 cu. ft. (255 L). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) NH male connectors. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 3 hp (2.25 kW). 6. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. F. Model No. UCT080: 1. Capacity: 80 lbs (36 kg). 2. Cylinder Volume: 12.9 cu. ft. (369 L). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) NH male connectors. 4. Number and Size of Drain Outlets: Drain Valves and Diameter: One, 3 inch (76 mm). 5. Drive Motor: 5 hp (3.75 kW). 6. G Force: 200. ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if no UYN washer extractor models are selected. 2.6 UY SERIES SOFTMOUNT COMMERCIAL WASHER EXTRACTORS ** NOTE TO SPECIFIER ** Use the following if any of the UYN washer extractor models are specified. Delete extractor model options not required. A. Model No. UYT020: 1. Capacity: 20 lbs (8 kg). 2. Wash Cylinder Volume: 2.6 cu ft (75 L) minimum. 3. Number and size of Water inlet Connections: Two, 3/4 inch (19 mm) BSP male connections. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 1 hp (0.75 kW). 6. G Force: 400. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. B. Model No. UYT025: 1. Capacity: 25 lbs (11.4 kg). 2. Cylinder Volume: 3.7 cu ft (105 L) minimum. 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) BSP male connections. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. G Force: 400. ** NOTE TO SPECIFIER ** Delete input voltage not required. 6. Electrical Requirements: 200 - 240 V / 60 Hz / 1 phase. 7. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. C. Model No. UYT030. 1. Capacity: 30 lbs (14 kg). 2. Wash Cylinder volume: 4.8 cu ft (135 L) minimum. 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) BSP male connections. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 2.01 hp (1.5 kW). 6. G Force: 400. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. D. Model No. UYT040: 1. Capacity: 40 lbs (18.1 kg). 2. Cylinder Volume: 6.4 cu ft (181 L) minimum. 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) BSP male connections. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 2.95 hp (2.2 kW). 6. G Force: 400. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. E. Model No. UYT055: 1. Capacity: 55 lbs (24 kg). 2. Cylinder Volume: 8.5 cu ft (240 L) minimum. 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) BSP male connections. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 4.02 hp (3 kW). 6. G Force: 400. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. F. Model No. UYT070: 1. Capacity: 70 lbs (31 kg). 2. Cylinder Volume: 9.9 cu ft (280 L) minimum. 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm) BSP male connections. 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 4.02 hp (3 kW). 6. G Force: 350. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. G. Model No. UYT100: 1. Capacity: 100 lbs (45 kg). 2. Cylinder Volume: 15.96 cu ft (452 L) minimum. 3. Number and Size of Water Inlet Connections: Three, 1-1/2 inch (38 mm) BSP male connections. 4. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 5. Drive Motor: 10.06 hp (7.5 kW). 6. G Force: 360. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 8. Electrical Requirements: 380 - 415 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. H. Model No. UYT135. 1. Capacity: 135 lbs (61 kg). 2. Cylinder Volume: 21.22 cu ft (601 L) minimum. 3. Number and Size of Water Inlet Connections: Three, 1-1/2 in 38 mm) BSP male connections. 4. Number and Size of Drain Outlets: Two, 3 inch (76 mm). 5. Drive Motor: 10.06 hp (7.5 kW). 6. G Force: 360. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 8. Electrical Requirements: 380 - 415 V / 60 Hz / 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. I. Model No. UYN180. 1. Capacity: 180 lbs (80 kg). 2. Cylinder Volume: 28.50 cu ft (807 L) minimum. 3. Number and Size of Water Inlet Connections: Three, 1-1/2 inch (38 mm) BSP male connections. 4. Number and Size of Drain Outlets: Two, 4 inch (102 mm). 5. Drive Motor: 14.75 hp (11 kW). ** NOTE TO SPECIFIER ** Delete input voltage not required. 6. Electrical Requirements: 208 - 240 V / 60 Hz / 3 phase. 7. Electrical Requirements: 400 - 480 V / 60 Hz / 3 phase. J. Model No. UYN230. 1. Capacity: 230 lbs (100 kg). 2. Cylinder Volume: 34.3 cu ft (972 L) minimum. 3. Number and Size of Water Inlet Connections: Three, 1-1/2 inch (38 mm) BSP male connections. 4. Number and Size of Drain Outlets: Two, 4 inch (102 mm). 5. Drive Motor: 20.12 hp (15 kW). 6. G Force: 350. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 208 - 240 V / 60 Hz / 3 phase. 8. Electrical Requirements: 400 - 480 V / 60 Hz / 3 phase. K. Model No. UYN275. 1. Capacity: 275 lbs (120 kg). 2. Cylinder Volume: 40.8 cu ft (1154 L) minimum. 3. Number and Size of Water Inlet Connections: Three, 1-1/2 inch (38 mm) BSP male connections. 4. Number and Size of Drain Outlets: Two, 4 inch (102 mm). 5. Drive Motor: 24.81 hp (18.5 kW). 6. G Force: 350. ** NOTE TO SPECIFIER ** Delete input voltage not required. 7. Electrical Requirements: 208 - 240 V / 60 Hz / 3 phase. 8. Electrical Requirements: 400 - 480 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if NAT models are not required. 2.7 NAT SERIES CABINET HARDMOUNT WASHER-EXTRACTORS ** NOTE TO SPECIFIER ** Delete model options not required. A. Model NAT030GN0MZAMPD0AA. 1. Capacity: 30 lbs (13.5 kg). 2. Cylinder Volume: 4.8 cu ft (135 L). 3. Number and Size of Water Inlet Connection: Three, 0.75 inch (19 mm). 4. Number and Size of Drain Outlets: One 3 inch (76 mm). 5. Drive Motor: 1 hp (0.75 kW). 6. G Force: 200. 7. Electrical Requirements: 208 - 240 V / 60 Hz / 1 phase. B. Model NAT040GN0MZAMPD0AA. 1. Capacity: 40 lbs (18 kg). 2. Cylinder Volume: 6.4 cu ft (180 L). 3. Number and Size of Water Inlet Connection: Three, 0.75 inch (19 mm). 4. Number and Size of Drain Outlets Diameter: One, 3 inch (76 mm). 5. Drive Motor: 1.48 hp (1.1 kW). 6. G Force: 200. 7. Electrical Requirements: 208 - 240 V / 60 Hz / 1 phase. C. Model NAT055GN0MZAMPD0AA. 1. Capacity: 55 lbs (24 kg). 2. Cylinder Volume: 8.5 cu ft (240 L). 3. Number and Size of Water Inlet Connection: Three, 0.75 inch (19 mm). 4. Number and Size of Drain Outlets: One, 3 inch (76 mm). 5. Drive Motor: 2.01 hp (1.5 kW). 6. G Force: 200. 7. Electrical Requirements: 208 - 240 V / 60 Hz / 1 phase. ** NOTE TO SPECIFIER ** Delete the following article if not required. 2.8 INDUSTRIAL TUMBLE DRYERS ** NOTE TO SPECIFIER ** Use the following if any of 30, 55, 75, F75, 120, 170, or 200 lb. dryer tumbler models are specified. A. Model 30, 55, 75, F75, 120, 170, and 200 lbs. Model Dryer Tumbler General Characteristics: 1. Construction: Heavy duty embossed steel with electrostatically applied baked enamel finish. 2. Door: High grade stainless steel door with 7/8 inch (22 mm) rubber gasket and heavy duty hinge. 3. Control System: Microprocessor touchpad control. a. Programming methods: Machine keypad, Infrared (PC or PDA). b. 48-Cycle Capability with graphic display of words and icons. c. PC software to program machine and/or audit machine performance with quick view performance reports. d. Record start, stop and idle time by date and time. e. Record last eight machine errors by date and time. f. Record machine service history. g. Internet connectivity for off-site diagnostic capabilities. h. Automatic maintenance reminders by day, week and month. i. Over Dry Prevention Technology (OPTidry) System utilizes one cylinder lifter as sensor. 4. Lint Filter: Self-cleaning, depositing lint to large storage area at bottom of tumbler. ** NOTE TO SPECIFIER ** OPTidry is an industry-exclusive, cutting-edge innovation that connects sensors located within the lifters to our revolutionary rotary transfer switch to offer unmatched levels of accuracy. The result is a pinpoint dryness reading throughout the entire load, eliminating costs associated with over-drying. Delete if not required. 5. Over-Dry Prevention: OPTidry technology. ** NOTE TO SPECIFIER ** Delete if not required. 6. Reversing Operation. ** NOTE TO SPECIFIER ** Delete the following model options not required. B. Tumble Dryer Model No. UTS30EVN: 1. Capacity: 30 lbs (14 kg). 2. Lint Filter: 480 sq. in. (3097 sq. cm.). Delf cleaning, depositing lint to large storage area at bottom of tumble dryer. ** NOTE TO SPECIFIER ** Delete the following exhaust size not required. 3. Exhaust Size, Standard: 6 inch (150 mm). 4. Exhaust Size, ProCapture: 8 inch (200 mm). 5. Heat Source: Electric (21 kW). ** NOTE TO SPECIFIER ** Delete the following electrical requirements not required. 6. Electrical Requirements: 230 - 240 V / 60 Hz / 3 phase. 7. Electrical Requirements: 460 - 480 V / 60 Hz / 3 phase. C. Tumble Dryer Model No. UTS30NVN: 1. Capacity: 30 lbs (14 kg). 2. Lint Filter: 480 sq. in. (3097 sq.cm.). Delf cleaning, depositing lint to large storage area at bottom of tumble dryer. ** NOTE TO SPECIFIER ** Delete the following exhaust size not required. 3. Exhaust Size, Standard: 6 inch (150 mm). 4. Exhaust Size, ProCapture: 8 inch (200 mm). ** NOTE TO SPECIFIER ** Delete the following heat source not required. 5. Heat Source: Natural Gas, Standard, 73,000 btu per hour. a. Gas Connection: 0.5 inch (13 mm) NPT. 6. Heat Source: Natural Gas, ProCapture, 65,000 btu per hour. a. Gas Connection: 0.5 inch (13 mm) NPT. ** NOTE TO SPECIFIER ** Delete the following electrical requirements not required. 7. Electrical Requirements: 100 - 120 V / 60 Hz / 1 phase. 8. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 9. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. D. Tumble Dryer Model No. UT055EVN: 1. Capacity: 55 lbs (25 kg). 2. Lint Filter: 576 sq. in. (3617 sq.cm.). Self-cleaning, depositing lint to large storage area at bottom of tumble dryer. 3. Exhaust Size: 8 inch (200 mm). 4. Heat Source: Electric 27 kW. ** NOTE TO SPECIFIER ** Delete the electrical requirement not required. 5. Electrical Requirements: 230 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 460 - 480 V / 60 Hz / 3 phase. E. Tumble Dryer Model No. UT055NVN: 1. Capacity: 55 lbs (25 kg). 2. Lint Filter: 576 sq. in. (3617 sq. cm.). Self-cleaning, depositing lint to large storage area at bottom of tumble dryer. 3. Exhaust Size: 8 inch (200 mm). 4. Heat Source: Natural Gas 112,000 btu per hour. a. Gas Connection: 0.5 inch (13 mm) NPT. ** NOTE TO SPECIFIER ** Delete the following electrical requirements not required. 5. Electrical Requirements: 100 - 120 V / 60 Hz / 1 phase. 6. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 7. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. F. Tumble Dryer Model No. UT055SVN: 1. Capacity: 55 lbs (25 kg). 2. Lint Filter: 576 sq. in. (3617 sq.cm.). Self-cleaning, depositing lint to large storage area at bottom of tumble dryer. 3. Exhaust Size: 8 inch (200 mm). 4. Heat Source: Steam 130,000 btu per hour. a. Steam Connection: 0.75 inch (19 mm) NPT. ** NOTE TO SPECIFIER ** Delete the following electrical requirements not required. 5. Electrical Requirements: 100 - 120 V / 60 Hz / 1 phase. 6. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 7. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. G. Tumble Dryer Model No. UT075EVN: 1. Capacity: 75 lbs (34 kg). 2. Lint Filter: 576 sq. inch (3716 sq. cm.). Self-cleaning, depositing lint to large storage area at bottom of tumble dryer. 3. Heat Source: Electric 36 kW. ** NOTE TO SPECIFIER ** Delete exhaust size not required. 4. Exhaust Size, Standard: 8 inch (200 mm). 5. Exhaust Size, ProCapture: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 6. Electrical Requirements: 230 - 240 V / 60 Hz / 3 phase. 7. Electrical Requirements: 460 - 480 V / 60 Hz / 3 phase. H. Tumble Dryer Model No. UT075NVN: 1. Capacity: 75 lbs (34 kg). 2. Lint Filter: 576 sq. inch (3716 sq. cm.). Self-cleaning, depositing lint to large storage area at bottom of tumble dryer. 3. Heat Source: Natural Gas 150,000 btu per hour. a. Gas Connection: 0.5 inch (13 mm) NPT. ** NOTE TO SPECIFIER ** Delete exhaust size not required. 4. Exhaust Size, Standard: 8 inch (200 mm). 5. Exhaust Size, ProCapture: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 6. Electrical Requirements: 100 - 120 V / 60 Hz / 1 phase. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. I. Tumble Dryer Model No. UT075SVN: 1. Capacity: 75 lbs (34 kg). 2. Lint Filter: 576 sq. inch (3716 sq. cm.). Self-cleaning, depositing lint to large storage area at bottom of tumble dryer. 3. Heat Source: Steam 133,900 btu per hour. a. Steam Connection: 3/4 NPT. ** NOTE TO SPECIFER ** Delete all but one exhaust size below. 4. Exhaust Size, Standard: 8 inch (200 mm). 5. Exhaust Size, ProCapture: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 6. Electrical Requirements: 100 - 120 V / 60 Hz / 1 phase. 7. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 8. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. J. Tumble Dryer Model No. UTF75NVN: 1. Capacity: 75 lbs (34 kg). 2. Lint Filter: 576 sq. inch (3716 sq. cm.). 3. Cylinder Drive: Reversing cylinder. 4. Heat Source: Natural Gas 225,000 btu per hour. a. Gas Connection: 3/4 inch (19 mm) NPT. 5. Exhaust Size: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 6. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 7. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. K. Tumble Dryer Model No. UT120EVN: 1. Capacity: 120 lbs (55 kg). 2. Lint Filter: 1301 sq. inch (8394 sq. cm.). 3. Heat Source: Electric. 60 kW. 4. Exhaust Size: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 230 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 460 - 480 V / 60 Hz / 3 phase. L. Tumble Dryer Model No. UT120NVN: 1. Capacity: 120 lbs (55 kg). 2. Lint Filter: 1301 sq. inch (8394 sq. cm.). 3. Heat Source: Natural Gas 270,000 btu per hour. a. Gas Connection: 1 inch (25 mm) NPT. 4. Exhaust Size: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. M. Tumble Dryer Model No. UT120SVN: 1. Capacity: 120 lbs (55 kg). 2. Lint Filter: 1301 sq. inch (8394 sq. cm.). 3. Heat Source: Steam 334,750 btu per hour. a. Steam Connection: 3/4 NPT. 4. Exhaust Size: 10 inch (254 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. N. Tumble Dryer Model No. UT170NVN: 1. Capacity: 170 lbs (77 kg). 2. Lint Filter: 1653 sq. inch (10664 sq. cm.). 3. Heat Source: Natural Gas 395,000 btu per hour. a. Gas Connection: 1 inch (25 mm) NPT. 4. Exhaust Size: 12 inch (305 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. O. Tumble Dryer Model No. UT170SVN: 1. Capacity: 170 lbs (77 kg). 2. Lint Filter: 1653 sq. inch (10664 sq. cm.). 3. Heat Source: Steam 502,125 btu per hour. a. Steam Connection: Inlet 3/4 inch (19 mm) NPT. Outlet: 1 inch (25 mm) NPT. 4. Exhaust Size: 12 inch (305 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. P. Tumble Dryer Model No. UT200NVN: 1. Capacity: 200 lbs (90 kg). 2. Lint Filter: 1653 sq. inch (10664 sq. cm.). 3. Heat Source: Natural Gas 425,000 btu per hour. a. Gas Connection: 1 inch (25 mm) NPT. 4. Exhaust Size: 12 inch (305 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. Q. Tumble Dryer Model No. UT200SVN: 1. Capacity: 200 lbs (90 kg). 2. Lint Filter: 1653 sq. inch (10664 sq. cm.). 3. Heat Source: Steam 502,125 btu per hour. a. Steam Connection: Inlet: 3/4 inch (19 mm) NPT. Outlet: 1 inch (25 mm) NPT. 4. Exhaust Size: 12 inch (305 mm). ** NOTE TO SPECIFIER ** Delete all but one of the following electrical requirements. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if UTT models are not required. 2.9 COMMERCIAL STACK TUMBLE DRYERS A. Tumble Dryer Model No. UTT30EVN: 1. Capacity: Two, 30 lbs (14 kg). 2. Lint Filter: Two, 405 sq. inch (2613 sq. cm.). System utilizes one cylinder lifter as a sensor. 3. Exhaust Size: One, 8 inch (200 mm) Oval. 4. Heat Source: Electric 21 kW. ** NOTE TO SPECIFIER ** Delete the following electrical requirement not required. 5. Electrical Requirements: 230 - 240 V / 60 Hz / 3 phase. 6. Electrical Requirements: 460 - 480 V / 60 Hz / 3 phase. B. Tumble Dryer Model No. UTT30NVN: 1. Capacity: Two, 30 lbs (14 kg). 2. Lint Filter: Two, 405 sq. in. (2613 sq. cm.). System utilizes one cylinder lifter as a sensor. 3. Exhaust Size: One, 8 inch (200 mm) Oval. 4. Heat Source: Natural Gas 73,000 btu per hour a. Gas Connection: 0.5 inch (13 mm) NPT. ** NOTE TO SPECIFIER ** Delete the following electrical requirements not required. 5. Electrical Requirements: 100 - 120 V / 60 Hz / 1 phase. 6. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 7. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. C. Tumble Dryer Model No. UTT45NVN: 1. Capacity: Two, 45 lbs (20 kg). 2. Lint Filter: Two, 558 sq. in. (3600 sq. cm.). System utilizes one cylinder lifter as a sensor. 3. Exhaust Size: One, 10 inch (250 mm) Oval. 4. Heat Source: Natural Gas 95,000 btu per hour. a. Gas Connection: 0.5 inch (13 mm) NPT. ** NOTE TO SPECIFIER ** Delete the following electrical requirements not required. 5. Electrical Requirements: 200 - 240 V / 60 Hz / 1 or 3 phase. 6. Electrical Requirements: 440 - 480 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if not required. 2.10 STACKED WASHER-EXTRACTOR/TUMBLE DRYERS A. Model UST030N 1. Capacity: Two, 30 lbs (13 kg). 2. Cylinder Volume, Washer-Extractor: 4.2 cu. ft. (119 liters). 3. Cylinder Volume, Tumble Dryer: 10.6 cu. ft. (300 liters). 4. Number and Size of Water Inlet Connections: Two, 0.75 inch (19 mm). 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor, Washer-Extractor: 1 hp (0.75 kW). 7. Drive Motor, Tumble Dryer: 0.3 hp (0.3 kW). 8. Fan Motor, Tumble Dryer: 0.5 hp (0.4 kW). 9. G Force: 200. 10. Heat Source: Natural Gas 73,000 btu per hour. 11. Exhaust Size: 8 inch (200 mm) Elliptical. 12. Electrical Requirements: 200 - 240 V / 60 Hz / 3 phase. B. Model UST050N: 1. Capacity: Two, 50 lbs (23 kg). 2. Cylinder Volume, Washer-Extractor: 6.3 cu. ft. (178 liters). 3. Cylinder Volume, Tumble Dryer: 14.8 cu. ft. (419 liters). 4. Number and Size of Water Inlet Connections: Two, 0.75 inch (19 mm). 5. Number and Size of Drain Outlets: One, 3 inch (76 mm). 6. Drive Motor, Washer-Extractor: 2 hp (1.5 kW). 7. Drive Motor, Tumble Dryer: 0.5 hp (0.4 kW). 8. Fan Motor, Tumble Dryer: 0.5 hp (0.4 kW). 9. G Force: 200. 10. Heat Source: Natural Gas 95,000 btu per hour. 11. Exhaust Size: 10 inch (254 mm) Elliptical. ** NOTE TO SPECIFIER ** Drying cabinets are specifically geared to the fire industry drying requirements. Delete the article below if automatic drying cabinets are not required. 2.11 FIREFIGHTER PPE DRYING CABINET A. Personal Protection Equipment (PPE) Drying Cabinets Model No. UTGC: Automatic drying cabinet for processing water-washed personal protection equipment. 1. NFPA 1851 Compliant. 2. Dry Capacity: 6 full sets of PPE and 15 boot / glove holders. 3. Heat Source: Electric 12 kW / 9 kW. 4. Exhaust Size: 6 inch (153 mm). 5. Airflow: 300 cfm (5.5 cmm). ** NOTE TO SPECIFIER ** Delete electrical requirements not required. 6. Electrical Requirements: 208 V / 60 Hz / 1 phase. 7. Electrical Requirements: 208 V / 60 Hz / 3 phase. 8. Electrical Requirements: 240 V / 60 Hz / 1 phase. 9. Electrical Requirements: 240 V / 60 Hz / 3 phase. ** NOTE TO SPECIFIER ** Delete the following article if light commercial washers and dryers are not required. Delete model options not required. 2.12 LIGHT COMMERCIAL WASHERS AND DRYERS A. Top Load Washer, Model No. UWMN2SP: 1. Capacity: 16 lbs (7.3 kg). 2. Cylinder Volume: 3.19 cu. ft. (90.3 liters). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm). 4. Number and Size of Drain Outlets: One, 1-1/2 inch (38 mm) outside diameter drain hose. 5. Drive Motor: 0.5 hp (0.37 kW). 6. G Force: 150. 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. B. Front Load Washer, Model No. UFNE5BJP: 1. Capacity: 21.5 lbs (9.5 kg). 2. Cylinder Volume: 3.42 cu. ft. (96.8 liters). 3. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm). 4. Number and Size of Drain Outlets: One, 1-1/4 inch (32 mm) outside diameter drain hose. 5. Drive Motor: 0.9 hp (0.67 kW) Variable Speed Induction. 6. G Force: 440. 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. C. Front Control Electric Dryer, Model No. UDEE5BGS: 1. Capacity: 18 lbs (8.2 kg). 2. Cylinder Volume: 7 cu. ft. (198 liters). 3. Heat Source: Electric. 4. Exhaust Size: 4 inch (102 mm). 5. Airflow: 220 cfm (105 liters per sec). 6. Drive Motor: 0.33 hp (0.25 kW). 7. Electrical Requirements: 120 V / 240 V / 60 Hz / 1 phase. D. Rear Control Electric Dryer, Model No. UDEMNRGS: 1. Capacity: 18 lbs (8.2 kg). 2. Cylinder Volume: 7 cu. ft. (198 liters). 3. Heat Source: Electric. 4. Exhaust Size: 4 inch (102 mm). 5. Airflow: 220 cfm (105 liters per sec). 6. Drive Motor: 0.33 hp (0.25 kW). 7. Electrical Requirements: 120 V / 240 V / 60 Hz / 1 phase. E. Front Control Gas Dryer, Model No. UDGE5BGS: 1. Capacity: 18 lbs (8.2 kg). 2. Cylinder Volume: 7 cu. ft. (198 liters). 3. Heat Source: Natural Gas 22,500 btu per hour. a. Gas Connection: 3/8 inch (9.5 mm). 4. Exhaust Size: 4 inch (102 mm). 5. Airflow: 220 CFM (105 liters per sec). 6. Drive Motor: 0.33 hp (0.25 kW). 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. F. Rear Control Gas Dryer, Model No. UDGMNRGS: 1. Capacity: 18 lbs (8.2 kg). 2. Cylinder Volume: 7 cu. ft. (198 liters). 3. Heat Source: Natural Gas 22,500 btu per hour. a. Gas Connection: 3/8 inch (9.5mm). 4. Exhaust Size: 4 inch (102 mm). 5. Airflow: 220 cfm (105 liters per sec). 6. Drive Motor: 0.33 hp (0.25 kW) 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. G. Commercial Stack Dryers - Electric, Model No. USEMNAGS: 1. Capacity: Two, 18 lbs (8.2 kg) x 2. 2. Cylinder Volume: Two, 7 cu. ft. (198 liters). 3. Heat Source: Electric. 4. Exhaust Size: Two, 4 inch (102 mm). 5. Airflow: Two, 220 CFM (105 liters per sec). 6. Drive Motor: Two, 0.33 hp (0.25 kW). 7. Electrical Requirements: 120 V / 240 V / 60 Hz / 1 phase. H. Commercial Stack Dryers - Gas, Model No. USGMNAGS: 1. Capacity: Two, 18 lbs (8.2 kg). 2. Cylinder Volume: Two, 7 cu. ft. (198 liters). 3. Heat Source, Natural Gas: Two, 22,500 btu per hour. a. Gas Connection: 3/8 inch (9.5 mm). 4. Exhaust Size: Two, 4 inch (102 mm). 5. Airflow: 220 cfm (105 liters per sec). 6. Drive Motor: 0.33 hp (0.25 kW). 7. Electrical Requirements: 120 V / 60 Hz / 1 phase. I. Stack Washer/Dryer - Electric, Model No. UTEE5ASP: 1. Capacity, Washer: 21.5 lbs (9.5 kg). 2. Capacity, Dryer: 18 lbs (8.2 kg). 3. Cylinder Volume, Washer: 3.42 cu. ft. (96.8 liters). 4. Cylinder Volume, Dryer: 7.0 cu. ft. (198 liters). 5. Number and Size of Water Inlet Connections: Two, 3/4 inch (19 mm). 6. Number and Size of Drain Outlets: One, 1-1/4 inch (32 mm) outside diameter drain hose. 7. Heat Source: Electric. 8. Exhaust Size: 4 inch (102 mm). 9. Airflow: 220 cfm (105 liters per sec). 10. Drive Motor, Washer: 0.9 hp (0.67 kW) Variable Speed Induction. 11. Drive Motor, Dryer: 0.33 hp (0.25 kW). 12. G Force: 440. 13. Electrical Requirements, Washer: 120 V / 60 Hz / 1 phase. 14. Electrical Requirements, Dryer: 120 V / 240 V / 60 Hz / 1 phase. J. Stack Washer/Dryer - Gas, Model No. UTGE5ASP: 1. Capacity, Washer: 21.5 lbs (9.5 kg). 2. Capacity, Dryer: 18 lbs (8.2 kg). 3. Cylinder Volume, Washer: 3.42 cu. ft. (96.8 liters). 4. Cylinder Volume, Dryer: 7.0 cu. ft. (198 liters). 5. Number and Size of Water Inlet Connections: Two, 3/4 inch (19mm). 6. Number and Size of Drain Outlets: One, 1-1/4 inch (32 mm) outside diameter drain hose. 7. Heat Source: Gas. 8. Exhaust Size: 4 inch (102 mm). 9. Airflow: 220 cfm (105 liters per sec). 10. Drive Motor, Washer: 0.9 hp (0.67 kW) Variable Speed Induction. 11. Drive Motor, Dryer: 0.33 hp (0.25 kW). 12. G Force: 440. 13. Electrical Requirements, Washer: 120 V / 60 Hz / 1 phase. 14. Electrical Requirements, Dryer: 120 V / 60 Hz / 1 phase. PART 3 EXECUTION 3.1 EXAMINATION A. Do not begin installation until substrates have been properly prepared. B. If substrate preparation is the responsibility of another installer, notify Architect of unsatisfactory preparation before proceeding. 3.2 PREPARATION A. Clean surfaces thoroughly prior to installation. B. Prepare surfaces using the methods recommended by the manufacturer for achieving the best result for the substrate under the project conditions. 3.3 INSTALLATION A. Install in accordance with manufacturer's instructions. B. System Startup and Commissioning: Arrange for a local manufacturer's representative to inspect machines prior to startup and operation. 3.4 PROTECTION A. Protect installed products until completion of project. B. Touch-up, repair or replace damaged products before Substantial Completion. END OF SECTION