Black Oxide, blackening, oxidizing, oxiding, black passivating, gun bluing . . . these terms all refer to the process of forming a black iron oxide on the surface of ferrous metals. The black oxide process is a chemical conversion coating. This means that the black oxide is not deposited on the surface of the substrate like nickel or zinc electroplating. Instead, the black oxide coating is produced by a chemical reaction between the iron on the surface of the ferrous metal and the oxidizing salts present in the black oxide solution. These oxidizing salts include penetrates, catalysts, activators and proprietary additives which all take part in the chemical reaction. The result of this chemical reaction is the formation of black iron oxide, magnetite (Fe3O4), on the surface of the metal being coated. Black oxide has a range of unique properties and benefits that can be applied to a variety of industries.
Black oxide architectural coatings give the architect, interior designer and merchandiser new ways to express themselves.
We work with professionals in creating the exact "look and finish" they are seeking for a given project.
Customers like the Ritz Carlton, Herman Miller and Liz Claiborne have incorporated blackened steel panels and fixtures into their designs.
These architectural industry case studies are just several ideas to show you how black oxide can make your designs stand out.
To learn more about black oxide finish for the architectural industry, call us today at 216-861-4431 (Bob McElwee x105 or Dave Tatham x113), or request a sample online.
|
|
In the case histories, you can see the features, advantages and benefits of black oxide coatings as they relate to specific jobs.
Black oxide is often the answer to the question, "How can I blacken this metal?" With over 50 years of experience, you can rely on Cleveland Black Oxide to develop the best black oxide coating solutions for your application.