Glass-Floor System

 

LITELAM is a fully tested Fire-rated Glass-floor system. The patented "load bi-pass" system gives LITEFLAM a superb range performance with over 90mins integrity/90mins insulation and /90mins load-bearing capability - meeting the requirements of US Building Regulations ASTM-E119, British Standards, European Norms.

Rated 5 based on 1 product reviews
As the leading single source manufacturer of structural glass floor panel systems, LITEFLOOR® offers unique and innovative product lines that can be designed into virtually any type of application to meet almost all structural, slip resistant and aesthetic design criteria. LITEFLOOR® is a walkable laminated safety glass with optional slip-resistant properties and/or structural integrity.

Rated 5 based on 1 product reviews

Glass For Leed

 

GLASSXcrystal - the solar glass that stores, heats and cools.

NEW materials for the architect's LEED construction set.

The basic approach to product development concerns optimisation of the glass architecture with self-regulating façade systems, reduction of energy costs, intelligent conversion of stored solar energy for comfortable heating and air-conditioning of interior spaces, independent of location and the sun's position in the various seasons of the year.

GLASS X Prism
GLASS X Crystal
GLASS X Store

Rated 5 based on 1 product reviews

Glass Wall Systems

 

Vast expanses of frameless, apparently weightless and transparent walls of light can be created using SGG LITEWALL®, the complete structural glazing system. LITEWALL blends versatility to a wide variety of sub-frame connection possibilities - steel elbows, steel spiders, or glass fin.

SGG LITEWALL® is a patented point-fixed glazing system - designed, engineered and manufactured by Eckelt Glas GmbH. Eckelt Glas is a wholly owned subsidiary of Saint-Gobain Glass - the world's largest glass company. Distributed in North America by Greenlite Glass Systems.

Rated 5 based on 1 product reviews
PRIVA-LITE is a laminated glass with a Liquid Crystal interlayer film. In their natural state, the Liquid Crystal molecules are randomly scattered, creating a translucent, frosted, effect that ensures privacy while still allowing light through. Once electricity is applied to the Liquid Crystal film, the molecules re-orient themselves and line up, turning the glass completely transparent.

Rated 5 based on 1 product reviews
LINIT Bendheim Wall Systems is a complete glazing system comprised of self-supporting glass channels within an extruded aluminum frame. Intermediate metal support bars are not necessary because of LINIT's 'U' shape, which gives it strength capable of withstanding high wind loads or large spans. LINIT is durable, maintenance free and fully recyclable.

Rated 5 based on 1 product reviews

Active Glass

 

An active glass panel that becomes a living material, glowing with pure, sensual light. PLANILUM draws on technological principles of fluorescent light sources, a principle that has been tried and tested for many years. The revolution introduced by PLANILUM is possible thanks to the advent of flat fluorescent light and the decision to avoid mercury in the plasma gas.

Rated 5 based on 1 product reviews

Glass Décor

 

Digital printing on glass allows what until now were unimaginable forms in design on facades, partitions and foyers. As an individual accent in modern rooms, photo-prints on glass give a coloured brilliance and play with transparency and refraction in the material. For everyone's affordable unique pieces such as POS, displays and advertising, LITEX PIX makes them easily possible.

Rated 5 based on 1 product reviews
Print any digital image on the laminated surface. STADIP ARTE allows the transformation of a multitude of artistic and creative ideas. From the stroke of a paintbrush to photo-realistic images, from Graphic data to colour graduations in all shades - the unrestricted use of glass is made possible. Colour definitions to RAL, Pantone etc. can be achieved. But also the blue of the ocean or the subtle yellow of the afternoon sun. Every desirable colour can be achieved.

Rated 5 based on 1 product reviews

Services

 

Greenlite Glass Systems Inc. offers consulting services from the design stage through engineering and installation of Specialty Glass projects in North America.

Greenlite Glass Systems represents some of the largest and most technically advanced glass factories in the world. GGS will assist in selecting the right product for the application and ensure that the product is delivered on time and on budget. GGS provides solutions for specialty glass challenges and in partnership with their clients is dedicated to 'making it work'.

Rated 5 based on 1 product reviews

Request Info

 

To request more information about our products or to order samples.

Rated 5 based on 1 product reviews