CONTACT INFO
150 Domorah Dr.
Montgomeryville, PA 18936
Toll Free: 800-250-2221
Phone: 215-616-0600
Would you like to see hosted content from Timberlane, Inc.?
EMAIL
Request for informationTimberlane, Inc. Contact Us / RFI

Shutter Materials  

Timberlane's Endurian line of shutters offers a state-of-the-art material that mimics wood in ways never imagined. Our Endurian line truly offers the world's first fully customizable maintenance-free shutters. Each Endurian shutter is hand-crafted and assembled by one of our meticulous artisans, and the end result is a masterpiece with a high level of detailing for which Timberlane is so well known.

Rated 5 based on 1 product reviews
Timberlane's Premium Wood line of shutters offers you the traditional beauty and flawless finish your home desires. We offer three types of wood: Western Red Cedar, Mahogany, and Spanish Cedar. All three wood types create beautiful piece of art. From the moment you order, your wooden shutters are completely custom made and hand-crafted.

Rated 5 based on 1 product reviews

Shutter Styles  

The most traditional shutter, but also the shutter most open to interpretation, our Panel styles come in many varieties. From raised to recessed, shaker to flat, ogee to quarter-round and bead trim, Panels offer something for everyone. Unlike applied moldings used by other companies, Timberlane uses and tongue and groove construction to secure the edge of the trim inside the stiles and the rails which ensures that our trim cannot fall off.

Rated 5 based on 1 product reviews
In the olden days, Louvered shutters were created for ventilation and privacy in homes. Today, they provide the same level of protection and come in three different styles: Faux, Fixed, and Operable. Timberlane's Louvered shutters are sanded to a glossy round finish, then hand-fitted into a slot so it can never flip in the wrong direction or fall out. These shutters are set with enough "float" so they can expand and contract in different types of weather conditions.

Rated 5 based on 1 product reviews
If you are head over heels for our Louvered style shutters, but are on a tighter budget, our Faux Louvers are a perfect fit for you! Available in Advantage and Fundamental materials, the Faux Louvers offer a unique approach to our original style of Louvered shutters. Since both Advantage and Fundamental materials have a single panel profile, these shutters do not have any space in between louvers, hence the "faux" term. The Timberlane Faux Louvered shutters have countless design configurations available and are all built to order.

Rated 5 based on 1 product reviews
If you admire Timberlane's Louvered style shutters, but want them solely for decoration purposes, Timberlane's Fixed Louvered style is a perfect match. Our Fixed Louvered shutters appear to be functional, but the slats do not operate the way they are constructed to.Each slat is hand cut and fitted to leave room for contraction and expansion during different weather climates. Fixed Louver shutters are only available in our Endurian and Premium Wood materials.

Rated 5 based on 1 product reviews
Timberlane's Operable Louvered style are an ideal match for those who want the traditional feel of shutters. Before the age of electricity, Louver style shutters were placed on the top level of a home to provide both ventilation and privacy. They have slats that move up and down, just like they did in the olden days. Our Operable Louvered shutters are fitted by hand, where each Louver has been cut to an exacting length to leave just enough room for expansion and contraction.

Rated 5 based on 1 product reviews
Traditionally used on barns, Board & Batten shutters have transformed into the pure beauty of the shutter world. Today these shutters are enlivened with beaded detail as seen on historic Northeastern brownstone homes and have created a presence in the rural communities. Substantial and heartfelt, Board & Batten are shutters that deeply satisfy the craving for authenticity.BR>
Rated 5 based on 1 product reviews
Originally designed for the tropics, Bermuda shutters are the most romantic of styles. Typically used for sun screening and storm protection, these shutters offer a classic vacation feel to your home. One shutter panel will usually cover the entire window. They are hinged from the top and are installed with a custom fit support arm to keep the shutter in an open position ||A||- perfect for capturing those nice coastal breezes! Bermuda shutters, also known as Bahama and Storm Shutters, are available in any louver size, with the option of small or large tilt-rods.

Rated 5 based on 1 product reviews
It's important to give your home a personal touch that distinguishes it from the rest of your neighborhood. Timberlane's line of custom Bahama shutters, also known as Bermuda shutters, will allow you to refresh the appearance of your home and make it tasteful and elegant. Our shutters can really accent your home's exterior and transform it from something that is just mediocre into something magnificent. Bahama shutters will give your home a unique style and allow those warm summer breezes through your windows.

Rated 5 based on 1 product reviews
Whether new or old, some homes just demand large shutters. Our Timberlane's Manor styles offer the largest shutters for the largest window casings. Our thicker collection of shutters designed to be proportionate to the size of your windows, will enhance the look of your home and certainly provide you with some curb appeal because they cannot be missed.

Rated 5 based on 1 product reviews
Give your home an elegant touch of class with custom made Cedar shutters from Timberlane. With the option of Western Red and Spanish Cedar, Timberlane's team of master shutter craftsmen go above and beyond to create exceptional wooden shutters. Cedar shutters, offered in our Premium Wood and Advantage materials, evoke a feeling of a simpler, more graceful time, when sipping lemonade on the front porch in the summer was the order of the day and the neighbors came by to visit regularly. Premium Wood Cedar shutters are available in all of our standard colors, and we have the ability to custom match any color. Our Advantage line is available primed only.

Rated 5 based on 1 product reviews
Shutters have been around for hundreds of years. Initially they were used to protect your windows from sunlight, drafts or unfavorable weather from entering your house. Today, shutters have become a part and parcel of home dA©cor. Shutters can complete the look of your home and add a unique style that truly will set it apart from the rest of the neighborhood. At Timberlane, we go out of our way for our customers. As a customer of Timberlane, not only can you design your shutters from scratch, but if we do not have something that you want, we will go above and beyond to make it possible. We create the finest custom shutters that are designed to make your home look its absolute best!

Rated 5 based on 1 product reviews
Timberlane creates custom home shutters that can accentuate the exterior dA©cor of any home or building, with both traditional wood and our maintenance-free Endurian line. Our Endurian shutters, although having a partial PVC composition, are far superior to standard PVC shutters because we have carefully selected the best raw material for the component of each shutter and candidly PVC is not a one size fits all raw material. Our Endurian shutters deliver durability and style while combining classic beauty with modern art. They are crafted with the same amazing attention to detail that our traditional wood shutters are designed with, but are more advanced and durable with respect to raw materials than standard PVC shutters you will find in the market.

Rated 5 based on 1 product reviews

Hand-Forged Shutter Hardware  

Timberlane offers the most extensive selection of shutter hardware available anywhere, and it's all in stock and ready to ship.

Rated 5 based on 1 product reviews
Heavy duty, stainless steel.

Rated 5 based on 1 product reviews
Lag mount.

Rated 5 based on 1 product reviews
Shutter Lock - Stainless Steel.

Rated 5 based on 1 product reviews
Dummy Strap Hinges, Jamb Hinges
"S" Beveled Shutter Tie-Back - Faux

Rated 5 based on 1 product reviews
Continuous Bermuda Hinge
Gravity Butt Style Hinge
Bermuda Shutter Support

Rated 5 based on 1 product reviews

Gallery  



Rated 5 based on 1 product reviews